PCB Materials Science & Properties
Explore a wide range of PCB materials—including FR-4 variants, copper and aluminum substrates, Rogers laminates, and PTFE composites—and understand how their properties impact performance, reliability, and manufacturability.
Featured Posts
PCB Materials Science
How to Select Tg of PCB ?
What is the Tg of PCB? In PCB manufacturing, "Tg" stands for Glass Transition Temperature. It is the temperature at which the PCB substrate material transitions from a rigid, glassy state to a soft, rubbery state. PCBs are flame-retardant (UL94 V-0) and do not burn easily; instead, they soften above Tg. The Critical Correlation Between Tg and Z-Axis CTE (Coefficient of Thermal Expansion) When the temperature exceeds the Tg point, the PCB substrate material (such as standard FR-4) undergoes a physical ......
Jan 12, 2024
PCB Materials Science
PCB Copper Pour BasicsAug 30, 2023PCB Materials Science
How to Choose the Thickness of PCBDec 19, 2023PCB Materials Science
Your Ultimate Guide to PCB RulersMar 08, 2024PCB Materials Science
Understanding the Materials Used in PCBs: Selection, Types, and ImportanceAug 01, 2023
Latest Posts
PCB Materials Science
Choosing the Right CTI Value for Safer High-Voltage PCBs
Key Takeaways Higher CTI (≥600V, Group I) allows shorter creepage distances while preventing surface tracking in high-voltage designs. Standard FR4 (CTI ~175V) is often inadequate for mains voltage — upgrade to high-CTI materials for safety and compactness. Always match CTI material group to your working voltage and pollution degree for IEC/UL compliance. Clean assembly and good layout practices are essential to realize the full benefits of high-CTI laminates. Choose certified high-CTI materials and e......
Nov 18, 2026
PCB Materials Science
Maximize Efficiency with PCB Panelization in High-Volume Manufacturing
Whenever a new PCB designer begins to spin the wheels, they are soon enough faced with the transition of creating a few prototypes into a volume production venture. As well as that, change brings a new idea that prototype-based engineers tend to forget: PCB panelization. In essence, panelization refers to loading a number of copies of your board design (or even a variety of designs) onto a single standardized production panel such that all of the fabrication and assembly processes treat them as a sing......
Nov 18, 2026
PCB Materials Science
Inside the PCB Structure : How Layers, Stackup, and Buildup Define Modern Circuit Board Performance
Printed circuit boards may look like flat green rectangles, but beneath the surface, they are sophisticated multi-layer structures. As devices get more compact and complex, engineers turn to multilayer boards with carefully chosen materials and stackups to meet electrical and mechanical demands. This article peels back those layers to explore how substrate choice, layer stackup, and buildup methods shape PCB performance. Here we’ll cover PCB design fundamentals from the base materials up to high-densi......
Nov 18, 2026
PCB Materials Science
The Benefits of Bed of Nails Testing in Professional PCB Manufacturing
Have you ever wondered how manufacturers can test thousands of PCBs daily and not make the production line crawl? The answer, as frequently as not, is a deceitful-appearing device called a bed of nails test set-up. The platform contains hundreds of little spring-loaded pins on it, and each of those pins is aligned very precisely to touch a specific test point on your circuit board. It can check the electrical integrity of a whole PCB, shorts, opens, and component defects in a few seconds, before the b......
Nov 18, 2026
PCB Materials Science
Understanding PCB Dielectric Constant : Choosing Materials for Optimal Signal Performance
Key Takeaways The PCB dielectric constant (Dk) is a critical factor that directly determines signal propagation speed, characteristic impedance, and transmission loss in high-frequency designs. Selecting the right material — from standard FR4 for general use to low-Dk Rogers, PTFE, and LCP for multi-gigahertz applications — enables better performance, tighter impedance control, and reduced signal degradation. Success ultimately comes from matching Dk to your frequency needs, optimizing layer stackup, ......
Nov 16, 2026
PCB Materials Science
PCB Adhesive : Types, Applications, and Best Alternatives for Circuit Board Assembly
A printed circuit board uses more than just solder to secure its components. PCB adhesives, or circuit board glue, bond layers and components together under extreme conditions. Good adhesives help hold parts in place during assembly, electrically insulate, moisture seal, and thermally spread from hot chips. In fact, adhesives are critical to performance by preventing micro components from loosening and shifting. In other words, the right adhesive keeps the puzzle of a device's electronic pieces reliab......
Nov 16, 2026
PCB Materials Science
A Complete Guide to Copper Clad Laminate (CCL) in PCB Manufacturing
Key Takeaways CCL is the base material: a cured resin-reinforcement sheet with copper foil bonded to one or both sides. Three parts control performance: Resin affects heat and loss, reinforcement controls stability, and copper foil affects conductor behavior. Choose by the main design stress: Heat, frequency, and cost usually determine the best laminate family. Slash sheets define the material: IPC-4101 uses numbered slash sheets to specify rigid PCB base materials. Tg alone is not enough: Td and time......
Nov 16, 2026
PCB Materials Science
FR4 PCB Deep Guide: Material Truth, Real Specs & When to Use (or Avoid) It
FR-4 isn't a secret code, it literally means Flame Retardant (grade 4). In PCB terms, FR-4 is a NEMA (National Electrical Manufacturers Association) grade designation for a glass-reinforced epoxy laminate. We can say it is a composite of woven fiberglass cloth bonded with an epoxy resin that contains flame-retardant additives. The “FR” stands for flame retardant, but note this doesn’t automatically mean UL94 V-0 certified. It just indicates the resin is formulated to self-extinguish if it catches fire......
Nov 10, 2026
PCB Materials Science
What is the Standard Thickness of a PCB?
Key Takeaways 1.6 mm Standard: 1.6 mm (0.062") is the universal industry standard, balancing rigidity, assembly ease, and component fit. 0.4mm–3.0mm Options: JLCPCB provides versatile FR-4 thicknesses from 0.4 mm for ultra-thin devices to 3.0 mm for high-power systems. Stackup Flexibility: Multilayer PCBs up to 12–16 layers can still maintain a 1.6 mm profile using thinner cores and prepregs. Impedance & Heat Balance: Dielectric thickness directly sets trace impedance (Z0), while thicker boards increa......
Nov 10, 2026
PCB Materials Science
How Laser Drilling Delivers Precision and Density in Advanced PCB Manufacturing
Key Takeaways Laser Drilling has become the cornerstone technology for precision and high-density PCB manufacturing, enabling microvias as small as 25-75μm — far beyond the 150μm limit of mechanical drilling. By delivering superior accuracy, contactless processing, excellent signal integrity, and reliable blind/stacked vias, it empowers advanced HDI board designs essential for modern electronics. From optimal stackup selection to professional plating and DFM practices, mastering laser drilling is key ......
Nov 09, 2026
PCB Materials Science
Why Sequential Lamination Delivers Superior HDI PCBs
Did you ever ask yourself how smartphone manufacturers can crust a thousand connections into a credit card-sized board? The process is referred to as sequential lamination, which is a multi-cycle process that is used to fabricate PCBs on a layer-by-layer basis, releasing microvia structures and routing densities that cannot be accessed by a single-press process. Without it, the slick, high-performance electronics that we all use on a daily basis would not appear the way that they do now. With data rat......
Nov 09, 2026
PCB Materials Science
Buried Vias in Advanced PCBs: Enabling Higher Density, Better Signal Integrity, and Compact Designs
Key Takeaways Hidden Routing: Buried vias connect only inner layers, keeping outer surfaces clear for dense components and traces. Better Signal Integrity: They eliminate via stubs, reducing parasitics and signal loss in high-speed designs. Higher Density: Essential for HDI boards, dense BGAs, and small form factors like wearables. Higher Cost: Sequential lamination and extra drilling steps make them ~3×-4× more expensive than standard through-holes. Ever wondered how a modern smartphone mainboard can......
Nov 09, 2026
PCB Materials Science
Unlocking Higher Density and Better Performance with Blind Vias in HDI PCBs
Key Takeaway Higher Density: Connects surface to inner layers without penetrating the whole board, freeing routing channels under fine-pitch BGAs. Improved Signal Integrity: Reduces via stub length to minimize impedance discontinuities in high-speed designs. Aspect Ratio Rule: Keep the depth-to-diameter ratio near 0.75:1 (max 1:1) for reliable laser drilling and void-free plating. Thermal Efficiency: Supports via-in-pad setups for better heat dissipation and compact component placement. Ever wonder ho......
Nov 09, 2026
PCB Materials Science
Stacked or Staggered Vias? Choosing the Best Option for Reliable HDI PCBs
Key Takeaways Structures: Stacked vias align vertically (need copper fill); staggered vias are offset laterally. Reliability: Staggered vias better resist thermal stress across 3+ layers. Cost & Yield: Staggered vias cut manufacturing steps, raising yield and saving cost. Space: Stacked vias fit tight, fine-pitch BGA breakouts best. Decision: Choose stacked for extreme density, staggered for reliable savings. Ever since taking a closer look at the guts of a smartphone motherboard, you may have thought......
Nov 09, 2026
PCB Materials Science
Understanding PCB Laminates Materials, Types, and Why They Matter
A PCB is a flat board made of a non-conductive substrate material with conductive pathways and components attached to it. One of the critical components of a PCB is the PCB laminate. A typical laminate PCB consists of a core material, such as fiberglass or composite epoxy. So what it actually do is ● Provides structural support ● Improves Signal Integrity ● Bond the layers to the core material The fiberglass layers are stacked on top of each other and pressed together with heat and pressure to create ......
Oct 30, 2026
PCB Materials Science
Why UL94 V0 Matters for Safe and Reliable PCB Manufacturing
Key Takeaways UL94 V0 is the highest flame rating for PCB materials, requiring self-extinguishing within 10 seconds with no flaming drips. It greatly reduces fire risk and has become the de facto standard for safe, reliable PCBs in consumer, industrial, automotive, and medical applications. JLCPCB offers UL94 V0 compliant FR4 and high-Tg materials by default, ensuring regulatory compliance (UL, CE, CCC) and long-term reliability without compromising performance or budget. Never sacrifice V0 rating for......
Oct 30, 2026
PCB Materials Science
PCB Material Guide : Types, Selection, and Impact on Performance
If PCB materials could talk, FR-4 would probably say, "I run 80% of the electronics industry, and still nobody appreciates me." Rogers would boast, "I'm expensive because I'm special," while Polyimide would flex literally and say, "I bend, but I don't break." The purpose of this blog is to introduce you to the types of PCB substrates available to you and how those materials affect your PCB's performance, thermal stability, signal integrity, and overall longevity. The choice of PCB material will be bas......
Oct 29, 2026
PCB Materials Science
The Critical Role of Copper Peel Strength in Durable PCB Performance
Key Takeaways Standard Test: Measured via the IPC-TM-650 90° pull test in N/mm. Core Function: Prevents pad lifting and delamination under thermal stress and CTE mismatch. Foil Types: ED foil provides higher adhesion; RA foil yields lower signal loss. Material Benchmarks: Standard FR4 averages 1.0–1.4 N/mm, while High-Tg FR4 achieves 1.2–1.6 N/mm. Design Tips: Add teardrops, eliminate unsupported copper slivers, and perform DFM checks. Ever wonder what's making the copper stay put on your circuit boar......
Oct 29, 2026
PCB Materials Science
Navigating Standard PCB Thickness: A Step-by-Step Guide to Selecting the Ideal Thickness for Your PCB Prototype
The thickness of a printed circuit board (PCB) may seem like a small detail, but it plays a crucial role in the performance and reliability of your electronic devices. Standard PCB thickness has become an industry norm, offering a range of benefits that impact mechanical stability, electrical performance, thermal management, and component compatibility.In this article, we will be taking a deep look at why the varying thickness of your PCB matters and provide you with a guide to choosing the right thic......
Oct 29, 2026
PCB Materials Science
How Modular PCB Design Simplifies Complex Electronics Projects
Key Takeaway Modular PCB design simplifies complex electronics by breaking boards into independent, reusable functional blocks with clear interfaces. It boosts reusability, speeds up debugging, enhances team collaboration, and reduces errors.Shift from flat to modular design for faster development and more scalable, reliable PCBs. Ever seen a 400+ component schematic and got your head scrambled before even beginning routing? You are not alone. With the ever-increasing density of electronics combined w......
Oct 29, 2026
PCB Materials Science
Metal Core PCB Materials: Thermal Truth & Design Rules
Metal-core PCBs (MCPCBs) are speciality boards where a metal substrate replaces the standard FR-4. This metal core acts as a built-in heatsink, improving heat dissipation in high-power electronics. The basic stackup is simple: A copper conductor layer on top. A thin dielectric insulator in the middle. A thick metal base at the bottom. This structure provides excellent thermal spreading and a convenient ground plane. But it comes at the cost of a much heavier and more expensive board than typical FR-4.......
Oct 29, 2026
PCB Materials Science
Mastering Mitered Corners for Superior High-Speed Signal Performance
Have you ever had the privilege of zooming into a PCB layout and noted those well-chamfered corners on high-speed signal traces? Mitered corners they are, and much more than a cosmetic preference. The geometry of each trace bend is directly proportional to impedance continuity, signal reflection, and the quality of your data being transmitted at the RF and high-speed digital frequencies. Having mitered corners on your PCB can be the difference between meeting your return loss target and trying to trac......
Oct 29, 2026
PCB Materials Science
Is FR4 the Best Board Material for Your Design
Key Takeaways Best All-Rounder: Ideal balance of strength, insulation, and low cost for standard PCBs. Clear Limits: Poor heat dissipation (~0.3 W/m·K) and high loss for RF (>3 GHz). Alternatives: Use Rogers for RF, Aluminum for high heat, and FPC for flexibility. Selection Essentials: Pick High-Tg (170°C+) for lead-free reflow and custom stackups for impedance. JLCPCB Advantage: 1–32 layer FR4 boards with ±10% impedance control and 24h fast dispatch. In the world of electronics and printed circuit bo......
Oct 28, 2026
PCB Materials Science
Heavy Copper PCBs : Harnessing Superior Power Handling and Thermal Performance
In my study, I discovered that in the PCB market, 1 oz/ft² (approximately 35µm) on the outer circuit boards and 0.5 oz/ft² on the inner circuit boards is typically referred to as standard copper weight. Another design that reverses the traditional is the use of copper weights of 3 oz/ft² (105µm) or higher, and in some radical designs, up to 20 oz/ft² or more. It is not a typo - we are talking of copper layers that are nearly a millimeter deep on one side of your heavy copper PCB. You may ask yourself ......
Oct 28, 2026
PCB Materials Science
How Design Rule Check Prevents Expensive PCB Production Mistakes
Have you ever sent Gerber files to your fab house, and you can get an email back saying that they need to fix clearance or annular ring issues, and only then can they start production? When that comes out like you, you know how frustrating that can be, days wasted, revision numbers rising, shipping dates falling. Catching all of that is actually the real MVP of good design, which is a solid design rule check in your PCB layout tool, that allows you to discover all of that before it even leaves your de......
Oct 28, 2026
PCB Materials Science
Choosing the Right PCB Solder Mask Material for Reliable PCBs
Key Takeaways Dual-Curing: UV defines openings; heat cures epoxy for durability. LPI vs. Coverlay: LPI for rigid boards; coverlay for flexible circuits. Color & Pitch: Green allows tighter dams (0.10 mm) than black/white (0.13 mm). Protection: Prevents solder bridges and seals copper from moisture. Cure Quality: Proper baking prevents mask peeling during plating and reflow. PCB solder mask material is a cured polymer film usually 10 to 30 µm (0.4 to 1.2 mil) thick. During reflow, it is the only barrie......
Oct 19, 2026
PCB Materials Science
Safeguarding Circuit Boards Against Breakdown Voltage Failure
Key Takeaways Construction Matters: Breakdown voltage depends on stackup and defects, not raw material ratings. Stress Causes Failures: Heat and moisture degrade insulation over time, leading to field defects. Four Main Failure Modes: Insulation fails via internal voids, treeing, CAF growth, or surface tracking. Layout Design Fixes: Use dual prepregs, wider hole spacing, rounded trace corners, and isolation slots. Testing Split: Bare-board testing checks low-voltage net continuity, while hi-pot tests ......
Oct 15, 2026
PCB Materials Science
Optimizing High-Voltage Circuit Safety with PCB Dielectric Strength
Key Takeaways Non-linear Scaling: Dielectric strength drops as thickness increases. Safety vs Signals: Dielectric strength ensures safety, while Dk controls signal speed. Material Selection: High-voltage safety depends on Tg, CTI, and moisture resistance. Spacing Rules: Clearance prevents air arcs, while creepage prevents surface tracking. Assembly Testing: Hi-pot testing requires finished assemblies, not bare boards. Dielectric strength is the number engineers quote to prove a board is safe at mains ......
Oct 09, 2026
PCB Materials Science
How Copper Foil Shapes PCB Performance and Manufacturing Quality
Key Takeaways Weight: 1 oz copper ≈ 35 µm thickness; higher weight increases current capacity. Types: ED for standard rigid boards, RA for dynamic flex circuits. DFM & Loss: Smoother foil lowers RF loss; thicker foil requires wider trace spacing. The part of a PCB that actually carries the electrical signal is the copper foil. The strength comes from the glass weave, the resin is used to keep the layers together, and the solder mask is used to provide protection and separation of exposed copper. But w......
Sep 28, 2026
PCB Materials Science
Why PCB Substrate Choice Matters More Than You Think
Key Takeaways Prevents Via Failures: Z-axis CTE expansion strains via barrels; right substrates prevent field failure. Specify Beyond FR-4: Name IPC-4101 sheets to guarantee proper Tg and lower thermal growth. Match Material to Need: Choose FR-4 for standard, Polyimide for flex, Aluminum for heat, and Rogers for >3 GHz. Use Real Fab Stackups: Prepreg weave alters Dk; compute impedance using real factory stackups. The PCB substrate is the one part of your board you never actually draw. You choose a thi......
Sep 28, 2026
PCB Materials Science
How to Select Tg of PCB ?
What is the Tg of PCB? In PCB manufacturing, "Tg" stands for Glass Transition Temperature. It is the temperature at which the PCB substrate material transitions from a rigid, glassy state to a soft, rubbery state. PCBs are flame-retardant (UL94 V-0) and do not burn easily; instead, they soften above Tg. The Critical Correlation Between Tg and Z-Axis CTE (Coefficient of Thermal Expansion) When the temperature exceeds the Tg point, the PCB substrate material (such as standard FR-4) undergoes a physical ......
Sep 09, 2026
PCB Materials Science
Beyond the Basics: The Role of PTFE PCBs
Polytetrafluoroethylene (PTFE) PCBs are integral to advanced electronic applications. Among various PCB materials, Teflon, the brand name for Polytetrafluoroethylene (PTFE). Teflon PCBs, known for their high frequency and heat resistance properties. All of this is achievable due to its exceptional dielectric properties. RF PCB designs often make use of low-loss PTFE-based materials thanks to their very low dielectric losses and huge range of possible Dk values. Low Dielectric Constant: Enables high-sp......
Sep 09, 2026
PCB Materials Science
Understanding PCB Copper Thickness: Standards and Conversions
When talking about copper thickness, there are some limited options available with manufacturing houses. When designers have to increase the current carrying capacity of a trace without making it wider, then copper weight or thickness is increased in the lateral dimension. There are only a few options, and most of the manufacturers have a standard thickness. Copper selection is all about power delivery, signal propagation, and thermal management. Copper width and length are always a concerning factor ......
Sep 09, 2026
PCB Materials Science
PCB Copper Pour Basics
What is Copper Pour in PCB Design? Copper pour refers to the technique of filling unused areas of a PCB's copper layers with solid copper planes. These planes are connected to power or ground nets, creating a continuous conductive path. Copper pour is typically used in the power and ground planes, as well as in signal layers for specific purposes. Purpose and Benefits of Copper Pour: Copper pour is primarily used to fill unused areas on PCB copper layers with solid (or hatched) copper connected to pow......
Sep 09, 2026
PCB Materials Science
How to Choose the Thickness of PCB
First, In the world of electronic products, the PCB is often referred to as the "heart" of the device. It interconnects all components, making board thickness one of the most important parameters. Choosing the right PCB thickness directly affects the electrical performance, mechanical stability, thermal management, and long-term reliability of the final electronic product. The process of selecting PCB thickness is influenced by various factors, such as product application scenarios, board material, an......
Sep 09, 2026
PCB Materials Science
Aluminum PCBs vs. Traditional FR4: A Comparative Analysis of Thermal Management
Key Takeaways Superior Thermal Conductivity: JLCPCB aluminum PCBs (1 W/m·K) provide 3–4x higher thermal conductivity than FR4 (~0.3 W/m·K). High-Voltage Safety: Features up to 3000V AC dielectric insulation against the metal base. Lower System Cost: Eliminates bulky external heatsinks, reducing total weight and cost. 1-Layer vs. Multilayer: Aluminum PCBs are 1-layer (SMT-focused), while FR4 supports up to 32 layers. Best Use Cases: Choose aluminum for high-power LEDs/power modules; choose FR4 for mult......
Sep 08, 2026
PCB Materials Science
PDN Design : Building Stable Power Delivery for High-Performance PCBs
Ever had to boot up a newly-built PCB only to discover that your FPGA won't boot up, your ADC inputs are not as clean as they should be, or your high-speed serial link is producing errors you did not get in simulation? Do not doubt your signal integrity work; just first review your PDN design. In many products that have failed to come to fruition, the problem is not the signal path but the power delivery to the signal path. A successful PCB is built upon a well-designed power distribution network, an ......
Sep 07, 2026
PCB Materials Science
Why Td Value Matters for Lead-Free and High-Reliability PCBs
Key Takeaways Td Definition: Td is the irreversible temperature where PCB laminate chemically breaks down (5% mass loss). Td vs. Tg: Tg is reversible softening; Td is permanent chemical destruction. Lead-Free Need: High lead-free reflow heat (245–260°C) requires high Td (≥340°C) to stop delamination. Reliability Metric: IPC Class 3 designs need high-Td materials and long T260/T288 delamination times. JLCPCB Solution: JLCPCB supplies high-Tg/Td laminates (Tg170/S1000-2) with optimized thermal DFM. Ever......
Aug 08, 2026
PCB Materials Science
Understanding Moisture Absorption: Choosing PCB Materials for Long-Term Reliability
Key Takeaways High Failure Risk: Absorbed moisture shifts trace impedance, causes signal loss, and leads to board delamination or CAF shorts during reflow. Material Differences: PTFE (<0.02%) offers top resistance, FR4 is moderate (~0.10–0.15%), while Polyimide absorbs the most (0.40–0.90%). Standardized Testing: Susceptibility is measured by weight gain using IPC-TM-650 (Method 2.6.2.1)—lower percentages are better. Effective Prevention: Prevent issues by using low-absorption substrates, pre-reflow b......
Aug 05, 2026
PCB Materials Science
Etched FPC: Manufacturing Process, Advantages, Applications, and Selection Guide
Ever noticed that thin, amber-coloured ribbon running between the boards in a smartphone camera module or a notebook's lid? That ribbon is almost surely an etched FPC, a flexible printed circuit that's created by chemically removing the unwanted copper to create a precise conductive pattern. It's one of the workhorses of modern electronics, and most people are unaware of the amount of engineering that goes into it. There are more than one flavor of flexible circuit, and the method of manufacture affec......
Jul 28, 2026
PCB Materials Science
Your Ultimate Guide to PCB Rulers
In the world of PCB design and manufacturing, having the right tools is crucial for achieving accuracy and precision. One such tool that has gained popularity among professionals and hobbyists is the PCB ruler. This specialized measuring tool is designed to provide accurate measurements, reference information, and component footprints, assisting designers, engineers, technicians, and assemblers in various stages of PCB development. In this guide, we'll explore what a PCB ruler is, the features and mea......
Jul 14, 2026
PCB Materials Science
Understanding the Materials Used in PCBs: Selection, Types, and Importance
Key Takeaways FR-4 is the go-to material for most cost-effective and reliable PCBs. Use Rogers for high-frequency and RF applications to reduce signal loss. Higher copper weight (2oz) improves current and heat handling. Choose High-Tg substrates for better thermal stability in multilayer boards. Green LPI soldermask offers the best balance of performance and inspection. Printed circuit boards (PCBs) are an essential component of modern electronics. These boards connect and support electronic component......
Jul 13, 2026
PCB Materials Science
How to Prevent Solder Bridges for Superior PCB Quality and Reliability
Key Takeaways Solder bridges are a leading cause of SMT failures on fine-pitch components. Prevent them with proper solder mask dams (0.075–0.1mm), optimized stencil design, and controlled reflow profiles. Combine good DFM practices with AOI + X-ray inspection for maximum reliability. Professional manufacturing and early DFM review significantly boost first-pass yield and reduce costly rework. You have experienced the post-reflow sadness and eyed the board that failed on the first reflow, if you have ......
Jul 09, 2026
PCB Materials Science
How PCB Functional Testing Ensures Your Product Works Flawlessly from Day One
Key Takeaways Looks right doesn’t mean it works right. Only PCB Functional Testing (FCT) verifies real-world performance that structural tests like AOI, ICT, and X-ray cannot catch. JLCPCB’s E-test, AOI, and X-ray ensure zero-defect hardware, so your FCT focuses on design and firmware issues. Design for testability: add clear test points and include a firmware test mode for fast verification. Final Tip: Always perform FCT before shipping — it prevents expensive field failures and builds product confid......
Jul 08, 2026
PCB Materials Science
Why Choosing the Right TG Value Leads to More Reliable PCBs
Key Takeaways Tg is key to PCB reliability — it determines when the material loses rigidity under heat. Choose high Tg (≥170°C) for automotive, industrial, or multilayer boards to reduce expansion stress and delamination. Standard Tg (130–140°C) is sufficient for low-power consumer electronics. Higher Tg delivers better thermal stability, especially during lead-free soldering and thermal cycling. Right Tg choice = fewer failures and lower long-term costs. Did you ever question how it's possible for 2 ......
Jun 25, 2026
PCB Materials Science
Choosing the PCB Laminate for Reliable High-Performance Boards
Key Takeaways Choosing the right PCB laminate is the foundation of a reliable high-performance board. Match your material to the application — standard FR4 for basic designs under 5 GHz, high-Tg FR4 for lead-free assembly, low-loss materials for high-speed digital, and Rogers/PTFE for RF and mmWave applications. Always prioritize stable Dk, low Df, high Tg, and low Z-axis CTE while recalculating your stackup for accurate impedance control. Partnering with an experienced manufacturer ensures optimal pr......
Jun 18, 2026
PCB Materials Science
Mastering BT Resin Packaging: Technical Insights & JLCPCB Capabilities
Key Takeaways BT resin is a high-performance thermoset polymer with Tg of 180°C–210°C, ultra-low Dk/Df, and under 0.05% moisture absorption — essential for advanced IC packaging substrates (BGA, CSP, SiP). Its dense cross-linked structure provides superior resistance to electromigration, dendrite growth, and chemical degradation, making it ideal for fine-pitch, high-reliability applications. Manufacturing BT resin PCBs requires specialized diamond-coated drilling, UV/CO2 hybrid laser systems, and prec......
Jun 16, 2026
PCB Materials Science
Selecting the Ideal Substrate Material for High-Performance PCBs
Key Takeaways Selecting the ideal PCB substrate material—balancing standard FR4 for general use with advanced Rogers or PTFE for high frequencies—is vital to prevent signal loss and thermal failure. Hybrid stackups perfectly optimize performance and cost , while JLCPCB guarantees a reliable, high-quality transition from rapid prototyping to volume production. Ever wonder what's under all those shiny copper traces on a printed circuit board? That layer is the substrate material, and it is probably the ......
Jun 09, 2026
PCB Materials Science
Low Df Materials: Reducing Dissipation Factor for Better High-Speed PCBs
Key Takeaways Low Df materials are essential for modern high-speed PCBs as they significantly reduce dielectric loss and signal attenuation at multi-gigabit frequencies. By choosing laminates with lower dissipation factor (such as Panasonic Megtron 6, Rogers, or Isola), designers can achieve cleaner eye diagrams, support higher data rates up to 112G, and maintain better signal integrity while balancing cost through hybrid stackup strategies. Selecting the right low Df material ultimately determines wh......
May 21, 2026
PCB Materials Science
Why High Tg FR4 Is the Smart Choice for Reliable High-Temperature PCBs
Key Takeaways High Tg FR4 is the smart choice for reliable high-temperature PCBs, offering a glass transition temperature of 170°C+, superior thermal stability, lower Z-axis CTE, and reduced warpage compared to standard FR4. It excels in lead-free assembly and demanding environments such as automotive, industrial, and 5G applications, significantly improving long-term reliability while minimizing defects like via cracking and delamination. For engineers seeking durable performance, specifying high Tg ......
May 20, 2026
PCB Materials Science
Unlocking Smaller, Smarter PCBs with Embedded Passive Components
Key Takeaways Embedded passive components are revolutionizing PCB design by integrating resistors, capacitors, and inductors directly into the board layers. This technology delivers smaller, thinner, and higher-performance boards with up to 30-50% space savings, significantly reduced parasitic inductance, superior signal integrity at high frequencies, better thermal distribution, and enhanced reliability through fewer solder joints. Ideal for 5G, wearable, automotive, and RF applications, embedded pas......
May 18, 2026
PCB Materials Science
Reducing CTE Mismatch Stress: Practical Ways to Build More Reliable PCBs
Key Takeaways CTE mismatch (FR4’s high Z‑axis CTE vs. copper) creates thermal stress that causes PCB warpage, via cracks, delamination, and solder fatigue—worse under lead‑free reflow and thermal cycling. Mitigate it with symmetric stackups and balanced copper, higher‑Tg/low‑CTE materials, and tight process control (lamination, cooling, moisture, and consistent via plating). Are you aware that the coefficient of thermal expansion of standard FR4 in the Z-axis can be up to 70 ppm/C, whereas copper has ......
Apr 29, 2026
PCB Materials Science
How to Choose the Right UL94 Rating for Safe and Reliable PCBs
Key Takeaways This article explains how to choose the right UL94 rating to ensure PCB fire safety and compliance: V-0 is the common baseline for most electronics, V-1/HB are typically for lower-risk or non-regulated uses. It also stresses that rating performance depends on material selection, thickness, and process control, so use UL-certified laminates and a traceable, UL-capable manufacturer. Have you heard that just one PCB that catches fire can produce poisonous fumes, annihilate an entire product......
Apr 27, 2026
PCB Materials Science
Why Glass Transition Temperature Is Key to Reliable PCB Performance
Ever had a load of freshly reflowed PCBs in the oven, then found out when you looked at it that there were delamination blisters or broken barrel vias? Should it be the case, it may not be your reflow profile or your solder paste. It could be baked into the substrate that you have your board composed of. One of the most important, yet often neglected, material characteristics of your PCB laminate that will make the difference between your board making it through the manufacturing process and making it......
Apr 22, 2026
PCB Materials Science
Heavy Copper PCBs: An Overview of Their Benefits and Applications
Printed circuit boards (PCBs) are the backbone of modern electronics, providing a platform for the connection of electronic components and the transmission of electrical signals. With the increasing demand for high-performance and reliable electronic devices, manufacturers are constantly seeking ways to improve the overall performance and durability of PCBs. Heavy Copper PCBs are a special type of PCBs that offers several advantages over the standard PCBs. They are designed to have thicker copper laye......
Apr 09, 2026
PCB Materials Science
PCB Troubleshooting : How to Diagnose Issues and Prevent Failures Through Professional Manufacturing
Modern PCBs can pass bench tests yet still fail later due to subtle defects. Faulty PCBs are unavoidable from time to time, which makes knowing troubleshooting techniques useful. Often, human error in manufacturing can cause problems from a slightly shifted trace to a tiny solder void. Identifying and fixing these issues early saves money and time because defective PCBs result in increased rework costs and delayed production. If a defect is caught in the early stages of prototyping, it can save thousa......
Apr 09, 2026
PCB Materials Science
Understanding PCB Thermal Conductivity : Material Choices, Calculation Methods, and High-Performance Solutions
When it comes to compact electronics, the challenge is power consumption, and thermal issues arise due to that. A PCB can pass DRC checks, SI simulations, and even functional testing, yet it may fail miserably in the field due to poor heat management. PCB thermal conductivity is no longer optional for electronics designers; it has become the core consideration in modern designs. As the component sizes shrink, the thermal margins disappear. When designing a PCB with complexities and compact assembly, o......
Apr 09, 2026
PCB Materials Science
Microstrip Line Design Techniques for High-Speed PCB Excellence
Have you ever routed a high-speed signal on an outer routing on your PCB and wondered whether the geometry of the traces you selected would actually work at multi-gigabit data rates? You’re definitely not alone. The most commonly used transmission line structure in PCB design is the microstrip line, but this line is immensely geometry-sensitive, material-sensitive, and manufacturer-tolerance-sensitive. The difference between a clean eye diagram and a signal-integrity nightmare is whether the microstri......
Mar 30, 2026
PCB Materials Science
The Foundation of Every Great PCB: Mastering Schematic Capture
Schematic capture is the process of creating an electronic circuit diagram using specialized software. Here we have to place component symbols (such as resistors, capacitors, ICs, and connectors) and connect them with wires to represent the electrical connection. Although it is not the real connection yet, but can be translated once it goes to layout. Hence, we can say on a big scale schematic capturing serves as the first step in the PCB design workflow, which allows designers to define how component......
Mar 22, 2026
PCB Materials Science
How to Choose the Right PCB Laminate: A Practical Guide for Performance, Cost & Reliability
Selecting the correct PCB laminate is one of the most important decisions in any board design. The laminate determines electrical performance, thermal behavior, mechanical strength, cost, and long-term reliability. A poor choice can lead to signal integrity problems, delamination during reflow, or excessive warpage in production. Engineers who understand laminate properties can avoid these issues and achieve better results at lower cost. Introduction: Why Laminate Selection Matters More Than Ever The ......
Mar 11, 2026
PCB Materials Science
Optimizing Return Paths in PCBs: Strategies for Minimal Noise and Maximum Integrity in High-Speed Designs
Here is a fundamental truth that every PCB designer should have tattooed on their forearm (figuratively, of course): every signal current requires a return current. Unless you take time to provide it with a low-impedance path, the current will simply seek whatever it can, and you are going to end up having some very undesirable hotspots. The entire concept of a current loop is the reason why the return is so difficult. In essence, when the signal passes between point A and point B, you now have a loop......
Feb 27, 2026
PCB Materials Science
Copper Weight and Trace Width: Finding the Optimal Balance
When it comes to printed circuit board (PCB) design, finding the optimal balance between copper weight and trace width is crucial. Copper weight and trace width directly impact the performance, reliability, and cost of your PCB. Whether you're an electronics enthusiast, hobbyist, engineer, student, or professional in the field, understanding the balance between them is essential for successful PCB design. Why Copper Weight Matters Copper weight refers to the thickness of the copper layer on a PCB. It ......
Feb 05, 2026
PCB Materials Science
PCB Repair Reality Check : Why It’s a Last Resort and How Proper Design and Manufacturing Prevent Most Issues
Printed circuit boards are like the heart and nervous system of electronic devices. When they start to fail, you need to know why. Standard failure modes include component breakdown, trace damage, and environmental stress. ICs can burn out, and tiny solder joints may crack under heat. Overheating can literally burn out circuit sections. A dropped device or dent often produces visible cracks in components. It can even corrode copper traces, causing shorts. In today's post, we will explore when to do re......
Feb 04, 2026
PCB Materials Science
OPAMP 101: Basics of Operational Amplifiers Every Engineer Should Know
Analog mathematics? Yes, it is what we are going to learn in this series of OPAMP 101. An operational amplifier is the most common and most widely used type of component in an analog circuit. We can not imagine an integrated circuit without amplifiers. It is common, but students, on the other hand, often have a love-hate relationship: “How can something that looks so simple (just a triangle!) cause so much confusion?” An operational amplifier can perform a lot of mathematical operations; we will see t......
Oct 24, 2025
PCB Materials Science
Rogers vs PTFE vs Teflon: Choosing the Best PCB Laminate for High-Frequency Design
FR4, being the most popular one, is not always used in high-frequency PCBs because this PCB laminate can degrade the signal performance at high frequencies. Not because they consist of any wrong conduction material, but the reality lies in the substrate dielectric properties. The dielectric itself attenuates the signal at high frequency. So, after a lot of research in this area, we got some really good materials. The three alternatives for high-performance PCBs are Rogers, PTFE, and Teflon laminates. ......
Oct 20, 2025
PCB Materials Science
Role of Prepreg in Multilayer PCB Manufacturing
A PCB stackup arrangement includes layers, planes, cores, base, substrate, laminate, and prepreg. From Core we can say FR4, Aluminum, Rogers and all. On the other hand prepregs are the dielectric material between the adjacent cores or the core and a layer. In multilayer PCBs, prepreg is a vital part that holds the PCB core and layers together. Once the difference between prepreg and core is clear, what exact material should you use for your application? How do the important electrical parameters chang......
Oct 20, 2025
PCB Materials Science
How Aluminum PCBs Improve Thermal Conductivity
Thermal management has become one of the most important issues in electronic design as contemporary electronics get smaller and more potent. PCBs have a variety of cores and materials. In the past, we have covered a wide range of materials. Today, however, metal core PCBs are the primary emphasis. Poor heat dissipation in basic PCBs causes electrical devices to perform worse, last less time, or possibly fail catastrophically. Compared to conventional FR-4 boards, aluminum PCBs have better heat conduct......
Jul 20, 2025
PCB Materials Science
The Impact of Inner Layer Residual Copper Rate on Board Thickness
When we were kids, we heard the children's story "The Crow Drinks Water," where a crow raises the water level by dropping stones into a fixed amount of water in a bottle. The same principle applies to multilayer PCB lamination, where during high temperature and high pressure, PP sheets flow in a liquid state to fill the gaps between the layers. This process is called "resin filling." As seen in the diagram, when the copper coverage in the inner layer is minimal, PP sheets of the same thickness need to......
Feb 05, 2025
PCB Materials Science
PCB Board Thickness: Importance and Considerations
An integral component of a printed circuit boards (PCB) design and utility is its thickness. It influences its mechanical stability, electrical performance, and simplicity of construction as well as mechanical strength. Knowing what thickness is optimum for each application is crucial since electronics must get ever smaller. This article discusses the importance of PCB board thickness, the elements affecting it, the accepted thicknesses, and how one should pick the best one. What is PCB Board Thicknes......
Jan 16, 2025
PCB Materials Science
Understanding the Importance of Coverlay in PCB Boards
Introduction: In the swiftly evolving realm of electronics, the significance of Printed Circuit Boards (PCBs) is immense. These crucial elements are the backbone of nearly all electronic devices. An essential feature that greatly boosts the performance and durability of PCBs is the coverlay. This article delves into the role, advantages, and innovations of coverlay in PCB boards. What is Coverlay? Coverlay, also called cover film, is a protective layer used mainly in flexible PCBs. Unlike the conventi......
Dec 06, 2024
PCB Materials Science
Aluminum PCBs: Transforming Thermal Management in Electronics
Introduction In the fast-paced world of electronics, managing heat effectively is crucial for maintaining the reliability and performance of devices. One major advancement in this field is the adoption of aluminum PCBs. Aluminum PCBs, celebrated for their exceptional thermal conductivity and heat dissipation capabilities, have become a vital solution for high-power applications. This article explores the benefits, applications, and design considerations associated with aluminum PCBs, highlighting how ......
Nov 20, 2024
PCB Materials Science
How Inner Layer Residual Copper Rate Affects PCB Thickness and Quality
In printed circuit board (PCB) manufacturing, precision is crucial for maintaining quality and performance. One key factor that significantly influences PCB quality is the residual copper rate in the inner layers. This concept becomes particularly critical in multilayer PCBs, where the balance of copper distribution impacts the final board thickness. This article explores how the inner layer residual copper rate affects board thickness and the importance of optimizing this rate to ensure robust and re......
Sep 24, 2024
PCB Materials Science
Unlocking the Power of Aluminum PCB: Enhancing Heat Dissipation in Electronics
In the fast-paced world of electronics, effective heat dissipation is crucial for ensuring the optimal performance and longevity of electronic devices. An aluminum PCB has emerged as a game-changer, offering superior heat dissipation and thermal transfer capabilities compared to standard FR-4 construction. At JLCPCB, we are thrilled to introduce our new product - Aluminum PCB Board, now available at an incredible price of only $2! In this comprehensive blog post, we will delve into the benefits of an ......
Sep 27, 2023
- 1
- 2
- 3
- 4
- 5
- 6
- 8