PCB Quality & Reliability Testing
A guide to AOI, flying probe, E-test, and reliability tests that ensure PCB performance and long-term durability.
Latest Posts
Quality & Reliability Testing
PCB Testing Methods: A Comprehensive Guide to Testing and Characterizing PCBs
Key Takeaways PCB testing helps identify manufacturing defects, verify electrical connections, and ensure product quality. Different testing methods serve different purposes: AOI and X-ray detect visual and hidden defects, while Flying Probe and ICT identify electrical issues. Functional and reliability testing help evaluate circuit performance under specific operating conditions. Combining appropriate inspection and testing methods improves quality control across PCB fabrication and PCBA assembly. JL......
Nov 06, 2026
Quality & Reliability Testing
How PCB Thermal Cycling Tests Reveal Manufacturing Reliability
Key Takeaways Exposes Hidden Faults: Thermal expansion opens tiny cracks, catching via failures that room tests miss. Expansion Mismatch Stress: Heat differences weaken vias and solder joints over time. Standardized Testing: Follows IPC and JESD rules, failing when resistance increases. Process Prevention: High Tg materials, thick copper, and filled vias boost board life. Destructive Test: Consumes board life, so tested samples must be scrapped. A PCB thermal cycling test can detect faults that a room......
Nov 05, 2026
Quality & Reliability Testing
Why PCB Inspection Microscopes Matter in Electronics Manufacturing
Key Takeaways Precise Faults: ICT tests individual components to report exact pin-level failures. Layout-Driven: Coverage relies on test pad size, pitch, and component clearance. Speed vs. Tooling: Bed-of-nails tests in seconds; flying probe requires no custom fixture. Guarded Isolation: Isolates components from parallel paths to catch early defects. Layered QA: Pairs with AOI and AXI for full quality coverage. A PCB inspection microscope earns its place on a production line because the costliest defe......
Nov 03, 2026
Quality & Reliability Testing
How Sustainable Materials and Expert Manufacturing Ensure RoHS Compliant PCBs
Have you ever experienced that a finished shipment of products was detained at the EU customs due to a single component on the board not passing the RoHS screening? It is higher than most engineers think, and the financial blow is far bigger than the impounded goods. Wasted time, remodeling expenses, and a compliance audit that is capable of halting your whole product introduction, that is the actual cost of doing RoHS wrong. The point is as follows: RoHS-compliant PCBs cease to be a checkbox exercise......
Oct 29, 2026
Quality & Reliability Testing
Ensuring Superior Solderability: The Critical Role of Testing in Reliable PCB Production
Key Takeaways Core Purpose: Verifies solder wetting before assembly to prevent yield drops and joint failures. Destructive Test: Per J-STD-002, tested components and coupons cannot be reused in production. Pass Standards: Requires 95 percent solder coverage on leads and 80 percent on exposed thermal pads. Key Defects: Catches non-wetting (exposed metal), dewetting (solder pulling back), and black pad on ENIG. DFM Prevention: Use thermal relief, keep silkscreen off pads, and select the right surface fi......
Oct 29, 2026
Quality & Reliability Testing
Solder Joint Inspection in PCB Manufacturing : A Complete Guide to Catching Defects Early
Key Takeaways Solder Joint Inspection is critical in modern PCB manufacturing to catch defects early and ensure product reliability. By combining Solder Paste Inspection (SPI), 3D AOI for visible joints, and X-ray for hidden BGA/QFN issues, manufacturers can effectively detect common defects such as bridging, cold joints, tombstoning, and head-in-pillow. Following IPC-A-610 standards with a layered inspection strategy significantly reduces field failures while improving first-pass yield. JLCPCB’s prof......
Oct 29, 2026
Quality & Reliability Testing
PCB Delamination Explained: Causes, Detection, and Prevention
Key Takeaways Causes: Moisture turns into steam during 260C reflow, causing layer separation under thermal expansion. Materials: High-temp lead-free builds require mid/high-Tg laminates instead of standard FR4. Detection: Surface blisters are visual, while internal voids need acoustic testing or microsectioning. Prevention: Protect bond strength using balanced copper, proper press profiles, and dry packaging. Fixes: Epoxy repair only works on minor surface defects; internal splits require board replac......
Oct 22, 2026
Quality & Reliability Testing
Key Benefits of In-Circuit Test in High-Yield PCB Manufacturing
Key Takeaways Precise Faults: ICT tests individual components to report exact pin-level failures without booting firmware. Layout-Driven: Coverage depends on layout rules like test pad size (0.9-1.0 mm), pitch, and clearances. Fixtures vs. Probes: Bed-of-nails runs in seconds for high volume; flying probes require zero tooling for prototypes. Guarded Accuracy: Guarding isolates components from parallel paths to detect bad values early and lower rework costs. Layered QA: Combining ICT with AOI and AXI ......
Oct 20, 2026
Quality & Reliability Testing
Why PCB Test Coupons Are Critical for Reliable Board Manufacturing
Key Takeaways Sacrificial Testing: Coupons allow destructive tests without harming active boards. True Process Mirror: They match the exact stackup and density to reflect panel quality. Clean Measurements: Straight lines enable precise TDR impedance and via inspection. Quality Shield: Coupon failures isolate flawed panels before shipping. A PCB test coupon is the one piece of your order that is intentionally destroyed. It rides in the panel border beside your boards, so it sees every drill, plating, a......
Sep 22, 2026
Quality & Reliability Testing
How to Master PCB Impedance Testing for High-Speed Designs
Key Takeaways Verification via TDR: Impedance testing uses Time-Domain Reflectometry (TDR) on test coupons to verify high-speed traces. Real-World Factors: Actual impedance is shifted by manufacturing variables, including trace undercut, solder mask, and pressed dielectric thickness. Design-to-Fab Loop: Use the manufacturer's exact stackup Dk values for layout and TDR reports to refine revisions within $\pm 10\%$ tolerance. An impedance test can be the difference between a USB 3.0 link that works reli......
Sep 15, 2026
Quality & Reliability Testing
Guardians of Quality: A Complete Walkthrough of PCB Inspection Standards
Key Takeaways Layered Defense: Combining AOI, AXI, ICT, and FCT covers all inspection blind spots. Paste Printing: Solder paste causes up to 60% of defects, making early checks vital. IPC Standards: IPC Class 3 tightens BGA void limits from 25% to 10%, raising costs. Thermal Balance: Equal layout heating balances reflow pull to prevent tombstoning. Design Control: Clear test pads and visible polarity marks ensure reliable automated checks. PCB inspection is not one check performed at the end of produc......
Aug 26, 2026
Quality & Reliability Testing
3D AOI Inspection Explained : How It Catches Defects That 2D Systems Miss
Key Takeaways 3D AOI Inspection has become essential in modern PCB assembly by using advanced height and volume measurement to detect critical solder defects that traditional 2D AOI systems routinely miss, such as lifted leads, insufficient solder, head-in-pillow, and component coplanarity issues. By delivering precise 3D data through structured light or Moire technology, it significantly reduces false calls, improves first-pass yield, and ensures long-term reliability according to IPC-A-610 standards......
May 20, 2026
Quality & Reliability Testing
Preventing PCB Warping: Best Practices for Design and Manufacturing
In the design and manufacturing process of electronic equipment, PCB (Printed Circuit Board) warpage is a common but troublesome problem. PCB warping not only affects the performance and reliability of the device but can also cause connectivity issues and other serious consequences. Therefore, it is crucial to understand how to prevent and resolve PCB warping. This article will explore some best practices in design and manufacturing to help you effectively prevent PCB warpage problems from occurring. ......
Apr 09, 2026
Quality & Reliability Testing
PCB Cleanliness in Professional Manufacturing : Preventing Contamination and Ensuring Long-Term Reliability
In the construction of PCBs, the boards are contaminated with all sorts of dirt at almost every stage. In the soldering process, the flux (either rosin-based or more recent organic forms) may cause residues or ionic salts to remain on the pads and traces and be sticky. Next there is etching, plating and micro-etching; the chemical processes will put metal ions on the copper unless the rinsing is complete. Tiny particles of metal shavings, fiberglass dust, and laminate fragments are also thrown out in ......
Apr 07, 2026
Quality & Reliability Testing
How PCB Cross Section Analysis Ensures Flawless Multilayer PCB Quality
Ever wondered what is really under a multilayer PCB? A completed board appears to us as a student as a flat and homogeneous slab of laminate and copper, yet internally a maze of plated vias, buried copper layers, thin dielectric films, and resin-filled structures, all of which must be within very strict tolerances. Cross-section analysis is the PCB equivalent of peeling back the layers and getting the true picture. Every person involved in PCB design or manufacturing, in a laboratory or on a productio......
Mar 24, 2026
Quality & Reliability Testing
Test PCB Board : Complete Testing Methods and Best Practices
As a PCB manufacturer, we always conduct testing with a number of stages, because if you’ve ever designed a PCB and sent a beautifully routed board to JLC, waiting eagerly for delivery, unboxing it like a new iPhone, only to find out later that a single microscopic solder bridge is enough to turn your masterpiece into a glorified coaster. This is exactly why PCB testing exists, and we are focused more extensively on it. PCB testing is like a basic “health checkup” of your electronic product before it ......
Feb 04, 2026
Quality & Reliability Testing
Quality Control and Testing in Bare Board Manufacturing
Bare printed circuit boards, or PCBs, are the foundation of almost all electronic devices made today, from computers and cellphones to industrial control systems and aeronautical electronics. Quality control and testing in bare board manufacturing have grown more important since these applications require more dependability. Defects at the PCB level might cause even the most sophisticated circuit designs to fail in the absence of adequate quality assurance. In order to guarantee long-term performance ......
Dec 02, 2025
Quality & Reliability Testing
How to Avoid Copper Peel Off
Hot Air Solder Leveling (HASL) involves coating the surface of the exposed copper with a layer of tin alloy to prevent oxidation and provide a good soldering surface for subsequent assembly. The basic process of HASL is to briefly immerse the PCB board into a high-temperature liquid tin bath. Through the action of flux and high-temperature tin, a copper-tin alloy (IMG) is formed. Then, on guide rails, the board is lifted out while high-pressure gas blows away excess tin from non-copper areas and level......
Jun 14, 2024
- 1
- 2