HDI PCB Design & Structure
An overview of HDI stackups, fabrication techniques, routing methods, and applications in compact, high-density electronics.
Latest Posts
HDI PCBs
How Stacked Vias Enable Higher Density and Better Performance in HDI PCBs
Key Takeaways Stacked vias are a critical technology that enables higher routing density and superior performance in HDI PCBs. By vertically aligning microvias in a single column, often combined with via-in-pad designs, they dramatically reduce breakout area, shorten signal paths, lower parasitic inductance, and improve thermal conductivity compared to traditional staggered vias. While requiring precise sequential lamination, via filling, and strict design rules, stacked vias help designers reduce lay......
Oct 30, 2026
HDI PCBs
HDI PCB vs Standard PCB: Key Differences and Benefits
Printed Circuit Boards (PCBs) constitute the core of any electronic system and provide mechanical and electrical connections to other electronic components. They are in the cars we drive, the capsules we open, and in what we put inside them, and use them in planes and rockets, with ever more unique aerospace solutions. Let’s face it: traditional PCB boards have served as an industry standard for decades; However, the need for smaller, faster products has sparked the rise of High-Density Interconnect (......
Oct 28, 2026
HDI PCBs
Comprehensive Guide to HDI PCBs: Design, Advantages, and Applications
Key Takeaways Core HDI Limits: Standard HDI uses 3/3 mil trace/space and 4 mil laser microvias for optimal yield and density. Via-in-Pad Benefits: Resin-filled microvias on SMT pads (JLCPCB's FPOV) eliminate fan-out and prevent solder wicking. Smart Stack-ups: Symmetrical 1+N+1 or 2+N+2 staggered microvias cut lamination costs and thermal stress. High Density Interconnect (HDI) printed circuit boards (PCBs) are circuit boards with a higher wiring density per unit area than traditional PCBs. HDI PCBs h......
Oct 20, 2026
HDI PCBs
Stack-Up Strategies for Effective HDI PCB Design
Whether you believe Moore's Law is dead or alive, the strong economic incentive to pack more processing power into ever smaller form factors is unlikely to abate any time soon. With the entry of the HDI stackup—a technology at the cutting edge of multilayer PCB design that promises to help PCB designers make smaller complex boards for years to come. The stack-up in a printed circuit board (PCB) design is a critical element that influences the board's performance, manufacturability, and reliability. In......
Oct 15, 2026
HDI PCBs
How to Optimize Layer Stack-Up in HDI PCB Boards
With the introduction of the HDI stackup, a cutting-edge technique in multilayer PCB design, PCB designers should be able to create increasingly complex, smaller boards in the years to come. Establishing your project's needs precisely is the first step in designing a PCB stackup. Determining the number of layers required is the first stage; this depends on the circuit's complexity, signal density, power distribution requirements, and if the design calls for RF or high-speed signals. In the late 1980s,......
Oct 15, 2026
HDI PCBs
High-Density Interconnect (HDI): Revolutionizing PCB Design for Modern Electronics
In the world of advanced electronics, High-Density Interconnect (HDI) technology has become a game-changer. As devices get smaller, faster, and more complex, traditional printed circuit boards (PCBs) often face limitations in handling these demands. That’s where HDI PCBs come into play. This article covers what HDI is, why it’s critical, and how it’s shaping the future of modern electronics. What is High-Density Interconnect (HDI)? A "HDI" printed circuit board (PCB) is one type whose wire count per u......
Oct 15, 2026
HDI PCBs
Comparing High-Density PCB Stack-Up With Normal PCB
High-density printed circuit boards (PCBs)are not the same as simple PCBs. Do you know what the difference is? PCBs with a larger number of layers and a higher density of traces are known as HDIs. These are not as common because they are not used in small prototypes or hobby work, but for more professional application. One of the best examples of an HDI board with a complex stack-up that you can see—or might have—is the motherboard of your PC. HDI changes the story completely when it comes into the pi......
Oct 15, 2026
HDI PCBs
Via in Pad (VIP) Technology : Driving Density and Reliability in Advanced PCB Fabrication
Via in pad is exactly what it sounds like: placing a via directly within a component’s soldering pad rather than routing it off to the side with a short trace. While this concept seems straightforward, it represents a significant evolution in PCB design philosophy that has become essential for modern high-density interconnect (HDI) boards. In traditional PCB design, vias were always placed outside the component pad area, connected by a short fanout trace. This approach works fine when you have plenty ......
Oct 15, 2026
HDI PCBs
Designing with Microvias: Stack-Ups, Reliability, and Via Filling
Have you ever wondered how designers pack so much functionality into such a small space? You can thank HDI design techniques and microvias in printed circuit design. High-Density Interconnect (HDI) PCB technology is at the forefront of modern electronics, enabling compact and powerful devices. These structures have been around for years, but they are becoming more common in a variety of systems that require multiple functions on a single circuit board. If you've done a size study and you've determined......
Sep 09, 2026
HDI PCBs
Via-in-Pad in PCB: Advantages and Challenges
In printed circuit board (PCB) design, via-in-pad has become a widely adopted technique, particularly in high-density interconnect (HDI) designs. It is particularly designed for BGAs with a package pitch of 0.8 mm or smaller. It involves placing a via directly within the surface mount pad of a component, offering several design and performance benefits. For example – placement of decoupling capacitors closer to IC pins, improving bypassing and noise performance. Proper via-in-pad implementation ensure......
Sep 09, 2026
HDI PCBs
Blind vs Buried Vias: A Comprehensive Guide for PCB Design
A printed circuit board (PCB) is made up of layers of copper foil circuits stacked on top of each other, and the connections between different circuit layers rely on vias. If the holes drilled by a drilling machine or laser are left as is, they will not conduct electricity, because the surface of the original drilled hole is only resin, which is not conductive. Therefore, a layer of conductive material (usually copper) must be plated on the surface of the drilled hole. In this way, current propagates ......
Sep 09, 2026
HDI PCBs
Enhancing PCB Reliability: A Deep Dive into VIA-in-PAD Design
Key Takeaways Space Saving: VIA-in-PAD (POFV) places vias directly inside SMD pads, maximizing routing channels and board miniaturization. Flawless Soldering: Epoxy filling and copper capping eliminate the risk of solder siphoning, ensuring flat, perfectly solderable pads. Maximum Performance: Direct vertical paths under components drastically lower thermal resistance and eliminate high-speed parasitic inductance. JLCPCB DFM Targets: Maintain mechanical via hole diameters between 0.25 mm and 0.35 mm, ......
Jul 16, 2026
- 1
- 2