Your Ultimate Guide to PCB Rulers
9 min
- What is a PCB Ruler?
- The Main Functions of a PCB Ruler
- PCB Ruler Features and Measurements
- How to choose the right PCB ruler?
- Making Your Own PCB Ruler
- FAQ about Guide to PCB Rulers
- Conclusion
- JLCPCB Ruler
In the world of PCB design and manufacturing, having the right tools is crucial for achieving accuracy and precision. One such tool that has gained popularity among professionals and hobbyists is the PCB ruler. This specialized measuring tool is designed to provide accurate measurements, reference information, and component footprints, assisting designers, engineers, technicians, and assemblers in various stages of PCB development. In this guide, we'll explore what a PCB ruler is, the features and measurements it offers, how to choose the right PCB ruler, and tips for creating a custom one.
What is a PCB Ruler?
A PCB ruler is a dedicated measuring tool specifically designed for PCB-related tasks. Crafted from durable materials like FR-4 or metal, these rulers ensure longevity and accuracy. They feature a wide range of markings, encompassing measurements, component footprints, and various reference guides. These elements are aimed at facilitating efficient PCB design and assembly processes.
The Main Functions of a PCB Ruler
A PCB ruler primarily serves two vital purposes in the PCB design process.
Firstly, it provides accurate measurements and reference information for electronic components and traces on a printed circuit board. This knowledge is essential to prevent mistakes during the welding process, ensuring precise component placement and proper circuit functionality.
Secondly, the ruler aids in visualizing and understanding the packages of components such as resistors, capacitors, inductors, and IC chips, allowing designers to make informed decisions during the design phase.
PCB Ruler Features and Measurements
The markings on a PCB ruler serve multiple purposes and offer valuable features to designers. Here are some key features of PCB rulers:
1. Measurement Precision for Component Layout
Accurate measurements provided by the ruler enable designers to plan and lay out components on the board with precision. This assists in avoiding design errors and optimizing component placement within the available space.
2. Optimizing Trace Width for Performance
Many PCB rulers include trace width references, helping designers determine the appropriate trace width based on factors like current carrying capacity. By utilizing these references, designers ensure that the PCB can handle the required electrical current without any performance issues or overheating.
Beyond conceptual calculations, a physical PCB ruler provides an immediate visual comparison for trace widths (e.g., 4 mil, 6 mil, 10 mil, up to 40 mil). This helps designers build intuition during layout. Based on JLCPCB's standard 1 oz copper weight manufacturing process, the following reference table can guide your trace width selection:
| Trace Width (mil) | Metric Equivalent (mm) | Max Current (A) at Delta T = 10°C | JLCPCB Process Role |
|---|---|---|---|
| 3.5 | 0.090 | 0.25 | Minimum trace width limit for multi-layer PCBs |
| 5.0 | 0.127 | 0.40 | Standard minimum trace width for double-sided PCBs |
| 8.0 | 0.203 | 0.70 | Safe and recommended width for general signal traces |
| 12.0 | 0.305 | 1.10 | Recommended width for low-power rails |
| 20.0 | 0.508 | 1.60 | Heavy trace width recommended for main power or GND |
3. Visualizing Component Size and Shape
PCB rulers offer more than just measurements and trace width references. They also incorporate component footprints, allowing designers to visualize the size and shape of electronic components. This enables them to ensure compatibility with the available space on the PCB and make informed decisions during the component selection process.
By utilizing the precise measurements, trace width references, and component footprints provided by PCB rulers, designers can achieve accurate component placement, optimal trace routing, and adherence to industry standards. The use of a PCB ruler not only saves time but also minimizes errors, resulting in high-quality PCB designs.
How to choose the right PCB ruler?
When selecting a PCB ruler, several factors should be considered to ensure its suitability. Here are four important factors to keep in mind:
1. Accuracy:
Choose a PCB ruler that provides accurate measurements and component footprints to ensure precise design and compatibility.
2. Durability:
Considering the demanding nature of PCB design, select a ruler made from durable materials such as
FR-4 fiberglass or Aluminum. This ensures its longevity and reliability throughout the design process.
3. Ease of use:
Opt for a PCB ruler with clear markings, easy-to-read fonts, and user-friendly features such as color-coded sections. These characteristics enhance the designer's experience and overall efficiency.
4. Compatibility with design software:
Some PCB rulers are designed to be compatible with popular design software, allowing designers to import measurements and footprints directly into their projects. This streamlines the design process and improves efficiency.
Making Your Own PCB Ruler
If you prefer a custom PCB ruler tailored to your specific needs, follow these steps:
Plan the design:
Determine the specific features and measurements you want to include on your ruler, such as trace widths, drill sizes, and component footprints.
Use PCB design software:
Utilize software like EasyEDA, KiCad, or Altium Designer to create your ruler design. Take advantage of precise measurement tools, component libraries, and design rule checks for accuracy.
Determine size and scale:
Choose a suitable size for your ruler, ensuring it fits within your workspace and is easy to read. Common dimensions include lengths of 15 centimeters (150 mm) or 6 inches.
Choose a suitable material:
Select a durable and stable material for your ruler, considering factors like rigidity and resistance to environmental factors. FR-4 fiberglass or aluminum are popular choices.
Ensure clear markings:
Use appropriate line thicknesses and font sizes to enhance readability on your ruler, ensuring the measurements are clear and legible.
Verify accuracy:
Compare your ruler to a calibrated reference or standard ruler, making adjustments as needed to ensure precise measurements.
Include alignment marks:
Add alignment marks or registration features to aid accurate positioning during PCB layout tasks.
Incorporate component footprints:
Optionally include commonly used component footprints to serves a quick reference during PCB layout.
Export and fabricate:
Export your PCB ruler design in Gerber format and choose a reliable manufacturer. Specify the material, layer stackup, copper weight, solder mask color, and silkscreen preferences. Provide the necessary files and specifications, following the manufacturer's guidelines for smooth fabrication.
When uploading Gerber files to JLCPCB, matching your order configuration to the ruler's dual role as an artwork and a reference tool is critical. Since a PCB ruler features numerous exposed copper areas for IC footprints and pad pitches, standard HASL (Hot Air Solder Leveling) may cause uneven padding. Specifying Electroless Nickel Immersion Gold (ENIG) as the surface finish is highly recommended; it ensures perfectly flat pads and prevents the exposed gold scales from oxidizing over time, ensuring long-term measurement precision.
| Manufacturing Option | Recommended Selection | Engineering Reason |
|---|---|---|
| Base Material | FR-4 / Aluminum | Maintains structural rigidity and prevents the ruler from bending |
| Board Thickness | 1.6 mm / 2.0 mm | Provides a solid, professional, and premium feel for handheld tools |
| Surface Finish | ENIG (Gold Plating) | Essential for perfectly flat component pads and excellent oxidation resistance |
| Solder Mask Color | Matte Black / Purple | Offers exceptionally high visual contrast against gold traces and white text |
| Silkscreen Color | White | Ensures maximum contrast and readability for fine fonts and sub-mil lines |
| Flying Probe Test | Fully Tested | Verifies electrical continuity if the ruler includes functional sample circuits |
Review and test:
Thoroughly review and test the accuracy of your custom PCB ruler upon receiving it. Verify the measurements against a calibrated reference and ensure that the markings are clear and legible. Make any necessary adjustments for future iterations if needed.
FAQ about Guide to PCB Rulers
Q: Why is ENIG surface finish highly recommended for a PCB ruler over HASL?
ENIG provides a perfectly flat surface and excellent oxidation resistance. Since a PCB ruler features exposed copper for IC footprints and fine-pitch pads, HASL can cause uneven solder bumps, making it difficult to use as a precise physical reference.
Q: What are the minimum trace width and clearance limits when manufacturing a ruler with JLCPCB?
For standard double-sided PCBs, JLCPCB supports a minimum trace width and spacing of 5 mil (0.127 mm). For advanced multi-layer boards, it can go down to 3.5 mil (0.09 mm). Ensure your ruler's calibration lines do not go below these manufacturing thresholds to avoid production errors.
Q: How can I prevent the automated JLCPCB order number from ruining my ruler's aesthetic design?
During the online ordering process on the JLCPCB website, you can select the "Specify Location" option and place the placeholder text on your silkscreen layer where you want the code hidden (e.g., under a large IC footprint). Alternatively, you can pay a small fee and select "Remove Order Number" to remove it entirely.
Q: How do I ensure the physical scale of the ruler remains 1:1 accurate after exporting Gerber files?
Always design using a 1:1 scale in your EDA software and verify that the export unit matches the standard CAM imperial/metric settings. Before submitting the order, use JLCPCB’s online Gerber Viewer to double-check that the calculated outline dimensions perfectly match your design intent.
Q: Can I design a ruler with custom cutouts, hanging holes, or curved slots via JLCPCB?
Yes, you can draw any custom shapes, internal slots, or hanging holes on the Mechanical or Outline layer. JLCPCB uses high-precision CNC routing to cut the board outline. Ensure that any internal slot width is at least 1.0 mm to accommodate the standard routing bit size.
Conclusion
In conclusion, PCB rulers remain essential tools in the realm of PCB design and manufacturing. Despite the availability of online tools, physical PCB rulers offer crucial advantages for real-world PCB design. They provide precise measurements, facilitate accurate component placement, and enhance the overall development process. By utilizing PCB rulers, designers and manufacturers can boost efficiency, minimize mistakes, and achieve superior quality PCBs.
JLCPCB Ruler
The JLCPCB ruler combines both imperial and metric units of measurement. It prominently displays numerical values from 0 to 20 centimeters, showcasing its accurate measurement capabilities. Additionally, smaller increments between the printed numbers allow for precise measurements. The ruler is also adorned with a cute cartoon bear.
Keep Learning
FR4 PCB Deep Guide: Material Truth, Real Specs & When to Use (or Avoid) It
FR-4 isn't a secret code, it literally means Flame Retardant (grade 4). In PCB terms, FR-4 is a NEMA (National Electrical Manufacturers Association) grade designation for a glass-reinforced epoxy laminate. We can say it is a composite of woven fiberglass cloth bonded with an epoxy resin that contains flame-retardant additives. The “FR” stands for flame retardant, but note this doesn’t automatically mean UL94 V-0 certified. It just indicates the resin is formulated to self-extinguish if it catches fire......
What is the Standard Thickness of a PCB?
Key Takeaways 1.6 mm Standard: 1.6 mm (0.062") is the universal industry standard, balancing rigidity, assembly ease, and component fit. 0.4mm–3.0mm Options: JLCPCB provides versatile FR-4 thicknesses from 0.4 mm for ultra-thin devices to 3.0 mm for high-power systems. Stackup Flexibility: Multilayer PCBs up to 12–16 layers can still maintain a 1.6 mm profile using thinner cores and prepregs. Impedance & Heat Balance: Dielectric thickness directly sets trace impedance (Z0), while thicker boards increa......
How Laser Drilling Delivers Precision and Density in Advanced PCB Manufacturing
Key Takeaways Laser Drilling has become the cornerstone technology for precision and high-density PCB manufacturing, enabling microvias as small as 25-75μm — far beyond the 150μm limit of mechanical drilling. By delivering superior accuracy, contactless processing, excellent signal integrity, and reliable blind/stacked vias, it empowers advanced HDI board designs essential for modern electronics. From optimal stackup selection to professional plating and DFM practices, mastering laser drilling is key ......
Why Sequential Lamination Delivers Superior HDI PCBs
Did you ever ask yourself how smartphone manufacturers can crust a thousand connections into a credit card-sized board? The process is referred to as sequential lamination, which is a multi-cycle process that is used to fabricate PCBs on a layer-by-layer basis, releasing microvia structures and routing densities that cannot be accessed by a single-press process. Without it, the slick, high-performance electronics that we all use on a daily basis would not appear the way that they do now. With data rat......
Buried Vias in Advanced PCBs: Enabling Higher Density, Better Signal Integrity, and Compact Designs
Key Takeaways Hidden Routing: Buried vias connect only inner layers, keeping outer surfaces clear for dense components and traces. Better Signal Integrity: They eliminate via stubs, reducing parasitics and signal loss in high-speed designs. Higher Density: Essential for HDI boards, dense BGAs, and small form factors like wearables. Higher Cost: Sequential lamination and extra drilling steps make them ~3×-4× more expensive than standard through-holes. Ever wondered how a modern smartphone mainboard can......
Unlocking Higher Density and Better Performance with Blind Vias in HDI PCBs
Key Takeaway Higher Density: Connects surface to inner layers without penetrating the whole board, freeing routing channels under fine-pitch BGAs. Improved Signal Integrity: Reduces via stub length to minimize impedance discontinuities in high-speed designs. Aspect Ratio Rule: Keep the depth-to-diameter ratio near 0.75:1 (max 1:1) for reliable laser drilling and void-free plating. Thermal Efficiency: Supports via-in-pad setups for better heat dissipation and compact component placement. Ever wonder ho......