PCB Components & Sourcing Guide
Articles covering PCB component types, SMD packages, part selection, sourcing strategies, availability risks, and BOM stability in electronics manufacturing.
Featured Posts
Components & Sourcing
SMD Resistor Package Sizes: Complete Size Chart, Footprints & How to Choose
Surface Mount Device (SMD) resistors are fundamental to modern electronics, and selecting the correct package size is a crucial engineering decision that impacts a PCB’s electrical performance, thermal reliability, and manufacturing cost. In this article, you will find practical, authoritative guidance on: The complete SMD resistor size chart (01005 to 2512) with exact dimensions and power ratings. Recommended PCB footprints and guidelines for reflow reliability. Critical trade-offs concerning power d......
Dec 08, 2025
Components & Sourcing
How to Solder SMD Components Like a Pro [2026 Updated]Sep 19, 2025Components & Sourcing
SMD Resistor Codes: How to Read 3-Digit, 4-Digit, and EIA-96 MarkingsDec 27, 2025Components & Sourcing
SMD Capacitor Codes: Identification, Markings, and PolarityDec 27, 2025Components & Sourcing
SMD Capacitor Sizes: Complete Size Chart and Selection Tips for PCB Design and AssemblyMar 13, 2026
Latest Posts
Components & Sourcing
What Are the Main Relay Types and Which One Should You Use?
Key Takeaways Two Main Types: Relays fall into two main categories: electromechanical relays, which use moving metal contacts to switch a circuit, and solid-state relays, which use electronic components with no moving parts. Choose Based on the Load: The load type determines which relay you need. Consider whether the load uses AC or DC, how much current it draws during normal operation and startup, and how frequently it needs to switch. Coil Behavior: A monostable relay returns to rest when its coil i......
Oct 23, 2026
Components & Sourcing
SMD MOSFET Code Guide: How to Identify, Test and Replace a MOSFET
Figure: AO3400A (C20917) in the JLCPCB parts library. The listing gives RDS(on) at 2.5 V gate drive, the number that matters in the replacement example later in this guide. An SMD MOSFET code is the two or three characters printed on top of the package, and on its own it rarely tells you which part you're holding. SMD resistors follow standard marking schemes, such as three- and four-digit codes and EIA-96. MOSFETs don't. The same short code can appear on unrelated parts from different manufacturers, ......
Oct 22, 2026
Components & Sourcing
ESP8266 vs ESP32: Which One Should You Use?
Key Takeaways ESP32: Dual-core 240 MHz CPU, Bluetooth Classic and BLE, 520 KB SRAM, and up to 34 GPIOs. ESP8266: Single-core CPU, no Bluetooth, and around 50 KB of free RAM for applications. Lifecycle status: Espressif marks the ESP8266 Not Recommended for New Designs (NRND) and names the ESP32-C2 (ESP8684) as its upgrade, although the ESP8266 remains in production with a longevity commitment. Which ESP32 to use: Choose the ESP32-C2 for simple Wi-Fi or Bluetooth LE firmware, the ESP32-C3 for more memo......
Oct 16, 2026
Components & Sourcing
What Is a Thermistor? A Practical Guide to NTC, PTC, Applications, and Circuit Design
Key Takeaways Definition: A thermistor is a thermally sensitive resistor whose resistance changes markedly and predictably with temperature, typically by about 4.4% per °C for a standard 10 kΩ NTC (B25/50 = 3950 K) near 25 °C. NTC vs. PTC: An NTC thermistor's resistance falls as temperature rises, which suits temperature sensing and inrush current limiting; a switching PTC's resistance rises steeply above its switch temperature, which suits circuit protection. Key Specifications: An NTC thermistor is ......
Oct 16, 2026
Components & Sourcing
What Is the ESP32-CAM, and How to Wire, Power, and Program It?
Key Takeaways Board, not chip: The ESP32-CAM is an AI-Thinker development board, not an Espressif product. It carries AI-Thinker's ESP32-S module, an OV2640 camera, PSRAM, a microSD slot, and a flash LED. No USB port: The board has no USB connector or USB-to-UART bridge, so you program it via its serial pins using a 3.3 V USB-to-serial adapter, with GPIO0 held low at reset. Few free pins: The camera, PSRAM, and microSD card occupy most GPIOs. With the microSD card unused, GPIO2, GPIO4, GPIO12, GPIO13,......
Oct 14, 2026
Components & Sourcing
ESP32 Versions: Which One Should You Use for Your Project?
Key Takeaways Radios decide first: ESP32 versions differ mainly in their radios, CPU cores, and peripherals. Common defaults: The ESP32-C3 suits low-cost Wi-Fi and Bluetooth LE, the ESP32-S3 suits camera, display, voice, and on-device AI. Original ESP32: The chip is still in production and remains the choice for Bluetooth Classic. Versions without Wi-Fi: The ESP32-H2 targets battery-powered Thread and Zigbee devices. Chip, module, or board: Prototype on a development board, then design a module onto y......
Oct 13, 2026
Components & Sourcing
SOIC Package: A Complete Guide to Specifications, Types, Uses, and SMT Assembly
As designs transition from legacy through-hole components to high-density Surface Mount Technology (SMT), the Small Outline Integrated Circuit (SOIC) remains the industry standard for operational amplifiers, flash memory, sensors, and microcontrollers. It reflects a well-balanced engineering design, offering a practical compromise between the miniaturisation demanded by modern consumer electronics and the ruggedness required for industrial applications. In this guide, you will learn: SOIC package dime......
Sep 29, 2026
Components & Sourcing
What Is a 100nF Capacitor and How Do You Choose the Right One
Key Takeaways Value: A 100nF capacitor has a nominal capacitance of 0.1 µF, or 100,000 pF, and all three names describe the same part value. Marking: Many through-hole ceramic and film capacitors use the three-digit code 104, while most SMD MLCCs are unmarked. Main use: Its most common function is local decoupling at an IC power pin, where it supplies fast transient current and shunts high-frequency noise to ground. Default choice: For general decoupling, an X7R or X5R MLCC is a common starting point;......
Sep 29, 2026
Components & Sourcing
SMD Resistor Package Sizes: Complete Size Chart, Footprints & How to Choose
Surface Mount Device (SMD) resistors are fundamental to modern electronics, and selecting the correct package size is a crucial engineering decision that impacts a PCB’s electrical performance, thermal reliability, and manufacturing cost. In this article, you will find practical, authoritative guidance on: The complete SMD resistor size chart (01005 to 2512) with exact dimensions and power ratings. Recommended PCB footprints and guidelines for reflow reliability. Critical trade-offs concerning power d......
Sep 28, 2026
Components & Sourcing
PCB Connector Types Explained: Categories, Comparison, Applications and How to Choose the Right One
PCB connectors are essential components for connecting circuit boards with external devices, cables, or other PCBs. Choosing the right connector type affects signal reliability, mechanical stability, and overall product performance. Factors such as current rating, frequency requirements, pitch size, and mounting method should be considered during selection. In this guide, you will learn: The major types of PCB connectors and their applications. How different connector types compare. How to select the ......
Sep 21, 2026
Components & Sourcing
What Is a System on a Chip (SoC)? A Complete Guide for PCB Designers
Nearly every electronic device you interact with today, from smartphones and IoT sensors to industrial controllers and AI edge systems, is powered by a System on a Chip (SoC). By integrating processors, memory controllers, communication interfaces, and specialized accelerators onto a single piece of silicon, SoCs deliver the performance, power efficiency, and compact form factors modern electronics demand. Whether you're selecting a processor for an embedded Linux design, evaluating an AI-capable plat......
Sep 21, 2026
Components & Sourcing
Capacitors in PCB Design_ A Complete Guide to All Types
Capacitors are indispensable components in PCB (Printed Circuit Board) design, providing functionality from energy storage and noise filtering to voltage regulation. Whether you're designing a simple circuit or a complex multi-layer board, understanding the different types of capacitors and their applications is crucial. The basic structure of a capacitor consists of two metal plates separated by a layer of dielectric. Capacitors can be of fixed or variable type. The ability of the capacitor to hold e......
Sep 09, 2026
Components & Sourcing
SMD LED Explained: Types, Packages, Applications, and How to Choose
SMD LED has become the standard light source in modern electronics and lighting products. From LED strips and displays to automotive dashboards and consumer devices, SMD LEDs are everywhere—but many designers and buyers still struggle to choose the right type. Package sizes, brightness, heat dissipation, color control, and assembly constraints all affect performance and reliability. Choosing the wrong SMD LED can lead to overheating, uneven lighting, or manufacturing issues. This guide breaks down wha......
Sep 09, 2026
Components & Sourcing
SMD Inductor Selection Guide: How to Choose the Right Inductor for Any Circuit
Choosing the wrong SMD inductor can quietly destroy your design - causing overheating, efficiency loss, noise, or even complete circuit failure. Yet most selection mistakes come from misunderstanding just a few key parameters. This guide cuts through the confusion and shows you exactly how to select the right SMD inductor with confidence. In this guide, you will learn: 1. How to choose an SMD inductor correctly for any circuit (not just guess from a datasheet) 2. The real difference between inductance......
Sep 09, 2026
Components & Sourcing
Ceramic Capacitor Types Explained: C0G, X7R, X5R, Y5V and How to Choose
Two ceramic capacitors can share the same capacitance value, the same voltage rating, and the same footprint, yet behave nothing alike on a powered board. The reason is the dielectric, not the number on the label. Ceramic capacitor types are defined by the dielectric, captured in codes like C0G, X7R, X5R, and Y5V. This guide decodes those codes, compares the dielectric classes, explains the DC bias and aging effects that catch designers off guard, and gives you a practical way to pick the right part f......
Sep 09, 2026
Components & Sourcing
Arduino vs Raspberry Pi: Which One Should You Actually Use for Your Project?
Note Quick Answer: Choose Arduino for robotics control, sensors, low-power builds, and direct hardware-level interaction where precise control loops matter. Choose Raspberry Pi for AI inference, Linux applications, multimedia, networking, and anything that needs a full operating system. If you have searched Arduino vs Raspberry Pi, you have probably found a dozen articles listing specs side by side without telling you what actually matters for your build. This guide is different. Whether you are proto......
Sep 08, 2026
Components & Sourcing
What is a Power Management IC (PMIC): Functions and Applications
A Power Management IC (PMIC) is a type of integrated circuit designed to manage the power requirements of the host system. It efficiently distributes, regulates, converts, and monitors electrical power for various components within a device, such as processors, memory units, and peripherals. As the demand for compact, battery-powered, and high-performance devices continues to grow, PMICs have become an essential part of system design across industries. Embedded and application processors and other com......
Sep 08, 2026
Components & Sourcing
Diode Type Guide: How to Choose the Right Diode for PCB and Product Design
Modern electronics rely on highly specialized diode types for power conversion, ESD protection, signal detection, and high-frequency switching. Choosing the wrong diode doesn't just reduce efficiency; it also generates excess heat, introduces switching losses, and can even damage sensitive circuits during voltage transients. Choosing the right component ensures a reliable board, whether you are wiring a prototype or scaling to low-volume PCB assembly. In this guide, you'll learn: How do different diod......
Sep 08, 2026
Components & Sourcing
Complete SMD Inductor Size Guide: Dimensions, Packages, and PCB Design Tips
SMD inductor size affects far more than PCB real estate. Package dimensions directly influence current handling, saturation behavior, DCR, and EMI characteristics. Picking the wrong package can mean a costly board respin, not just inefficiency. One challenge is that SMD inductor package sizes use multiple naming conventions and the fundamental split between RF chip inductors (compact footprint, high Q-factor) and power inductors (low DCR, magnetic shielding, high saturation current). This guide covers......
Sep 08, 2026
Components & Sourcing
Capacitor Polarity Explained: How to Identify It, Read Markings, and Avoid Reverse Failures
In modern electronics, the board is dominated by non-polarized components like MLCCs (Multilayer Ceramic Capacitors). Yet, for any application requiring high capacitance in a small volume - such as power supply filtering or DC-DC converters - engineers invariably turn to polarized capacitors. These components, namely aluminum electrolytic and tantalum capacitors, are the workhorses of power integrity. But they come with one critical, non-negotiable rule: they must be installed in the correct orientati......
Sep 08, 2026
Components & Sourcing
The Ultimate Guide to Wafer Level Packaging (WLP): Process, Types, Benefits, and Applications
Modern electronics are hitting a hard limit: you can’t keep shrinking devices without rethinking how chips are packaged. As PCB space tightens and signal speeds increase, traditional packaging methods introduce too much size, parasitic loss, and inefficiency. Wafer-level packaging (WLP) addresses this by forming interconnects directly on the wafer before singulation, eliminating substrates and shortening signal paths. The result is a chip-scale package with higher integration density, lower parasitics......
Sep 08, 2026
Components & Sourcing
The Engineering Guide to Capacitor Symbols: Schematic Standards and Polarity
In high-frequency PCB design and precision analog circuitry, the capacitor is not merely a charge storage device governed by the fundamental equation C = Q/V; it is a complex component possessing Equivalent Series Resistance (ESR) and Inductance (ESL). However, before a design reaches the simulation or layout stage, it begins as a symbol on a schematic. For the PCB design engineer, the capacitor symbol is a critical element, serving as the main instruction for both the layout team and the manufacturin......
Sep 08, 2026
Components & Sourcing
ESP32-C3 vs ESP32-S3 Explained: Performance, Features, and How to Choose the Right Chip
Note Pick the ESP32-C3 for low-cost, low-power, connected sensors. Pick the ESP32-S3 for anything involving a camera, a display, on-device AI, or USB. If you are making a prototype that connects to the internet using WIFI or transmits data over BLE, the most popular option among designers is ESP32. The two most popular chips from the ESP32 series are: ESP32-c3 and ESP32-s3. The pain point is to choose the one as per the required application. The ESP32-c3 vs ESP32-s3 decision trips up beginners and sea......
Sep 08, 2026
Components & Sourcing
How to Read SMD Resistor Values: Codes, Charts, and Identification Guide
An SMD resistor value is identified using numeric or alphanumeric marking codes printed on the surface of chip resistors. These codes represent resistance in ohms using standardized 3-digit, 4-digit, or EIA-96 systems. This guide breaks down the 3-digit, 4-digit, and EIA-96 marking systems so you can decode, calculate, and replace any SMD resistor with confidence. Quick Checklist to Identify SMD Resistor Value Understanding SMD resistor values simply requires recognizing which standardized system is p......
Sep 08, 2026
Components & Sourcing
How to Solder SMD Components Like a Pro [2026 Updated]
Soldering is a core skill to know, and when it comes to SMD, things become more complex and smaller. Soldering is similar to welding, but instead of welding two iron/steel pieces, we are now welding small components. To develop a circuit, the best way to join two components is by soldering. There are two main types of components in electronics: one is a through hole with long legs covered with tin, which can be easily inserted onto a PCB and then soldered, and the other is SMDs (surface mount devices)......
Sep 08, 2026
Components & Sourcing
A Beginner’s Guide to STM32 vs ESP32: Key Differences and Best Uses
STM32 vs ESP32 is the most-asked microcontroller comparison on r/embedded for a reason: they look interchangeable on paper, but solve completely different engineering problems. STM32 is an industrial-grade MCU family built on ARM Cortex-M cores and precision peripherals. ESP32 is a connectivity-first SoC built around Wi-Fi, Bluetooth, and out-of-the-box IoT. This guide breaks down where each platform wins in real engineering projects, using datasheet numbers, production design trade-offs, and practica......
Sep 08, 2026
Components & Sourcing
What Is an SMD Capacitor? A Complete Guide to Types, Sizes, Markings, and Applications
SMD capacitors are essential components in modern electronic circuits, enabling compact PCB design, high-frequency performance, and efficient automated manufacturing. As surface-mount technology has become the industry standard, understanding how these capacitors work and how to select them is crucial for engineers, students, and electronics enthusiasts. In this guide, we will explore: What SMD capacitors are and how they differ from through-hole capacitors The main types of SMD capacitors and their e......
Sep 08, 2026
Components & Sourcing
Capacitor Value Guide: Charts, Codes, Selection & Practical Uses
Whether you're adding a 100nF bypass capacitor to a microcontroller, sizing a smoothing capacitor for a power supply, or selecting a capacitor for an RC filter, choosing the wrong value can lead to noise, instability, or poor circuit performance. Capacitor selection is one of the most frequent decision points in hardware engineering, yet finding the right balance between theory and physical constraints is rarely straightforward. In this guide, you'll learn how capacitor values work, how to read capaci......
Sep 08, 2026
Components & Sourcing
SMD Diode Polarity Guide: How to Identify Cathode Marking & Prevent PCB Damage
Installing an SMD diode in the wrong orientation can instantly damage a PCB or prevent a circuit from working. Whether you are assembling a prototype or troubleshooting hardware, understanding SMD diode polarity is a fundamental electronics skill. In this guide, you will learn: 1. how to visually identify SMD diode polarity markings 2. how to find the anode and cathode direction on different packages 3. how to test diode polarity using a digital multimeter 4. how polarity appears in schematics and PCB......
Sep 08, 2026
Components & Sourcing
LED Sizes Explained: Complete LED Size Chart, Types, Dimensions, and Applications
LEDs come in multiple package types, and choosing the wrong LED size affects brightness, PCB footprint, thermal performance, and assembly method. Whether you are placing an indicator on a breadboard, designing an LED strip PCB, or specifying a COB module for a spotlight, size is the first decision to get right. This guide covers every major LED size category, through-hole dimensions, SMD package codes, COB module sizes, and the difference between chip size and package size, with a quick-reference char......
Sep 08, 2026
Components & Sourcing
The Ultimate Guide to SMD Transistor Package: Sizes, Footprints, Thermal Performance & Selection
Choosing the wrong transistor package, thermal limitations, or excessive PCB area quickly becomes a problem. SMD transistor packages range from compact SC-70 and SOT-523 devices to much larger DPAK and D2PAK power packages, each optimized for different current, thermal, and assembly requirements. This guide compares common SMD transistor package sizes, including SOT-23, SOT-89, SOT-223, SC-70, DPAK, and D2PAK. You'll find nominal dimensions, footprint sizes, thermal characteristics, current capabiliti......
Sep 08, 2026
Components & Sourcing
ESP32 vs Arduino: Differences, Performance, and How to Choose the Right Board
When deciding between ESP32 vs Arduino for your next electronics project, the right choice depends heavily on your specific engineering requirements. To put it directly: the ESP32 is the best choice for IoT, wireless connectivity, and high-performance computing, while Arduino remains the gold standard for beginners, simple hardware control, and deterministic timing. Which is better, ESP32 or Arduino? The answer lies in your project’s demands for processing power, power consumption, and connectivity. L......
Sep 08, 2026
Components & Sourcing
SMD Resistor Codes: How to Read 3-Digit, 4-Digit, and EIA-96 Markings
SMD resistor codes are compact markings used to identify the resistance value of surface-mount resistors. Instead of traditional color bands, SMD resistors typically use a combination of numbers and letters printed directly on the component. Knowing how to read these markings is useful for engineers, technicians, and electronics hobbyists when identifying components, troubleshooting circuits, or replacing resistors during rework. This guide explains the three most common SMD resistor code systems: 3-d......
Sep 08, 2026
Components & Sourcing
Complete SMD Diode Size Guide: Package Dimensions, Charts, and Selection Tips
Picking the wrong SMD diode package usually shows up late, either during layout when footprints mismatch, or during testing when junction heating climbs past safe limits. Package size dictates how much current a diode carries, how efficiently it sheds heat, and whether your assembly line can solder it reliably. This guide details common SMD diode package families (SMA, SMB, SMC, SOD-123, SOD-323, SOD-523, and SOD-923). You will find our comprehensive SMD diode package size chart, layout recommendation......
Sep 08, 2026
Components & Sourcing
SMD Capacitor Codes: Identification, Markings, and Polarity
Identifying SMD capacitor codes is a unique and often confusing challenge. Unlike components with clear, standardized labels, capacitor markings depend entirely on capacitor type, and in most cases, the marking is a complete absence of one. As fundamental components for storing charge, capacitors are essential for every part of an embedded system, from filtering power supply noise (decoupling) and setting oscillator timing to coupling signals between ICs. Correctly identifying them is a critical skill......
Sep 08, 2026
Components & Sourcing
SMD Transistor Code Lookup: Identify Markings, Pinout & Multimeter Test Guide
Repairing a circuit board often brings a familiar frustration: staring at a tiny, three-legged black component with an obscure two- or three-letter code. Whether troubleshooting a bare prototype or a mass-produced PCBA, knowing how to quickly decode these surface-mount device (SMD) markings is an essential skill for any electronics engineer or repair technician. In this comprehensive guide, you will learn: 1. How to decode SMD transistor marking codes 2. How to identify BJT vs MOSFET types 3. How to f......
Sep 08, 2026
Components & Sourcing
What Is the ESP32? A Complete Guide to Features, Architecture, Modules, Programming, and Applications
From Wi-Fi-enabled temperature sensors and wearable health monitors to industrial gateways and AI-powered cameras, the ESP32 microcontroller has become one of the world's most widely adopted wireless embedded platforms. Combining a powerful processor with integrated Wi-Fi and Bluetooth, it lets engineers build connected devices without separate networking hardware. This guide covers ESP32 specifications, architecture, the full family of variants, development boards, programming tools, and real-world E......
Sep 08, 2026
Components & Sourcing
SMD Capacitor Sizes: Complete Size Chart and Selection Tips for PCB Design and Assembly
In the world of modern electronics, surface mount devices (SMDs) have revolutionized board design, allowing for smaller, faster, and more efficient printed circuit boards. When designing a PCB, selecting the correct SMD capacitor sizes is one of the most critical decisions an engineer must make to ensure both electrical reliability and manufacturability. In this article, you will find practical, authoritative guidance on: Comprehensive SMD capacitor size charts for quick reference. How to read imperia......
Sep 08, 2026
Components & Sourcing
SMD Diode Code Lookup: Full List, Marking Guide & Identification [2026 Guide]
In modern electronics, surface-mount diodes are used everywhere - from power input protection circuits to high-speed signal routing. Because these components are extremely small, manufacturers cannot print full part numbers on their bodies. Instead, they use short marking codes such as A2, M7, SS14, or SL, which often confuse beginners during PCB repair, reverse engineering, or component replacement. This guide explains how to decode SMD diode codes, identify polarity, test components using a multimet......
Sep 08, 2026
Components & Sourcing
Ball Grid Array (BGA): Definition, Types, Advantages, and PCB Assembly Guide
Ball Grid Array (BGA) is a leadless surface-mount package widely used in high-density and high-speed PCB designs. It features an array of solder balls on the underside, providing high I/O density, better signal integrity, and thermal performance. This guide covers what is BGA, different types of BGA packages, advantages and disadvantages, assembly requirements, inspection methods, and common defect solutions, helping engineers make informed decisions in PCB manufacturing. What is Ball Grid Array (BGA)......
Sep 04, 2026
Components & Sourcing
Capacitor Types Explained: Applications, Differences, and Selection Guide
Capacitors are the most widely used parts in electronics design, from input/output coupling to bypassing and decoupling networks; they find applications everywhere. And if you get the wrong part/value placed, the consequences may be you get an audible whine from a supply rail, a bootloader that won't start, or a capacitor that lights up like a match. The question that never comes up is "which brand?" It's always “which type and what value.” This tutorial does not waste time on a textbook explanation o......
Sep 04, 2026
Components & Sourcing
Complete Guide to Resistor Types: Fixed, Variable, and Non-Linear Resistors
The decision becomes difficult even for designers when a circuit board involves different types of resistors. Knowing which one your circuit actually needs solves half of the design problem. In this guide, you will go through: The full resistor types chart — fixed, variable, and non-linear families. How to choose between carbon film, metal film, wirewound, and foil resistors. When to use a potentiometer, thermistor, LDR, or varistor in design. SMD/through-hole resistor types and what each costs you. H......
Aug 13, 2026
Components & Sourcing
Thin Film vs. Thick Film Resistors: Key Differences, Advantages & Applications
Key Takeaways Default to thick film resistors for most designs. They are cost-effective, robust, and ideal for pull-ups, LED current-limiting, digital circuits, and surge-prone applications. Choose thin-film resistors whenever a resistor defines an analog quantity, such as a voltage divider, reference network, gain-setting circuit, or current-sensing signal chain. Their tight tolerance and low TCR help maintain measurement accuracy over temperature and time. Most PCB designs use thick film or thin fil......
Jul 30, 2026
Components & Sourcing
How to Choose the Right STM32 Microcontroller: Compare Series, Cortex-M Cores, and Key Features
STMicroelectronics ships thousands of STM32 MCU part numbers across more than a dozen series, and that variety is exactly what makes STM32 microcontroller selection difficult. Pick the wrong family, and you pay for it later: oversized BOM cost, wasted power budget, or a board respin when a peripheral turns out to be missing. This STM32 microcontroller selection guide breaks the decision into a five-step framework built on practical engineering criteria, not datasheet marketing copy, so you can match a......
Jul 23, 2026
Components & Sourcing
PoP Package (Package on Package) Explained: Architecture, Assembly, and SMT Challenges
In the race for miniaturization, fitting more processing power into smaller footprints is the ultimate challenge for PCB designers. Package on Package (PoP) technology answers this by integrating logic and memory vertically, becoming the standard for modern mobile processors. However, this 3D architecture demands advanced SMT assembly capabilities beyond standard fabrication. JLCPCB specializes in the high-precision manufacturing required to master these complex stacks. This guide covers how PoP packa......
Jul 01, 2026
Components & Sourcing
What Is a PQFP Package? Plastic Quad Flat Package Design, Footprint, and Assembly Guide
The Plastic Quad Flat Package (PQFP) is a widely used IC package in industrial, automotive, and embedded designs. This article provides a practical, engineering-focused guide to PQFP package. It explains how PQFP is built, when it makes sense to use it, how it compares with newer package types, and what designers should consider in terms of footprint design, thermal performance, signal integrity, manufacturing, and reliability. What Is a PQFP Package (Plastic Quad Flat Package)? A Plastic Quad Flat Pa......
Jul 01, 2026
Components & Sourcing
A Complete Guide to Surface Mount Device (SMD)
Imagine holding a smartphone in your hand. Inside that sleek device lies a complex network of thousands of miniature components — resistors smaller than a grain of rice, capacitors thinner than a fingernail, and integrated circuits containing millions of transistors. Without Surface Mount Technology (SMT) and its compact Surface Mount Devices (SMDs), none of this would exist. Just a few decades ago, electronics were bulky. Radios filled desks, computers filled rooms, and assembling a circuit meant dri......
Jun 30, 2026
Components & Sourcing
Circuit Breaker Types Explained: MCB, MCCB, RCCB, RCBO, ACB, VCB & SF6 Circuit Breakers
A circuit breaker automatically disconnects power when it detects faults such as overloads or short circuits, protecting equipment and reducing fire risk. Different circuit breaker types are designed for different voltage levels, current ratings, and applications, from household distribution boards to high-voltage substations. This guide explains the most common types - including MCBs, MCCBs, RCCBs, RCBOs, ACBs, VCBs, and SF6 breakers and helps you choose the right one for your application. Figure: Ci......
Jun 30, 2026
Components & Sourcing
Quad Flat Package (QFP): The Engineer's Guide to Design, Assembly and Thermal Management
What is QFP Package? The Quad Flat Package (QFP) is one of the most popular surface mount technology (SMT) package formats throughout the history of electronic manufacturing. After it became standard in the 1980s, the QFP has been the industry standard for integrated circuits (ICs) with moderate to high pin counts that typically range from 32 to 304 pins, so it was a good alternative for simple SOIC packages and complex Ball Grid Arrays (BGAs) at the same time. Defined by its "gull-wing" leads extendi......
Jun 30, 2026
Components & Sourcing
System on a Chip vs. System on Module: Which Is Right for Your Product?
A System on a Chip (SoC) integrates processing units, memory controllers, and peripheral interfaces into a single integrated circuit (IC), whereas a System on Module (SoM) combines an SoC with RAM, storage, power management, and supporting circuitry on a compact, pre-validated circuit board. Deciding between these two integration paths is one of the most critical structural decisions in embedded hardware engineering. The optimal path depends on production volume, cost targets, in-house layout expertis......
Jun 29, 2026
Components & Sourcing
NPN vs PNP Transistor: Key Differences, Working Principles, and Applications
Both NPN and PNP transistors are Bipolar Junction Transistors (BJTs) used for switching and amplification. They share the same three-layer construction but operate with opposite current and voltage polarities. Mixing up the two is a common source of design errors, from a relay that never switches to a high-side load that stays permanently on. This guide breaks down the structure, symbols, switching behavior, and selection criteria you need to pick the right transistor for your circuit. NPN vs PNP Tran......
Jun 23, 2026
Components & Sourcing
STM32 vs ESP32: A Deep Technical Comparison for Embedded and IoT Design
Choosing between STM32 and ESP32 is not just a question of price. Many engineers start with the same doubt: if ESP32 is cheaper and already has Wi-Fi/Bluetooth, why would anyone still choose STM32? The real answer depends on what your product must do. If you are building a connected smart-home device, ESP32 may be the fastest and most cost-effective path. But if your design needs deterministic control, accurate ADC sampling, low-power operation, industrial interfaces, motor control, or long-term avail......
Jun 10, 2026
Components & Sourcing
Zener Diode vs Schottky Diode: Which One Should You Use?
Zener and Schottky diodes may look identical in their physical surface-mount packages, but they serve completely different purposes in electronic design. A Zener diode is engineered specifically to operate in its reverse breakdown region for voltage regulation and overvoltage protection. Conversely, a Schottky diode is optimized for low forward voltage drop and high-speed switching in the forward conduction region. This guide provides a comprehensive comparison of their operating principles, electrica......
Jun 08, 2026
Components & Sourcing
How Engineers Choose Capacitor Voltage Ratings for PCB Circuits
Choosing a capacitor's voltage rating looks trivial on a schematic, but it quietly drives reliability, board size, and BOM cost. Pick too low, and the cap fails. Pick too high carelessly, and you waste space and (for MLCCs) may still lose capacitance you didn't know you had. Balancing these factors is critical for successful hardware development. In this guide, you will learn: How to apply voltage derating (the 1.5x and 2x rules) How to select the right rating for 3.3 V, 5 V, 12 V, 24 V, and 48 V rail......
May 28, 2026
Components & Sourcing
What Is System in Package? Architecture, Benefits, and Applications in Modern Electronics
System in Package (SiP) is a semiconductor packaging approach that combines multiple ICs, passive components, and interconnects inside a single package, delivering a complete functional subsystem in the footprint of one component. SiP has become a foundational technology in smartphones, wireless modules, wearables, and IoT devices. It lets engineers integrate a processor, memory, RF circuitry, and power management into one compact, pre-tested unit, reducing board complexity and shortening time to mark......
May 12, 2026
Components & Sourcing
Supercapacitor vs Capacitor: Differences, Performance, Applications and How to Choose
Key Takeaways The main difference between a capacitor and a supercapacitor lies in energy density versus power delivery speed. While standard capacitors discharge rapid bursts of power in milliseconds, supercapacitors store massive amounts of energy for longer durations to act as short-term battery replacements. Choose a supercapacitor if: You need short-term energy backup Choose a capacitor if: You need high-frequency noise filtering When designing modern electronic power systems, engineers frequentl......
Apr 22, 2026
Components & Sourcing
Supercapacitor vs Battery: Differences, Advantages, and When to Use Each
Key Takeaways Supercapacitor vs Battery: Quick Answer Batteries provide sustained energy for long-duration operation, supercapacitors (ultracapacitors) deliver rapid bursts of high current with exceptional cycle life. Understanding the difference between supercapacitor and battery technologies is essential for designing reliable PCB-based systems. Decision Rule: Battery: For sustained energy storage (Wh). Supercapacitor: For rapid power delivery (W). Hybrid: For optimized, resilient system design. In ......
Apr 22, 2026
Components & Sourcing
TQFP vs LQFP: Differences, Specs, Applications & Which to Choose
Key Takeaways Quick Selection Guide Use the following guidelines to choose the right package for your project: Prototyping & Early Testing → LQFP Easier soldering, inspection, and rework Mass Production → TQFP Better suited for automated assembly and compact layouts High Pin Count Designs → LQFP Longer leads improve yield and solder reliability Ultra-Thin & Space-Constrained Products → TQFP Lower profile enables slimmer device designs The TQFP (Thin Quad Flat Package) and LQFP (Low-Profile Quad Flat P......
Apr 21, 2026
Components & Sourcing
Capacitor vs Battery: Key Differences, Energy Storage, and When to Use Each
Key Takeaways Capacitors deliver high power in microseconds but store very little energy Batteries hold large amounts of energy but respond more slowly to load transients Capacitors are ideal for filtering, decoupling, and transient suppression Batteries are best for sustained, long-duration power Are capacitors better than batteries? Neither is universally superior - they are optimized for different roles. Capacitors excel in power delivery and speed; batteries excel in energy storage and runtime. Th......
Apr 17, 2026
Components & Sourcing
BJT vs MOSFET: Differences, Advantages, Applications and When to Use Each
In modern electronics, choosing between a BJT and MOSFET directly impacts switching speed, power efficiency, and PCB layout - especially in SMD designs. While BJTs are current-controlled devices ideal for analog circuits, MOSFETs are voltage-controlled and dominate high-speed switching applications. In this guide, we compare BJT vs MOSFET in terms of switching speed, SMD packaging, thermal performance, and real-world PCB applications to help you choose the right component. What is the Difference Betwe......
Apr 15, 2026
Components & Sourcing
Microcontroller vs Microprocessor: Differences, Applications, and How to Choose
Key Takeaways The fundamental difference between microprocessors and microcontrollers comes down to integration. A microcontroller bundles a CPU, memory (Flash + SRAM), and peripherals (GPIO, ADC, UART, SPI, I2C, timers) into a single chip for dedicated control tasks. A microprocessor provides only the CPU core - you must add RAM, storage, and peripherals externally, This single architectural difference cascades into cost, power, complexity, and performance trade-offs throughout your entire design. Fi......
Apr 15, 2026
Components & Sourcing
Types of BGA Packages: Differences, Applications, and Selection Guide
If you’re searching for the types of BGA packages, you’re likely trying to understand which one fits your PCB design, performance, or manufacturing needs. With options like PBGA, CBGA, and FBGA, each package comes with different trade-offs in thermal performance, cost, and reliability. Choosing the wrong type can lead to routing challenges, assembly defects, or even product failure. In this guide, we break down all major BGA package types, compare their key differences, and explain how to select the r......
Apr 01, 2026
Components & Sourcing
TQFP vs. QFN: A Comprehensive Comparison Guide for PCB Designers
Deciding between TQFP and QFN isn't just about aesthetics; it’s a high-stakes trade-off between board space, thermal management, and manufacturability. While TQFP’s visible leads make it a favorite for prototyping and easy inspection, QFN’s compact, leadless design dominates high-performance, space-constrained applications. But which one fits your specific project? This comprehensive TQFP vs. QFN comparison breaks down the technical specs, pros, and cons to ensure your next PCB design is both efficien......
Mar 31, 2026
Components & Sourcing
What Is a BGA Chip? A Complete Guide to Ball Grid Array Packaging
Modern electronics require compact packages with high connection density and efficient heat dissipation. Ball Grid Array (BGA) technology has become a key solution for high-performance PCB design. Because of these advantages, BGA chips are widely used in processors, graphics devices, memory modules, networking hardware, and compact embedded systems. This guide explains how BGA packages work, the common types available, their key benefits and challenges, and the essential PCB design and assembly consid......
Mar 27, 2026
Components & Sourcing
Resistor Power Rating: How to Calculate Wattage for SMD and Through-Hole Resistors
Every electronic circuit generates heat. Resistors, as their name implies, restrict current by converting electrical energy into thermal energy. But how much heat is too much? Understanding the resistor power rating is critical for any hardware designer. It defines the maximum continuous power (in watts) a component can safely dissipate without degrading. If you don't know how to calculate resistor wattage accurately, you risk thermal runaway, damaged components, or even a completely burned PCB. Wheth......
Mar 20, 2026
Components & Sourcing
QFP vs QFN: Which IC Package Is Right for Your PCB?
QFP and QFN are two widely used IC packages in modern PCB design, each offering different advantages in size, assembly, and performance. Choosing between QFP vs QFN directly impacts layout complexity, soldering reliability, thermal management, and manufacturing cost. An improper package selection may lead to low production yield, higher rework rates, and long-term reliability issues. In this guide, we compare QFP and QFN in terms of structure, PCB footprint, assembly process, and typical applications,......
Feb 27, 2026
Components & Sourcing
TQFP Package Explained: Dimensions, Pin Pitch, PCB Design & Comparisons
The constant push for miniaturization in modern electronics demands highly efficient PCB layouts. As surface-mount technology (SMT) has evolved, engineers have constantly sought component packages that balance high pin density with manufacturability. For mid-to-high I/O density applications where the extreme routing complexity and X-ray inspection requirements of a BGA (Ball Grid Array) are unnecessary, the TQFP package remains an industry-standard go-to. This guide explores everything you need to kno......
Feb 26, 2026
Components & Sourcing
LQFP Package Explained: Pin Pitch, Dimensions & Applications
The LQFP package (Low-Profile Quad Flat Package) is a widely used surface-mount IC package known for its fine pitch, compact size, and reliable performance in modern electronics. Commonly found in microcontrollers, embedded systems, and industrial devices, LQFP packages offer a balance between high pin density and easy inspection. In this guide, we’ll explain what an LQFP package is, how it works, its dimensions, applications, and PCB design considerations—helping engineers and manufacturers choose th......
Feb 05, 2026
Components & Sourcing
Ceramic Quad Flat Package (CQFP): Design, Reliability, Assembly, and When to Use It
When system failure is not acceptable, IC package selection becomes a reliability-driven engineering decision rather than a cost-driven one. In such scenarios, the limitations of plastic IC packages quickly emerge under sustained thermal stress, vibration, and harsh environmental exposure. This is precisely where the Ceramic Quad Flat Package (CQFP) remains a deliberate choice. Unlike plastic QFPs, CQFP packages offer hermetic sealing, superior dimensional stability, and predictable long-term aging—ch......
Feb 05, 2026
Components & Sourcing
SMD Resistor Selection Guide: Types, Package Sizes, Applications and Tips
Selecting the right SMD resistor is crucial for ensuring stable circuit performance. Because resistance, tolerance, power rating, and package size directly affect voltage control, current flow, and overall reliability, choosing an unsuitable SMD resistor may lead to overheating or unstable operation. To help beginners make the right decision, this guide explains the fundamentals of SMD resistors—including common types, key selection factors, size codes, tolerance ratings, and special-purpose resistor ......
Feb 05, 2026
Components & Sourcing
Understanding the Function of Electronic Parts in Circuit Design
Introduction The basic building blocks of modern electronics, electronic parts are important in forming reliable and efficient circuits. From small resistors to complex integrated circuits, these parts which range in value are critically important for the design and running of different electronic equipment. The importance of electronic parts in circuit design, their varieties, uses, and best practices for choosing the appropriate components to guarantee excellent performance in your projects are disc......
Oct 20, 2025
Components & Sourcing
Exploring PCB Connectors: Types, Features, and Applications for Optimal Electronic Connectivity
In the world of electronic circuits, PCB connectors quietly ensure that our devices work smoothly. These little components play a big role in connecting electronic parts on a printed circuit board (PCB). This article aims to explain why PCB connectors matter and why choosing the right ones is crucial for making electronic systems perform at their best. Let's explore the basics and see how picking the right PCB connectors can make a big difference in the functionality of our electronic devices. What is......
Oct 20, 2025
Components & Sourcing
GaN vs Silicon: Which Power Device Should You Use
Have you heard something about GaN? It is quite popular nowadays. Not because it is a different technology that saves power, but because today electronics are moving towards miniaturization. And we need small power supplies that can handle a lot more current and power and dissipate less heat. This is all possible due to GaN MOSFETs available in SMT packages out there. There are a lot of new companies that took this idea and implemented it into small mobile and laptop chargers, and generated a lot of r......
Oct 16, 2025
Components & Sourcing
How Nixie Tubes Work: The Glow Behind the Glass
Let me take you in the past, when there were no LED or LCD lights for display, rather a technology that consumes a lot of power but looks awesome. Nixie tubes, a softly glowing orange digits inside a glass tube. But nowadays these have just become obsolete, for some electronics hobbyists still keep them alive as a vintage piece from history. In this article, we’ll dive into how Nixie tubes work. Moreover, we will know the technology behind them and the history that brought them from laboratory equipme......
Sep 14, 2025
Components & Sourcing
Types and Packages of SMD Electronic Components
Due to circuit complexity and other factors, the use of SMD components has significantly expanded as electronics, as we all know, are becoming smaller. These days, we need alternatives that offer the same performance in a smaller form factor rather than components that require more room. Comparing SMD components to conventional through-hole components reveals a number of benefits. Due to their tiny leads they perform better at high frequencies and easier automated assembly. First of all, because they ......
Aug 13, 2025
Components & Sourcing
Microprocessor vs. Integrated Circuit: Key Differences, Types, and Applications
In electronics things origin from silicon and today we will discuss two different silicon pieces. It is not a type of battle, but a race of price to performance ratio. An integrated circuit is a piece of a semiconductor chip that houses thousands to billions of transistors in it. Integrated circuits house the basic structure of MOS transistors on a small piece of a silicon wafer. The MOS transistors are connected in a way that achieves the same functionality of a larger setup. And these MOS transistor......
Jul 23, 2025
Components & Sourcing
What is a HDMI RF Modulator? A Complete Guide
1. What is an HDMI RF Modulator? An HDMI RF modulator is a device that converts high-definition multimedia interface (HDMI) signals into Radio frequency (RF) signals. This allows HDMI-compatible devices, such as Blu-ray players, gaming consoles, and streaming devices, to transmit audio and video content over coaxial cables, making them compatible with older television sets or distribution systems that use RF signals. These modulators are particularly useful in settings where legacy TV systems are stil......
Jun 15, 2025
Components & Sourcing
Understanding the Role of PCB Controllers in Electronic Design
A PCB Controller is an important part of designing and building electrical systems. It controls the functions of different mechanical parts on a printed circuit board (PCB) and makes sure they can talk to each other easily. People use PCB controllers in a lot of different situations, from home technology to factory automation. The purpose of this article is to discuss the importance of PCB controllers, including the different kinds, their uses, and the best ways to choose and use them. 1. What is a PC......
Apr 14, 2025
Components & Sourcing
Capacitors 101: How They Work, Their Functions, and Types
Capacitors are indispensable components in PCB (Printed Circuit Board) design, providing functionality from energy storage and noise filtering to voltage regulation. Whether you're designing a simple circuit or a complex multi-layer board, understanding the different types of capacitors and their applications is crucial. The basic structure of a capacitor consists of two metal plates separated by a layer of dielectric. Capacitors can be of fixed or variable type. Capacitance is a fundamental concept i......
Mar 13, 2025
Components & Sourcing
PCB Controllers in Electronic Circuit Design
PCB controllers are the vital part of modern electronics and they are found on printed circuit boards (PCBs). These controllers are like the brains of electronic systems. They handle data, keep voltages stable, and make sure that all the parts on the circuit board can talk to each other easily. It is impossible to overstate how important they are, especially since computer designs are getting more complicated all the time. There are different kinds of PCB controllers and different uses for them. This ......
Feb 19, 2025
Components & Sourcing
PCB Board Connectors: Essential Components for Reliable Connections
PCB board connectors are important parts of electronics because they make it possible for different circuit elements to connect to each other electrically. These connectors make sure that data and power flow smoothly through the system. You can find them in everything from consumer electronics to heavy machinery. This article discusses about the types of PCB board connectors, their uses, and the best ways to choose and place them. What are PCB Board Connectors? PCB board connectors called electrical p......
Feb 17, 2025
Components & Sourcing
Essential Components Found on Every PCBA
Printed Circuit Board Assembly (PCBA) is the heart of modern electronic devices, facilitating the seamless function of various systems by connecting multiple electronic components on a board. While the design and complexity of PCBAs vary based on the application ranging from consumer electronics to industrial systems. But some common core components are consistently found across virtually every assembly. With the evolution of components used in circuit boards over several years, it is essential for ev......
Nov 28, 2024
Components & Sourcing
PCB Fuse Ensuring Circuit Protection in Modern Electronics
Introduction In the world of electronics, the PCB fuse is a critical component that safeguards circuits from damage due to overcurrent protection and short circuit prevention. As electronic devices become more complex and compact, the importance of effective circuit protection cannot be overstated. A PCB fuse, whether in the form of a Surface Mount Device (SMD) fuse or a through-hole fuse, plays a pivotal role in maintaining the integrity and functionality of electronic circuits. This article delves i......
Nov 26, 2024
- 1
- 2
- 3
- 4
- 5
- 6
- 9