PCB Surface Finishes & Coatings
Explore different PCB finishes, their benefits, limitations, and how they impact solderability, durability, and cost.
Featured Posts
Surface Finishes & Coating
The Ultimate Guide to OSP Surface Finish in PCB Manufacturing: Advantages, Process, and Selection
Key Takeaways OSP (Organic Solderability Preservative) is a water-based, cost-effective PCB surface finish that deposits a 0.2-0.5μm organic film directly onto copper pads. Unlike metallic finishes such as ENIG or HASL, OSP provides superior surface flatness for fine-pitch SMT components at no extra process charge, making it ideal for high-density consumer electronics. However, OSP requires controlled handling and a limited assembly window (24-48 hours after opening vacuum packaging). It is best suite......
Jul 30, 2026
Latest Posts
Surface Finishes & Coating
Why Copper Oxidation Matters in PCB Design & How to Prevent It
Key Takeaways Copper oxidation is a critical concern in PCB design that directly impacts solderability, contact resistance, and long-term reliability. By understanding how oxidation forms and damages copper surfaces, designers can effectively prevent it through appropriate surface finishes (such as HASL, ENIG, and OSP), strategic solder mask application, and strict adherence to proper storage and handling practices per IPC-1601 guidelines. Protecting copper from oxidation ensures better assembly yield......
Oct 28, 2026
Surface Finishes & Coating
Choosing the Right Surface Finish for Your PCB: An Overview of HASL, ENIG, OSP, Immersion Tin and Immersion Silver
Key Takeaways Lead-Free HASL: Best low-cost, RoHS-compliant finish for general PCB builds. ENIG: Superior flatness and 12+ month shelf life for fine-pitch BGAs. OSP: Ultra-flat, lowest-cost option for high-volume SMT (3–6 month shelf life). Immersion Silver: Ideal for high-frequency RF by eliminating nickel signal loss. Immersion Tin: Best for press-fit connectors and fine-pitch assembly. Printed Circuit Boards (PCBs) are essential components in the manufacturing of electronic devices ranging from sma......
Oct 08, 2026
Surface Finishes & Coating
Conformal Coating in PCB Technology: Benefits, Challenges, and Future Developments
If you're searching for conformal coating, you're likely looking for a reliable way to protect your PCB from moisture, dust, chemicals, or harsh environments. Choosing the right coating directly affects product reliability, performance, and lifespan. In this guide, you'll learn what conformal coating is, the main types available, and how to select the best option for your application. We'll also cover key benefits, application methods (manual, automated, and selective), as well as inspection, rework, ......
Sep 28, 2026
Surface Finishes & Coating
PCB Gold Fingers: Why They Matter and How to Design Them
Key Takeaways PCB gold fingers provide reliable electrical and mechanical contact for PCBs that connect to external connectors or card slots. ENIG is suitable for general contact applications, while electroplated hard gold offers higher wear resistance for repeated insertion and removal. Gold fingers should remain fully exposed, with solder mask and silkscreen kept away from the contact area. Proper chamfering and gold finger orientation are essential to ensure smooth insertion and prevent damage duri......
Sep 11, 2026
Surface Finishes & Coating
Comparing HASL and ENIG Surface Finishes for PCBs
Selecting the right surface finish for a printed circuit board (PCB) is crucial to ensuring its performance, reliability, and longevity. Two of the most commonly used finishes are Hot Air Solder Leveling (HASL) and Electroless Nickel Immersion Gold (ENIG). Each of these surface finishes offers distinct advantages and disadvantages, making them suitable for different applications. In this article, we will compare HASL and ENIG to help you determine which finish is best suited for your PCB project. What......
Sep 09, 2026
Surface Finishes & Coating
Avoid PCB Assembly Failures: Mastering Solder Mask Expansion Rules and Best Practices
Solder mask protects copper traces and pads from oxidation, bridges, and contamination during assembly. Incorrect solder mask expansion—the clearance around features where mask is pulled back—leads to defects like shorts or exposed copper. Engineers must set expansion values precisely to ensure reliable soldering and long-term performance. Introduction: Why Solder Mask Expansion is Critical for PCB Reliability Understanding Solder Mask and Expansion Basics Solder mask is a polymer layer applied over t......
Sep 08, 2026
Surface Finishes & Coating
The Ultimate Guide to OSP Surface Finish in PCB Manufacturing: Advantages, Process, and Selection
Key Takeaways OSP (Organic Solderability Preservative) is a water-based, cost-effective PCB surface finish that deposits a 0.2-0.5μm organic film directly onto copper pads. Unlike metallic finishes such as ENIG or HASL, OSP provides superior surface flatness for fine-pitch SMT components at no extra process charge, making it ideal for high-density consumer electronics. However, OSP requires controlled handling and a limited assembly window (24-48 hours after opening vacuum packaging). It is best suite......
Sep 04, 2026
Surface Finishes & Coating
PCB Encapsulation: Design Rules, Material Selection, and Reliable Manufacturing
Key Takeaways Encapsulation vs. Potting: Potting uses a permanent shell; encapsulation produces a free-standing resin-coated module. Both deliver full environmental isolation. Encapsulation vs. Conformal Coating: Conformal coating is lightweight and reworkable but limited to mild environments. Encapsulation provides IP67/IP68 submersion-grade protection at the cost of repairability. Resin Selection: Epoxy offers rigidity and chemical resistance; polyurethane provides flexibility for thermal cycling; s......
Aug 11, 2026
Surface Finishes & Coating
Hard Gold PCB Finish: Achieving Exceptional Wear Resistance and Contact Performance
Surface finishes are not all the same thing, and this is obvious beyond mention when you are dealing with parts that are beaten against one another over and over. Hard gold. The most common finish used when PCBs must complete hundreds or even thousands of insert-and-remove operations before going out of service is essentially a hard alloy of gold electroplated over a nickel barrier coating. The prototypical piece of evidence that demonstrates why this is important is the edge connector, otherwise know......
Aug 08, 2026
Surface Finishes & Coating
Optimizing Plating Thickness for Superior PCB Durability and Performance
Key Takeaways Plating thickness directly determines PCB durability, via reliability, and current-carrying capacity. Minimum hole wall copper: 20 µm (Class 2) / 25 µm (Class 3) per IPC-6012. Thicker copper (2 oz) significantly improves thermal performance and mechanical strength. Uniform plating requires good aspect ratio and process control to prevent cracking. Proper surface finish selection and reliable manufacturing are essential for long-term performance. Why do two boards that are the same act di......
Jul 29, 2026
Surface Finishes & Coating
Preventing Black Pad Defects: Ensuring Reliable ENIG Finish in Professional PCB Manufacturing
Key Takeaways Black Pad is caused by excessive nickel corrosion during the ENIG immersion gold step, leading to brittle solder joints and hidden BGA/QFN failures. Key prevention methods: tight chemistry control (temperature, pH, time), consistent phosphorus content, and regular bath monitoring. High-reliability alternatives: ENEPIG (lowest risk) or nickel-free finishes like Immersion Silver and OSP. Always source ENIG from manufacturers with strict process controls. Ever get a great-looking board, wor......
Jun 29, 2026
Surface Finishes & Coating
Solder Mask Colors: Boost Your PCB Performance, Style & Reliability
Key Takeaways Solder mask color directly impacts AOI accuracy, thermal performance, and PCB reliability — it is not purely cosmetic. Green remains the industry benchmark for the highest manufacturing yields and fastest turnaround at no extra cost. White maximizes light reflection for LED applications, while black offers a premium aesthetic for high-end consumer products. Red and yellow provide superior visual contrast for prototyping, debugging, and safety-critical inspections. JLCPCB offers all seven......
Jun 16, 2026
Surface Finishes & Coating
Comparing OSP Plating with Other PCB Surface Finishes
Key Takeaways OSP stands out as a cost-effective, ultra-flat, and environmentally friendly PCB surface finish with excellent solderability for fine-pitch components, making it ideal for high-volume consumer electronics. However, its short shelf life (3–6 months), sensitivity to handling and oxidation, and limited multi-reflow durability require careful storage and process control. When compared to HASL, ENIG, Immersion Silver, and Immersion Tin, OSP offers superior planarity and lower cost but trades ......
May 16, 2026
Surface Finishes & Coating
Copper Coin PCB : A Solution for Heat Dissipation
In the fast-evolving electronics industry, devices are becoming smaller, faster, and more powerful, while also coming in a compact size. Power is no longer a problem, but packing the device into a smaller form factor presents a serious challenge. Whether we are working on a power converter, LED lighting module, automotive ECU, or 5G communication device, the excessive heat reduces performance. It shortens the component lifespan. This is where Copper Coin-Embedded PCBs become a smart, modern solution f......
Apr 17, 2026
Surface Finishes & Coating
Technical Guidance: Five Via Finishes: Exposed, Tented, Plugged, Epoxy and Copper Paste Filled
Definition and Universal Inspection Standards In response to customer requests, we have added the processes of "plugged vias," "epoxy-filled vias," and "copper paste filled vias," which can be selected in the ordering interface. Refer to the rules for via-in-pad filled vias (click here to view). When ordering a PCB there are generally five via covering options available: Untented (Exposed), Tented, Plugged, Epoxy-Filled & Capped, and Copper-Paste-Filled & Capped. Finish Type Appearance Key Advantages ......
Apr 08, 2026
Surface Finishes & Coating
How to Waterproof a PCB: A Step-by-Step Potting Guide
PCBs are everywhere, they are an integral part of nowadays essential things. We can not imagine a world without them. Almost all the things which have power or that can take power have at least a PCB. Because they are used so often the circuit needs to operate in challenging environments. Mostly we are talking about outdoors, under the hood or in humid industrial settings. The term potting becomes a crucial solution for all this. Potting a printed circuit board (PCB) helps protect it from moisture, du......
Apr 07, 2026
Surface Finishes & Coating
HASL Surface Finish : Proven Reliability and Cost Efficiency in High-Quality PCB Manufacturing
In case you have ever been confused by seeing the acronym HASL on the PCB spec sheet and wondered what it means, here is the brief description: HASL is the abbreviation of Hot Air Solder Leveling, and it is one of the oldest, and still most dependable, surface finishes in the printed circuit board. You simply put the board into a pot of molten solder, typically a tin-lead or lead-free blend, and blow hot air over the solder to remove the excess and leaving a thin coat of solder on each exposed copper ......
Apr 07, 2026
Surface Finishes & Coating
Design and Surface Finish of Coil Boards
Circular coils are a wiring method sometimes used in PCB layout. They serve primarily as inductors, transformers, antennas, and more. Considering the production of PCBs containing coiled traces, please take note of the following points: 1. Compared to conventional circuits, it might not be possible to detect short circuits between windings of circular coils if the coil is a closed circuit. Therefore, the requirement for trace width and spacing is 0.254 mm (with a limit of 0.15 mm, but only when the co......
Apr 03, 2026
Surface Finishes & Coating
All you need to know about PCB Gold Fingers
In today's highly connected, tech-driven world, seamless communication between devices is essential, and it all starts at the circuit board level. A critical element in enabling this communication is the use of gold fingers, the gold-plated connectors that link circuit boards to motherboards, making the flow of signals possible. Although it looks nice, gold plating is not merely for aesthetic purposes, it serves a practical function critical to the connector performance. Without gold fingers, critical......
Mar 31, 2026
Surface Finishes & Coating
Considerations for Gold Finger Bevel Design
In our daily lives, we often come across products with a row of contacts on the PCB edge used for connections, which are known as PCB gold fingers. They are also referred to as "edge connectors", typically serving as the external connection interface for a PCB board when inserted into a slot. Technical Guidance So, what should you keep in mind when designing PCBs with gold fingers? Excessive beveling of PCB gold fingers can result in the fingers not making proper contact with the mating equipment duri......
Mar 31, 2026
Surface Finishes & Coating
Solder Mask on PCBs : Protecting Traces, Guiding Assembly, and Boosting Long-Term Reliability
As we wear masks to save us from pollution, in the same way, the ones used by PCB to avoid contamination and oxidation. It became a very important step in PCB manufacturing over the years. In the early days, the manufacturers were more focused on one type of color, but today we have multicolor PCBs. That’s how the soldermask process evolved over the years. From protecting delicate copper traces to ensuring precise soldering during assembly. The solder masks directly influence yield and long-term field......
Feb 04, 2026
Surface Finishes & Coating
PCB Silkscreen Explained : From Design Intent to Professional Application and Manufacturing Precision
Let’s come to the topmost layer of a PCB, which is about annotations. We all need some reference material to work on, and the same applies to the assembler, from component assembly to referencing different section legends and silkscreen plates; it plays an important role. In a finished printed circuit board, the silkscreen layer is the least technically appreciated element. It is the most helpful layer for the end user because we can not look into the layout, datasheets, and schematics. That’s how som......
Feb 04, 2026
Surface Finishes & Coating
PCB Coating Spray: Conformal Layers for Bulletproof Circuit Protection
Conformal coating is like giving your printed circuit board an invisible raincoat or even a bulletproof vest. It’s a thin polymer film applied over the PCB and its parts to protect against moisture, dust and vibration. This shield is lightweight and flexible, which means it conforms closely to every contour of the board. The goal is to extend the board’s life and reduce failure rates in harsh conditions. Spray application is one popular method to lay down this protective coat. In this article, we will......
Feb 04, 2026
Surface Finishes & Coating
What is ENEPIG and How Does it Compare to ENIG in PCB Finishing?
ENEPIG (Electroless Nickel Electroless Palladium Immersion Gold) is a type of surface plating applied on a Printed Circuit Board to protect it from environmental factors during storage and operation. ENEPIG is prepared by depositing electroless Nickel (Ni 3-5 μm), followed by electroless Palladium (Pd 0.05-0.1μm), and an immersion Gold layer (Au 0.03-0.05 μm). It is good for solder joint strength, gold wire bonding, aluminium wire bonding, and provides low contact resistance. It can easily be deposite......
Oct 20, 2025
Surface Finishes & Coating
Understanding the Role of Solder Resist Materials in PCB Fabrication
Solder resist, also known as solder mask, Yes they are the same. Again two different names for the same thing but the solder mask one is adapted globally. The protective coating used on PCBs to stop solder from bridging undesired places is referred to by both designations. Although the term "solder mask" is frequently used, "solder resist" is more technically correct since the resist material opposes the solder as it is being assembled. Nonetheless, in the business, both phrases are frequently used in......
Jul 14, 2025
Surface Finishes & Coating
How to Choose the Right Surface Finish for Your PCB
When it comes to designing and manufacturing of printed circuit boards (PCBs), considering the element of your surface finish is a critical decision. In addition to influencing the PCB's aesthetics, surface finish is essential to the functionality, dependability, solderability and longevity of the electronic equipment it powers. The surface finish serves as a protective layer on the exposed copper traces of a PCB. It prevents oxidation, promotes solderability, enhances conductivity, and provides a lev......
Feb 27, 2024
Surface Finishes & Coating
Comprehensive Guide to Exploring PCB Surface Finish
The PCB surface treatment process is a crucial step in PCB manufacturing. Its purpose is to protect the copper surface from oxidation and ensure that it can bond well with the solder during the soldering process. The following are some common PCB surface treatment processes and their advantages and disadvantages: HASL (Hot Air Solder Leveling) Hot air leveling (HASL) is a traditional method for treating the surface of PCBs. The process involves immersing the PCB in molten tin and then using hot air to......
Jan 31, 2024
Surface Finishes & Coating
Protective Measures for PCBs: Safeguarding Electronics from Environmental Factors and Electrical Hazards
Printed Circuit Boards (PCB’s) serve as crucial parts of electronic devices providing the framework for connecting various electrical components. Put in place strong protection measures to guarantee the dependable and durable operation of PCBs. PCB protection means preventing external influences, electrical problems, mechanical stress, and excessive temperatures from harming the board and it’s components. In the subsequent sections, we will delve into nine methods, which are summarized into five major......
Dec 07, 2023
Surface Finishes & Coating
Demystifying Conformal Coating
Welcome to JLCPCB's blog, your ultimate resource for all things related to conformal coating for printed circuit boards (PCBs). In this article, we will explore the significance of conformal coating, the different types of coating materials available, the application process, and the importance of quality assurance and testing. Whether you're a seasoned PCB designer or a beginner in the field, this article will provide valuable insights to help you understand and utilize conformal coatings effectively......
Oct 20, 2023
- 1
- 2
- 3