Advanced PCB Packaging & Integration
Explore cutting-edge techniques for dense packaging, miniaturization, and multi-functional PCB integration.
Latest Posts
Advanced Packaging & Integration
QFN Package: Structure, PCB Design, and Assembly
Key Takeaways Choose the correct PCB footprint: Follow the QFN manufacturer’s recommended land pattern and package datasheet. Optimize thermal management: Use appropriate thermal pads and thermal vias to improve heat transfer. Control solder paste application: Design stencil apertures to achieve suitable solder volume and reduce assembly defects. Inspect hidden solder joints: Use X-ray inspection when required by the product’s reliability needs and inspection plan. Design for manufacturability (DFM): ......
Oct 12, 2026
Advanced Packaging & Integration
Navigating Automotive PCB Manufacturing Standards and High-Reliability Fabrication
Key Takeaways Harsh Operating Environments: Engineered to survive 15 years under thermal cycling (-40 °C to 150 °C) and severe vibration. Strict Compliance: Guided by IATF 16949, AEC-Q200 components, and IPC Class 3 standards. Targeted Materials: Leverages high-Tg/heavy copper for power and Rogers substrates for 77 GHz radar. Zero-Defect Inspection: Employs 3D AOI and X-ray testing to eliminate hidden solder joints failures. An automotive PCB has to keep working for fifteen years in the same place. Bo......
Sep 23, 2026
Advanced Packaging & Integration
Battery PCB Board: What You Need to Know
Key Takeaways Battery PCB boards support power distribution, protection, monitoring, and cell balancing. PCB types include single-layer, multilayer, flexible, and HDI designs. Current capacity, thermal management, and routing density are key design considerations. Reliable manufacturing depends on proper materials, fabrication, assembly, and testing. Battery PCB boards are used in a wide range of battery-powered electronics, from smartphones and laptops to electric vehicles and energy storage systems.......
Sep 21, 2026
Advanced Packaging & Integration
Medical PCB Manufacturing: Key Standards, Types, and High-Reliability Fabrication
Key Takeaways Strict Compliance: Demands ISO 13485 QMS certification, IPC Class 3 specs (25 µm copper barrels), and IEC 60601-1 safety rules. Targeted Substrates: High-Tg FR-4 handles autoclave heat, polyimide flex serves wearables, and metal/ceramic cores manage high power. Quality & Traceability: Layered AOI, X-ray inspection, and full IPC-1782 lot tracking prevent critical field failures. A medical PCB carries a level of responsibility that consumer electronics rarely face, because a patient’s diag......
Sep 19, 2026
Advanced Packaging & Integration
A Complete Guide to Package Substrates: Materials, Structure, Types, and PCB Differences
Key Takeaways Definition: A package substrate is the fine-pitch organic carrier connecting a bare die to the system board. Not a PCB: Substrates are routed several times finer than advanced HDI and use entirely different dielectrics. Materials: BT resin cores carry wire-bond and CSP work, while glass-free ABF build-up film carries flip chip. Process: Semi-additive plating, not etching, is what makes single-digit micrometer lines possible. Constraint: Substrate capacity, not wafer supply, now limits hi......
Sep 18, 2026
Advanced Packaging & Integration
Comprehensive Guide to QFN Packages: Advantages, Types, and Applications in Electronics
Key Takeaways Thermal Vias: Place 0.3mm vias in the exposed pad to draw heat away from the IC. Voiding Control: Apply a window-pane stencil (50–75% coverage) to prevent solder voids. Prevent Wicking: Use tented vias or Via-in-Pad to stop solder from leaking. Hidden Joints: Require X-ray inspection (AXI) since QFN leads are under the package. JLCPCB SMT: Fully supports 0.4mm pitch QFNs, Via-in-Pad, and AXI quality checks. Quad flat no-lead (QFN) packages are a type of IC package that are small, lightwe......
Sep 10, 2026
Advanced Packaging & Integration
Unlocking Smaller and Smarter PCBs with Embedded Components
Have you ever opened a smartwatch or a pair of wireless earbuds, looked at the miniature chip inside, and wondered how engineers could pack so much functionality into such a small enclosure? While surface-mount technology (SMT) has become incredibly sophisticated—with the advent of ultra-small 0201 and 01005 packages—there is a physical limit to how many components can be crammed onto the surface of a board. To bypass this bottleneck, the electronics manufacturing industry is increasingly turning to e......
Jul 01, 2026
Advanced Packaging & Integration
Improving Heat Dissipation : The Smart Use of Thermal Pads in PCB Design
Key Takeaways Optimizing PCB thermal pad design and via arrays is essential to prevent semiconductor failures caused by FR4's low thermal conductivity. By implementing a 1.0–1.2 mm via pitch and keeping solder voiding below 25% through segmented stencils, designers can eliminate localized hot spots and boost board reliability from prototype to high-volume production. Have you ever considered that the thermal conductivity of a normal FR4 PCB is only about 0.3 W/mK? That is an acceptable number for low-......
Jun 04, 2026
Advanced Packaging & Integration
A Complete Guide to IC Package: Types, Properties, PCB Design Rules & Selection Tips
What is an IC Package? An IC package is the physical enclosure that houses an integrated circuit or electronic component, providing mechanical protection, electrical connections, and thermal management. It ensures that the component can be reliably mounted on a PCB and integrated into circuits. Key Functions of an IC Package: 1. Mechanical protection: Shields the chip from physical damage and environmental factors. 2. Electrical connections: Provides pins or solder balls to connect the IC to the PCB. ......
Apr 22, 2026
Advanced Packaging & Integration
BGA vs LGA: Understanding the Differences and Choosing the Right Package
In the world of electronic components, the choice of package type plays a crucial role in the overall performance, reliability, and manufacturability of a printed circuit board (PCB). Two popular package types that are widely used in modern PCB design are BGA (Ball Grid Array) and LGA (Land Grid Array). Understanding the differences between these two packages is instructive for electronics enthusiasts, hobbyists, engineers, students, and professionals in the field of electronics and PCB design. This a......
Apr 03, 2026
Advanced Packaging & Integration
Technical Guidance: BGA Design Rules
With the advancement of the electronics industry, chip integration continues to increase, the number of IO pins quickly rises, and power consumption grows accordingly, leading to stricter requirements for integrated circuit packaging. To meet the demands of this progress, Ball Grid Array (BGA) packaging technology is introduced. This technology involves the creation of an array of solder balls on the bottom of the package substrate as the I/O interface for the circuit, connecting it to the printed cir......
Apr 03, 2026
Advanced Packaging & Integration
What is Chip-on-Board (COB) in PCB Design? Full Guide to Benefits and Manufacturing Process
In this tutorial, we will get the detailed concept of "Chip On Board" or COB. If you have ever thought about how cheaper, durable and compact electronic devices are made, the answer is chip-on-board technology. Chip on board is a solution from chip manufacturing to prototyping and development board. Today we will provide a deep understanding of COB and profitable insights for the electronic miniaturization future. A finished semiconductor wafer is cut into dies. Each die is then physically bonded to t......
Jun 30, 2025
Advanced Packaging & Integration
Optimizing BGA Fanout in PCB Design for High-Performance Electronics
In the world of high performance electronics, Ball Grid Array (BGA) packages have become very common and popular, due to their high pin density and compact footprint. However, effectively routing signals from BGAs to the rest of the PCB represents significant challenges, particularly when dealing with devices with hundreds or even thousands of pins. In this article, we'll dive into the world of BGA fanout in PCB design and explore strategies for optimizing signal routing, ensuring signal integrity, an......
May 10, 2024
Advanced Packaging & Integration
DIY IoT Arduino PCB: Building a Customized Platform for Smart Projects
Embarking on the thrilling journey of custom Arduino PCB design opens a world of possibilities, allowing enthusiasts to craft unique solutions and bring their imaginative projects to life. This venture involves an immersive exploration of Arduino schematic design, meticulous component selection, strategic PCB layout, considerations for shield compatibility, and the critical aspect of power supply design. In this exciting endeavor, we will specifically delve into the integration of an Arduino Uno with ......
Apr 24, 2024
- 1
- 2