PCB DFM Guidelines
Learn DFM rules that improve manufacturability, reduce defects, and ensure high-quality PCB fabrication.
Featured Posts
Design for Manufacturing
The Ultimate Guide to PCB Panelization: Tools and Techniques
Printed circuit boards (PCBs) are the backbone of modern electronics. One critical aspect of PCB manufacturing is panelization — the process of arranging multiple PCBs onto a single larger panel for efficient manufacturing and assembly. This technique allows multiple boards to be processed simultaneously, significantly reducing costs and improving production efficiency. In this article, we will provide a comprehensive guide to PCB panelization, covering the tools and techniques required for successful......
Jul 28, 2023
Latest Posts
Design for Manufacturing
Implications of border lines and 3D footprint lines on Mechanical Layer 1
Key Takeaways Mastering Mechanical Layer 1 is essential for accurate PCB manufacturing. Always place the complete board outline, mounting holes, and irregular slots on Mechanical Layer 1 (GM1), as JLCPCB prioritizes the lowest-numbered Mechanical Layer while ignoring KEEP-OUT and higher Mechanical Layers. 3D footprint lines serve only as design references and will not be fabricated. Following these layer priority rules and best practices ensures correct board dimensions, proper slot formation, and avo......
Oct 30, 2026
Design for Manufacturing
The Role of PCB Test Fixtures in High-Volume Manufacturing
In high-volume manufacturing of Printed Circuit Boards (PCBs), quality, efficiency, and reliability are paramount. One of the most crucial tools in achieving these goals is the PCB test fixture. These fixtures play a vital role in ensuring that PCBs meet the required performance standards before they are integrated into electronic devices. This article delves into the importance of PCB test fixtures, their types, and how they contribute to the efficiency of high-volume manufacturing. Specialized and c......
Oct 30, 2026
Design for Manufacturing
SMT or Through Hole Technology?Which is Better for Your Project?
When designing and manufacturing electronics, one of the most important steps is selecting the appropriate assembly method. Nowadays we have through-hole technology and surface mount technology, which become the industry standards and are the two main approaches. The surface-mount technology (SMT) uses components that are perfectly aligned with the PCB surface. On the other hand through-hole technology (THT) uses leads that are placed into pre-drilled holes in the PCB and thereafter soldered. Consider......
Oct 30, 2026
Design for Manufacturing
PCB temperature: Tips regarding improving the thermal management of PCBs
Thermal management is of utmost importance while designing PCBs. This is because the temperature of PCBs can guarantee the reliability, performance, and longevity of PCBs and the electronic equipment of which they are an integral component. Thus, enhanced Printed Circuit Board heat management is a necessity for reliable operation and to protect against damage to electronic components. In the upcoming chapter, we will discuss several approaches to strengthen PCB temperature management. Reasons of heat ......
Oct 29, 2026
Design for Manufacturing
Design for Manufacturing (DFM): A Comprehensive Guide for Optimizing Production
Maintaining quality while improving the manufacturing process is critically important in the competitive fields of electronics and industry. Design for Manufacturing (DFM) here comes in handy. DFM is a design tool stressing the simplicity of manufacturing during the product development stage. Early on manufacturing limitations help DFM to guarantee that goods are not only useful but also reasonably priced, dependable, and easily produced at large-scale production. This article covers the importance of......
Oct 28, 2026
Design for Manufacturing
Design for Manufacturing and Assembly: A Complete DFMA for PCB Design Guide
Key Takeaways DFMA covers both PCB fabrication and assembly: DFM addresses bare-board fabrication, while DFA addresses component assembly and related process constraints. The biggest decisions happen early: Package choice, layer count, and board outline are usually set well before Gerber export and become expensive to change later. Passing DRC does not guarantee a good footprint: Design rules can verify clearances and copper geometry, but they cannot confirm that a footprint matches the component data......
Sep 28, 2026
Design for Manufacturing
Get More From Every PCB Panel: Choosing the Right Panel Size
Key Takeaways Panel Drives Cost: Fabs price the whole panel, so maximizing utilization lowers per-board cost. 3 Panel Types: Distinguish raw sheets, fab working panels, and your delivery array. Keep Clearances: Reserve 5 mm process rails and 1–2 mm spacing around V-scores. Match Depaneling Method: Use V-cut (0 mm gap) for rectangles, tab routing for complex shapes. Test Both Orientations: Rotate boards 90° to find the best fit before ordering. PCB panel size is the one number on your order that you ne......
Sep 20, 2026
Design for Manufacturing
Free DFM Tool: Enhancing PCB Design Efficiency
Design for Manufacturability (DFM) guarantees that the design is best suited for manufacturing and assembly, it is a key process in printed circuit board (PCB) design. Using a Free DFM Tool will improve accuracy and efficiency, by greatly streamlining this process. The advantages of Free DFM Tools, their place in PCB design, and how they could affect your projects are discussed in this article. We will also discuss some typical problems and fixes related to using these tools, highlighting their applic......
Sep 10, 2026
Design for Manufacturing
Understanding the Importance of DFM Analysis in PCB Design
Design for Manufacturing (DFM) analysis helps you on whether a printed circuit board (PCB) is fit for manufacturing, assembly, and sales. Early in the planning process, it looks for and fixes any possible problems arising throughout production. This will increase manufacturing efficiency and help to save expenses. DFM analysis is quite vital in the complex world of electronics, where even little design errors can create delays costing a lot of money. This article discusses the different types of DFM i......
Sep 10, 2026
Design for Manufacturing
Thermal Vias in PCB Design for Heat Management
Thermal vias are specialized vias designed to transfer heat from one layer of a PCB to another. These vias are placed near heat-generating components to create a thermal pathway, helping to dissipate heat and reduce the risk of overheating. They are often used with heat sinks, thermal pads, or copper planes to enhance their effectiveness. They are simply plated through holes (PTHs) that are located under a surface-mounted heat source component in a printed circuit board (PCB) that allow heat transfer.......
Sep 09, 2026
Design for Manufacturing
The Ultimate Guide to PCB Panelization: Tools and Techniques
Printed circuit boards (PCBs) are the backbone of modern electronics. One critical aspect of PCB manufacturing is panelization — the process of arranging multiple PCBs onto a single larger panel for efficient manufacturing and assembly. This technique allows multiple boards to be processed simultaneously, significantly reducing costs and improving production efficiency. In this article, we will provide a comprehensive guide to PCB panelization, covering the tools and techniques required for successful......
Sep 09, 2026
Design for Manufacturing
Common Design Issues and Recommendations for PCB Optimized Design
To help customers avoid common issues that may arise during the PCB production process due to design problems, we' ve summarized the most frequent cases below. These issues have been detailed on our website to assist customers in identifying and addressing them more effectively. The following points include important design considerations and suggested modifications: 1. Missing Slots, Cutouts, Millings and V-Cut Issue: Missing Slots, Cutouts, Millings and V-Cut due to improper design. Recommendation: ......
Sep 09, 2026
Design for Manufacturing
PCB File Formats
Ordering printed circuit boards (PCBs) involves providing precise and detailed information about the design and specifications of the board. This is why specific PCB file formats are necessary. Manufacturing can only take place successfully with a completed PCB file. Designing a PCB and communicating those design decisions depends on files such as circuit schematic designs, Bill-of-Materials, PCB layouts, and stack-up design information. To ensure interoperability among various electronics design soft......
Sep 09, 2026
Design for Manufacturing
How to Run a Design Rule Check (DRC) for Your PCBs
Any time you design a PCB, and you want to turn it into a real product, you will have to make sure the design obeys all the constraints within the standard PCB manufacturing process. These constraints in the PCB design are known as Design rules and to check these rules in a CAD software we have to run the DRC(Design Rule Check) algorithm. The ever-increasing complexity of boards has made it nearly impossible to carry out the design rule verification process manually, so designers have to program the r......
Sep 09, 2026
Design for Manufacturing
Using Via-in-Pad Technology: What You Need to Know, Design Guidelines, and More…
In the world of multi-layer PCB (Printed Circuit Board) design, vias are essential parts that connect different layers of a board. As electronic devices become more compact and complex, designers must employ advanced technologies to optimize board space and performance. One such technology is via-in-pad technology, which has become increasingly popular in high-density and high-performance PCB designs. This article explores the essentials of via-in-pad technology, including guidelines for its implement......
Sep 08, 2026
Design for Manufacturing
Castellated PCBs: Introduction and Design Requirements
With the rapid development of electronic technology, electronic products are moving towards miniaturization, portability, multi-functionality, high integration, and high reliability.Consequently, printed circuit boards (PCBs) are frequently designed to integrate pre-existing, off-the-shelf modules. For example, IoT Bluetooth modules or NB-IoT modules, which are indispensable communication modules, can be soldered onto PCBs just like chips. These carrier boards are characterized by their small size and......
Sep 08, 2026
Design for Manufacturing
Why Tolerance Analysis Is Key to Reliable and Cost-Effective PCB Production
Key Takeaways Tolerance analysis bridges CAD perfection and manufacturing variations to ensure reliable PCB assembly. Focus on critical areas: annular rings, hole tolerances, trace/space, layer registration, and solder mask alignment. Apply Worst-Case, RSS, or Monte Carlo methods for effective tolerance stack-up. Proper analysis boosts yield, cuts respins and costs — start with JLCPCB’s DFM review. Have you ever sent a board to fabrication, which appeared flawless on the computer screen, but then foun......
Jun 30, 2026
Design for Manufacturing
Copper Balancing in PCBs: Achieving Optimal Performance and High Yields with JLCPCB
Key Takeaways Copper balancing strategically distributes copper across PCB layers to create uniform density, preventing warpage, uneven plating, inconsistent etching, and signal integrity issues. The ideal copper density target sits within the 40%–60% golden ratio, with mirrored layers maintaining density variation within 15%–20% per IPC-6012 standards. Copper thieving (dot patterns or crosshatch meshes) equalizes current density during electroplating without introducing parasitic capacitance on spars......
Jun 12, 2026
Design for Manufacturing
PCB Design : How to Resolve Short Circuit Defects Caused by HASL
Key Takeaways In high-density PCB designs, HASL frequently causes solder bridging and short circuits due to its uneven surface and molten solder flow, especially on fine-pitch and dense traces. The most effective solution is to switch to ENIG (Electroless Nickel Immersion Gold), which provides superior planarity, significantly reduces bridging risks, and improves assembly yield. By selecting ENIG for dense layouts, optimizing solder mask design, and running DFM checks, designers can effectively elimin......
May 15, 2026
Design for Manufacturing
Design Process of a Surface Mount PCB
Key Takeaways Mastering the surface mount PCB design process is essential for creating compact, high-density, and reliable electronic boards. This comprehensive guide walks through the complete SMT workflow — from schematic capture and component selection to optimized layout, precise routing, DRC/ERC verification, and Gerber file generation — enabling designers to achieve superior performance, better manufacturability, and cost efficiency compared to traditional through-hole methods. By following thes......
May 14, 2026
Design for Manufacturing
How to Avoid Shorts and Open Circuits in Dry Film Etching Process
When utilizing the dry film etching process, it is crucial to take precautions to prevent short circuits and open circuits in printed circuit boards (PCBs). JLCPCB emphasizes specific considerations to ensure the integrity and functionality of PCB designs. This article provides guidelines for maintaining adequate trace width and spacing as well as utilizing hatched copper pours effectively to avoid defects during the dry film etching process. Maintaining Adequate Trace Width and Spacing JLCPCB employs......
Apr 18, 2026
Design for Manufacturing
How to Set PCB Via Tenting in PCB Design Software
Introduction Via tenting refers to covering the via pads and holes with solder mask ink (also known as solder resist), preventing solder from adhering to the pads. This is a process widely used in most circuit boards. It's a critical part of PCB design, protecting the vias and enhancing the board’s durability and performance. In this guide, we'll show you how to configure PCB via tenting in commonly used software such as Altium Designer (AD) and Protel 99 to ensure your Gerber files meet the required ......
Apr 17, 2026
Design for Manufacturing
FPC Panelization Design Standards and Requirements
FPC (Flexible Printed Circuit Board) panelization is the process of arranging multiple FPC boards onto a single panel for efficient production. Proper panelization is crucial for optimizing material utilization, reducing production costs, and ensuring product quality. JLCPCB recommends following these standards to achieve the best yield and compatibility with SMT processes. General Panelization Guidelines Irregularly Shaped Frames: For irregularly shaped FPC frames, consider using JLC's irregular pane......
Apr 14, 2026
Design for Manufacturing
Enhanced PCB Design Efficiency with Mouse Bites
PCB design is a crucial aspect of electronics manufacturing, and optimizing the design can significantly enhance manufacturing efficiency while reducing costs and waste. One design element that can improve efficiency is the implementation of mouse bites. Mouse bites are small cuts or grooves made in a PCB to facilitate its separation into individual pieces during the manufacturing process. In this article, we will explore the role of mouse bites in PCB design, their advantages and disadvantages, desig......
Apr 08, 2026
Design for Manufacturing
Critical Aspect of PCB Panel Size
PCB panel size is a major factor in designing printed circuit boards because it directly affects how quickly they can be manufactured, how they are assembled, and how much they generally cost. From home electronics to heavy industrial, PCBs are the building blocks of practically all devices in the modern electronics. This article covers the importance of PCB panel size, the elements affecting it, the best approaches to maximize it, and its applications in multiple sectors. 1. What is PCB Panel Size? P......
Apr 03, 2026
Design for Manufacturing
Understanding the Importance of Annular Rings in PCB Design
Annular rings play a crucial role in printed circuit board (PCB) design, ensuring the proper electrical connection of two pads. The signal and current flow are characterized based on the placement of annular rings between two layers. Incorrect calculation of size and improper placement can lead to transient behavior and flicker noise in electronic components. In this article, we will consider all important steps to improve our design from annular ring issues, tangency, and breakout. An annular ring in......
Mar 30, 2026
Design for Manufacturing
How to Prevent Solder Defects During Reflow Soldering
Reflow soldering is a critical step in surface mount technology (SMT) assembly, where solder paste is melted to form strong and reliable joints between components and the PCB. However, defects during this process can lead to assembly failures, rework, and reduced reliability. Understanding the causes of solder defects and implementing preventive measures can significantly improve yield and quality. Know how PCB assembly is done in JLCPCB factory. Common Solder Defects in Reflow Soldering: Solder Bridg......
Jan 30, 2026
Design for Manufacturing
What's the Difference: Countersink VS Counterbore Holes in PCBs?
When designing printed circuit boards (PCBs), engineers often need to create holes in the board to mount components or attach connectors. Two common hole types are countersunk and counterbored. While they may seem similar at first glance, there are important differences between countersink and counterbore holes that impact their use in PCBs. Both terms are commonly used in CNC machining. Normally countersink is a cone-shaped hole and the counterbore is a cylindrical flat-bottomed hole. This article wi......
Aug 15, 2025
Design for Manufacturing
Understanding DRC Testing in PCB Design
Design Rule checking (DRC) must be used throughout design and production of printed circuit boards (PCBs). Design rule and constraint compliance (DRC) testing helps eliminate issues that could arise during manufacturing and during the usage of the produced good. A good DRC test makes sure that the design is reliable, reduces mistakes, and meets the manufacturer's requirements, even though PCBs are getting more complicated in modern electronics. In this article, we will talk about why DRC testing is im......
Apr 30, 2025
Design for Manufacturing
RoHS Compliance in PCBs: What Designers Need to Know
RoHS-compliant in the context of PCBs (Printed Circuit Boards) means that the board and its components adhere to the Restriction of Hazardous Substances (RoHS) directive. RoHS is a set of regulations that restrict the use of certain hazardous materials commonly found in electronic and electrical equipment. The primary goal is to reduce environmental impact and improve health safety during manufacturing, usage, and disposal. To know how PCBs are made in JLPCB fab, visit our comprehensive guide on PCB m......
Jan 19, 2025
Design for Manufacturing
The Role of Pad Soldering in PCB Design
Introduction Pad soldering is a vital method used in the manufacturing of Printed Circuit Boards (PCBs), especially in relation to Surface Mounted Devices (SMDs). Pad soldering's reliability and precision have grown more crucial as electronic devices keep getting smaller and more complicated. The value of pad soldering in PCB design, varieties of solder pads, optimum techniques for obtaining dependable connections, and typical process difficulties are discussed in this article. What is Pad Soldering? ......
Dec 25, 2024
Design for Manufacturing
Thermal Vias in PCB: A Comprehensive Guide to Heat Management
Introduction In the world of PCB design, managing heat is essential for the reliability and performance of electronic devices. Thermal vias in PCBs play a vital role in heat dissipation, ensuring components last longer. As electronic devices become more compact and powerful, understanding the design and placement of PCB thermal vias and other thermal management techniques is crucial. This guide delves into thermal vias in PCBs, focusing on their design, placement, and effectiveness in thermal manageme......
Nov 26, 2024
Design for Manufacturing
A Comprehensive Guide to Countersunk Holes in PCB Design
When designing printed circuit boards (PCBs), engineers often need to create holes in the board to mount components or attach connectors. Two common hole types are countersunk and counterbored. While they may seem similar at first glance, there are important differences between countersunk and counterbore holes that impact their use in PCBs. Both terms are commonly used in CNC machining. Normally countersunk is a cone-shaped hole and the counterbore is a cylindrical flat-bottomed hole. This article wi......
Sep 29, 2024
Design for Manufacturing
Addressing Panelization Issues with Irregular Shapes and Structures
In production, JLCPCB has frequently had to process panel designs which have insufficient consideration for V-cutting. Simply tiling multiple boards together is suitable for uniformly sized and regularly shaped rectangular boards. However, for irregularly shaped boards with varying sizes, such a naive panel design is not feasible. Instead, it requires a consideration of the capabilities and requirements of the machines involved in production. Below, we will provide specific analyses using real-world e......
Mar 26, 2024
Design for Manufacturing
Design Optimization: How to Avoid Incomplete Milling of Internal Corners in PCB Panels
When panelizing PCBs with no gap between boards, the outlines of adjacent boards can sometimes form sharp internal corners that cannot be accurately routed without artefacts such as spurs or indents. Panels like this need to be redesigned to ensure complete, spur-free board outlines. Example V-Cut Panel With Three Boards Two Possible Routing Strategies And Results Because the router bit is round, it's unable to reach into tight corners. The unreached parts become sharp spurs after separating the board......
Jan 09, 2024
Design for Manufacturing
Maximizing PCB Design and Manufacturing Success with Effective PCB Pad Implementation
Within the realm of PCB (Printed Circuit Board) design and manufacturing, the significance of PCB pads cannot be overstated. These small, yet vital parts play a crucial role in ensuring reliable and secure connections for optimal performance. In this article, we dig further into the essential aspects of PCB pads, including what they are, different pad types, and their design considerations, impact on manufacturing, and material choices, all aimed at enhancing the overall quality of PCBs. I. What Are P......
Nov 27, 2023
Design for Manufacturing
Avoiding Ambiguities for Non-Standard PCB Shapes
Typically, PCBs have regular rectangular shapes. However, nowadays, many PCBs are becoming smaller in size, and with the changing market, they are incorporating more functions and accommodating more diverse casing shapes. This has led to more complex designs, especially for non-standard shapes that often require more care in design and manufacture. Now, let's explore the different outcomes that can arise due to the improper design of non-standard shapes. 1. Routing Only Along the Outer Layer (Green li......
Sep 21, 2023
Design for Manufacturing
PCB Design Tips: How to Avoid Damaged Traces and Pads
PCB Design Tips: All machining operations have finite errors, and milling in PCB production is no exception. JLCPCB’s regular milling tolerance is ±0.2 mm, with a precision ±0.1 mm option available. Due to these errors, it’s necessary to leave at least a 0.3 mm safety margin between any copper and a milled edge. Insufficient clearance can lead to damaged traces and pads, resulting in defective boards. Problem and Solution A milled slot on the board (purple) is placed too close to a nearby trace and cu......
Aug 17, 2023
Design for Manufacturing
PCB Design Tips: The Introduction of L Special-shaped Board
PCB Design Tips: L special-shaped board upside-down jigsaw puzzle. In actual production, there are L special-shaped boards, which can be rotated 180 degrees to increase the utilization rate of the boards and reduce costs. The conventional boarding methods include V-cut boards and stamp hole boards.The V-cut processing is linear, from one end of the V-cut to the other end, and it is necessary to pay attention not to the V-cut to the PCB circuit pattern when assembling the board. GET FREE QUOTE>>
Aug 04, 2023
Design for Manufacturing
PCB Design Tips: Why Perfboard is Not Suitable for Soldering
PCB Design Tips: Perfboard should be made of immersion gold instead of HASL. HASL is also called hot air leveling (HSAL). Its processing method is to immerse the board vertically down into the liquid tin liquid through the guide rail, then lift it up, and blow the flat surface with strong hot air. The residual tin liquid in the hole of the "board" flows out from the hole under the action of hot air, and part of it may stick to the adjacent pad, thus forming a short circuit failure. For this kind of "p......
Aug 04, 2023
Design for Manufacturing
PCB Design Tips: How to Avoid Solder Splatter
PCB Design Tips: Immersion gold should be used to avoid tin blast holes. HASL is also called hot air leveling (HSAL). Its processing method is to immerse the board vertically down through the guide rail into the liquid high-temperature tin liquid, and then lift it up, and use strong hot air to blow the tin liquid on the surface of the slot hole plate. If the tin hole is too large (round hole or oval hole), the copper surface of the hole wall will sometimes fall off from the base material, which will c......
Aug 04, 2023
Design for Manufacturing
PCB Design Tips: How to Prevent Breakage of Traces during Board Bending
PCB Design Tips: How to avoid breaking the board when the thin and narrow connection is broken? In actual production, sometimes there are narrow and long connections, some of which may be wired. After the PCB is processed by V-cutting, the customer's force is uneven when dividing the board, and the force on the narrow place is weak. It is easy to break when breaking the board (at A in the figure below). At this time, we can change the way of jigsaw puzzles, and open a gap of 1.6-2MM between the boards......
Aug 04, 2023
- 1
- 2
- 3
- 4
- 5