How Inner Layer Residual Copper Rate Affects PCB Thickness and Quality
4 min
- How Inner Layer Copper Affects Board Thickness
- Importance of Residual Copper Rate
- The Role of PP Sheets in Multilayer Lamination
- Consequences of Low Residual Copper Rate
- JLCPCB Recommendations
- Common Issues in Gold Finger Design
- Common Issues in PCB Gold Finger Design
In printed circuit board (PCB) manufacturing, precision is crucial for maintaining quality and performance. One key factor that significantly influences PCB quality is the residual copper rate in the inner layers. This concept becomes particularly critical in multilayer PCBs, where the balance of copper distribution impacts the final board thickness. This article explores how the inner layer residual copper rate affects board thickness and the importance of optimizing this rate to ensure robust and reliable PCBs.
How Inner Layer Copper Affects Board Thickness
As shown in the diagram, when the copper coverage in the inner layer is minimal, the (PP prepreg) sheets, regardless of their thickness, must spread evenly to fill the gaps between layers. Once the PP sheets cool and solidify, the reduced resin volume leads to a thinner overall board thickness.
Importance of Residual Copper Rate
So, how much copper should be laid in the inner layer to ensure that the board thickness doesn’t fall below tolerance limits? This is where the "residual copper rate" comes in. The residual copper rate refers to the percentage of the inner layer's copper circuit patterns relative to the entire surface area of the board.
Residual copper rate = the area of copper in the current layer / total area of the board.
The Role of PP Sheets in Multilayer Lamination
In multilayer board lamination, PP sheets are cut into pieces and placed between the inner core board and another core board, or between the core board and copper foil. The resin on the PP melts under high temperature and pressure, filling the copper-free areas on the core board. After cooling, the resin solidifies, bonding the core board and copper foil together.
Consequences of Low Residual Copper Rate
If the residual copper rate is too low, the overall board thickness decreases, and uneven copper distribution across layers can lead to board warping.
This is especially critical for boards with gold fingers, as their thickness must be precise to ensure a proper fit in slots. A thinner board may result in a loose fit or poor contact when inserted into the slot.
JLCPCB Recommendations
JLCPCB enginners strongly recommend :
1. For Gold Finger Multilayer Boards
Cover the blank areas with copper, especially in the inner layers near the gold finger region. This prevents issues such as the board being too thin to fit into the slot or variations in line widths.
2. For Residual Copper Rates Below 25%
To minimize uneven electroplating, which can cause inconsistent line widths and excessive board thickness deviations, add copper to the blank areas.
Common Issues in Gold Finger Design
For the golden finger areas in both the inner and outer layers, ensure that there is an open window (i.e., no solder mask bridge between each golden finger pad) to prevent frequent insertion and removal from causing ink to fall into the golden finger slot, which can result in poor contact and other functional issues.
For all types of PCBs, add copper to blank areas whenever possible, as long as it does not affect the board's performance. For boards with a residual copper rate below 25%, ensure that copper is added. In gold finger boards, copper should be applied to the inner layer near the gold finger area, and the outer layer should have a solder mask with a properly open window in the gold finger area.
Common Issues in PCB Gold Finger Design
For the golden finger areas in both the inner and outer layers, ensure that there is an open window (i.e., no solder mask bridge between each golden finger pad) to prevent frequent insertion and removal from causing ink to fall into the golden finger slot, which can result in poor contact and other functional issues.
For all types of PCBs, add copper to blank areas whenever possible, as long as it does not affect the board's performance. For boards with a residual copper rate below 25%, ensure that copper is added. In gold finger boards, copper should be applied to the inner layer near the gold finger area, and the outer layer should have a solder mask with a properly open window in the gold finger area.
Keep Learning
How to Select Tg of PCB ?
What is the Tg of PCB? In PCB manufacturing, "Tg" stands for Glass Transition Temperature. It is the temperature at which the PCB substrate material transitions from a rigid, glassy state to a soft, rubbery state. PCBs are flame-retardant (UL94 V-0) and do not burn easily; instead, they soften above Tg. The Critical Correlation Between Tg and Z-Axis CTE (Coefficient of Thermal Expansion) When the temperature exceeds the Tg point, the PCB substrate material (such as standard FR-4) undergoes a physical ......
Choosing the Right CTI Value for Safer High-Voltage PCBs
Key Takeaways Higher CTI (≥600V, Group I) allows shorter creepage distances while preventing surface tracking in high-voltage designs. Standard FR4 (CTI ~175V) is often inadequate for mains voltage — upgrade to high-CTI materials for safety and compactness. Always match CTI material group to your working voltage and pollution degree for IEC/UL compliance. Clean assembly and good layout practices are essential to realize the full benefits of high-CTI laminates. Choose certified high-CTI materials and e......
Maximize Efficiency with PCB Panelization in High-Volume Manufacturing
Whenever a new PCB designer begins to spin the wheels, they are soon enough faced with the transition of creating a few prototypes into a volume production venture. As well as that, change brings a new idea that prototype-based engineers tend to forget: PCB panelization. In essence, panelization refers to loading a number of copies of your board design (or even a variety of designs) onto a single standardized production panel such that all of the fabrication and assembly processes treat them as a sing......
Inside the PCB Structure : How Layers, Stackup, and Buildup Define Modern Circuit Board Performance
Printed circuit boards may look like flat green rectangles, but beneath the surface, they are sophisticated multi-layer structures. As devices get more compact and complex, engineers turn to multilayer boards with carefully chosen materials and stackups to meet electrical and mechanical demands. This article peels back those layers to explore how substrate choice, layer stackup, and buildup methods shape PCB performance. Here we’ll cover PCB design fundamentals from the base materials up to high-densi......
The Benefits of Bed of Nails Testing in Professional PCB Manufacturing
Have you ever wondered how manufacturers can test thousands of PCBs daily and not make the production line crawl? The answer, as frequently as not, is a deceitful-appearing device called a bed of nails test set-up. The platform contains hundreds of little spring-loaded pins on it, and each of those pins is aligned very precisely to touch a specific test point on your circuit board. It can check the electrical integrity of a whole PCB, shorts, opens, and component defects in a few seconds, before the b......
Understanding PCB Dielectric Constant : Choosing Materials for Optimal Signal Performance
Key Takeaways The PCB dielectric constant (Dk) is a critical factor that directly determines signal propagation speed, characteristic impedance, and transmission loss in high-frequency designs. Selecting the right material — from standard FR4 for general use to low-Dk Rogers, PTFE, and LCP for multi-gigahertz applications — enables better performance, tighter impedance control, and reduced signal degradation. Success ultimately comes from matching Dk to your frequency needs, optimizing layer stackup, ......