PCB Sourcing & Procurement Essentials
Understand sourcing factors, pricing considerations, lead times, and how to choose dependable PCB fabrication partners.
Latest Posts
PCB Sourcing & Procurement
Breaking Down PCB Pricing: How is the Cost Determined
PCB quote packaging involves gathering and organizing all the necessary details to estimate the cost of manufacturing a PCB. This process includes not only design specifications but also material selection, manufacturing methods, and engineering considerations. It goes beyond a simple financial estimate and provides a thorough engineering analysis to ensure the quote is accurate, feasible, and optimized for production. Every aspect affecting production such as material type, size, complexity, and prod......
Nov 16, 2026
PCB Sourcing & Procurement
Flex PCB Manufacturers for Compact Electronics: Sourcing Guide
When choosing a flex PCB manufacturer for your compact electronics application, be sure to consider not only their maximum trace density, maximum stackup thickness, maximum bend radius, and stiffener thickness, but also whether they routinely build such parts. Since a design based on the manufacturer's best-case fabrication limits may be very tight in terms of production yield and/or dimensional tolerances, and long-term reliability, particularly in compact devices where space may be limited and repea......
Nov 02, 2026
PCB Sourcing & Procurement
Quick Turn PCB: How to Get High-Quality Prototypes Fast
Printed Circuit Boards (PCBs) are a vital part of modern electronics, and the demand for faster and more efficient development made a quick turn PCB services extremly important. In this article, we will discuss what quick turn PCB is, its importance, the lead time for JLCPCB's quickturn PCB fabrication, how quick turn PCB can help businesses, and how to choose a good quick turn PCB manufacturer. What is Quick Turn PCB? Quick turn PCB refers to the process of manufacturing and delivering PCBs within a ......
Oct 29, 2026
PCB Sourcing & Procurement
How to Build a Bulletproof Bill of Materials for Flawless PCB Production
Have you ever sent a PCB design to be assembled only to receive an email requesting why you have not provided a part number or the package has not been matched? In that case, you are already aware that a single slip in your bill of materials will bring a flawless board down. Take a small CH32V003-based dev board consisting of 29 components distributed on 11 different footprints on a 2-layer copper PCB. It has an MCU, USB-C input, 24MHz crystal, USB-to-TTL bridge, indicator LEDs, and programming/GPIO h......
Oct 28, 2026
PCB Sourcing & Procurement
The True Cost of Custom PCBs: Understanding the Factors that Affect the Bottom Line
Key Takeaways Optimize Layout & Size: Simplify circuit design and keep board size within 100mm x 100mm for basic promo rates. Stick to Standard Specs: Use 1.6mm board thickness and 1 oz copper weight to avoid material surcharges. Respect DFM Limits: Maintain trace width/spacing ≥ 5/5 mil and via drills ≥ 0.3mm to prevent fine-feature fees. Select Low-Cost Finishes: Choose HASL over ENIG for prototypes unless fine-pitch BGAs are required. Printed circuit boards (PCBs) are integral to modern technology,......
Oct 28, 2026
PCB Sourcing & Procurement
Crafting Success: Choosing the Right PCB Manufacturer for Hobbyist
As a PCB hobbyist or engineer, finding a reliable and professional PCB manufacturer is crucial to ensure the success of your projects. The right PCB manufacturer can provide you with valuable guidance, access to advanced manufacturing technologies, and the support needed to excel in the dynamic world of PCB design and manufacturing. In this article, we will explore key characteristics to consider when selecting a PCB manufacturer, with a focus on professional instruction, customization options, qualit......
Oct 28, 2026
PCB Sourcing & Procurement
PCB Mount Techniques, Methods, and Best Practices
Key Takeaways SMT vs. THT: SMT fits micro-packages (down to 01005), while THT provides high mechanical strength for heavy components. Selective Wave DFM: Requires a 5mm keep-out zone around THT pads to protect bottom-side SMT parts from thermal shock. Mounting Hole Clearance: Keep a 0.5mm minimum clearance around screw heads on NPTH/PTH holes to prevent trace shorts. FPC Stiffeners: Use PI/FR4 stiffeners behind FPC pads with a 1.0mm edge clearance to prevent joint fatigue. Introduction In the electron......
Oct 13, 2026
PCB Sourcing & Procurement
What Is a Protoboard and Why Engineers Use It
Key Takeaways Core Concept: Protoboards use a 2.54 mm perforated copper grid for hand-soldered, semi-permanent circuit prototypes. Protoboard vs. Breadboard: They offer far better physical durability and joint stability than solderless breadboards. Key Limitations: Manual wiring creates high parasitic noise, lacks impedance control, and supports no direct SMD chips. JLCPCB Upgrade: Custom PCBs provide 0.3 mm drill accuracy, 5 mil traces, multi-layer stackups, and heavy copper. I used protoboards when ......
Sep 09, 2026
PCB Sourcing & Procurement
Why Specific File Formats Are Essential for Ordering PCBs
Ordering printed circuit boards (PCBs) involves providing precise and detailed information about the design and specifications. Without the right file formats, even the most brilliant PCB design can lead to manufacturing delays, costly errors, or complete production failure. This is why specific PCB file formats are necessary. Manufacturing can only proceed successfully with a complete set of production files, including schematic designs, Bill of Materials (BOM), PCB layouts, and stack-up information.......
Apr 16, 2026
PCB Sourcing & Procurement
How to Choose the Right Solder Wire for Your Projects
Solder hails from the middle english word soudur, which derives from the latin word solidare, meaning "to make solid." It's a fusible alloy (i.e. low melting point) used to bond metal workpieces together. Solder is a material that is used to bond objects, such as pipes or wires, together permanently. The primary application for soldering in the plumbing industry is leak-free connections. In the electronics industry, soldering is used to fuse wires for circuit components. Soldering is an essential skil......
Apr 01, 2026
PCB Sourcing & Procurement
Lead-Free vs Lead Solder: What’s the Real Difference?
Solder is used by the majority of electrical devices to connect components to PCBs. The procedure of soldering is, when a solder melts down it will make a connection. This connection can be between pads or wires. Soldering is not like welding, we can attach the two joints by heating them again a lil bit. Although after performing the soldering step the curing and cooling is required. If during the cooling step there is any disturbance occur in the system it will lead to dry joints. Two main varieties ......
Apr 01, 2026
PCB Sourcing & Procurement
The Importance of a PCB Supplier in the Electronics Industry
Introduction: Printed circuit boards (PCBs) are found in almost all electronic devices, as they are the backbone of modern electronics. They give the mechanical support and electrical connection to run complicated systems. Particularly with regard to large-scale manufacturing, choosing the correct PCB supplier is absolutely vital for guaranteeing the performance, durability, and cost-effectiveness of these boards. This article covers the function of PCB Suppliers, the criteria that should be considere......
Oct 20, 2025
PCB Sourcing & Procurement
Understanding PCB Quote and Packaging Engineering
In the era of electronics miniaturization, which everyone needs, we want lower form factors, lower power consumptions and higher performance. A field “packaging” which also evolves as the things shrink. In the early days electronics were shipped in big boxes with no need of high end packaging because components were not so delicate at that point. But the small components need quality packaging. The field of packaging becomes a type of engineering as well. Which keeps the things inside the package inta......
Aug 19, 2025
PCB Sourcing & Procurement
Understanding PCB Printer vs. PCB Manufacturer: Which Option Suits Your Needs?
PCB printers are becoming more popular for quick prototyping on-site and small-scale production, especially among artists and new businesses. Traditionally, companies hired skilled PCB manufacturers to make a lot of boards for them. This article will discuss about the differences between using a PCB printer and depending on a manufacturer. It will cover the pros and cons of each and what you should think about when making your choice. 1. What is a PCB Printer? A PCB printer is a special kind of machin......
Mar 28, 2025
PCB Sourcing & Procurement
Custom PCBs: The Ultimate Guide to Designing and Ordering Your Own PCB
Custom PCBs (Printed Circuit Boards) are customized circuit boards designed to meet specific requirements or applications that standard off-the-shelf PCBs cannot fulfill. They are utilized in a broad array of electronic devices and systems, serving as a base for mounting and connecting electronic components like resistors, capacitors, integrated circuits, and connectors. Custom PCBs facilitate the creation of specialized and innovative electronic devices, offering the adaptability to fulfill particula......
Jan 03, 2025
PCB Sourcing & Procurement
The Dos and Don'ts of Choosing a PCB Manufacturer
Choosing the right printed circuit board (PCB) manufacturer is a critical decision for electronics engineers, designers, and manufacturers. With so many options available, it can be overwhelming to decide which manufacturer to trust with your PCB assembly needs. The quality of the PCBs you use can make a significant impact on the performance, reliability, and safety of your electronic devices. Therefore, it is essential to choose a manufacturer that can meet your specific requirements while providing ......
Jul 24, 2023
- 1
- 2