This website requires JavaScript.
Coupons
Ship to
Blog

Understanding PCB Laminates Materials, Types, and Why They Matter

Published Jul 27, 2025, updated Oct 30, 2026

6 min

A PCB is a flat board made of a non-conductive substrate material with conductive pathways and components attached to it. One of the critical components of a PCB is the PCB laminate. A typical laminate PCB consists of a core material, such as fiberglass or composite epoxy. So what it actually do is

● Provides structural support

● Improves Signal Integrity

● Bond the layers to the core material

The fiberglass layers are stacked on top of each other and pressed together with heat and pressure to create a solid sheet of material. The result is a rigid, flat board that can support the conductive pathways and components that make up the PCB. This article explores what PCB laminates are, the different types available.

What Is a PCB Laminate?

A PCB laminate is basically a composite material consisting of one or more layers impregnated with resin. Without lamination, a PCB would be too fragile to function properly  ruining the circuitry and making the board unusable. The laminate also includes additional layers of insulating material known as prepreg. Prepreg is placed between the copper layers to provide electrical insulation and to maintain the desired spacing between layers. The number of copper layers and prepreg layers in a laminate can vary depending on the complexity of the PCB. Overall, the laminate in a PCB is the composite structure that consists of:

● Core material

● Copper foil layers

● Prepreg layers

It provides the foundation for the circuit board, enabling the proper functioning of electrical connections and ensuring the mechanical stability of the PCB.

Types of PCB Laminates

The choice of PCB laminate material depends on the application's requirements. Which includes mechanical strength, thermal resistance and electrical performance. Below are some common types of PCB laminates:

Some of the features are:

FR-4:

● Flame retardant (self-extinguishing)

● Good mechanical strength (tensile, flexural, compressive)

● Low moisture absorption (typically <0.1%)

● Good electrical insulation and reliable performance in dry/humid conditions

● Relatively low cost and widely available

● Moderate thermal stability (glass transition temperature ~130–140°C, high-Tg variants up to ~180°C)

PTFE (Teflon):

● Excellent high-frequency performance (low dielectric constant, low dissipation factor)

● Good thermal and chemical resistance

● Low moisture absorption

● Low surface energy (requires special treatment for copper adhesion)

● Dimensional instability and mechanical sensitivity

● Used in RF/microwave and high-speed digital circuits

Polyimide:

● Exceptional thermal stability (operates above 260°C)

● High mechanical strength and flexibility (ideal for flexible and rigid-flex PCBs)

● Low coefficient of thermal expansion (CTE)

● Good chemical resistance

● Low dielectric constant and dissipation factor (suitable for high-frequency and high-reliability applications)

● Higher cost compared to FR-4

PCB Laminate Factors to Consider

Power and energy efficiency will also be critical factors in ensuring a PCB’s compatibility with the end-use application. Depending on the application and desired results, other important factors to consider include:

● Glass Transition Temperature (Tg)

● Thermal conductivity (k)

● Coefficient of thermal expansion (CTE)

● Dielectric constant (Dk)

● Surface resistivity (pS)

● Flame retardancy

● Moisture absorption

● Density

● Chemical resistance

● Time to delaminate

Finally, you should take the certifications of a PCB manufacturer and the company’s research and development capabilities into account to guarantee the highest quality product.

Types of PCB Lamination Process:

Different electronic applications require different types of PCB components that fit the requirements of your operation. Choosing the right method will improve product reliability and decrease layer-to-layer registration. These types are:

Multilayer PCB Lamination:

Multilayer PCB lamination uses heat and pressure on prepreg material to bond layers together. The prepreg material is typically made from glass fiber or paper infused with a thermosetting resin. This provides:

● Good dimensional stability

● Excellent layer-to-layer registration

● High reliability

Sequential PCB Lamination

Sequential lamination is the best choice when bonding two to four substrates. Sequential lamination involves a step-by-step process that builds up the layers of the board one at a time. This process is done by adding and curing layers of dielectric material and copper until the desired board thickness is achieved. Some advantages are:

● The ability to fine-tune the properties of each layer

● Improved dimensional stability

● Low warpage

● Excellent layer-to-layer registration

Teflon (PTFE) Microwave Lamination

Teflon has good dimensional stability, can withstand extreme temperatures, and is an excellent electrical insulator. It is resistant to moisture and heat, making it ideal for use in high-frequency applications. Some advantages includes:

● High signal speed

● Minimal connection interruption

● Tight depth tolerance

● Excellent dimensional stability

Step-By-Step PCB Lamination

While the various specifics of each lamination process vary from one type to another, some general steps are followed in all cases:

Preparation:

Cleaning the substrates, metalization layers, and dielectric material ensures the components are free of any contaminants.

Micro-etching:

Once the materials are clean, the next step is to etch micro features into the metalization layers. Taking this action helps make sure that the layers bond together properly.

Black Oxide Treatment:

This step is used to improve the adhesion of the metalization layers to the substrate. Which avoids common issues like delamination.

Inner Layer Stack-Up:

The next step is to build the inner layer stack-up. This process involves bonding the layers and prepreg on a gluing machine to ensure inner layers and the prepreg won’t move during cure.

Stack-Up:

The layer creation is completed through the stack-up of copper and dielectric material. The application requirements will determine the number of layers.

Lamination:

You can do this step manually or automatically, depending on the size and complexity of the board. As it is the final step to run the stack-up through a lamination process to bond all the layers together.

Common PCB Lamination Issues

Blistering:  Blistering occurs when too much humidity or heat is present in the lamination process. This issue can cause bubbles and gaps. Solutions include proper drying of the materials before lamination and using lower temperatures during the process.

Voiding: A PCB lamination void can occur due to resin gaps between bonding materials.  Excessive moisture on layers prior to lamination, or due to air pockets between layers. Oven drying or increasing resin pressure can be the solutions.

From everyday consumer gadgets to sophisticated aerospace systems, the quality of PCB laminates plays a vital role in the success of electronic products worldwide.JLCPCB provides quality PCBs using industry-standard laminates.

Keep Learning