PCBA Quality Control & Testing
Explore PCBA quality control and testing practices, including inspection methods, electrical testing, defect detection, and reliability validation.
Featured Posts
Quality Control & Testing
PCB X-Ray Inspection Explained: Non-Destructive Testing for PCB Assembly Quality Control
In the era of miniaturization, modern printed circuit boards (PCBs) face an invisible challenge: verifying the quality of solder joints hidden beneath components. With Ball Grid Array (BGA) packages featuring pitch sizes down to 0.3mm and Quad Flat No-lead (QFN) components concealing critical thermal connections, traditional optical methods are blind to the most critical failure points. PCB X-ray inspection has emerged as the definitive solution. This guide explores the technical foundations, applicat......
Feb 03, 2026
Quality Control & Testing
Flying Probe Testing: Revolutionizing PCB Quality Assurance in Modern Electronics ManufacturingNov 26, 2025Quality Control & Testing
Solder Paste Inspection (SPI): A Complete Guide to Process Control in SMT AssemblyNov 27, 2025Quality Control & Testing
What Is PCBA Testing? Complete Guide to Inspection Methods, Process, and Quality ControlNov 25, 2025Quality Control & Testing
Automated Optical Inspection (AOI): Principles, Defects, and PCB ApplicationsSep 11, 2024
Latest Posts
Quality Control & Testing
PCB X-Ray Inspection Explained: Non-Destructive Testing for PCB Assembly Quality Control
In the era of miniaturization, modern printed circuit boards (PCBs) face an invisible challenge: verifying the quality of solder joints hidden beneath components. With Ball Grid Array (BGA) packages featuring pitch sizes down to 0.3mm and Quad Flat No-lead (QFN) components concealing critical thermal connections, traditional optical methods are blind to the most critical failure points. PCB X-ray inspection has emerged as the definitive solution. This guide explores the technical foundations, applicat......
Nov 18, 2026
Quality Control & Testing
Flying Probe Testing: Revolutionizing PCB Quality Assurance in Modern Electronics Manufacturing
The process for manufacturing printed circuit boards (PCBs) includes a critical testing phase. Each board must undergo testing to ensure manufacturers detect every electrical or circuitry problem before leaving the center. When a PCB passes this testing, it further ensures that it performs reliably. The most common types of testing methods include in-circuit testing (ICT) and flying probe testing (FPT). 6 high-precision probes (needles), 4 on top and 2 on the bottom are programmatically able to contac......
Nov 12, 2026
Quality Control & Testing
Transistor Pin Identification Using a Multimeter: Complete Step-by-Step Guide
Identifying transistor pins correctly is one of the first checks every engineer, hobbyist, and EE student needs before placing a bipolar junction transistor (BJT) into a circuit. A wrong base, collector, or emitter assignment can destroy the part on first power-up or leave a prototype board silently non-functional. This guide explains how to identify transistor pins using a multimeter when no datasheet is available. The method works because a BJT is internally built from two PN junctions sharing a com......
Nov 10, 2026
Quality Control & Testing
Solder Paste Inspection (SPI): A Complete Guide to Process Control in SMT Assembly
In today's Surface Mount Technology (SMT) manufacturing world, the consistency of the solder paste deposit is the element that drives electrical performance, mechanical shear strength, and long-term reliability of assembled Printed Circuit Boards. The solder paste is the medium that bonds the component terminations to the copper pads on the PCB. Therefore, any variations in the solder paste deposit in terms of volume, thickness, or placement will drastically impact the quality of the solder joints in ......
Nov 03, 2026
Quality Control & Testing
What Is PCBA Testing? Complete Guide to Inspection Methods, Process, and Quality Control
In modern electronics, the performance and long-term reliability of a finished product are directly tied to its Printed Circuit Board Assembly (PCBA) quality control. Even small defects at the board level—such as microscopic solder cracks, misaligned components, or incorrect passive values—can cascade into costly field failures, product recalls, and long-term damage to a brand's reputation. High-quality PCBA is not achieved through a single final inspection; it is the result of a repetitive and system......
Jun 30, 2026
Quality Control & Testing
Automated Optical Inspection (AOI): Principles, Defects, and PCB Applications
What Is Automated Optical Inspection (AOI)? Automated Optical Inspection (AOI) is a machine-based inspection method that uses high-resolution cameras, controlled lighting, and image-processing software to automatically detect visual defects on printed circuit boards (PCBs). It is widely used in PCB fabrication and PCB assembly to inspect components, solder joints, and conductor patterns without physical contact. By comparing captured images with design data or reference models, AOI systems can quickly......
Apr 23, 2026
Quality Control & Testing
What Are the Different Types of SMT Tests in PCB Assembly
Full-fledged electronics solutions that aim to minimize size and space use surface mount components. Although the SMT components function similarly to the TH, they are generally chosen due to their small size and compatibility with both side assemblies. When developing for mass manufacturing, cost is also the primary issue because of their low cost, which allows us to use them in large quantities. Due to their small size, inspection methods and repair operations are now more challenging. A product is ......
Sep 29, 2025
Quality Control & Testing
What is a Bed of Nails Test Fixture
Testing is important when it comes to electronics product manufacturing. It is the most crucial yet deciding the working condition of a product. There are many testing procedures a product wants to go through. When working with an assembly company the testing may take a lot of time to reduce the manpower and time there should be a set of instructions to follow. For this the BED OF NAILS test is designed, so that we can make a type a zig and test the prototypes directly by connecting the testing points......
Aug 20, 2025
Quality Control & Testing
Electrostatic Discharge (ESD): The Hidden Threat to Electronics
It's possible your next electronic device could be deployed in an area where it is exposed to high voltages or static electricity. In these cases, a system’s vulnerability to ESD should be determined through testing and simulation. Electrostatic Discharge (ESD) is the sudden transfer of static electricity from one object to another. This phenomenon occurs when there is a difference in electrical potential between two surfaces, leading to an abrupt discharge of energy. The charge can be accumulated par......
Mar 25, 2025
Quality Control & Testing
PCB Failure Analysis: Understanding the Causes and Solutions
Printed circuit board (PCB) failure analysis is vital for finding and resolving issues causing electronics to stop working. PCBs are highly complex and feature numerous layers of circuitry that interact with one another, hence it can be difficult to understand why something is not working. A damaged component may bring down the entire system. By doing a failure analysis, makers can make PCB designs more reliable and stop problems from happening again. This article goes into detail about why PCB failur......
Mar 10, 2025
Quality Control & Testing
AOI Detection Working Principle
#1 What is AOI Detection? Automated Optical Inspection (AOI) is a technology that uses optical principles and image processing techniques to inspect component solder joints on PCBA boards. It can quickly identify subtle defects in solder joints, effectively overcoming the limitations of manual visual inspection. (Image source: Internet) #2 AOI Detection Working Principle AOI detection equipment mainly relies on the principle of light reflection to identify and inspect component solder joints on PCBA b......
Feb 05, 2025
Quality Control & Testing
Understanding PCBA Manufacturing Standards and Certifications
In the world of electronics manufacturing, ensuring the quality and reliability of printed circuit board assemblies (PCBAs) is of utmost importance. To meet industry standards and deliver high-quality products, PCBA manufacturers adhere to specific manufacturing standards and certifications. In this article, we will delve into the realm of PCBA manufacturing standards and certifications, shedding light on their significance and how they contribute to the overall quality assurance process. The Importan......
Dec 26, 2023
- 1
- 2