This website requires JavaScript.
Coupons
Ship to
Blog

FR4 PCB Deep Guide: Material Truth, Real Specs & When to Use (or Avoid) It

Published Dec 27, 2025, updated Nov 10, 2026

12 min

Table of Contents
  • FR4 Material Properties That Actually Matter
  • FR4 PCB Specifications: What Manufacturers Really Offer
  • FR4 PCB Manufacturing: Process Differences & Limitations
  • When FR4 Is Perfect (and When You Should Run Away)
  • Material Quick Decision Matrix:
  • Conclusion: Your 30-Second FR4 Checklist Before Ordering

hdi pcb coupons

FR-4 isn't a secret code, it literally means Flame Retardant (grade 4). In PCB terms, FR-4 is a NEMA (National Electrical Manufacturers Association) grade designation for a glass-reinforced epoxy laminate. We can say it is a composite of woven fiberglass cloth bonded with an epoxy resin that contains flame-retardant additives. The “FR” stands for flame retardant, but note this doesn’t automatically mean UL94 V-0 certified. It just indicates the resin is formulated to self-extinguish if it catches fire. FR-4 was named in 1968 by NEMA and has since displaced older grades like G-10 because of its flame-resistant brominated epoxy.

NEMA FR-4 Grade Explained:

The NEMA LI-1 standard defines FR-4 as "industrial laminated thermosetting products" and was harmonized with Military Specification (MIL-I-24768) beginning in 1999. Essentially this means that in order for a board to be able to carry the designation of FR-4, it must meet certain mechanical, thermal and flammability requirements as per its Manufacturer's Specifications (MIL-I-24768). Other grades like FR-5 and FR-6 still exist but the FR-4 grade has become the industry standard. "FR-4" designates a particular grade of laminate material (epoxy/glass combination) that has been engineered to resist fire. It does not mean it makes its components "fireproof."

Epoxy + Glass Fabric + Flame Retardant Chemistry:

FR-4 is literally layers of fiberglass and epoxy. Embedded in the cured green epoxy resin, we can think of them like the “noodles” in a PCB lasagna. The resin itself is typically bromine-filled epoxy (often using TBBPA or similar brominated compounds). Which makes it self-extinguish when burned.

In summary, FR-4 = Fiberglass + Resin (epoxy) with flame-resistant bromine chemistry. It combines lightweight strength with low cost. You might joke that FR-4 stands for “Fires Reduced grade 4”. The important part is that FR-4’s epoxy resins are specially formulated to stop burning, which is why this grade became the PCB industry staple.

FR4 Material Properties That Actually Matter

Not all material specs are created equal. For PCB designers, the crucial FR-4 properties include its glass transition (Tg), decomposition temperature (Td), thermal expansion (CTE), dielectric constant (Dk), and loss tangent (Df). Here are typical ballpark values for a standard FR-4 (values vary by manufacturer):

  • Glass Transition (Tg): It is 130–140 °C for standard FR-4. This is the temperature at which the board starts to soften. High-Tg FR-4 materials may get up to 170–180 °C for lead-free processes.
  • Decomposition Temp (Td): Around 300–350 °C (e.g. some FR-4 variants list Td as 355 °C). This is where the resin chemically breaks down.
  • CTE (Coeff. of Thermal Expansion): It is 12–17 ppm/°C in-plane (X/Y) and 60–80 ppm/°C through-plane (Z). FR-4’s fiber weave keeps X/Y expansion modest, but in Z it can be 5× higher.
  • Dielectric Constant (Dk): Roughly 4.2–4.8 at 1 MHz, dropping slightly to 4.4 at 1 GHz. This affects signal speed/impedance.
  • Dissipation Factor (Df): Low (0.015 to 0.03 at 1 MHz to 1 GHz). Lower Df means less loss. FR-4 boards aren't great for RF, but works well up to a few GHz.
ParameterTypical Value (FR-4)
Glass Transition Temperature (Tg)130–140 °C (standard FR-4)170–180 °C (High-Tg FR-4)
Decomposition Temperature (Td)300–350 °C (up to ~355 °C for some grades)
CTE – In-Plane (X/Y)12–17 ppm/°C
CTE – Through-Plane (Z)60–80 ppm/°C
Dielectric Constant (Dk)4.2–4.8 @ 1 MHz4.4 @ 1 GHz
Dissipation Factor (Df)0.015–0.03 @ 1 MHz–1 GHz

Many boards just use these “typical FR-4” values as a baseline. Of course, actual values vary by supplier, so critical high-frequency or high-reliability designs should always check the exact datasheet.

Standard FR-4 vs High-Tg vs Halogen-Free

Even within FR-4 grade, there are variants tailored for different needs. Standard FR-4 (Tg around 130 °C) is the cheapest and is used in most consumer PCBs. High-Tg FR-4 variants are engineered for lead-free soldering and extreme environments. These may have Tg up to 170–180 °C or higher to survive multiple 260 °C reflow cycles.

Finally, halogen-free FR-4 uses phosphorus and nitrogen flame retardants instead of bromine. All this to meet RoHS and environmental rules. Its Tg and basic properties are similar, but it avoids toxic bromine. If you need extra temperature margin or greener chemistry then go for it.

FR4 PCB Specifications: What Manufacturers Really Offer

When you order FR-4 PCBs, what can you actually get from fabs?

Thickness Range (0.2–3.2 mm), Copper Weights & Tolerances

Most rigid FR-4 laminates come in sheets from about 0.127 mm (0.005″) up to 3.175 mm (0.125″) thickness. In practice, boards are commonly built from 0.4–2.0 mm. Manufacturers often stock core laminates at 0.2, 0.4, 0.8, 1.0, 1.2, 1.6, 2.0, 2.4, 3.2 mm, etc.

Copper foil weights are typically ½ oz, 1 oz, or 2 oz per side (17 μm, 35 μm, 70 μm). Inner layers are often ½ to 1 oz; outer layers can go up to 3–4 oz in extreme cases. Per IPC-4562 tolerances, a nominal 1 oz (35 μm) copper foil may legally be as low as 31 μm, meaning boards should expect about ±10% thickness variation on base copper. In plating, buildup or etch processes, the actual finished copper may end up slightly different, so designers generally allow some margin.

Surface Finishes Compatibility:

FR-4 substrates are compatible with all the usual PCB surface finishes. Standard finishes include HASL (hot-air solder leveling, tin-lead or lead-free) and ENIG (electroless nickel/immersion gold). Some others are Immersion Silver/Tin, OSP and ENEPIG.

HASL (lead or lead-free solder) is the classic low-cost finish. On the other hand, ENIG gives a flat gold surface for fine-pitch assembly. OSP is a low-cost organic coating often used on consumer boards. The key point is FR-4 boards can be plated or coated with any finish that PCB shops offer; there's no special limitation here.

FR4 PCB Manufacturing: Process Differences & Limitations

FR-4 boards are made using standard rigid-board processes. However, its glassy nature does impose some rules.

Drilling, Plating & Multilayer Pressing on FR-4

Drilling FR-4 is typically done with carbide bits. Unlike flexible or metal-core boards, FR-4 is rigid enough for conventional CNC drill presses. The glass fibers in FR-4 are abrasive, so carbide drills are essential to avoid rapid wear. Drilled holes (vias and TH components) are then electrolytically plated with copper. In multilayer production, FR-4 cores (copper-clad panels) are alternated with prepreg sheets. This stack is heat-pressed, and the prepreg epoxy melts and flows to bond the layers. In short, FR-4 lamination is the familiar layered stackup with high-temperature pressing and the same process used for any rigid PCB.

Aspect Ratio, Minimum Trace/Space & Hole Size Rules

Typical board shops design around an aspect ratio (board thickness : hole diameter) of about 8:1 to 10:1 for reliable plating. For example, one manufacturer allows up to 13:1 on a 2 mm board (i.e. 0.2 mm holes). In practice, many fabs quote 10:1 as a safe rule.

Hole sizes: Microvias (non-plated) can be 0.1–0.15 mm, but standard plated vias are usually ≥0.2–0.3 mm diameter. Drills smaller than 0.15 mm become very costly or impractical.

Line/space: With 1 oz copper, many fabs guarantee 0.1–0.15 mm (4–6 mil) minimum trace and spacing. As an example, one fab’s table shows outer-layer limits from 0.2–0.3 mm down to 0.125 mm with higher copper weights requiring wider space. Your fab will specify its actual capabilities, but FR-4 itself doesn’t magically allow finer lines than any other substrate.

Why FR4 Starts to Fail Above 8–12 Layers

Stacking more layers stresses FR-4’s limits. Each layer adds epoxy resin and copper, so total thickness and internal heat increase. Standard FR-4 (Tg around 130 °C) can actually soften if overcooked or warped in multiple laminations/reflows. Many fabhouses find that around 8–12 layers (especially thick boards) is the practical limit for standard FR-4.

Beyond that, panels are prone to warping, or delamination under thermal cycling. In fact, nearly every additional lamination step “pushes” the epoxy more, requiring stricter process control. That’s why high-layer-count boards often specify high-Tg FR-4 or more rigid laminates. In short, above 10 layers FR-4 itself isn't “failing” but it’s just that standard material needs an upgrade to keep up with the build.

When FR4 Is Perfect (and When You Should Run Away)

No material is perfect for every job. Let’s be practical about when FR-4 is a hero – and when it’s a zero.

Cost-Sensitive Consumer & IoT Projects

This is FR-4’s sweet spot. When you need an affordable general-purpose PCB. It’s ubiquitous and cheap, the industry makes zillions of FR-4 boards every day. So as economies of scale kick in, the prices will be low. If your design runs at low frequencies (kHz to low MHz) with moderate voltages, FR-4 will do the job with minimal fuss. In other words, if cost is king and performance demands are modest then FR-4 is a perfect fit.

High-Frequency & High-Power – Better Alternatives

For RF and microwave above a few GHz, FR-4’s dielectric losses and Dk variability wreak havoc on signals. Most RF/5G/Wi-Fi (>2 GHz) systems instead use Rogers, Duroid, PTFE, or ceramic substrates.

These materials have much lower loss and tighter Dk specs than FR-4. Similarly, if your board works in LED drivers, the FR-4 isn’t ideal. Its thermal conductivity is only 0.3 W/mK. Metal-core or thick-copper boards with aluminum or copper heat spreaders are common replacements for high-power applications.

Lead-Free Reflow & Automotive Temperature Requirements

Modern assembly and automotive standards press FR-4 hard. Lead-free soldering requires 260 °C peak reflow, far above standard FR-4’s Tg. A board heated beyond Tg risks “exploding” (delamination).

To survive this, PCBs often use high-Tg FR-4 (170–180 °C) when lead-free is specified. Automotive and industrial environments can also demand 150–175 °C operation. Designers either choose high-Tg FR-4 or switch to polyimide because it can handle 300 °C. If your board sees extreme soldering or high-temp use then you'll most probably use a high-Tg  FR-4 variant.

Material Quick Decision Matrix:

A quick comparison can help decide when to stick with FR-4 or switch materials. Consider cost, frequency range, thermal performance, and flexibility:

MaterialCostTypical Frequency UseThermal Conductivity
FR-4LowUp to a few GHz (fine for DC–1 GHz; marginal beyond 2 GHz)0.3 W/mK (low)
Rogers/High‑fHighRF/microwave (several GHz up to 40+ GHz)0.4–0.6 W/mK (moderate)
Aluminum (MCPCB)MedPower/DC (not used for RF)1–2 W/mK (very high)
CEM-3Very lowSimilar to FR-4 (a few GHz max)Slightly lower than FR-4
PolyimideHighUp to 1–2 GHz (used in flex)~0.12–0.17 W/mK (low)

FR-4 is cheapest and covers most DC/low‑frequency needs. Rogers or PTFE laminates cost more but excel at high-frequency. Aluminum-core is chosen for its superior heat spreading used in LEDs and motor controllers. CEM-3 is a budget FR-4 equivalent (UL V-0 rated glass/epoxy with finer weave), offering lower cost for simple boards. Polyimide (Kapton) is expensive but can be used if you require a truly bendable board with extreme thermal stability.

Conclusion: Your 30-Second FR4 Checklist Before Ordering

Before you click “order PCB,” give your design the FR-4 sniff test. Here’s a quick checklist:

  • Material Grade: Are you using the right FR-4 variant? Standard FR-4 is fine for general use, but choose high-Tg FR-4 for lead-free temperatures.
  • Board Stackup: Check your total thickness and copper. FR-4 is offered 0.2–3.2 mm. Pick the closest standard core and prepreg combo. Make sure copper weights (0.5/1/2 oz) match your thermal/power needs, and remember IPC ±10% tolerances.
  • Layer Count & Features: More layers mean more FR-4 stress. If you’re going above 10 layers, talk to the fab about high-Tg or reinforced laminates. Ensure hole sizes and trace/space are realistic.
  • Performance Requirements: Is your board compatible with high-speed? FR-4 works well up to the low-GHz range. But above 2 GHz you’ll want a Rogers‑type laminate. Does your design pump out a lot of heat or use thick copper? Consider a metal-core FR4 alternative.

If all your boxes check out and none of the “run away” warnings apply (extreme GHz, extreme power, extreme flex/temperature). Then FR-4 is your safe and budget-friendly choice. Otherwise, it might be time to explore Rogers, aluminum-core, polyimide, or other specialized laminates for that “just right” PCB base.


Keep Learning