The Impact of Inner Layer Residual Copper Rate on Board Thickness
3 min
When we were kids, we heard the children's story "The Crow Drinks Water," where a crow raises the water level by dropping stones into a fixed amount of water in a bottle. The same principle applies to multilayer PCB lamination, where during high temperature and high pressure, PP sheets flow in a liquid state to fill the gaps between the layers. This process is called "resin filling."
As seen in the diagram, when the copper coverage in the inner layer is minimal, PP sheets of the same thickness need to be evenly distributed into the gaps between the layers. This leads to a thinner overall thickness after the PP sheets cool and solidify, resulting in a thinner overall board thickness.
So, how much copper should be laid in the inner layer to ensure that the board thickness doesn’t fall below tolerance limits? This is where the "residual copper rate" comes in. The residual copper rate refers to the percentage of the inner layer's copper circuit patterns relative to the entire surface area of the board. Residual copper rate = the area of copper in the current layer / total area of the board.
In multilayer board lamination, PP sheets are cut into pieces and placed between the inner core board and another core board, or between the core board and copper foil. The resin on the PP melts under high temperature and pressure, filling the copper-free areas on the core board. After cooling, the resin solidifies, bonding the core board and copper foil together.
If the residual copper rate is too low (as shown below), the overall board thickness will be thinner, and the uneven copper distribution across layers can lead to board warping.
Here, a special reminder for golden finger boards: since golden finger boards need to be inserted into slots, they are more sensitive to thickness. If the board is too thin, it may result in a loose fit or poor contact when inserted into the slot.
Therefore, we strongly recommend:
1) For golden finger multilayer boards, cover the blank areas with copper, especially the inner layers at the golden finger region, to avoid issues such as boards being too thin to fit into the slot or inconsistent line widths.
2) When the residual copper rate is below 25%, to reduce the uneven electroplating that causes inconsistent line widths and excessive board thickness deviations, cover the blank areas with copper.
【Commonly Overlooked Issues in Golden Finger Design】
For the golden finger areas in both the inner and outer layers, ensure that there is an open window (i.e., no solder mask bridge between each golden finger pad) to prevent frequent insertion and removal from causing ink to fall into the golden finger slot, which can result in poor contact and other functional issues.
Summary:
For all types of boards, whenever possible, add copper to blank areas as long as it doesn't affect the design performance. Particularly when the residual copper rate is below 25%, ensure that copper is laid. In golden finger boards, copper must be laid in the inner layer at the golden finger area, and the outer layer should have a solder mask with a solid open window at the golden finger area.
Keep Learning
Choosing the Right CTI Value for Safer High-Voltage PCBs
Key Takeaways Higher CTI (≥600V, Group I) allows shorter creepage distances while preventing surface tracking in high-voltage designs. Standard FR4 (CTI ~175V) is often inadequate for mains voltage — upgrade to high-CTI materials for safety and compactness. Always match CTI material group to your working voltage and pollution degree for IEC/UL compliance. Clean assembly and good layout practices are essential to realize the full benefits of high-CTI laminates. Choose certified high-CTI materials and e......
Maximize Efficiency with PCB Panelization in High-Volume Manufacturing
Whenever a new PCB designer begins to spin the wheels, they are soon enough faced with the transition of creating a few prototypes into a volume production venture. As well as that, change brings a new idea that prototype-based engineers tend to forget: PCB panelization. In essence, panelization refers to loading a number of copies of your board design (or even a variety of designs) onto a single standardized production panel such that all of the fabrication and assembly processes treat them as a sing......
Inside the PCB Structure : How Layers, Stackup, and Buildup Define Modern Circuit Board Performance
Printed circuit boards may look like flat green rectangles, but beneath the surface, they are sophisticated multi-layer structures. As devices get more compact and complex, engineers turn to multilayer boards with carefully chosen materials and stackups to meet electrical and mechanical demands. This article peels back those layers to explore how substrate choice, layer stackup, and buildup methods shape PCB performance. Here we’ll cover PCB design fundamentals from the base materials up to high-densi......
The Benefits of Bed of Nails Testing in Professional PCB Manufacturing
Have you ever wondered how manufacturers can test thousands of PCBs daily and not make the production line crawl? The answer, as frequently as not, is a deceitful-appearing device called a bed of nails test set-up. The platform contains hundreds of little spring-loaded pins on it, and each of those pins is aligned very precisely to touch a specific test point on your circuit board. It can check the electrical integrity of a whole PCB, shorts, opens, and component defects in a few seconds, before the b......
Understanding PCB Dielectric Constant : Choosing Materials for Optimal Signal Performance
Key Takeaways The PCB dielectric constant (Dk) is a critical factor that directly determines signal propagation speed, characteristic impedance, and transmission loss in high-frequency designs. Selecting the right material — from standard FR4 for general use to low-Dk Rogers, PTFE, and LCP for multi-gigahertz applications — enables better performance, tighter impedance control, and reduced signal degradation. Success ultimately comes from matching Dk to your frequency needs, optimizing layer stackup, ......
PCB Adhesive : Types, Applications, and Best Alternatives for Circuit Board Assembly
A printed circuit board uses more than just solder to secure its components. PCB adhesives, or circuit board glue, bond layers and components together under extreme conditions. Good adhesives help hold parts in place during assembly, electrically insulate, moisture seal, and thermally spread from hot chips. In fact, adhesives are critical to performance by preventing micro components from loosening and shifting. In other words, the right adhesive keeps the puzzle of a device's electronic pieces reliab......