SMT Stencil Types, Coatings & Manufacturing
Explore stencil technologies and how they're made — framed vs frameless (foil) structures, nano-coating and electropolishing, and material choices — plus the manufacturing flow of laser cutting, electroforming, chemical etching, tensioning, and finishing, and how each affects print quality and life.
Latest Posts
SMT Stencil Types & Manufacturing
Why PCB Stencil Are Key to High-Quality SMT Assembly
PCB(Printed Circuit Board) stencil is a critical component of Surface Mount Technology (SMT) assembly. It plays a vital role in ensuring the accuracy and consistency of SMT assembly results, which directly affects the functionality and performance of the final product. PCB stencil also called SMT stencil, Circuit Board stencil is used to apply solder paste to the PCB, which is then used to attach SMT components to the board. Without the use of PCB stencil, it becomes challenging to achieve high-qualit......
Oct 30, 2026
SMT Stencil Types & Manufacturing
Nano-Coating vs Electropolishing for SMT Stencils
Key Takeaways Electropolishing improves the underlying metal surface by smoothing aperture walls. Nano-coating adds a low-friction, hydrophobic surface that helps paste release and reduces residue. Both treatments can improve fine-pitch paste release and support more consistent deposits and higher first-pass yield. Nano-coating is especially useful for BGA/QFN assemblies and high-volume runs, where cleaning frequency and paste-release consistency matter more. Electropolishing and nano-coating are comp......
Aug 24, 2026
SMT Stencil Types & Manufacturing
Stencil in PCB: A Comprehensive Guide to PCB Stencil Design, Fabrication, and JLCPCB Solutions
Figures 1 Solder paste application using a stainless steel stencil to achieve high-precision results. In PCB assembly based on Surface-Mount Technology (SMT), precision is a key factor that determines the final quality of electronic products. One critical element that strongly influences soldering accuracy is the stencil. The stencil functions as a physical template that controls the distribution of solder paste onto PCB pads before components are placed. Accurate solder paste application produces rel......
Aug 12, 2026
SMT Stencil Types & Manufacturing
Unlocking the Secrets of Nano-Coated Stencil Manufacturing
Nano-Coated Stencil Manufacturing Process The manufacturing of nano-coated stencils involves a series of precision engineering steps including design and drafting, laser cutting, polishing, nano-coating deposition, and quality inspection. Below is a detailed description of each process stage: 1. Design and Drafting (1) Data Acquisition: Accurate data is obtained from customer-supplied design files (e.g., Gerber files, PCB layouts) or physical product samples. This includes stencil dimensions, pad layo......
Aug 12, 2026
SMT Stencil Types & Manufacturing
The ROI of Nano-Coated Stencils in PCB Assembly Lines
Nano coatings offer several benefits. They are hydrophobic and repel water-based chemistry or flux, and some are also oleophobic and repel oil-based chemistry or flux. When applied to the bottom or board side of the stencil, these coatings will prevent solder paste squeeze-out during the print process between the stencil and PCB from sticking to the bottom of the stencil when the stencil separates from the board. As a result, the next print will be as good as the initial print, and bridging is reduced......
Aug 12, 2026
SMT Stencil Types & Manufacturing
What Are Laser Cut Stencils? A Guide for PCB Assembly
Traditional PCB assembly processes require the manual placement of electronic components before soldering. However, the increasing complexity of electronic printed circuit boards, combined with the need for miniaturisation, necessitates mechanical assembly and solder paste application using SMT stencils. Placing and soldering many small components on a small circuit board is no longer practical.Stencils replace the hand soldering of surface mount components and the inconsistencies caused by hand solde......
Aug 12, 2026
SMT Stencil Types & Manufacturing
Stencil Cutting Machine Guide: Choosing the Best Solution for PCB Stencil Manufacturing
In the PCB assembly process using Surface-Mount Technology (SMT), precision plays a critical role in determining the final quality of a market-ready product. One of the most crucial stages in SMT is the solder paste printing process, which is the first step in the SMT production line. In this process, the stencil functions as the medium that distributes solder paste onto each component pad. At this stage, the stencil cutting machine plays a vital role in determining the overall success of the assembly......
Aug 12, 2026
SMT Stencil Types & Manufacturing
The Essential Guide to SMT Stencils in PCB Assembly
Introduction In the dynamic world of electronics manufacturing, Surface Mount Technology (SMT) plays a crucial role in achieving efficiency and precision in printed circuit board (PCB) assembly. Central to the SMT process is the SMT stencil, an indispensable tool for the accurate application of solder paste. This ensures solid electrical connections between components and PCBs. This guide delves into the specifics of SMT stencils, examining their types, materials, manufacturing methods, advantages, ch......
Mar 23, 2026
SMT Stencil Types & Manufacturing
Nano-Coatings in PCB Manufacturing: How They Outperform Traditional Stencils
Nano coating is a thin hydrophobic (water repellent) and oleophobic (oil repellent) treatment used on the undersides and edges of solder paste stencils. With this the surface becomes non-stick which reduces the number of cleaning cycles required for the solder paste printing process. Upon application, the less than 5 nanometer coating bonds with the stencil foil at the microscopic level, which does not change the size and shape of the stencil. Nano coating is an industry proven process which shows imm......
Mar 23, 2026
SMT Stencil Types & Manufacturing
Laser Cut Stencil for PCB Assembly: Materials, Machines, and Key Advantages
Modern surface mount assembly relies on precise solder paste transfer across dense PCB pad arrays. Inconsistent paste volume produces opens, solder bridges, and unstable joints during reflow. PCB stencils control paste deposition through apertures that match copper land patterns, ensuring accurate and repeatable printing. Laser cut stencils achieve high dimensional accuracy with uniform aperture walls, which improve paste release for fine pitch components. These stencils handle prototype and productio......
Jan 23, 2026
SMT Stencil Types & Manufacturing
How does Electropolishing Work in PCB Stencil
To ensure optimum solder paste release, PCB stencil producers must offer superior finishes. One method for enhancing the functionality of stencils is electropolishing. How does electropolishing improve PCB stencils, and what is it? The continuous application of laser beams during the PCB stencil-making process causes the opening or aperture wall to become rough. This occurs as a result of the sheet material being melted by the laser beam, which causes certain surface irregularities. Electropolishing i......
Dec 29, 2025
SMT Stencil Types & Manufacturing
Types of Solder Stencils: Laser-Cut, Electroformed and Etched
I had covered a lot of stencils in the past, they are awesome tools for an electronics designer. At this point everyone knows they are a simple thin piece of steel which acts as a mask for soldering paste. Once applied we can put the components and heat them. And we have our PCB ready! Too simple. Although there are some steps which we have to look into such as soldering paste thermal profile and heating process of the PCB. If heated in the wrong way components can also be damaged. Today we are not go......
Dec 29, 2025
SMT Stencil Types & Manufacturing
When to Choose Electroformed Stencils
A high-quality PCB stencil is necessary for accurate solder paste application. Ordering PCB stencil is simple with JLCPCB, no matter whether you're working on small-scale production or prototypes. The method of electroforming involves depositing atoms one after the other to create metal, stencils, or pieces. This method turns a mandrel or master surface into an extremely exact duplicate. Another notable feature of electroforming is its repeatability. With 0.01-mil increments, electroform stencils can ......
Dec 29, 2025
SMT Stencil Types & Manufacturing
How Nano Coatings Affect Stencil Performance in SMT Printing
The undersides and edges of solder paste stencils are treated with a thin layer of nano coating, which is oleophobic (oil repellent) and hydrophobic (water resistant). This makes the surface non-stick, which lowers the number of cleaning cycles needed for the printing process using solder paste. The less than 5 nanometer coating does not alter the stencil's size or shape upon application; instead, it forms a tiny bond with the stencil foil.JLCPCB offers nano-coated stencils that leverage this technolo......
Dec 29, 2025
SMT Stencil Types & Manufacturing
SAM vs Ceramic: Choosing the Right Nano-Coating for Your PCB Stencil
As SMT designs evolve, tighter pitches and smaller components are introduced in electronics. Traditional stencil services can be used for bigger SMD pads but as the innovation goes on nano coated stencils comes to the market. Nano coatings are hydrophobic and oleophobic and repel water, oil and solder paste flux. Some benefits of using these coatings are improved transfer efficiency, reduced need (or frequency) of underside cleaning, and reduced bridging after print. There are two types of Nano-coatin......
May 13, 2025
SMT Stencil Types & Manufacturing
Reducing Solder Bridging and Cleaning Costs with Nano-Coated Stencils
The ongoing trend for miniaturization of electronic devices ensures that the surface mount assembly process will continue to provide new challenges. Components and stencil apertures are getting smaller and tighter in pitch. The demands on the solder paste printing process require improvements in technology. Nano-coatings for stencils have been available for many years. The coatings are supplied in two common forms. The most common form is a multiple step liquid coating which is applied by wiping onto ......
May 13, 2025
- 1
- 2