Metal Core PCB Materials: Thermal Truth & Design Rules
10 min
- What “Metal Core PCB Material” Actually Means
- Thermal Performance Numbers You Can Trust
- Available Metal Core PCB Material Grades (2025)
- Design Rules That Separate Pros from Burnt Boards
- Manufacturing Limits & Cost Drivers
- When to Choose MCPCB vs FR4 + Heatsink vs Ceramic
- Conclusion
Metal-core PCBs (MCPCBs) are speciality boards where a metal substrate replaces the standard FR-4. This metal core acts as a built-in heatsink, improving heat dissipation in high-power electronics. The basic stackup is simple:
- A copper conductor layer on top.
- A thin dielectric insulator in the middle.
- A thick metal base at the bottom.
This structure provides excellent thermal spreading and a convenient ground plane. But it comes at the cost of a much heavier and more expensive board than typical FR-4. MCPCBs are widely used in LED lighting and power supplies. The applications where there is a lot of heat generated by the components. In this article, we will bust some myths about different core metals, highlighting how the dielectric layer really controls heat flow. Finally, compare real thermal conductivity numbers.
What “Metal Core PCB Material” Actually Means
The metal forms the structural base of the board and doubles as a giant heatsink. The copper layer, often 1–3 oz, carries the circuit traces on the top. Underneath sits a thin dielectric, typically 25–100 µm, which electrically insulates the copper from the metal. Finally, the bottom is the metal core, a 1.0–3.2 mm aluminium plate that spreads heat laterally.
Because aluminium has a thermal conductivity of 150–235 W/mK, compared to copper, 380–400 W/mK. These two metal bases can whisk heat away much faster than FR-4 (0.3 W/mK).
Copper-core boards sound amazing, but copper is heavy and expensive. So nearly all MCPCBs use aluminium instead. Steel core PCBs exist for mechanical strength or EMI shielding, but their thermal performance is much worse. The metal core provides mechanical support and acts as a natural ground plane/shield. The tricky part is that the heat must travel through the thin dielectric insulation first. So we will see why that dielectric layer is the real thermal bottleneck next.
Aluminium vs Copper vs Steel Core – Structure & Myths
| Material | Thermal Conductivity (W/m·K) |
| FR-4 (Epoxy Glass) | 0.3 |
| Aluminum | 150 – 235 |
| Copper | 380 – 400 |
| Steel | 20 - 60 |
Aluminium core (Al): Aluminium is relatively cheap, lightweight, and has good thermal conductivity. Most generic MCPCBs use a 1.0–1.6 mm Al base. Aluminium’s thermal performance is not as high as copper's, but it is usually good enough. Designers love aluminium MCPCBs for general lighting and consumer power electronics.
Copper core (Cu): Extremely high thermal conductivity makes copper an attractive heat spreader. In theory, a copper-core board with no insulating layer means die-attached directly to copper. In practice, copper MCPCBs are rare, expensive and heavier. JLCPCB even has a special 'copper PCB' service where chips are mounted on copper plates.
Steel core: Steel is only used if you need a super-strong or magnetic board. Its thermal conductivity is far lower. In other words, a steel core board runs hotter than an aluminium one. Use a steel core only if you have special mechanical needs, and even then, expect worse heat spreading.
Dielectric Layer Role (The Real Thermal Bridge)
A thin dielectric/insulation layer, typically 50–150 µm, sits between the hot copper circuitry and the metal base. This layer electrically insulates the copper from the metal, but it also greatly limits heat flow. In fact, the dielectric is usually the biggest thermal bottleneck in an MCPCB. Many people forget this: the copper-on-metal looks shiny, but there’s always a gooey glue in between. It has a thermal conductivity, ranging from 5 to 10 W/mK only.
The result: a conventional MCPCB (with a standard dielectric) effectively only achieves a few W/mK overall. Only ultra-high-performance IMS boards with specialized ceramic-filled dielectrics can push that above 10 W/mK. If ultimate thermal conductivity is needed, designers sometimes skip the insulation altogether in a COB-MCPCB (Chip-On-Board metal-core PCB). There, the die is glued directly to the metal base, so the heat sees the full metal conductivity. This can yield an effective thermal conductivity greater than 200 W/mK.
Thermal Performance Numbers You Can Trust
When evaluating or comparing MCPCBs, rely on measured conductivity figures – not just the raw metal numbers. A few key thermal numbers:
| Category | Thermal Conductivity (W/m·K) |
| Dielectric (MCPCB insulation) | 1–10 (premium) |
| Aluminum base | 138–235 |
| Copper base | 380–400 |
| Overall MCPCB stack | 1–4 |
How thickness matters: A thicker metal base has more bulk to absorb heat and a slightly lower thermal resistance path to its edges. However, heat still primarily flows laterally in the plane of the plate. If your heat source is small, even a 1mm plate spreads the heat widely. Doubling to 2mm might only modestly lower the hotspot temperature. It does increase mass, so the board heats up more slowly.
Available Metal Core PCB Material Grades (2025)
In practical terms, MCPCB boards fall into tiers by insulating-layer conductivity:
- Standard (1–3 W/m·K): Basic MCPCBs use generic FR-4-based dielectric or simple fillers. These achieve a thermal conductivity of roughly 1–3 W/m·K.
- Mid-Range (3–6 W/m·K): Better boards use speciality polymers or silicone layers to bump the conductivity to a few W/m·K. These appear in automotive modules or industrial converters.
- Extreme (6–12+ W/m·K): The cutting-edge MCPCBs use high-performance insulated metal substrates (IMS) with ceramic fillers or even a ceramic base. Materials like aluminium nitride or aluminium oxide ceramic layers push the board’s thermal conductivity into the high single digits or low tens.
Design Rules That Separate Pros from Burnt Boards
Even with the right materials, a poor layout can spoil your MCPCB. Here are critical rules:
Via Types (Through, Blind, Thermal) & Current Limits
| Via Type | Use in MCPCB |
| Through-Hole Vias | Signals, mounting |
| Blind / Buried Vias | Rare/impractical |
| Thermal Vias | Heat transfer only |
| Via-in-Pad | Thermal optimization |
Current Capacity: As a rough guide, 1 oz of copper on a 0.254 mm trace carries 1 A. Doubling the copper weight or trace width roughly doubles the current. For MCPCBs handling 50–200 W, expect tens of amps; 16 A at 12 V is equivalent to 200 W. To carry 15–20 A continuously, you’ll need on the order of several-millimetre traces.
Minimum Dielectric Thickness vs Voltage Rating
The insulating layer must also meet electrical requirements. Industry rule-of-thumb is 2–3 kV per millimetre of dielectric. JLCPCB’s specifications list a 1.0 mm Al-MCPCB with a 3000 V breakdown. A thicker dielectric roughly increases the breakdown proportionally.
Always verify the manufacturer’s breakdown spec. If your design has high isolation needs, use thicker cores or additional insulating gaps. If the metal base is grounded, ensure soldermask or barriers prevent arcing between copper and base.
Copper Weight & Track Width for 50–200 W Applications
Handling dozens of watts means high currents. Here are typical design choices:
Copper Weight: Heavy copper reduces trace resistance dramatically. In a metal-core stack, the copper only lives on the topside. So, thicker foil directly improves conduction and lowers I²R losses. Heavy copper applications (2 oz, 3 oz, or higher) require special processing, which increases costs by 50–200%.
Trace Width: IPC data shows that a 6.35 mm trace at 2 oz can carry 20 A (at a 20°C rise). Suppose you need 20 A, budget 6–8 mm of width in 2 oz copper. Always consult an IPC trace-current chart.
Thermal Vias / Planes: If using double-sided MCPCBs, distribute heavy currents across both sides. On single-sided boards, you essentially have only one conductor layer, so you are also your own “heat sink.”
Manufacturing Limits & Cost Drivers
Why MCPCB Is 2–4× More Expensive Than FR4
Most PCB buyers notice that MCPCB quotes are shockingly higher. Indeed, industry guides list MCPCBs as roughly 2–4 times the price of ordinary FR-4 boards:
Material Cost: Aluminum sheet and high-k dielectrics cost several times more per square meter than FR-4 laminate. A 1 mm Al plate is much pricier than glass epoxy for the same area.
Process Complexity: Fabricating MCPCB involves extra laminations and sometimes special plating. You must bond copper-dielectric-aluminium under heat/pressure. Drilling through the metal core is also tougher than drilling FR-4.
Yield/Testing: One defect in a thermal bond or dielectric void often ruins an MCPCB's hot spots. Yields can be lower than FR-4. Many boards require 100% thermal/mechanical inspection.
Volume and Expertise: FR-4 proto boards are a high-volume commodity. MCPCBs are still niche, so the economies of scale aren’t there. Only a few board houses possess the necessary equipment and expertise.
When to Choose MCPCB vs FR4 + Heatsink vs Ceramic
Choosing the right approach for thermal management can be done in 60 seconds with this decision path:
| Solution | Example Cost (typical) | Approx. Heat Capacity | Cost per Watt |
| FR4 PCB + Heatsink | $15 | 50 W | $0.30/W |
| Aluminum MCPCB | $25 | 150 W | $0.17/W |
| High-end Ceramic PCB | $100 | 200 W | $0.50/W |
Estimate Power & Heat Flux: Is your design dissipating lots of watts per area? If total power is less than 20–50 W total and you have space, a standard FR-4 PCB with a heatsink or thermal vias might suffice. Below 20 W, FR-4 + fan/heatsink is usually cheapest. If you’re pushing 50–200 W on a small board, MCPCB deserves serious consideration.
Space and Integration: Do you need a compact solution? MCPCB integrates the heatsink into the board, saving space. FR-4 + heatsink takes extra volume and clips. If size is constrained, MCPCB often wins.
Mechanical/Environmental: Is weight a concern? Aluminium MCPCBs are lighter than bulky steel or some ceramic boards. Are you in a high-reliability or high-temp environment? MCPCBs outperform FR-4 in terms of vibration and heat resistance.
Budget: FR-4 is the cheapest per square inch. If cost is the top driver and your heat load is moderate, try FR-4 with an external heatsink. If the heatsink and assembly cost is high, the MCPCB’s higher board cost may be justified.
60‑Second Flowchart:
Conclusion
Metal-core PCBs are a powerful tool for thermal management in high-power electronics. Follow key rules, such as keeping the dielectrics thick enough for the required voltage and placing thermal vias correctly. Size the traces for amps to keep the board from burning itself out. Designers choose just enough metal thickness to fit the power budget and mechanical strength, because extra metal is heavy and expensive. For example, JLCPCB’s standard aluminium MCPCBs top out at 1.6 mm. Some vendors offer 3.2 mm when panelizing or stiffening an entire power assembly. Use at least 1 mm for modest power, 1.5–2 mm for high-power modules, and only go beyond if structural.
If your PCB design needs to shed more than a few dozen watts in a small area, consider a metal core. If you only need modest cooling, FR-4 + heatsink is cheaper. And if you truly need the maximum MCPCB thermal management, look to high-performance IMS or direct-bonded ceramic boards. By following the guidelines above and consulting real spec sheets, engineers can confidently choose the right board type.
Keep Learning
How to Select Tg of PCB ?
What is the Tg of PCB? In PCB manufacturing, "Tg" stands for Glass Transition Temperature. It is the temperature at which the PCB substrate material transitions from a rigid, glassy state to a soft, rubbery state. PCBs are flame-retardant (UL94 V-0) and do not burn easily; instead, they soften above Tg. The Critical Correlation Between Tg and Z-Axis CTE (Coefficient of Thermal Expansion) When the temperature exceeds the Tg point, the PCB substrate material (such as standard FR-4) undergoes a physical ......
Choosing the Right CTI Value for Safer High-Voltage PCBs
Key Takeaways Higher CTI (≥600V, Group I) allows shorter creepage distances while preventing surface tracking in high-voltage designs. Standard FR4 (CTI ~175V) is often inadequate for mains voltage — upgrade to high-CTI materials for safety and compactness. Always match CTI material group to your working voltage and pollution degree for IEC/UL compliance. Clean assembly and good layout practices are essential to realize the full benefits of high-CTI laminates. Choose certified high-CTI materials and e......
Maximize Efficiency with PCB Panelization in High-Volume Manufacturing
Whenever a new PCB designer begins to spin the wheels, they are soon enough faced with the transition of creating a few prototypes into a volume production venture. As well as that, change brings a new idea that prototype-based engineers tend to forget: PCB panelization. In essence, panelization refers to loading a number of copies of your board design (or even a variety of designs) onto a single standardized production panel such that all of the fabrication and assembly processes treat them as a sing......
Inside the PCB Structure : How Layers, Stackup, and Buildup Define Modern Circuit Board Performance
Printed circuit boards may look like flat green rectangles, but beneath the surface, they are sophisticated multi-layer structures. As devices get more compact and complex, engineers turn to multilayer boards with carefully chosen materials and stackups to meet electrical and mechanical demands. This article peels back those layers to explore how substrate choice, layer stackup, and buildup methods shape PCB performance. Here we’ll cover PCB design fundamentals from the base materials up to high-densi......
The Benefits of Bed of Nails Testing in Professional PCB Manufacturing
Have you ever wondered how manufacturers can test thousands of PCBs daily and not make the production line crawl? The answer, as frequently as not, is a deceitful-appearing device called a bed of nails test set-up. The platform contains hundreds of little spring-loaded pins on it, and each of those pins is aligned very precisely to touch a specific test point on your circuit board. It can check the electrical integrity of a whole PCB, shorts, opens, and component defects in a few seconds, before the b......
Understanding PCB Dielectric Constant : Choosing Materials for Optimal Signal Performance
Key Takeaways The PCB dielectric constant (Dk) is a critical factor that directly determines signal propagation speed, characteristic impedance, and transmission loss in high-frequency designs. Selecting the right material — from standard FR4 for general use to low-Dk Rogers, PTFE, and LCP for multi-gigahertz applications — enables better performance, tighter impedance control, and reduced signal degradation. Success ultimately comes from matching Dk to your frequency needs, optimizing layer stackup, ......