High-Speed PCB Layout Fundamentals
Understand impedance control, timing, skew, return paths, and routing rules essential for high-speed digital design.
Latest Posts
High-Speed Layout
HDMI PCB Pinout: A Complete Guide to Types A, C, and D
Key Takeaways The HDMI connector for Type A, C, and D connectors has got 19 pins, however each connector has its own pin configuration. Either side of the female connector has its pins arranged in reverse order according to which side is used for viewing. Thus, it is necessary to correctly select the footprints. TMDS pairs take place at pins 1-12, which creates important high-speed video and audio channels. A good schematic and reliable high-speed layout should start with an accurate pin table specifi......
Nov 06, 2026
High-Speed Layout
SFP Pinout Explained: PCB Layout & Design Guide
Key Takeaways The SFP pinout follows a standard 20-pin edge connector, with dedicated pins for power, ground, differential data pairs, and I2C control signals. The Tx and Rx differential pairs carry the high-speed optical or copper signal and need controlled 100 ohm differential impedance through the entire routing path. Low-speed control pins (TX_FAULT, TX_DISABLE, MOD_ABS, LOS, Rate Select/RS1) use standard single-ended routing and don't need impedance matching. Placing the SFP cage near the board e......
Nov 04, 2026
High-Speed Layout
Crosstalk in PCB Design: Causes, Types, and How to Reduce It
Key Takeaways Crosstalk starts at an edge: a changing aggressor voltage and current produce electric and magnetic fields that couple energy into a neighboring victim trace. Edge rate matters more than clock frequency alone. A modest-rate bus with fast I/O edges can still create a serious coupling problem. More spacing and a smaller signal-to-reference-plane distance usually provide the cleanest layout improvements, but the result depends on the complete cross-section. NEXT and FEXT do not scale in the......
Oct 28, 2026
High-Speed Layout
Signal Integrity Fundamentals in PCB Layout
In the world of PCB design, signal integrity plays a crucial role in ensuring the reliable and accurate transfer of electronic signals. Understanding the fundamentals of signal integrity is essential for electronics enthusiasts, hobbyists, engineers, students, and professionals involved in PCB design. This article will delve into the key concepts of signal integrity and explore how they influence PCB layout. By following best practices, you can optimize signal integrity and enhance the overall perform......
Oct 28, 2026
High-Speed Layout
HDMI PCB Layout Guidelines:Impedance & Length Matching
Key Takeaways Route the four TMDS pairs as 100 Ω differential pairs, and hold that value through vias, pads, and the connector. Match the P and N traces in each pair first, then match the pairs to each other within your silicon vendor's limits. Keep a solid reference plane under the whole route. Never cross a split. Put ESD protection as close to the connector as practical, so surge current is diverted early. Check the signaling type first. TMDS matching rules do not apply to HDMI 2.1 FRL. Introductio......
Oct 16, 2026
High-Speed Layout
RGMII Routing Guidelines for Reliable Gigabit PCB Design
Key Takeaways RGMII is a 12-signal, single-ended, source-synchronous parallel interface; its TX and RX paths are separate timing groups. Match TXD[3:0] and TX_CTL to TXC. Match RXD[3:0] and RX_CTL to RXC. Do not match TX against RX. Budget the aggregate clock-to-data skew separately in each direction, and avoid unintentionally stacking a full PCB delay with an enabled silicon delay. Treat 50 Ω ±10%, 20 mil matching and a 6 inch route limit as TI layout guidance, not universal clauses of the RGMII spec......
Oct 15, 2026
High-Speed Layout
Ethernet PCB Routing: Guidelines for MAC, PHY, and RJ45
Key Takeaways Route every MDI pair as a 100 Ω differential transmission line with ±10% control, unless the selected PHY or cable specification requires a different target. TI recommends keeping each MDI route below 2 in and matching P to N within 20 mil for 1 Gb/s or 50 mil for 10/100 Mb/s. Keep metal out from under discrete magnetics, separate chassis ground from board ground, and preserve a continuous reference beneath the routed pairs. TI’s Ethernet-specific guidance places suitable ESD protection ......
Oct 14, 2026
High-Speed Layout
DDR5 PCB Layout Guidelines: Design Rules and Best Practices
Key Takeaways DDR5 raises the stakes on layout: 1.1V rails and data rates up to 8800 MT/s leave far less margin for error than DDR4 did. Target around 40–45 Ω single-ended for DQ/CA and 80 Ω differential for CLK/DQS — exact values come from vendor guidelines — and hold them through every via and connector. Keep DQ and DQS length matching within about 5 mil per byte lane, and never route a DDR5 signal over a gap in its reference plane. Plan for 8 to 12 layers with dedicated ground references next to ev......
Sep 21, 2026
High-Speed Layout
Via Stitching in PCB Design: A Complete Guide
Key Takeaways Via stitching bonds same-net copper across layers with repeated plated vias, most often ground, to cut high-frequency impedance between regions. A grounded via next to a signal layer transition gives return current a short local path and helps confine the field around the via. Via fences along board edges and RF cavities suppress edge radiation, but their isolation is geometry- and frequency-dependent, with no universal dB value. Keep stitching pitch at or below one-twentieth of the in-b......
Sep 14, 2026
High-Speed Layout
Mastering IC Board Design: Layout Rules & Best Practices
Key Takeaways Placement is the foundation of good layout. Position ICs, decoupling capacitors, and crystals to minimize trace lengths before routing anything — placement quality determines most of your signal performance. Respect the physics, not just the schematic. High-speed designs demand controlled impedance (e.g., 90-ohm USB differential pairs), length matching, and a well-planned layer stackup to prevent reflections, crosstalk, and power noise. Handle power and heat deliberately. Size power trac......
Sep 02, 2026
High-Speed Layout
LVDS PCB Layout Guidelines: Design Tips and Worked Example
Key Takeaways 100 Ω Differential Impedance: LVDS PCB layout starts with one number: 100 Ω of differential impedance. Trace width, spacing, and board thickness all set that number. Route Pairs Together: Route the two traces of a pair together, side by side, and keep their lengths within 5 to 10 mil of each other. Solid Ground Plane: Never let an LVDS pair cross a gap in the ground plane. It breaks the return path and hurts the signal. 4-Layer Minimum: A 4-layer board with a solid ground plane is enough......
Aug 26, 2026
High-Speed Layout
High Speed PCB Layout Guide for Reliable Signal Control
Key Takeaways 1. High-speed ≠ high frequency alone — it's defined by signal edge rates and trace electrical length. Treat traces as transmission lines with controlled impedance, not simple wires. 2. Placement is an electrical decision — clustering drivers/receivers, matching differential pairs symmetrically, and keeping decoupling capacitors tight to power pins directly govern signal integrity. 3. Continuous ground planes are non-negotiable — never route high-speed traces across split planes; use stit......
Aug 24, 2026
High-Speed Layout
High-Speed PCB Routing: Guidelines, Techniques & Examples
Key Takeaways 1. Define "High-Speed" by Rise Time, Not Clock Frequency. Per IPC-2251, traces longer than 2 x rise_time require controlled impedance routing. Even sub-100 MHz signals with fast edges demand transmission-line treatment. 2. Plan the Stackup Before Routing. Every high-speed signal needs an uninterrupted reference plane. Use the fabricator's actual impedance data—JLCPCB guarantees ±10% tolerance on controlled impedance. 3. Route Critical Nets in Priority Order. Route clocks, differential pa......
Jul 25, 2026
High-Speed Layout
RF PCB Layout: Common Design Mistakes and Practical Guidelines
Key Takeaways Impedance control is non-negotiable: Maintain consistent 50Ω impedance across all transitions, including vias, connector launches, and trace bends, to prevent reflections and signal loss. Return path integrity determines RF success: Never route RF traces over ground plane splits or slots. Provide continuous return paths with stitch vias at every layer change. Functional zoning prevents interference: Physically separate RF front-end circuitry from digital logic and power management to kee......
May 15, 2026
High-Speed Layout
Microstrip v/s Stripline: Layout Difference and When to Use Them
RF (Radio Frequency) PCB design is where engineering meets art. Among the tools in an RF designer's toolkit, microstrip and stripline transmission lines are the unsung heroes. They ensure signals travel seamlessly across PCBs without succumbing to interference, loss, or impedance mismatches. But what are these lines, and how do you choose between them? Let's dive in, and to know more about PCB, see our detailed blog on PCB manufacturing. What Are Microstrip and Stripline Transmission Lines? Microstrip......
Dec 26, 2025
- 1
- 2