Understanding PCB Copper Thickness: Standards and Conversions
6 min
- What Is PCB Copper Thickness?
- How to Measure PCB Copper Thickness
- Standard Copper Thickness Values in PCBs
- How the Number of Layers Affects Copper Thickness
- Why Copper Thickness Matters (Practical Implications)
- What is Copper Balancing
- What are Copper Pours
- Conclusion
When talking about copper thickness, there are some limited options available with manufacturing houses. When designers have to increase the current carrying capacity of a trace without making it wider, then copper weight or thickness is increased in the lateral dimension. There are only a few options, and most of the manufacturers have a standard thickness. Copper selection is all about power delivery, signal propagation, and thermal management. Copper width and length are always a concerning factor for designers because if the traces are too thin, and your traces burn under high current. Too thick, and your etching process turns into an expensive nightmare. Somewhere in between lies the sweet spot. In the article, we will see some standards, measurement methods, and unit conversion related to copper thickness.
What Is PCB Copper Thickness?
In simple terms, PCB copper thickness is the height of the copper layer deposited on the laminate of a PCB. It can be expressed in three different units:
- Micrometers (µm)
- Mils (1 mil = 0.001 inches)
- Ounces per square foot (oz/ft²)
Ounces are adopted as the industry standard because PCB manufacturers historically measured copper by weight spread over one square foot.
1 oz/ft2 ≈ 35 μm ≈ 1.37 mils.
This means a 1-oz copper PCB layer has a thickness of about 35 µm.
How to Measure PCB Copper Thickness
There are two main contexts for measuring copper thickness:
1. Before fabrication, we specify the thickness to the manufacturer (e.g, 1 oz). Manufacturers supply laminates pre-coated with base copper.
2. After fabrication, the actual thickness of the PCB is determined; the thickness increases because copper is plated during via formation. Measurement is done using a cross-sectional analysis (cutting a PCB slice and measuring under a microscope). We can also use surface profilometry for more accurate and precise results. The finished copper thickness is always slightly higher than the base copper due to plating.
Standard Copper Thickness Values in PCBs
PCB copper thicknesses are usually standardized to simplify manufacturing. Some of the common values here are:
- 0.5 oz (17 µm) – Often used for fine-pitch inner layers in multilayer PCBs.
- 1 oz (35 µm) – The industry standard for most PCBs.
- 2 oz (70 µm) – Power electronics, automotive, industrial boards.
- 3 oz (105 µm) and above – Heavy copper PCBs for high-current designs.
The table below follows the IPC-6012 defines acceptance criteria and tolerances for finished copper thickness.
How the Number of Layers Affects Copper Thickness
The copper thickness difference between the outer and inner layers can be seen when moving from a 2-layer PCB to a multilayered one. Typically, 1 oz copper is used for top and bottom layers, and somehow, if it is a compact power board, we can use 2 oz. Inner Layers use 0.5 oz copper to save space and ensure manufacturability.
The more layers, the more copper will be used in the board, and thicker copper requires a thicker and higher K dielectric for the insulation. The higher the gap between layers, will cause the impedance mismatch and the overall cost of the system. But overall, we get better heat dissipation and thermal conductivity.
Why Copper Thickness Matters (Practical Implications)
1. Current Carrying Capacity: The Thicker the copper higher the current that can be supported without overheating the system. The thickness can be chosen on the basis of IPC-2152.
2. Thermal Management: Extra copper helps to spread the heat from the power components and make the PCB more rigid for automotive applications.
3. Signal Integrity & Impedance: Copper trace length, width, spacing, and thickness decide the impedance of a circuit and trace, and for better signal integrity, we have to consider the weight of copper when designing.
4. Mechanical Strength: The more copper better the strength of the PCB and the stronger the whole PCB.
5. Cost and Manufacturability: Thicker copper costs more because of more etching and plating time. Fine pitch routing of traces became harder as the copper became thicker.
What is Copper Balancing
If copper distribution is uneven across the board, it can create problems during fabrication. More during the plating and etching processes. Areas with dense copper can behave differently from sparse ones and may lead to warping or twisting. This is where copper balancing comes in. The process involves adjusting the copper distribution across the PCB so that both sides and different regions have more uniform copper coverage. Designers often add “dummy copper” or patterned fills in low-density areas that are not electrically connected. The practice is done to simply even out the copper thickness. The goal is not to change circuit behavior but to ensure that the board goes through manufacturing steps.
What are Copper Pours
A copper pour is essentially a large, continuous area of copper that fills unused spaces on a PCB layer. Instead of leaving the non-routed areas as bare substrate, designers “pour” copper over these regions. The connection is made to a specific net and is often grounded. This poured copper serves multiple purposes. Electrically, it lowers the overall impedance of return paths and improves signal integrity by creating a broad reference plane. It also helps with thermal management. A larger copper area can spread heat away from components and dissipate it more effectively. From a manufacturing perspective, using copper pours minimizes the amount of copper that must be etched away during fabrication.
Conclusion
From the article, it is clear that the copper thickness may seem like a minor specification when ordering a PCB. But in reality, it decides current handling capabilities of your board, how well it dissipates heat, and how reliable it will be in the field. For students, it’s essential to understand the unit conversions and IPC standards. So, the next time you’re configuring a PCB order, don’t just click “1 oz” by default. Ask yourself: Does my design need more copper to handle current or heat? Will thicker copper affect impedance or manufacturability? You can always calculate the thickness according to the current and length/width of the trace from the signal integrity point of view.
If you want to explore how copper thickness affects your PCB design in practice, you can easily experiment through JLCPCB’s online ordering system. Their real-time quotation tool lets you adjust copper weight and instantly see the cost difference — a great way for students and engineers to learn through experience.
Keep Learning
FR4 PCB Deep Guide: Material Truth, Real Specs & When to Use (or Avoid) It
FR-4 isn't a secret code, it literally means Flame Retardant (grade 4). In PCB terms, FR-4 is a NEMA (National Electrical Manufacturers Association) grade designation for a glass-reinforced epoxy laminate. We can say it is a composite of woven fiberglass cloth bonded with an epoxy resin that contains flame-retardant additives. The “FR” stands for flame retardant, but note this doesn’t automatically mean UL94 V-0 certified. It just indicates the resin is formulated to self-extinguish if it catches fire......
What is the Standard Thickness of a PCB?
Key Takeaways 1.6 mm Standard: 1.6 mm (0.062") is the universal industry standard, balancing rigidity, assembly ease, and component fit. 0.4mm–3.0mm Options: JLCPCB provides versatile FR-4 thicknesses from 0.4 mm for ultra-thin devices to 3.0 mm for high-power systems. Stackup Flexibility: Multilayer PCBs up to 12–16 layers can still maintain a 1.6 mm profile using thinner cores and prepregs. Impedance & Heat Balance: Dielectric thickness directly sets trace impedance (Z0), while thicker boards increa......
How Laser Drilling Delivers Precision and Density in Advanced PCB Manufacturing
Key Takeaways Laser Drilling has become the cornerstone technology for precision and high-density PCB manufacturing, enabling microvias as small as 25-75μm — far beyond the 150μm limit of mechanical drilling. By delivering superior accuracy, contactless processing, excellent signal integrity, and reliable blind/stacked vias, it empowers advanced HDI board designs essential for modern electronics. From optimal stackup selection to professional plating and DFM practices, mastering laser drilling is key ......
Why Sequential Lamination Delivers Superior HDI PCBs
Did you ever ask yourself how smartphone manufacturers can crust a thousand connections into a credit card-sized board? The process is referred to as sequential lamination, which is a multi-cycle process that is used to fabricate PCBs on a layer-by-layer basis, releasing microvia structures and routing densities that cannot be accessed by a single-press process. Without it, the slick, high-performance electronics that we all use on a daily basis would not appear the way that they do now. With data rat......
Buried Vias in Advanced PCBs: Enabling Higher Density, Better Signal Integrity, and Compact Designs
Key Takeaways Hidden Routing: Buried vias connect only inner layers, keeping outer surfaces clear for dense components and traces. Better Signal Integrity: They eliminate via stubs, reducing parasitics and signal loss in high-speed designs. Higher Density: Essential for HDI boards, dense BGAs, and small form factors like wearables. Higher Cost: Sequential lamination and extra drilling steps make them ~3×-4× more expensive than standard through-holes. Ever wondered how a modern smartphone mainboard can......
Unlocking Higher Density and Better Performance with Blind Vias in HDI PCBs
Key Takeaway Higher Density: Connects surface to inner layers without penetrating the whole board, freeing routing channels under fine-pitch BGAs. Improved Signal Integrity: Reduces via stub length to minimize impedance discontinuities in high-speed designs. Aspect Ratio Rule: Keep the depth-to-diameter ratio near 0.75:1 (max 1:1) for reliable laser drilling and void-free plating. Thermal Efficiency: Supports via-in-pad setups for better heat dissipation and compact component placement. Ever wonder ho......