Understanding the Materials Used in PCBs: Selection, Types, and Importance
13 min
- Types of materials used in PCBs
- Types of Substrates Used in PCBs
- Types of Copper Foils Used in PCBs
- Types of soldermask Used in PCBs
- Types of adhesives Used in PCBs
- FAQ about Materials Used in PCBs
- Conclusion
Key Takeaways
- FR-4 is the go-to material for most cost-effective and reliable PCBs.
- Use Rogers for high-frequency and RF applications to reduce signal loss.
- Higher copper weight (2oz) improves current and heat handling.
- Choose High-Tg substrates for better thermal stability in multilayer boards.
- Green LPI soldermask offers the best balance of performance and inspection.
Printed circuit boards (PCBs) are an essential component of modern electronics. These boards connect and support electronic components, providing a stable platform for the transfer of electrical signals and power. A typical PCB consists of multiple layers of materials that are laminated together to form a single unit.
PCBs are an integral part of the electronics manufacturing process. They are used in everything from consumer electronics to automotive and aerospace applications, and are critical to the functioning of electronic devices.
Types of materials used in PCBs
1. Substrates
Substrates are the base material for PCBs, and serve as the foundation on which other materials are deposited. Substrates are typically made of fiberglass-reinforced epoxy resin, also known as FR-4. Other types of substrates include CEM-1, CEM-3, Polyimide (PI), and Rogers. The choice of substrate depends on specific requirements such as operating temperature, dielectric strength, and cost.
Some common criteria for choosing substrates include:
- Dielectric constant: The dielectric constant is a measure of the substrate's ability to store electrical energy. A high dielectric constant can result in signal loss and interference, especially in high-speed digital or RF circuits.
- Tg (Glass Transition Temperature): Tg is the temperature at which the substrate changes from a rigid to a flexible state. A high Tg is required for high-temperature applications, such as automotive and aerospace electronics, because it helps the board maintain mechanical stability during soldering and operation.
- CTE (Coefficient of Thermal Expansion): CTE is a measure of the substrate's tendency to expand or contract with changes in temperature. A low CTE is required for applications where the PCB must maintain its shape and dimensions over a wide temperature range, reducing the risk of solder joint failure and via cracking.
- Moisture absorption: Substrates that absorb moisture can lead to delamination and other problems during assembly and operation. Low moisture absorption is desirable for most applications, particularly in humid or outdoor environments.
In practice, selecting the right substrate often involves trade-offs. For example, a material with excellent high-frequency performance may have higher cost or lower mechanical strength. Understanding these properties helps designers achieve better reliability and signal integrity in the final product.
2. Copper Foils
Copper foils are used to create the conductive traces on the surface of the PCB. Copper foils are available in two types: rolled copper foil and electrodeposited copper foil. The choice of copper foil depends on factors such as the thickness, purity, and surface roughness required for the PCB.
- Thickness: The thickness of the copper foil determines the current-carrying capacity of the traces. Thicker foils are required for high-current applications.
- Purity: Higher purity copper foils are more conductive and have better adhesion to the substrate.
- Surface roughness: The surface roughness of the copper foil affects the adhesion of the soldermask and the quality of the solder joints.
3. Soldermask
Soldermask is a protective coating applied to the surface of the PCB to prevent solder bridges and other defects during the soldering process. Types of soldermask include liquid photoimageable soldermask (LPI), dry film soldermask (DFSM), or thermal cure soldermask (TCS). The choice of soldermask depends on factors such as the chemical resistance, adhesion, and insulation resistance required for the PCB.
- Chemical resistance: The soldermask must be resistant to the chemicals used in the PCB assembly process.
- Adhesion: The soldermask must adhere well to the substrate and the copper foils to prevent delamination and other problems.
- Insulation resistance: The soldermask must provide adequate insulation around the traces to prevent short circuits.
4. Silkscreen
Silkscreen is used to print text and graphics onto the surface of the PCB. Silkscreen is typically divided into two types:
Component silkscreen: This type of silkscreen is used to print reference designators, component outlines, and other information that helps identify the components on the PCB. Component silkscreen is usually printed in white or black ink and is located on the component side of the PCB.
Legend silkscreen: This type of silkscreen is used to print text and graphics that provide additional information about the PCB, such as the name of the board, the company logo, and any other relevant information. Legend silkscreen is usually printed in white or black ink and is located on the solder side of the PCB.
- Legibility: The silkscreen must be legible under various lighting conditions and from different angles.
- Durability: The silkscreen must be resistant to wear and tear during the assembly and operation of the PCB.
5. Adhesives
Adhesives are used to bond the different layers of the PCB together. The most common types of adhesives used in PCBs are epoxy resin and acrylic adhesive. The choice of adhesive depends on factors such as thermal stability and chemical resistance.
- Thermal stability: The adhesive must maintain its bond strength over a wide temperature range.
- Chemical resistance: The adhesive must be resistant to the chemicals used in the PCB assembly process.
- Moisture resistance: The adhesive must be resistant to moisture to prevent delamination and other problems.
Choosing the materials for a PCB often involves a trade-off between different properties. For example, a substrate with a high Tg may have a lower CTE, but it may also be more expensive. Similarly, a copper foil with a high purity may be more conductive, but it may also be more expensive. The choice of materials depends on the specific requirements of the PCB, and a balance between different properties is often required.
Types of Substrates Used in PCBs
FR-4 Substrates
FR-4 substrates are the most common type of substrate used in PCBs. They are made of woven fiberglass cloth impregnated with epoxy resin. FR-4 substrates have excellent electrical properties, including a low dielectric constant and good insulation resistance. They also have a high Tg, which makes them suitable for high-temperature applications. FR-4 substrates are relatively low cost and are widely available in the market.
Due to its well-balanced performance, FR-4 has become the workhorse material for the electronics industry. It offers good mechanical strength, flame retardancy, and processability, making it ideal for everything from simple single-layer boards to complex multilayer designs. In real-world applications, FR-4 performs reliably in consumer electronics, industrial controls, and automotive systems where operating temperatures are moderate.
Polyimide (PI) Substrates
Polyimide (PI) substrates are used in applications where high-temperature resistance is required. They have a higher Tg than FR-4 substrates, making them suitable for use in aerospace and industrial electronics applications. PI substrates are also flexible, making them suitable for use in flexible PCBs. However, PI substrates are more expensive than FR-4 substrates and have a higher moisture absorption rate.
The flexibility and thermal endurance of Polyimide make it particularly valuable in applications involving repeated bending or extreme temperature swings. Although the higher cost and moisture sensitivity require careful design considerations (such as proper sealing or coatings), PI enables the creation of thin, lightweight, and highly reliable flexible circuits that rigid materials cannot achieve.
Rogers Substrates
Rogers substrates are a type of high-frequency substrate used in applications where signal loss is a concern. They have a low dielectric constant and low loss tangent, which makes them suitable for high-frequency applications. Rogers substrates are more expensive than FR-4 substrates and have a lower Tg.
In high-frequency designs, even small differences in dielectric properties can cause significant signal degradation, impedance mismatch, and increased insertion loss. Rogers materials address these challenges effectively, providing stable electrical performance across a wide frequency range and temperature variations. This makes them essential for advanced applications such as 5G base stations, radar systems, and high-speed data transmission equipment, where standard FR-4 would no longer suffice.
Types of Copper Foils Used in PCBs
Rolled Copper Foil
Rolled copper foil is produced by processing a sheet of copper through a series of rollers. Rolled copper foil is thinner than electrodeposited copper foil and has a smoother surface. Rolled copper foil is used in applications where a thin, high-quality copper surface is required, such as fine-pitch circuits and high-frequency circuits.
Electrodeposited Copper Foil
Electrodeposited copper foil is created by depositing a layer of copper onto a thin substrate using an electroplating process. Electrodeposited copper foil is thicker than rolled copper foil and has a rougher surface. Electrodeposited copper foil is used in applications where high current-carrying capacity is required, such as power supplies and high-current circuits.
The thickness of copper foil (commonly expressed in ounces, such as 1oz or 2oz) directly determines the current-carrying capacity and heat dissipation ability of the traces. Designers must balance copper weight with trace width, manufacturing capability, and cost to achieve optimal electrical and thermal performance.
Types of soldermask Used in PCBs
Here are the three most common types of soldermask used in PCBs:
Liquid Photoimageable Soldermask (LPI)
LPI soldermask is a liquid material that is applied to the surface of the PCB and then exposed to ultraviolet (UV) light through a photomask. The areas that are not exposed to UV light are then washed away, leaving the desired soldermask pattern on the PCB. LPI soldermask is popular due to its ease of application, high resolution, and excellent adhesion to the substrate. It is also available in a range of colors, making it suitable for color-coding PCBs. However, LPI soldermask can be more expensive than other types of soldermask, and it can affect the signal integrity in high-frequency applications.
Dry Film Soldermask (DFSM)
DFSM soldermask is a dry film material that is laminated onto the surface of the PCB. The film is then exposed to UV light through a photomask, and the unexposed areas are removed, leaving the desired soldermask pattern on the PCB. DFSM soldermask is popular due to its low cost, ease of application, and excellent adhesion to the substrate. However, DFSM soldermask can be less precise than LPI soldermask, and it may have a slightly rougher surface finish.
Thermal Cure Soldermask (TCS)
TCS soldermask is a liquid material that is applied to the surface of the PCB and then cured by exposure to heat. TCS soldermask is typically used in high-temperature applications, as it can withstand temperatures of up to 300°C. TCS soldermask is popular due to its high chemical resistance and excellent adhesion to the substrate. However, TCS soldermask can be more difficult to apply than other types of soldermask, and it may require additional processing steps.
Types of adhesives Used in PCBs
Here are the three most common types of adhesives used in PCBs:
Epoxy Resin Adhesive
Epoxy resin adhesive is a common type of adhesive used in PCB manufacturing. It provides excellent adhesion and thermal stability, making it suitable for high-temperature applications. Epoxy resin adhesive is also resistant to chemicals and moisture, making it ideal for harsh environments. Epoxy resin adhesive is typically applied by spreading a thin layer of the adhesive onto the surface of the PCB, and then curing it by exposure to heat.
Acrylic Adhesive
Acrylic adhesive is another common type of adhesive used in PCB manufacturing. It provides good adhesion and chemical resistance, making it suitable for use in harsh environments. Acrylic adhesive is also resistant to UV light and moisture, making it ideal for outdoor applications. Acrylic adhesive is typically applied as a thin film onto the surface of the PCB, and then cured by exposure to heat.
Polyurethane Adhesive
Polyurethane adhesive is a type of adhesive used in PCB manufacturing for its excellent bonding strength and flexibility. It is commonly used in flexible PCBs and other applications where flexibility is required. Polyurethane adhesive is also resistant to chemicals and moisture, making it ideal for harsh environments. Polyurethane adhesive is typically applied as a thin film onto the surface of the PCB, and then cured by exposure to heat.
Beyond these adhesives, in multilayer PCB construction, Prepreg sheets (B-stage epoxy resin impregnated glass cloth) are extensively used as the primary bonding material. Prepreg not only bonds the layers together but also provides consistent dielectric spacing between copper layers, which is critical for impedance control and overall board reliability. Proper selection and processing of bonding materials are essential to prevent delamination and ensure long-term performance under thermal and mechanical stress.
FAQ about Materials Used in PCBs
Q: What is the most commonly used PCB substrate and why?
FR-4 is by far the most commonly used substrate. It offers an excellent balance of electrical performance, mechanical strength, cost, and manufacturability, making it suitable for the vast majority of consumer electronics, industrial, and general-purpose applications.
Q: When should I choose Rogers material instead of FR-4?
You should choose Rogers substrates when designing high-frequency, RF, or microwave circuits (typically above 1 GHz). Rogers materials provide lower dielectric constant and much lower signal loss compared to FR-4, which is critical for maintaining signal integrity in 5G, antennas, and high-speed applications.
Q: What is the difference between standard FR-4 and High-Tg FR-4?
Standard FR-4 usually has a Tg of around 130–140°C, while High-Tg FR-4 offers a Tg of approximately 150–170°C or higher. High-Tg material provides better thermal stability, reduced risk of delamination, and improved reliability during lead-free soldering and in high-temperature operating environments.
Q: How does copper thickness (weight) affect PCB performance?
Thicker copper (e.g., 2oz instead of 1oz) increases current-carrying capacity and improves heat dissipation, which is beneficial for power electronics. However, it may limit the minimum trace width/spacing and increase manufacturing cost. 1oz is the standard choice for most general designs.
Q: Which soldermask color is recommended and why?
Green soldermask is the most recommended and widely used. It provides the best contrast for automated optical inspection (AOI), excellent readability of silkscreen, and is usually the most optimized and cost-effective option. Other colors (Blue, Black, White, etc.) are available when aesthetics or visual requirements are important.
Conclusion
As technology continues to advance, the demand for smaller, faster, and more powerful electronic devices will continue to drive the development of new materials and technologies for PCBs. The importance of material selection in PCB design and manufacturing will only increase, and designers and manufacturers will need to stay up-to-date with the latest developments in materials science and technology.
In summary, the selection of materials for PCBs is a critical step in the design and manufacturing process, and it is essential to choose materials that meet the specific requirements of the PCB while balancing trade-offs between different properties. The use of high-quality materials, along with careful design and manufacturing processes, will result in PCBs that are reliable, perform well, and have a long lifespan.
Keep Learning
FR4 PCB Deep Guide: Material Truth, Real Specs & When to Use (or Avoid) It
FR-4 isn't a secret code, it literally means Flame Retardant (grade 4). In PCB terms, FR-4 is a NEMA (National Electrical Manufacturers Association) grade designation for a glass-reinforced epoxy laminate. We can say it is a composite of woven fiberglass cloth bonded with an epoxy resin that contains flame-retardant additives. The “FR” stands for flame retardant, but note this doesn’t automatically mean UL94 V-0 certified. It just indicates the resin is formulated to self-extinguish if it catches fire......
What is the Standard Thickness of a PCB?
Key Takeaways 1.6 mm Standard: 1.6 mm (0.062") is the universal industry standard, balancing rigidity, assembly ease, and component fit. 0.4mm–3.0mm Options: JLCPCB provides versatile FR-4 thicknesses from 0.4 mm for ultra-thin devices to 3.0 mm for high-power systems. Stackup Flexibility: Multilayer PCBs up to 12–16 layers can still maintain a 1.6 mm profile using thinner cores and prepregs. Impedance & Heat Balance: Dielectric thickness directly sets trace impedance (Z0), while thicker boards increa......
How Laser Drilling Delivers Precision and Density in Advanced PCB Manufacturing
Key Takeaways Laser Drilling has become the cornerstone technology for precision and high-density PCB manufacturing, enabling microvias as small as 25-75μm — far beyond the 150μm limit of mechanical drilling. By delivering superior accuracy, contactless processing, excellent signal integrity, and reliable blind/stacked vias, it empowers advanced HDI board designs essential for modern electronics. From optimal stackup selection to professional plating and DFM practices, mastering laser drilling is key ......
Why Sequential Lamination Delivers Superior HDI PCBs
Did you ever ask yourself how smartphone manufacturers can crust a thousand connections into a credit card-sized board? The process is referred to as sequential lamination, which is a multi-cycle process that is used to fabricate PCBs on a layer-by-layer basis, releasing microvia structures and routing densities that cannot be accessed by a single-press process. Without it, the slick, high-performance electronics that we all use on a daily basis would not appear the way that they do now. With data rat......
Buried Vias in Advanced PCBs: Enabling Higher Density, Better Signal Integrity, and Compact Designs
Key Takeaways Hidden Routing: Buried vias connect only inner layers, keeping outer surfaces clear for dense components and traces. Better Signal Integrity: They eliminate via stubs, reducing parasitics and signal loss in high-speed designs. Higher Density: Essential for HDI boards, dense BGAs, and small form factors like wearables. Higher Cost: Sequential lamination and extra drilling steps make them ~3×-4× more expensive than standard through-holes. Ever wondered how a modern smartphone mainboard can......
Unlocking Higher Density and Better Performance with Blind Vias in HDI PCBs
Key Takeaway Higher Density: Connects surface to inner layers without penetrating the whole board, freeing routing channels under fine-pitch BGAs. Improved Signal Integrity: Reduces via stub length to minimize impedance discontinuities in high-speed designs. Aspect Ratio Rule: Keep the depth-to-diameter ratio near 0.75:1 (max 1:1) for reliable laser drilling and void-free plating. Thermal Efficiency: Supports via-in-pad setups for better heat dissipation and compact component placement. Ever wonder ho......