SMD Resistor Codes: How to Read 3-Digit, 4-Digit, and EIA-96 Markings
11 min
- Why SMD Resistor Codes Matter
- How to Read 3-Digit and 4-Digit SMD Resistor Codes (E-Series) System
- Understanding Resistor Tolerance Letter Codes (J, F, G)
- EIA-96: The 1% SMD Resistor Code System
- Unmarked SMD Resistors: When SMD Resistor Codes Are Not Available
- Common Challenges in Reading SMD Resistor Codes
- Conclusion: How to Correctly Identify Any SMD Resistor Code
- FAQs about SMD Resistor Codes
SMD resistor codes are compact markings used to identify the resistance value of surface-mount resistors. Instead of traditional color bands, SMD resistors typically use a combination of numbers and letters printed directly on the component.
Knowing how to read these markings is useful for engineers, technicians, and electronics hobbyists when identifying components, troubleshooting circuits, or replacing resistors during rework.
This guide explains the three most common SMD resistor code systems: 3-digit, 4-digit, and the EIA-96 standard for 1% tolerance components.
Why SMD Resistor Codes Matter
In a densely populated PCB, the surface mount resistor codes provide a quick way to identify a physical component and verify it against the schematic and BOM. They are useful in several engineering activities:
- Assembly Verification: When markings are present, they can help operators and inspection systems verify that the correct resistor has been placed during assembly.
- Debugging & Rework: During troubleshooting and rework, resistor markings can help engineers quickly verify whether the installed component matches the intended value in the schematic and BOM—for example, whether a 10 kΩ resistor in a feedback network was mistakenly replaced with a 1 kΩ resistor.
- Field Repair: For technicians, visible resistor markings can provide a quick reference for identifying a damaged component and selecting a suitable replacement.
For example, confusing a 100 code (10 Ω) with a 101 code (100 Ω) can significantly alter circuit behavior and, in a current-sensing application, may result in incorrect measurements or excessive current.
Understanding these marking systems helps engineers identify resistor values quickly and avoid component selection, assembly, and troubleshooting errors. This guide covers the three common SMD resistor marking systems: 3-digit, 4-digit, and EIA-96 codes.
How to Read 3-Digit and 4-Digit SMD Resistor Codes (E-Series) System
This is the most straightforward system, typically used for 5% (E24) and 2% (E48) tolerance resistors. The logic is simple: all but the last digit are significant figures, and the last digit is the multiplier (the number of zeros to add).
3-Digit Code (E24): Two significant figures and a multiplier.
- 103 = 10 x 103 = 10,000Ω = 10kΩ
- 472 = 47 x 102 = 4,700Ω = 4.7kΩ
- 560 = 56 x 100 = 56Ω
4-Digit Code (E48/E96): Three significant figures and a multiplier. This system is used for 1% or 2% resistors that have more precise values.
- 2201 = 220x 10¹ = 2,200Ω = 2.2kΩ
- 1001 = 100 x 101 = 1,000Ω = 1.00kΩ
- 4992 = 499 x 102 = 49,900Ω = 49.9kΩ
- 7500 = 750 x 100 = 750Ω
The "R" for Decimals: For values under 100Ω (and sometimes 10Ω for 3-digit), the letter R is used to indicate the decimal point's position.
- R102 = 0.102Ω
- 4R7 = 4.7Ω
- 0R22 = 0.22Ω
0-Ohm Resistors (Jumpers): A 0-ohm resistor, or jumper, is used to connect traces and is typically marked with a single 0 or multiple zeros (000, 0000).

3-Digit and 4-Digit (E-Series) resistor code identification
Understanding Resistor Tolerance Letter Codes (J, F, G)
While the 3-digit and 4-digit systems often imply a 5% or 1% tolerance, you will sometimes see a letter code added, especially on 0603 or larger packages. This letter explicitly states the tolerance.
- 103J = 10kΩ, 5%
- 1001F = 1.00kΩ, 1%
Here is a chart for the most common codes:
| Code | Tolerance |
|---|---|
| F | ±1% |
| G | ±2% |
| J | ±5% |
| K | ±10% |
| M | ±20% |
Resistor Tolerance Letter Codes
Note
Do not confuse the tolerance letter F with the EIA-96 multiplier F. They are used in different systems.
EIA-96: The 1% SMD Resistor Code System
As components shrank, even 3-digit codes became too large. The EIA-96 system was introduced for 1% tolerance (E96 series) resistors, fitting a precise value into a three-character code.
This system consists of two parts:
- Two-Digit Code: A number from 01 to 96 that corresponds to a 3-digit value.
- One-Letter Multiplier: A letter that sets the power of 10.
| Code | Value (Ω) | Code | Value (Ω) | Code | Value (Ω) | Code | Value (Ω) |
|---|---|---|---|---|---|---|---|
| 01 | 100 | 25 | 178 | 49 | 316 | 73 | 562 |
| 02 | 102 | 26 | 182 | 50 | 324 | 74 | 576 |
| 03 | 105 | 27 | 187 | 51 | 332 | 75 | 590 |
| 04 | 107 | 28 | 191 | 52 | 340 | 76 | 604 |
| 05 | 110 | 29 | 196 | 53 | 348 | 77 | 619 |
| 06 | 113 | 30 | 200 | 54 | 357 | 78 | 634 |
| 07 | 115 | 31 | 205 | 55 | 365 | 79 | 649 |
| 08 | 118 | 32 | 210 | 56 | 374 | 80 | 665 |
| 09 | 121 | 33 | 215 | 57 | 383 | 81 | 681 |
| 10 | 124 | 34 | 221 | 58 | 392 | 82 | 698 |
| 11 | 127 | 35 | 226 | 59 | 402 | 83 | 715 |
| 12 | 130 | 36 | 232 | 60 | 412 | 84 | 732 |
| 13 | 133 | 37 | 237 | 61 | 422 | 85 | 750 |
| 14 | 137 | 38 | 243 | 62 | 432 | 86 | 768 |
| 15 | 140 | 39 | 249 | 63 | 442 | 87 | 787 |
| 16 | 143 | 40 | 255 | 64 | 453 | 88 | 806 |
| 17 | 147 | 41 | 261 | 65 | 464 | 89 | 825 |
| 18 | 150 | 42 | 267 | 66 | 475 | 90 | 845 |
| 19 | 154 | 43 | 274 | 67 | 487 | 91 | 866 |
| 20 | 158 | 44 | 280 | 68 | 499 | 92 | 887 |
| 21 | 162 | 45 | 287 | 69 | 511 | 93 | 909 |
| 22 | 165 | 46 | 294 | 70 | 523 | 94 | 931 |
| 23 | 169 | 47 | 301 | 71 | 536 | 95 | 953 |
| 24 | 174 | 48 | 309 | 72 | 549 | 96 | 976 |
EIA-96 Resistor Code and Corresponding Resistance Values
| Letter | Multiplier | Letter | Multiplier |
|---|---|---|---|
| Y | 10⁻² (0.01) | C | 10² (100) |
| X or S | 10⁻¹ (0.1) | D | 10³ (1k) |
| A | 10⁰ (1) | E | 10⁴ (10k) |
| B or H | 10¹ (10) | F | 10⁵ (100k) |
EIA-96 Multiplier Chart
Example: A resistor marked 01C is 100 (from code 01) x 100 (from letter C) = 10,000Ω or 10kΩ.

EIA96 resistor code identification
Unmarked SMD Resistors: When SMD Resistor Codes Are Not Available
Be aware that as package sizes shrink to 0201 (0.6mm x 0.3mm) and 01005, most resistors are unmarked. At this scale, the only way to identify the component is by referencing the assembly documentation (BOM and pick-and-place data).
Common Challenges in Reading SMD Resistor Codes
Even with these standards, you will face challenges in the real world.
Challenge 1: Misreading Similar SMD Resistor Codes
Problem: The risk of misreading 101 (100Ω) as 100 (10Ω) is very high, or 102 (1kΩ) as 120 (12Ω), which can happen as well. A tiny error in the feedback loop might lead to the destruction of a part.
Solution: Use good magnification and lighting all the time. If you are not sure, use a multimeter. A quick in-circuit resistance check (with the board powered off) can often confirm a value. For 100% accuracy, desolder one leg of the resistor to measure it out of the circuit, thereby removing any parallel paths.
Challenge 2: Confusing Different SMD Resistor Marking Systems
Problem: Different marking systems can use similar combinations of numbers and letters, making identification confusing. For example, an EIA-96 marking such as 10F consists of the two-digit code 10 and the multiplier F. In the EIA-96 system, 10 corresponds to 124, while F represents a multiplier of 10⁵, giving a resistance of 12.4 MΩ.
Solution: Always identify the marking system before interpreting the code. EIA-96 markings use two digits followed by a letter multiplier and are primarily used for 1% tolerance resistors. Three-digit markings, such as 103, use the first two digits as the significant value and the third digit as the power-of-ten multiplier, giving 10 kΩ. When a marking includes an additional letter, refer to the manufacturer's datasheet or marking convention rather than assuming its meaning.
Challenge 3: Obscured or Damaged Resistor Markings
Problem: The component is either covered in conformal coating, flux residue, or is partially damaged (burnt).
Solution: Using a cotton swab and 99% isopropyl alcohol (IPA), slowly clean the part. For damaged codes, you have to regard it as an "unmarked" component: find a similar part on the board to measure, or refer to the schematic/BOM, which is the final source of truth.
Conclusion: How to Correctly Identify Any SMD Resistor Code
Correctly reading SMD resistor codes is a fundamental skill for anyone working at the PCB level. These standardized markings provide a direct link between the physical component and the schematic, making them essential for assembly verification, debugging, rework, and field repair. Once you understand the underlying logic, even compact SMD markings become clear, reliable, and actionable.
While decoding SMD resistors is critical when diagnosing existing boards, the most effective way to avoid resistor-related issues is to ensure correctness from the design and assembly stage.
FAQs about SMD Resistor Codes
Q: What's the difference between 3-digit and 4-digit codes?
The number of digits denotes precision. The 3-digit codes are meant for 5% tolerance resistors, commonly known as the E24 series, and have two significant figures along with one multiplier (i.e., two significant figures and one multiplier). The 4-digit codes represent higher precision (1% or 2% E48 or E96 series) resistors with more particular values and have three significant figures and one multiplier (i.e., three significant figures and one multiplier).
Q: I see a resistor marked with just a single '0'. What is that?
That is a "zero-ohm" or "0-ohm" resistor. It is, in fact, a jumper link placed inside a resistor package. Engineers generally use them to link the traces on a PCB, especially as a configurable jumper (to be "stuffed" or "not stuffed") or to connect two traces during layout.
Q: What do the terms E24, E48, and E96 mean?
The terms "E-series" characterize the standard resistor "preferred values" grouped according to tolerance.
- E24 (5%): It offers 24 different values for each decade (e.g., 1.0, 1.1, 1.2, 1.3, 1.5...).
- E48 (2%): It presents 48 different values for each decade.
- E96 (1%): It provides 96 different values for each decade.
The 3/4-digit system is usually employed for E24/E48, while the EIA-96 code system is intended for the E96 values only.
Q: Does the color of an SMD resistor (black vs. blue/green) mean anything?
The vast majority of standard chip resistors are black, with a white/light protective overglaze. You may occasionally see other colors, such as blue or green, which often signify a special type, such as a high-precision thin-film resistor or a specialty resistor. However, this is not standardized, so you should always rely on the code, not the body color.
Q: Does the SMD resistor code (like 103 or 01C) also indicate the power rating?
No, this is a critical point of confusion. The code only indicates the resistance and tolerance. The power rating (e.g., 1/16W, 1/10W, 1/8W) is determined by the physical package size of the component. For example:
- 0402 Package: Typically 1/16W
- 0603 Package: Typically 1/10W
- 0805 Package: Typically 1/8W
An engineer must select the correct package size for the design based on their power dissipation (P = I²R) calculations.
Q: I see a component marked 102, but it has 8 pins. What is it?
That is almost certainly an SMD resistor array or resistor network. The code (102 = 1kΩ) typically applies to all the individual resistors housed inside the single package. These are used to save space (e.g., for pull-up resistors on a data bus). It could be an "isolated" array (four 1kΩ resistors with 8 pins, 2 per resistor) or a "bussed" array (seven 1kΩ resistors, each tied to one common pin). You would need to check the schematic or trace the pins to know which.
Q: My EIA-96 code is ambiguous, like 06. Is it 06 (113Ω) or 90 (845Ω) read upside-down?
This is a real problem, especially with 2-digit codes. To solve this, some high-quality manufacturers will add a small underline or bar to the code to indicate orientation. For example, 06 (underlined) means 06, while a non-underlined 06 might be interpreted as 90 (or vice-versa, depending on the manufacturer). If no orientation mark is present, you must fall back to using your multimeter or consulting the schematic. Never assume the orientation.
Q: Why does the EIA-96 multiplier chart have duplicate letters (like A/Z, X/S, Y/R)?
This is an artifact of merging different standards (EIA and JIS) over time. While the chart lists all of them, in practice, you will most commonly see A (x1), B (x10), C (x100), and X (x0.1). The other letters (Z, S, R) are less common but are still valid. For all practical purposes, you can treat A and Z as the same (x1), X and S as the same (x0.1), and Y and R as the same (x0.01).
Popular Articles
• SMD Resistor Codes: How to Read 3-Digit, 4-Digit, and EIA-96 Markings
• SMD Capacitor Codes: Identification, Markings, and Polarity
• SMD Resistor Package Sizes: Complete Size Chart, Footprints & How to Choose
• SMD Capacitor Sizes: Complete Size Chart and Selection Tips for PCB Design and Assembly
• SMD Diode Code Lookup: Full List, Marking Guide & Identification [2026 Guide]
Keep Learning
Ceramic Capacitor Types Explained: C0G, X7R, X5R, Y5V and How to Choose
Two ceramic capacitors can share the same capacitance value, the same voltage rating, and the same footprint, yet behave nothing alike on a powered board. The reason is the dielectric, not the number on the label. Ceramic capacitor types are defined by the dielectric, captured in codes like C0G, X7R, X5R, and Y5V. This guide decodes those codes, compares the dielectric classes, explains the DC bias and aging effects that catch designers off guard, and gives you a practical way to pick the right part f......
ESP32-C3 vs ESP32-S3 Explained: Performance, Features, and How to Choose the Right Chip
Note Pick the ESP32-C3 for low-cost, low-power, connected sensors. Pick the ESP32-S3 for anything involving a camera, a display, on-device AI, or USB. If you are making a prototype that connects to the internet using WIFI or transmits data over BLE, the most popular option among designers is ESP32. The two most popular chips from the ESP32 series are: ESP32-c3 and ESP32-s3. The pain point is to choose the one as per the required application. The ESP32-c3 vs ESP32-s3 decision trips up beginners and sea......
PCB Connector Types Explained: Categories, Comparison, Applications and How to Choose the Right One
PCB connectors are essential components for connecting circuit boards with external devices, cables, or other PCBs. Choosing the right connector type affects signal reliability, mechanical stability, and overall product performance. Factors such as current rating, frequency requirements, pitch size, and mounting method should be considered during selection. In this guide, you will learn: The major types of PCB connectors and their applications. How different connector types compare. How to select the ......
Complete Guide to Resistor Types: Fixed, Variable, and Non-Linear Resistors
The decision becomes difficult even for designers when a circuit board involves different types of resistors. Knowing which one your circuit actually needs solves half of the design problem. In this guide, you will go through: The full resistor types chart — fixed, variable, and non-linear families. How to choose between carbon film, metal film, wirewound, and foil resistors. When to use a potentiometer, thermistor, LDR, or varistor in design. SMD/through-hole resistor types and what each costs you. H......
The Engineering Guide to Capacitor Symbols: Schematic Standards and Polarity
In high-frequency PCB design and precision analog circuitry, the capacitor is not merely a charge storage device governed by the fundamental equation C = Q/V; it is a complex component possessing Equivalent Series Resistance (ESR) and Inductance (ESL). However, before a design reaches the simulation or layout stage, it begins as a symbol on a schematic. For the PCB design engineer, the capacitor symbol is a critical element, serving as the main instruction for both the layout team and the manufacturin......
What Is the ESP32? A Complete Guide to Features, Architecture, Modules, Programming, and Applications
From Wi-Fi-enabled temperature sensors and wearable health monitors to industrial gateways and AI-powered cameras, the ESP32 microcontroller has become one of the world's most widely adopted wireless embedded platforms. Combining a powerful processor with integrated Wi-Fi and Bluetooth, it lets engineers build connected devices without separate networking hardware. This guide covers ESP32 specifications, architecture, the full family of variants, development boards, programming tools, and real-world E......