Capacitors in PCB Design_ A Complete Guide to All Types
9 min
- What Is a Capacitor and How Does It Work?
- Factors That Affect Capacitance
- Polarized vs Non-Polarized Capacitors
- Functions of Capacitors in Electronic Circuits
- Capacitor Types and Their Applications in PCB Design
- Understanding Capacitor Markings and Codes
- How to Select the Right Capacitor for PCB Design
- Best Practices for PCB Capacitors in High-Frequency Circuits
- How To Reduce Parasitic Capacitance in Circuit Board Layout
- Conclusion
Capacitors are indispensable components in PCB (Printed Circuit Board) design, providing functionality from energy storage and noise filtering to voltage regulation. Whether you're designing a simple circuit or a complex multi-layer board, understanding the different types of capacitors and their applications is crucial. The basic structure of a capacitor consists of two metal plates separated by a layer of dielectric. Capacitors can be of fixed or variable type.
The ability of the capacitor to hold electric charge is called capacitance and is measured in Farads. Like resistors, capacitors can be arranged in series or parallel combinations, and thus effective capacitance can be varied. There are several types of capacitors that have been developed for use in electronic circuits. In this complete guide, we'll explore the roles of capacitors in PCB design, discuss the various types available, and look at how to choose the right one for your projects. See the other type of components required on a PCB.
What Is a Capacitor and How Does It Work?
Capacitors are passive electrical components that store and release electrical energy in the form of an electric field. They are made of two conductive plates separated by an insulating material called a dielectric. When a voltage is applied, the plates store electric charge. The charges stored on the plates are complementary to each other. Capacitors play many roles in electronic circuits. The capacitor terminals are taken out from the metal plates for external connections.
The capacitance of the structure can be given by the following equation:
C = εA / D
Where:
ε is the permittivity (Dielectric constant) measured in
C is the capacitance measured in farads
D is the distance between the plates
A is the overlapped area between two plates
The capacitance is the ratio of charge (Q) to voltage (V), and its mathematical expression is as follows:
C = Q / V
Where:
C is the capacitance measured in farads
Q is the charge accumulated on the plates
V is the voltage applied to capacitor
Factors That Affect Capacitance
The capacitance of a capacitor can be varied by changing the following parameters:
- Area of the plate: The capacitance increases by increasing the area of the plate.
- Overlap of the plates(A): As the parallel plate overlap area increases, the capacitance value increases.
- Distance between the plates(D): The closer the proximity of the parallel plates, the greater the capacitance value.
- The nature of the dielectric(ε): Choosing a dielectric material of high permittivity increases the capacitance value.
Polarized vs Non-Polarized Capacitors
Polarized capacitors: They are the capacitor that has positive and negative two different terminals. Common examples include aluminum electrolytic and tantalum electrolytic capacitors. These capacitors have distinct positive and negative terminals, and it’s crucial to connect the positive terminal to the positive side of the power source, and the negative terminal to the negative side.
Non-polarized capacitors: These capacitors can be connected in either direction without any concern for polarity. They are often used in applications where the voltage direction changes frequently.
Functions of Capacitors in Electronic Circuits
- Decoupling and Bypassing: They prevent noise from propagating in the circuit by acting as small reservoirs of charge.
- Filtering: Capacitors smooth out fluctuations in voltage, often used in power supply circuits to filter out AC ripple.
- Timing Circuits: Combined with resistors, capacitors are used to create timing intervals.
- Energy Storage: They temporarily store electrical energy and release it when needed, particularly in backup applications.
Capacitor Types and Their Applications in PCB Design
Capacitors come in various shapes, sizes, and materials, each suited for different applications. Below is a comprehensive overview of the most common types of capacitors used in PCB design.
1. Ceramic Capacitors
- Material: Made from ceramic as the dielectric.
- Types: Multilayer ceramic capacitors (MLCC) are most commonly used.
- Capacitance Range: Typically from a few picofarads (pF) to microfarads (µF).
- Voltage Ratings: Available in a wide range of voltage ratings.
- Applications: Ceramic capacitors are used in high-frequency circuits for bypassing and decoupling, due to their low equivalent series resistance (ESR) and low inductance.
- Pros: Low cost, small size, and good stability.
- Cons: Limited capacitance value compared to other types.
2. Electrolytic Capacitors
- Material: Aluminum or tantalum with an electrolyte as the dielectric.
- Capacitance Range: High capacitance values, typically in the range of 1 µF to several thousand µF.
- Voltage Ratings: Medium to high voltage ratings.
- Applications: Commonly used for bulk energy storage and filtering in power supplies due to their large capacitance.
- Pros: High capacitance in a compact size.
- Cons: Higher ESR, polarized (must be connected correctly in terms of polarity).
3. Tantalum Capacitors
- Material: Tantalum metal with a conductive oxide as the dielectric.
- Capacitance Range: Medium to high capacitance values.
- Voltage Ratings: Typically lower voltage ratings than aluminum electrolytics.
- Applications: Tantalum capacitors are used where a stable capacitance is needed, such as in decoupling and filtering applications.
- Pros: High stability, longer life, and compact size.
- Cons: More expensive and sensitive to voltage spikes.
4. Film Capacitors
- Material: Plastic film, often polyester, polypropylene, or PTFE.
- Capacitance Range: Generally low to medium capacitance, from a few nanofarads (nF) to several µF.
- Voltage Ratings: High voltage ratings.
- Applications: Preferred in audio circuits, signal coupling, and filtering applications due to their low distortion and high accuracy.
- Pros: Very stable, low ESR, and high reliability.
- Cons: Larger size compared to ceramic capacitors.
5. Supercapacitors (Ultra-Capacitors)
- Material: Electrochemical double-layer technology.
- Capacitance Range: Farads (F), much higher than traditional capacitors.
- Voltage Ratings: Typically low voltage.
- Applications: Energy storage in applications requiring quick charge and discharge cycles, such as backup power and power smoothing.
- Pros: Extremely high capacitance.
- Cons: Low voltage rating, often requiring series combinations for higher voltage applications.
Understanding Capacitor Markings and Codes
A capacitor's markings provide crucial information for its use in PCB assembly and testing. These markings include:
- Capacitance Value: Indicates the charge capacity, usually in μF, nF, or pF.
- Voltage Rating: The maximum voltage the capacitor can handle, often noted like "5V5" for 5.5V.
- Tolerance: The acceptable capacitance variance, typically ±1%, ±5%, or ±10%.
- Temperature Coefficient: Shows how capacitance changes with temperature.
- Date Code: Indicates the manufacturing or batch date.
- Polarity: For polarized capacitors, positive and negative terminals are marked.
- Logo: Manufacturer branding and sometimes a part number.
Some capacitors also indicate the insulating material, ripple current, and lifetime hours.
How to Select the Right Capacitor for PCB Design
When selecting a capacitor for PCB design, consider the following factors:
1. Capacitance Value: Determine the required capacitance for your application, which can range from picofarads to farads.
2. Voltage Rating: Choose a capacitor with a voltage rating at least 1.5 times higher than the expected operating voltage.
3. Temperature Coefficient: For precision circuits, a low temperature coefficient is important to maintain stability.
4. Size and Form Factor: Space limitations may require using a smaller component, like an MLCC, instead of bulkier types like film capacitors.
5. ESR (Equivalent Series Resistance): Low ESR is critical in high-frequency and power applications where efficiency is paramount.
6. Dielectric material type: A capacitor's dielectric material dictates its capacitance and thermal stability.
7. Tolerance: The tolerance value shows how far a capacitor can deviate from its nominal value in both directions.
8. Capacitor Mounting Types: SMD for the smaller designs and Through hole where more capacitance required and space is not a constraint.
9. Supplier Considerations: When sourcing capacitors, always choose reputable suppliers to avoid counterfeit components that may have incorrect specifications.
Best Practices for PCB Capacitors in High-Frequency Circuits
While a capacitor's behavior is predictable at low frequencies, it becomes less ideal at higher frequencies. Use these tips to maintain stable operation and avoid issues such as Equivalent Series Inductance (ESL) and self-resonance. Here are some key factors to consider while working on high frequency circuit
- Instead of electrolytes, use ceramic caps or ESR films.
- Tiny case sizes have a lower ESL, with chip caps being better than Lead.
- Reduce trace lengths and return paths to the ground plane.
- Avoid large loop areas to prevent parasitic inductance.
- Simulate the circuit using S-parameter models.
- Test for ringing and other frequency-dependent issues during prototyping.
- The distance between capacitor pads on the PCB affects resonant frequency.
- If the capacitor operates near the self-resonant frequency, characterize its impedance.
How To Reduce Parasitic Capacitance in Circuit Board Layout
The parasitic capacitance on a PCB is due to the high-frequency signals and different adjacent traces passing through the circuit board. This capacitance then introduces EMI, which propagates down to adjacent traces. To keep this capacitance minimum:
- A guard ring reduces the capacitive effect between two traces.
- Increase the space between adjacent traces.
- Use low permittivity dielectric materials since they produce less stray capacitance.
- Avoid routing the traces in parallel, as this leaves a maximum area between the two traces.
Conclusion
Capacitors are fundamental components in PCB design, providing various functionalities essential for circuit stability, noise reduction, and energy management. Understanding the different types of capacitors, their properties, and best practices for placement can make a significant difference in the performance and reliability of your circuits. In summary:
- PCB capacitors store energy between conducting plates separated by a dielectric.
- Different capacitor types suit various applications and conditions.
- Proper rating of voltage, capacitance, ESR, and other factors prevents failures.
- Correct selection, placement, and handling ensure stable PCB performance.
- Bypass and decoupling capacitors need careful design for clean power delivery.
Whether you're working on high-speed digital designs, audio circuits, or power electronics, selecting the right capacitor type and placement is key to achieving your design goals. By mastering the use of capacitors, you'll be better equipped to handle complex PCB projects and avoid common pitfalls.
Popular Articles
• SMD Resistor Codes: How to Read 3-Digit, 4-Digit, and EIA-96 Markings
• SMD Capacitor Codes: Identification, Markings, and Polarity
• SMD Resistor Package Sizes: Complete Size Chart, Footprints & How to Choose
• SMD Capacitor Sizes: Complete Size Chart and Selection Tips for PCB Design and Assembly
• SMD Diode Code Lookup: Full List, Marking Guide & Identification [2026 Guide]
Keep Learning
Complete SMD Inductor Size Guide: Dimensions, Packages, and PCB Design Tips
SMD inductor size affects far more than PCB real estate. Package dimensions directly influence current handling, saturation behavior, DCR, and EMI characteristics. Picking the wrong package can mean a costly board respin, not just inefficiency. One challenge is that SMD inductor package sizes use multiple naming conventions and the fundamental split between RF chip inductors (compact footprint, high Q-factor) and power inductors (low DCR, magnetic shielding, high saturation current). This guide covers......
Circuit Breaker Types Explained: MCB, MCCB, RCCB, RCBO, ACB, VCB & SF6 Circuit Breakers
A circuit breaker automatically disconnects power when it detects faults such as overloads or short circuits, protecting equipment and reducing fire risk. Different circuit breaker types are designed for different voltage levels, current ratings, and applications, from household distribution boards to high-voltage substations. This guide explains the most common types - including MCBs, MCCBs, RCCBs, RCBOs, ACBs, VCBs, and SF6 breakers and helps you choose the right one for your application. Figure: Ci......
What is a Power Management IC (PMIC): Functions and Applications
A Power Management IC (PMIC) is a type of integrated circuit designed to manage the power requirements of the host system. It efficiently distributes, regulates, converts, and monitors electrical power for various components within a device, such as processors, memory units, and peripherals. As the demand for compact, battery-powered, and high-performance devices continues to grow, PMICs have become an essential part of system design across industries. Embedded and application processors and other com......
How to Read SMD Resistor Values: Codes, Charts, and Identification Guide
An SMD resistor value is identified using numeric or alphanumeric marking codes printed on the surface of chip resistors. These codes represent resistance in ohms using standardized 3-digit, 4-digit, or EIA-96 systems. This guide breaks down the 3-digit, 4-digit, and EIA-96 marking systems so you can decode, calculate, and replace any SMD resistor with confidence. Quick Checklist to Identify SMD Resistor Value Understanding SMD resistor values simply requires recognizing which standardized system is p......
What Is a BGA Chip? A Complete Guide to Ball Grid Array Packaging
Modern electronics require compact packages with high connection density and efficient heat dissipation. Ball Grid Array (BGA) technology has become a key solution for high-performance PCB design. Because of these advantages, BGA chips are widely used in processors, graphics devices, memory modules, networking hardware, and compact embedded systems. This guide explains how BGA packages work, the common types available, their key benefits and challenges, and the essential PCB design and assembly consid......
SOIC Package: A Complete Guide to Specifications, Types, Uses, and SMT Assembly
As designs transition from legacy through-hole components to high-density Surface Mount Technology (SMT), the Small Outline Integrated Circuit (SOIC) remains the industry standard for operational amplifiers, flash memory, sensors, and microcontrollers. It reflects a well-balanced engineering design, offering a practical compromise between the miniaturisation demanded by modern consumer electronics and the ruggedness required for industrial applications. In this guide, you will learn: SOIC package dime......