How Nixie Tubes Work: The Glow Behind the Glass
4 min
- What is a Nixie Tube?
- A Brief History of Nixie Tubes
- The Technology Behind Nixie Tubes
- Drivers and Digit controllers for Nixie Tubes:
- Conclusion
Let me take you in the past, when there were no LED or LCD lights for display, rather a technology that consumes a lot of power but looks awesome. Nixie tubes, a softly glowing orange digits inside a glass tube. But nowadays these have just become obsolete, for some electronics hobbyists still keep them alive as a vintage piece from history. In this article, we’ll dive into how Nixie tubes work. Moreover, we will know the technology behind them and the history that brought them from laboratory equipment to nostalgic collectibles.
What is a Nixie Tube?
A Nixie tube is an electronic display device invented in the 1950s. In that time, there were no devices like LEDs, but they used cold cathode glow discharge to display numerals. It looks like a glass tube similar to a vacuum tube filled with a low-pressure neon gas. Inside it, there are shaped metal cathodes (usually digits 0–9), stacked one behind another. When a cathode is energized with ~170 V DC, it glows with an orange-red light due to neon gas discharge, making the digit visible. Because it is made to glow from discharge back then to make a pixel, separate shaped cathodes for each number (0–9) are used.
The signature warm orange glow is due to neon gas emitting light when excited by an electric field. Neon’s emission spectrum is dominated by orange-red wavelengths. When argon or mercury vapor is added, it changes the brightness and adds a bluish tint near the electrodes.
A Brief History of Nixie Tubes
Nixie tubes were first developed in 1955 by the Haydu Brothers Laboratories. The name "Nixie" is said to come from "Numeric Indicator eXperimental No. 1". They became popular in scientific instruments and calculators in the early 60s. At the time, they were the way to display numeric data. Around 70s LEDs and LCDs emerged, offering lower voltages, smaller sizes, and greater durability. Nixie production rapidly declined. Today, they are just used as vintage pieces. Today you'll find them in:
- Custom Nixie clocks
- Retro-style instrumentation
- Art installations
- Unique timepieces for collectors
The Technology Behind Nixie Tubes
A Nixie tube is essentially a cold cathode gas discharge tube, operating on a principle similar to neon signs. The key components of a nixie tube are:
- Cathodes: These are the shaped metal electrodes for each numeral or symbol.
- Anode: A fine wire mesh surrounding the cathodes completes the circuit.
- Gas Fill: Typically, neon for the orange glow, with trace amounts of argon or mercury for longevity, is used.
- Glass Envelope: Sealed to maintain low pressure for gas.
Usually, a positive voltage (around 170–200 V DC) is applied to the anode. It is huge! We need some DC-DC converters and some specialized electronics to handle the voltage. The cathode is connected to ground and ionizes the gas, which produces a glow discharge. This much voltage/ electric field between the cathode and the anode is enough to ionize the gas in the glass chamber. Only the chosen cathode lights up and others remain dark, so there is no concept of a pixel. And there is no filament; instead, we are using the glow that is caused by ionized gas. This becomes the main reason they do not produce much heat.
Drivers and Digit controllers for Nixie Tubes:
Nixie tubes need special driver circuits because they operate at ~170–200 V DC. But requires a very low current, typically 1–5 mA per digit. They cannot be connected directly to low-voltage microcontrollers like Arduino or Pi. To use these nixie properly, we need to convert low-voltage DC (e.g., 5 V or 12 V) into ~170–200 V DC. We have to use a DC-DC boost converter, and the output must be regulated to avoid overdriving and damaging the tube.
List of some commonly used drivers:
These drivers can be connected to high-voltage digit controllers, which can be used to light up the required digit at a time.
Conclusion
Nixie tubes are more than just display devices. Their warm glow connects us to a time when even functional components were works of art. Though nixies are replaced in mainstream use by LEDs and LCDs, the Nixie tube lives on in retro designs. We have seen the types of drivers required to power them up. If you ever get the chance to see one in person, take a moment to appreciate the glow behind the glass.Want to build your own retro-style Nixie clock or display? Upload your design files to JLCPCB and get high-quality PCBs manufactured fast, so you can bring vintage electronics back to life.
Popular Articles
• How to Solder SMD Components Like a Pro [2026 Updated]
• SMD Resistor Codes: How to Read 3-Digit, 4-Digit, and EIA-96 Markings
• SMD Capacitor Codes: Identification, Markings, and Polarity
• SMD Resistor Package Sizes: Complete Size Chart, Footprints & How to Choose
• SMD Capacitor Sizes: Complete Size Chart and Selection Tips for PCB Design and Assembly
Keep Learning
How to Solder SMD Components Like a Pro [2026 Updated]
Soldering is a core skill to know, and when it comes to SMD, things become more complex and smaller. Soldering is similar to welding, but instead of welding two iron/steel pieces, we are now welding small components. To develop a circuit, the best way to join two components is by soldering. There are two main types of components in electronics: one is a through hole with long legs covered with tin, which can be easily inserted onto a PCB and then soldered, and the other is SMDs (surface mount devices)......
The Ultimate Guide to Wafer Level Packaging (WLP): Process, Types, Benefits, and Applications
Modern electronics are hitting a hard limit: you can’t keep shrinking devices without rethinking how chips are packaged. As PCB space tightens and signal speeds increase, traditional packaging methods introduce too much size, parasitic loss, and inefficiency. Wafer-level packaging (WLP) addresses this by forming interconnects directly on the wafer before singulation, eliminating substrates and shortening signal paths. The result is a chip-scale package with higher integration density, lower parasitics......
Diode Type Guide: How to Choose the Right Diode for PCB and Product Design
Modern electronics rely on highly specialized diode types for power conversion, ESD protection, signal detection, and high-frequency switching. Choosing the wrong diode doesn't just reduce efficiency; it also generates excess heat, introduces switching losses, and can even damage sensitive circuits during voltage transients. Choosing the right component ensures a reliable board, whether you are wiring a prototype or scaling to low-volume PCB assembly. In this guide, you'll learn: How do different diod......
How to Read Capacitor Symbols in Electronic Schematics
Introduction A capacitor symbol represents a capacitor in an electronic schematic, but its appearance can vary depending on the component type and drawing standard. Recognizing these differences is essential for reading circuit diagrams, identifying polarized components, and avoiding design mistakes. This guide covers common capacitor symbols, explains the differences between ANSI and IEC representations, and shows how to identify capacitor polarity. It also explores how schematic symbols relate to PC......
Complete SMD Inductor Size Guide: Dimensions, Packages, and PCB Design Tips
SMD inductor size affects far more than PCB real estate. Package dimensions directly influence current handling, saturation behavior, DCR, and EMI characteristics. Picking the wrong package can mean a costly board respin, not just inefficiency. One challenge is that SMD inductor package sizes use multiple naming conventions and the fundamental split between RF chip inductors (compact footprint, high Q-factor) and power inductors (low DCR, magnetic shielding, high saturation current). This guide covers......
Circuit Breaker Types Explained: MCB, MCCB, RCCB, RCBO, ACB, VCB & SF6 Circuit Breakers
A circuit breaker automatically disconnects power when it detects faults such as overloads or short circuits, protecting equipment and reducing fire risk. Different circuit breaker types are designed for different voltage levels, current ratings, and applications, from household distribution boards to high-voltage substations. This guide explains the most common types - including MCBs, MCCBs, RCCBs, RCBOs, ACBs, VCBs, and SF6 breakers and helps you choose the right one for your application. Figure: Ci......