This website requires JavaScript.
Coupons
Ship to
Blog

Via Stitching Guide : Core Functions, Pitch Rules & Placement

Published Nov 06, 2026, updated Nov 06, 2026

17 min

Table of Contents
  • What Is Via Stitching and How Does It Work?
  • Core Functions of Via Stitching in PCB Layout
  • Best Practices for Via Stitching Placement
  • Manufacturing High-Density Via Stitching Boards
  • FAQs About Via Stitching
  • Conclusion

key takeaway

  • Core Purpose: Ties ground layers together to cut EMI, reduce impedance, and shorten return paths.
  • Pitch Rules: Space vias at λ/10 for ground grids and λ/20 for edge rings and shielding fences.
  • Layer Transitions: Place stitching vias adjacent to signal vias to minimize return current loop area.
  • Avoid Over-Stitching: Overuse perforates power planes, alters trace impedance, and increases drilling costs.
  • DFM Control: Follow hole spacing rules, tent non-test vias, and maintain proper edge copper setbacks.

Via stitching connects ground copper across different PCB layers using rows or grids of vias, helping the layers form a continuous, low-impedance ground reference. These stitching vias create short return current paths, enhance grounding, and help reduce electromagnetic interference (EMI). The distance between vias, or via pitch, depends on the highest significant signal frequency, the signal's wavelength in the PCB material, and the board layout.

In this guide, we will discuss how stitching vias work, how they carry return current, and why they're so important in PCB layout. Also included are instructions on calculating pitch using the signal wavelength, where to place stitching vias along the board edges, and how to avoid excessive stitching.

What Is Via Stitching and How Does It Work?

Via stitching is the act of inserting a "via" between two copper areas on different layers; these vias are typically plated, tied to the same net, and grounded. The vias cause those areas to behave as a single conductor, keeping the return current and fields where the layout wants them.

Via Stiching Guide Oct 1. (1)

Figure 1: Via stitching on a four-layer PCB with a ground via grid, a via fence along

Understanding Via Stitching in High-Frequency Design

A stitching via is a via that is not included in the signal. It brings together the ground copper of each layer it crosses: outer-layer pours, inner ground planes, and a ground area that might not be connected. Because the copper resistance is low, a single via at DC connects two ground layers that are at nearly the same potential. Each via also introduces a small series inductance to the connection, in the high-frequency case.

Howard Johnson's approximation for a via of height h and drill diameter d, both in inches, is L ≈ 5.08h[ln(4h/d) + 1] nH.

Example: A 0.3 mm (12 mil) via through a 1.6 mm (63 mil) board results in about 1.3 nH.

This is approximately 8 Ω of reactance at 1 GHz. So at high frequency, one via can't maintain two planes at the same potential, and via stitching solves this problem in two ways:

  • Parallel vias: Many vias in parallel reduce the net inductance between layers.
  • Short spacing: Closely spaced vias keep the gaps between them small enough to limit field leakage and to raise the plane-pair resonance.

Via Stitching for Ground Plane Continuity and Return Current Paths

When the frequency is high, the return current will flow in the reference plane immediately under the signal line. This path has the smallest loop area and hence the lowest inductance. When moving a trace from one layer to another, the reference plane often changes. The return current then has to travel between the two planes at the transition, and the layout determines the path:

  • Ground-to-ground transition: A via stitch that connects the signal via to the return path that provides a short path with minimal inductance between the planes.
  • Ground-to-power transition: A via cannot connect planes on different nets; instead, a decoupling capacitor is placed near the transition where the return current flows.
  • No nearby return path: Return current is diffused through the plane-pair cavity and finds a path that widens the loop and introduces noise into other vias.

For a single-ended signal via, the distance to the nearest stitching vias is a major factor in the via's impedance. Return vias are not an independent grounding detail, but are part of the transmission line.

Via Stiching Guide Oct 1. (5)

Figure 2: Return current crossing between two ground planes through a stitching via

Stitching vs. Thermal vs. Shielding Vias

These are all plated holes, which may be the same size drill. The shielding vias are stitching vias used in series to contain fields; they are not necessarily different from stitching vias, but vary in placement and pitch. Thermal vias serve different purposes and therefore have different locations and pitches.

Via TypePrimary FunctionTypical LocationWhat Sets the Pitch
Stitching viaTie the ground copper on several layers into one low-impedance referenceAcross ground pours and planes, and next to signal vias that change layersWavelength at the highest frequency of concern
Thermal viaConducts heat from a component's thermal pad into the inner or bottom copperArrays under exposed pads of QFNs, regulators, LEDs, and power MOSFETsPad size, heat load, and solder-wicking limits
Shielding via (via fence)Confines fields around a trace or circuit to reduce coupling and emissionRows along RF or high-speed traces and around sensitive circuitsWavelength, typically λ/20 or tighter

Core Functions of Via Stitching in PCB Layout

In PCB layout, there are three primary functions of via stitching. It manages EMI, minimizes the impedance between ground layers, prevents plane-cavity resonance, dissipates heat, and ensures power integrity. The electrical functions are the primary ones, with heat spreading as a secondary effect.

Minimizing EMI with Via Stitching and Via Fences

A via fence is a line of vias that are connected to ground along a trace or around a circuit. Every segment between two vias acts as an aperture in a shield and radiates efficiently when it is nearly half a wavelength long.

Gary Fenical's aperture rule of thumb is that the shielding effectiveness of a single slot of length L is approximately SE = 20·log10(λ/2L) dB. It was applied to a gap in a fence and provided these estimates:

  • Gap of λ/10: about 14 dB for a single gap.
  • Gap of λ/20: about 20 dB for a single gap.
  • Several gaps: the estimate decreases by 20·log10(n) when n gaps lie within half a wavelength, so a long fence shields less than one gap would suggest.

According to the same source, apertures should be chosen to be smaller than λ/50, but no larger than λ/20. These figures are for comparison of pitches only and do not indicate a result in an emissions test.

There are 3 common locations for the use of fences:

  • RF and high-speed traces: Coupling into adjacent traces is minimized by a fence tied to the plane below, on each side of the trace.
  • Grounded coplanar waveguide: The fence is used to lower the coplanar ground to the plane potential to ensure that the unwanted parallel plate modes between the two ground layers are suppressed.
  • Noisy circuits: A ring around a switching regulator or clock generator limits field coupling into analog circuits.

Via Stiching Guide Oct 1. (3)

Figure 3: Via fence on both sides of a high-speed microstrip trace, with the fence pitch marked as a fraction of wavelength.

Reducing Ground Impedance Between Inner Layers

Stitching reduces the impedance between ground layers by using multiple parallel vias in series. A 1 GHz connection with the 8 Ω connection is made through ten 1.3 nH vias that are a large distance apart so that the mutual inductance is small.

A cavity is created by two parallel ground planes or a plane and a large pour. The cavity is allowed to couple noise between the vias that pass through it at resonance. The cavity is broken up into smaller cells by a stitching grid, which increases the lowest resonance.

There are three layout settings to accommodate this:

  • Direct connection: Make stitching vias directly connected to planes and pours, since the thermal-relief spokes introduce inductance.
  • All ground layers: Stitch each stitching to all ground layers that it passes through.
  • No floating copper: Stitch or remove isolated areas of ground, as floating copper can lead to noise coupling between nearby traces.

Best Practices for Via Stitching Placement

The stitching placement begins with the highest frequency the board must have. Take that frequency and calculate the wavelength in the dielectric, and use a fraction of that as the maximum pitch. Edge rules and over-stitching then refine the grid.

Via Stitching Pitch and Spacing Rules for High-Speed Signals

There is no one-size-fits-all solution when it comes to pitch. The distance between maximum points is suggested to be < λ/8 and < λ/20 of the wavelength at the highest frequency of interest:

  • λ/8: Writing in EDN, Steve Hageman says that if the ground vias are spaced 1/8 λ or less, the ground plane acts as a solid ground.
  • λ/10: A common general-purpose limit for ground stitching in fabricator and design guides.
  • λ/20: The common rule of thumb for via fences and shielding, consistent with Fenical's limit for apertures.

The pitch for a specific board follows four steps:

  1. Find the highest frequency of concern. For digital signals, estimate bandwidth from the 10–90% rise time with f ≈ 0.35 / tr; a 100 ps edge gives 3.5 GHz.
  2. Calculate the wavelength in the dielectric. Use λ = c / (f × √Dk). For stripline, use the laminate Dk.
  3. Choose the fraction. Use λ/10 for general ground stitching, and λ/20 for via fences and board edges.
  4. Check the result against the fabricator's limits. Confirm the minimum via size and hole-to-hole spacing before committing to a dense grid.
Highest FrequencyWavelength in FR4, Dk 4.2 (mm)λ/10 Pitch (mm)λ/20 Pitch (mm)
1 GHz14614.67.3
2.4 GHz616.13.0
5 GHz29.32.91.5
10 GHz14.61.50.73

The effective Dk for microstrip is less than that of the laminate and is typically 3.2-3.3 for a 50 Ω line on FR4 laminate. A shorter wavelength, and hence a conservative pitch, is obtained with the laminate Dk.

Via Stiching Guide Oct 1. (6)

Figure 4: Via stitching pitch versus frequency on FR4, comparing λ/10 and λ/20 spacing

Edge Via Stitching Rules for Board-Level EMI Control

Edge is a stitching method that lays a row of ground vias along the board edge, thereby joining all ground layers at that edge. It helps to reduce fields radiating between pairs of planes along the board edge, which are a major source of radiation at high frequencies.

The rules of the edge ring are 5-fold:

  • Pitch: λ/20 at the highest frequency of concern (same as via fence).
  • Layers: Connect the ring to all ground layers, and connect a ground pour strip around the outside of the top layers, to allow vias to connect to copper.
  • Setback: Copper distance from the routed edge is at least 0.2 mm (8 mil), and the V-cut edge is 0.4 mm (16 mil), according to JLCPCB's capabilities.
  • Continuity: Stitch in the same direction around ring openings and cut-outs, and don't break the stitching inside the ring.
  • Power planes: If possible, place power planes between ground planes, as stitching cannot connect a power plane to a ground plane. A power plane sandwiched between two edge-stitched ground planes has less radiation leakage from the edges.

Via Stiching Guide Oct 1. (2)

Figure 5: Edge via stitching ring along a PCB perimeter, with the copper setback from the routed edge marked.

Avoiding Signal Degradation from Over-Stitching

Over-stitching provides more vias than needed by return paths and fields. This reduces the power planes, alters the impedance of adjacent traces, and introduces drill count, so stitching vias should be stitched in where a return path or a fence is required.

Over-Stitching EffectMechanismLayout Fix
Perforated power planesEach through via crossing a power plane needs an antipad, a clearance opening in the plane copper, and dense rows of antipads merge into a slotUse the pitch the frequency requires, and no tighter, and stagger rows
Shifted trace impedanceGround pour, and vias close to a trace add capacitance, which turns a microstrip into a grounded coplanar waveguideInclude the pour and fence in the field-solver model, or widen the gap
Routing blockageVia grids occupy inner-layer routing channelsKeep channels clear under dense routing areas
Drill count and costMore holes and smaller drill lengths lengthen drilling timeUse the pitch the frequency requires, with 0.3 mm or larger holes, where the pitch allows

JLCPCB (0.2 mm inner-layer via-to-copper clearance) will clear a 0.7 mm (28 mil) circle in a power plane with a 0.3 mm (12 mil) via. The copper webs between antipads are 0.3 mm (12 mil) wide, at 1 mm (39 mil) pitch.

Via Stiching Guide Oct 1. (4)

Figure 6: Comparison showing antipads in a power plane at 1 mm pitch and merging into a slot at 0.75 mm pitch.

Manufacturing High-Density Via Stitching Boards

These dense via-stitching arrays create three design-for-manufacturability (DFM) concerns: drill-position error when drilling small holes, thin or cracked barrel plating when drilling deep holes, and narrower solder-mask dams than the fabricator's minimum. Each design decision is performed before release.

Drilling Accuracy and Layer Registration for Dense Via Arrays

Position errors in the holes during drilling and layer-to-layer registration errors both cause the holes to be displaced relative to the pads. The annular ring in each layer must absorb that energy transfer; otherwise, the drill can break out of the pad.

JLCPCB's PCB capabilities page lists these drilling capabilities for vias:

  • Minimum via: 0.15 mm hole with a 0.25 mm pad; 0.1 mm or 0.2 mm is available only for boards 1 mm thick or less with an ENIG or OSP finish.
  • Surcharge: 0.1 or 0.15 mm holes at any pad size, and 0.2 or 0.25 mm holes with pads under 0.45 mm cost more.
  • Hole position tolerance: ±0.075 mm.
  • Via hole-to-hole spacing: 0.2 mm.
  • Via hole to track: 0.2 mm.

A 0.25/0.15 mm via does not leave much room for drill-position errors, as it allows only a 0.05 mm annular ring. A 0.3 mm (12 mil) hole in a 0.6 mm (24 mil) pad leaves a 0.15 mm ring and avoids both surcharges.

Hole Wall Plating Thickness and Barrel Reliability

The thickness of the barrel plating will influence whether the stitching via cracks during repeated thermal cycling. All of the expansion in the barrel is due to the laminate's expansion through its thickness compared to copper, and it occurs with every reflow and temperature cycle.

A common lead-free FR4 material, Isola 370HR, has a Z-axis expansion rate of 45 ppm/°C below its Tg and 230 ppm/°C above its Tg. Copper has an expansion rate of approximately 17 ppm/°C, causing the barrel to stretch and potentially crack thin plating, usually in the middle of the hole.

Three design features protect the barrel:

  • State the class: IPC-6012F defines the minimum copper thickness for each performance class, and Class 3 has a thicker copper wall than Class 2. Indicate the class on the fabrication drawing.
  • Understand the default value: JLCPCB provides an average hole plating thickness of 18µm.
  • High aspect ratio: Plating solution does not flow as easily into high-aspect-ratio holes. A 0.3 mm hole in a 1.6 mm board is about 5:1, while a 0.15 mm hole is nearly 11:1.
Ready to Bring Your PCB Ideas to Life?

Turn designs into working hardware with expert fabrication, assembly, and component services from a trusted industry leader. Upload your files, choose your options, and get boards that are ready to test, ready to ship, and ready to scale.

Get Quote Now >

DFM Checks for Solder Mask Dams and Via Tenting'

When a stitch array is dense and near a pad, the solder mask will form narrow dams between openings. If it's smaller than the fabricator's minimum solder mask bridge, a dam is not reliable, and solder can flow from a pad to an exposed via.

DFM CheckJLCPCB CapabilityRelevance to Via Stitching
Minimum pad spacing that keeps a mask dam, 1 oz copper0.10 mm (green, red, yellow, blue, purple); 0.13 mm (black, white)A narrower gap between a pad and an exposed via loses its dam
Minimum pad spacing that keeps a mask dam, 2 oz copper0.20 mm (any color)Thicker copper needs a wider gap
Via plugging with solder maskVia 0.5 mm or smaller, no mask opening on either side, at least 0.35 mm from other openingsPlugged stitching vias near pads must respect the opening clearance
Copper to routed or V-cut edgeAt least 0.2 mm or 0.4 mmEdge stitching rings must respect the setback
Inner-layer via hole to copper0.2 mmSets the antipad size and the web width between vias

Four checks complete the DFM review:

  • Tent stitching vias: Cover vias that are not test points with solder mask (via tenting) to remove the mask openings that create narrow dams.
  • Keep exposed vias out of pads: Place vias in pads only with a via-in-pad process that fills and caps them.
  • Run DRC with fabricator rules: Check hole-to-hole spacing, via-to-track clearance, mask dam width, and edge setback before export.
  • Verify the Gerber output: The Gerber solder mask layer, not the EDA setting, defines which vias are tented.

FAQs About Via Stitching

Q: How Many Stitching Vias Does a PCB Need?

No fixed count applies because the count follows from the pitch and the area. A 100 mm square pour stitched on a 7.3 mm grid, λ/20 at 1 GHz in FR4, needs about 200 vias.

Q: Should Stitching Vias Be Tented?

In most designs, yes. Tenting removes the mask openings that create narrow dams between stitching vias and nearby pads. Leave a via exposed only when it serves as a test point.

Q: Do Stitching Vias Need Thermal Relief Connections?

No. Stitching vias need a direct, solid connection to planes and pours, because thermal-relief spokes add inductance. Thermal reliefs belong on component pads, where they limit heat sinking during soldering.

Q: Can Blind or Buried Vias Be Used for Via Stitching?

Yes. Blind and buried vias stitch only the layers they span, which keeps routing channels free on other layers. They add fabrication cost, so through-vias remain the usual choice when every ground layer must be bonded.

Conclusion

Stitching is effective when its pitch matches the wavelength at the board's highest frequency and when the vias are located where return current and fields are required. Measure the pitch within the dielectric, then use λ/10 for general stitching, and λ/20 for via fences and board edges, and add a return via at any place where the signal changes ground reference.

This stitching array reduces the ground impedance and edge radiation without destroying power planes or routing channels. After your fabricator approves the array for drilling, plating, and solder mask, upload your Gerber files to receive an instant quote.

Keep Learning