Step-by-Step Guide to Create Custom PCB Footprints
5 min
If you need a PCB footprint, but it does not exist in EasyEDA's component library, then you can create it yourself. And creating a device also requires a footprint library to complete. The usage method of the footprint library tool is the same as that of the PCB tool under PCB, but there are some unnecessary functions in the toolbar.
The footprint library is the various parameters of electronic components, chips, etc. (such as the size of components, length and width, in-line, patch, pad size, length and width of pins, spacing between pins, etc.) in a graphical way. Manifested so that it can be called when drawing the PCB. Creating a footprint library is almost identical to creating a symbol library. EasyEDA, a popular online PCB design tool, simplifies the process of creating custom footprints with its intuitive interface. In this guide, we’ll walk you through the step-by-step process of creating custom PCB footprints in EasyEDA. See more detail about electrical schematics design, from our latest blog.
PCB Pad Design and Development of Footprint?
PCB design and development involve creating the board’s layout, selecting the appropriate components, and designing the interconnections between them. Different components come with different pin configurations, numbers and package types. The uncovered metal area on an electrical circuit board where the factor lead has been soldered is known as the PCB pad. Aligning these pads together creates the component footmark PCB design model. The pad design involves two main factors:
- Symbol design
- Footprint design
We are using EasyEDA for the design because of its open source library and online environment.
Symbol Design:
Launch EasyEDA and go to the Schematic Editor. Open the Symbol Editor on the top menu, click on Libraries > Create Symbol.
- Use the drawing tools like Rectangle, Line, and Pin from the left toolbar to create the visual representation of your component.
- Add pins by selecting the "Pin" tool and placing them on your symbol. Make sure to number them according to your component’s datasheet.
- Label the pins with pin numbers and names to match the component’s specifications.
- Right-click the symbol and choose Properties. Here, you can enter the name, description, and other properties like reference designators (e.g., R for resistors, C for capacitors).
- Once your symbol is complete, click on Save and name your symbol appropriately. It will be saved to your personal library.
Footprint Design:
Step 1: Gather Component Data
Before you begin, collect the following data for the component:
- Datasheet: This provides the pin layout, dimensions, and other critical details.
- Mechanical Drawing: Look for the package type (e.g., SOIC, QFN, or TO-220).
- Pin Configuration: Verify the pin count and numbering.
- Recommended Footprint: Most datasheets include a recommended PCB layout.
Step 2: Open EasyEDA and Start a New Footprint
- Log in to your EasyEDA account and navigate to the "Library" section.
- Click “Create New Footprint” to open the footprint editor. This is where you’ll design the layout.
Step 3: Define the Basic Settings
- Name Your Footprint: Assign a descriptive name that corresponds to the component (e.g., “Custom-TO-220”).
- Unit Settings: Set the unit to millimeters (mm) or inches, depending on the datasheet.
- Grid Size: Adjust the grid size to match your design requirements. Smaller grids (e.g., 0.1 mm) are ideal for precise placement.
Step 4: Draw the Pad Layout
- Add Pads: Use the “Pad” tool to place pins on the editor canvas.
- Position Pads Accurately: Refer to the datasheet for exact coordinates and spacing. Adjust the pad size and shape (circular, rectangular, or oval) as specified.
- Number the Pads: Double-click each pad to assign the corresponding pin number from the datasheet.
Step 5: Define the Silkscreen Outline
The silkscreen layer provides visual cues for assembly.
- Use the “Line” tool on the silkscreen layer to draw the component outline.
- Include alignment markers or notches to indicate pin 1 or orientation.
- Add labels such as the part number or other identifying information.
Step 6: Add Courtyard and Assembly Layers
The courtyard defines the space the component occupies, ensuring no overlap with neighboring parts.
- Switch to the Courtyard Layer and draw a rectangle around the pads and outline.
- Ensure the courtyard is slightly larger than the component dimensions.
Step 7: Validate and Save the Footprint
- Use the “Design Rule Check (DRC)” tool to verify that your footprint adheres to standard PCB design rules.
- Save the footprint to your personal library with a unique name.
Step 8: Test the Footprint in a PCB Design
- Open or create a schematic in EasyEDA.
- Associate your custom footprint with the corresponding component.
- Place the component in the PCB layout to ensure proper fit and alignment.
Tips for Accurate Custom Footprints
- Double-Check Measurements: Verify all dimensions against the datasheet before finalizing.
- Follow IPC Standards: Use IPC-7351 guidelines for footprint design when in doubt.
- Test with a Prototype: Print the footprint on paper to check against the actual component.
Conclusion
Creating custom PCB footprints in EasyEDA is a straightforward process once you understand the basics. With the right datasheet and careful attention to detail, you can design footprints that ensure accurate and reliable PCB designs. Mastering this skill opens the door to handling a wide range of components, from common to custom-made parts, enhancing your PCB design capabilities.
Start designing today and unlock the full potential of your EasyEDA projects!
Popular Articles
• GPT-6 Astra PCB Design in EasyEDA Pro: What Worked, What Failed, and What We Learned
• Altium MCP with Claude Code: From Setup to PCB Design
• KiCad MCP: How to Design a PCB with Claude Code [Step-by-Step]
• Altium MCP: AI PCB Design with GPT-6 and Codex [Step-by-Step Guide]
• AI PCB Design: From Prompt to PCB with EasyEDA Pro
Keep Learning
Choosing the Right PCB Shape
key takeaway Choose a PCB shape based on layout, space, and application requirements. Consider edge clearance, cutouts, and manufacturing feasibility early. Select suitable routing and panelization methods for reliable production. Work with JLCPCB to turn custom PCB designs into manufacturable products. Selecting the right PCB shape is an important part of electronic product design. Beyond determining how a circuit board fits inside an enclosure, its geometry also affects component placement, signal r......
Designing Durable Custom Keyboard PCBs: Tailored Solutions and Expert Fabrication
So what's a keyboard PCB? In simple terms, it is the printed circuit board that is contained in the center of any keyboard, connecting the key switches to the controller, which communicates with your computer. Hitting a key closes a circuit on the PCB, which the controller records what key it was and transmits that keycode back to your host device. The mechanical-keyboard community is a subculture that has developed out of a niche hobby to become a successful subculture in the mechanical-keyboard worl......
GPT-6 Astra PCB Design in EasyEDA Pro: What Worked, What Failed, and What We Learned
Key Takeaways What was tested: GPT-6 Astra was given access to a native EasyEDA Pro 3.2.149 installation and asked to design a stereo TPA3116D2 amplifier from a four-line written brief. What it produced: The run resulted in a 44 × 34 mm, two-layer PCB with 40 SMD components and an editable native EasyEDA Pro project with embedded libraries. Where it failed: The first complete import opened cleanly and looked plausible, yet the initial native verification reported 50 association mismatches involving 12......
Claude Code PCB Design: Can It Build a Real Board in EasyEDA Pro?
Key Takeaways Claude Code PCB design: Using Claude Opus 5.5 and EasyEDA Pro 3.2.149, I converted a 47-component, three-page schematic from a PDF into a fully routed, two-layer PCB with zero DRC errors. EasyEDA Pro integration: The EasyEDA API skill connects Claude Code to EasyEDA Pro through a local bridge server and the Run API Gateway extension. This allows Claude to control the editor via JavaScript, with a 30-second timeout per API call. Design verification: A successful API response doesn't alway......
Guide to PCB Via Design: Best Practices, Tips, and Key Considerations
High-quality PCB design not only requires innovative concepts but also relies on a deep understanding of PCB manufacturing processes. Via design, as one of the critical steps in PCB design, is crucial for both PCB performance and manufacturing efficiency. Can vias be designed in any size? To answer this question, let’s first understand how holes on a PCB are created. 1. Cutting the Material: PCB manufacturers use automatic cutting machines to slice large copper-clad laminates into substrates of specif......
AI PCB Design: From Prompt to PCB with EasyEDA Pro
Key Takeaways AI PCB design uses AI agents to automate schematic creation, component selection, layout, and verification inside a real EDA editor — not just generate images. The workflow connects EasyEDA Pro to an AI coding agent (Claude Code or Codex) through the EasyEDA API Gateway, the open-source API Skill, and a local bridge server. Setup takes about ten minutes and is fully local-first: designs, API calls, and intermediate code never leave your machine. Because the agent places real library part......