Choosing the Right PCB Shape
10 min
- Rectangular PCB Shape: The Classic Choice
- Circular PCB Shape: Optimal for Compact Designs
- Triangular PCB Shape: Precision and Space Efficiency
- Irregular PCB Shapes: Tailored for Specific Applications
- Other PCB Shapes: Specialized Applications
- PCB Shape Design and Manufacturing Considerations
- Conclusion
key takeaway
- Choose a PCB shape based on layout, space, and application requirements.
- Consider edge clearance, cutouts, and manufacturing feasibility early.
- Select suitable routing and panelization methods for reliable production.
- Work with JLCPCB to turn custom PCB designs into manufacturable products.
Selecting the right PCB shape is an important part of electronic product design. Beyond determining how a circuit board fits inside an enclosure, its geometry also affects component placement, signal routing, mechanical integration, and manufacturing requirements.
While rectangular PCBs remain the most widely used option due to their straightforward layout and manufacturing advantages, circular, triangular, and irregular-shaped boards are better suited to certain space-constrained or application-specific designs.
This guide explores common PCB shapes, their practical applications, and the key design considerations involved in manufacturing them. It also explains how board outlines, routing, and panelization influence the production of custom-shaped PCBs.
Rectangular PCB Shape: The Classic Choice
Rectangular PCBs are the tried-and-true choice across a wide range of industries. Their regular geometry simplifies board layout, component placement, signal routing, and integration into standardized enclosures.
The straight edges and right-angle corners also make rectangular boards relatively straightforward to manufacture and panelize. During PCB fabrication, the board outline can be processed using CNC routing or V-scoring, depending on the panel design and separation requirements. For applications requiring multiple boards to be processed together, rectangular PCBs are generally easier to arrange in regular panel configurations.
For example, laptops commonly use rectangular PCBs to accommodate processors, memory, storage devices, and power management circuits within a defined enclosure. Their geometry provides a practical balance between available board space, component arrangement, and mechanical integration.
However, the rectangular shape is not always the most space-efficient option. When a product has a circular housing, curved enclosure, or other non-standard mechanical constraints, a custom PCB outline may provide a better fit.
Circular PCB Shape: Optimal for Compact Designs
Circular PCBs are particularly useful in products with round housings or rotationally symmetrical structures. Their geometry allows the board outline to follow the shape of the enclosure, making them suitable for compact devices such as smartwatches, fitness trackers, LED lighting products, and certain medical electronics.
Unlike rectangular boards, circular PCBs can distribute available layout space around a central area. This arrangement may be useful when positioning sensors, indicator LEDs, connectors, or other components around a central mounting point.
However, mechanical reliability depends on more than board geometry. Mounting-hole locations, PCB thickness, material selection, enclosure support, and external mechanical loads must all be considered during design.
From a manufacturing perspective, circular board outlines are generally produced using CNC routing rather than conventional V-scoring. For multiple circular boards, panelization must also account for board spacing, tooling edges, and the requirements of the selected separation method.
For example, JLCPCB specifies a minimum single-board size of 20 × 20 mm for its circular PCB panelization option. Stamp holes and tooling strips are used to support the panel structure and subsequent separation.
Triangular PCB Shape: Precision and Space Efficiency
Triangular PCBs are useful for electronic products with triangular housings, angled mounting spaces, or geometric design requirements. Their non-rectangular outlines allow designers to adapt the board to specific enclosure shapes and make use of areas that may be difficult to accommodate with conventional rectangular boards.
One example is LED lighting. A triangular PCB can be designed to match the geometry of a lighting fixture, allowing LED modules and their associated driver circuits to be positioned according to the required illumination layout. However, lighting performance and energy efficiency depend primarily on LED selection, drive conditions, thermal management, and optical design rather than PCB shape alone.
When designing triangular PCBs, engineers should pay particular attention to component clearances near the board edges, mounting-hole positions, and the routing paths required for manufacturing. Sharp corners and narrow sections may also affect mechanical strength and material utilization during production.
Irregular PCB Shapes: Tailored for Specific Applications
Irregular PCB shapes are designed to meet specific mechanical and spatial requirements that standard rectangular boards cannot always accommodate. They are commonly used in products with complex enclosures, curved internal boundaries, restricted installation areas, or multiple mounting points.
Automotive electronics provide a typical example. Instrument clusters, dashboard control systems, and infotainment modules may require custom-shaped PCBs to fit around displays, connectors, structural supports, and other internal components.
Manufacturing these boards requires careful attention to the PCB outline and its mechanical features. CNC routing is commonly used to create irregular external contours, internal cutouts, and slots. Designers should also ensure sufficient clearance between copper features and routed edges to prevent exposed copper or unwanted damage during edge processing.
For example, JLCPCB specifies a minimum copper-to-routed-edge clearance of 0.2 mm and a minimum copper-to-routed-slot clearance of 0.2 mm for its standard PCB routing process. These requirements should be considered when defining board outlines and internal cutouts.
Panelization is another important consideration. Irregular boards may not fit efficiently into standard rectangular panel arrangements, so their placement, spacing, tooling edges, and separation tabs should be evaluated before production. Boards with irregular shapes or large aspect ratios may also require additional manufacturability review.
Other PCB Shapes: Specialized Applications
Beyond conventional rectangular, circular, triangular, and irregular designs, several specialized PCB shapes are used to meet particular product and system requirements.
Hexagonal PCBs
Hexagonal PCBs can be used in modular electronic systems and antenna array structures where repeated geometric arrangements are required. Their six-sided geometry allows multiple boards or antenna modules to be arranged in a structured pattern. However, antenna performance depends on factors such as element spacing, operating frequency, feed network design, and electromagnetic coupling, rather than board shape alone.
Curved and Flexible PCBs
Products with curved surfaces, such as automotive displays and wearable electronics, may require circuit boards that follow non-flat mechanical contours. Flexible PCBs (FPCs) are particularly suitable for applications where the circuit must bend or fold within a specified mechanical design. Rigid-flex PCBs can also combine rigid component-mounting sections with flexible interconnections.
When designing flexible circuits, engineers must consider the minimum bending radius, copper-layer construction, material properties, and whether the bend is static or dynamic. A conventional rigid PCB should not be assumed to support repeated bending simply because its outline follows a curved shape.
Star-Shaped PCBs
Star-shaped PCBs may be used in specialized products that require a central section with multiple outward extensions. These extensions can accommodate distributed sensors, connectors, or other functional modules. Their layout should be determined by electrical connectivity, component placement, and mechanical constraints rather than the geometric shape alone.
PCB Shape Design and Manufacturing Considerations
CNC Routing vs. V-Cut: Choosing the Right Outline Process
The PCB outline processing method should be selected according to the board geometry and panel separation requirements.
CNC routing uses a rotating cutting tool to follow a programmed path, making it suitable for irregular contours, circular boards, internal cutouts, and routed slots. It provides greater flexibility when manufacturing boards with complex external profiles.
V-Cut, also known as V-scoring, creates V-shaped grooves along straight separation lines in a PCB panel. It is commonly used for separating rectangular or other boards with compatible straight edges. Unlike CNC routing, V-Cut cannot follow curved or irregular contours.
When selecting an outline process, designers should consider the board shape, copper clearance, panel layout, board thickness, and final separation requirements.
PCB Edge Clearance and Mechanical Design
PCB edge clearance is an important design consideration, particularly for boards with irregular outlines, narrow sections, and internal cutouts.
Copper traces, pads, and other conductive features should maintain sufficient clearance from routed edges to avoid exposed copper after milling. The location of mounting holes and connectors should also be checked against the mechanical enclosure to prevent interference during assembly.
For JLCPCB standard routed PCBs, the minimum copper clearance from routed board edges and routed slots is 0.2 mm. For V-scored boards, the required copper clearance from V-cut edges is 0.4 mm.
These manufacturing requirements should be incorporated into the PCB layout before Gerber file generation to reduce the risk of fabrication issues.
| Manufacturing Parameter | JLCPCB Capability |
|---|---|
| Routed Edge Copper Clearance | ≥ 0.2 mm |
| Routed Slot Copper Clearance | ≥ 0.2 mm |
| Regular CNC Routing Tolerance | ±0.2 mm |
| High-Precision CNC Routing Tolerance | ±0.1 mm |
| V-Cut Edge Copper Clearance | ≥ 0.4 mm |
| V-Cut Dimension Tolerance | ±0.4 mm |
| Minimum Panel Size for V-Cut | 70 × 70 mm |
| Maximum Panel Size for V-Cut | 475 × 475 mm |
| Panel Spacing (with spacing) | ≥ 2 mm |
Panelization for Custom-Shaped PCBs
Panelization combines multiple individual PCBs into a larger production panel, helping improve manufacturing and assembly efficiency.
For custom-shaped PCBs, panelization requires additional consideration of board spacing, connecting tabs, tooling edges, and the selected separation method. CNC routing with breakaway tabs or mouse bites can be used to connect individual boards within a panel, while V-Cut is suitable for compatible straight separation lines.
For JLCPCB panelization, the spacing between boards in a panelized design with spacing should be at least 2 mm. When using mouse-bite connections, the recommended hole diameter is 0.5–0.8 mm, with a recommended spacing of 0.2–0.3 mm between adjacent mouse bites.
A suitable panel design helps maintain board stability during manufacturing and provides a more practical structure for subsequent PCB assembly and separation.
| PCB Shape | Typical Applications | Recommended Manufacturing Considerations |
|---|---|---|
| Rectangular | Computers, control boards, consumer electronics | CNC routing or V-scoring, depending on panel design |
| Circular | Wearables, LED lighting, compact devices | CNC routing and suitable panelization |
| Triangular | Specialized lighting, geometric enclosures | CNC routing and careful edge clearance |
| Irregular | Automotive electronics, custom enclosures | CNC routing, internal cutouts, and mechanical verification |
| Hexagonal | Modular systems, antenna arrays | CNC routing and geometric panel arrangement |
| Curved/Flexible | Wearables, curved electronic assemblies | FPC or suitable mechanical integration design |
| Star-shaped | Specialized control systems, distributed modules | CNC routing and customized panel design |
Conclusion
Choosing the right PCB shape involves more than matching a circuit board to an enclosure. Designers must also consider component placement, electrical layout, mechanical requirements, edge clearance, and manufacturing feasibility.
From conventional rectangular boards to circular and irregular-shaped designs, each PCB geometry presents different opportunities and manufacturing considerations. Selecting an appropriate outline process, maintaining sufficient copper clearance, and planning panelization are essential steps toward reliable PCB production.
With CNC routing, V-cut processing, and customized panelization options, JLCPCB supports a range of PCB outline and production requirements. By following the relevant design specifications and manufacturing guidelines, engineers can turn custom PCB shapes into production-ready circuit boards.
Popular Articles
• GPT-6 Astra PCB Design in EasyEDA Pro: What Worked, What Failed, and What We Learned
• Altium MCP with Claude Code: From Setup to PCB Design
• KiCad MCP: How to Design a PCB with Claude Code [Step-by-Step]
• Altium MCP: AI PCB Design with GPT-6 and Codex [Step-by-Step Guide]
• AI PCB Design: From Prompt to PCB with EasyEDA Pro
Keep Learning
Choosing the Right PCB Shape
key takeaway Choose a PCB shape based on layout, space, and application requirements. Consider edge clearance, cutouts, and manufacturing feasibility early. Select suitable routing and panelization methods for reliable production. Work with JLCPCB to turn custom PCB designs into manufacturable products. Selecting the right PCB shape is an important part of electronic product design. Beyond determining how a circuit board fits inside an enclosure, its geometry also affects component placement, signal r......
Designing Durable Custom Keyboard PCBs: Tailored Solutions and Expert Fabrication
So what's a keyboard PCB? In simple terms, it is the printed circuit board that is contained in the center of any keyboard, connecting the key switches to the controller, which communicates with your computer. Hitting a key closes a circuit on the PCB, which the controller records what key it was and transmits that keycode back to your host device. The mechanical-keyboard community is a subculture that has developed out of a niche hobby to become a successful subculture in the mechanical-keyboard worl......
GPT-6 Astra PCB Design in EasyEDA Pro: What Worked, What Failed, and What We Learned
Key Takeaways What was tested: GPT-6 Astra was given access to a native EasyEDA Pro 3.2.149 installation and asked to design a stereo TPA3116D2 amplifier from a four-line written brief. What it produced: The run resulted in a 44 × 34 mm, two-layer PCB with 40 SMD components and an editable native EasyEDA Pro project with embedded libraries. Where it failed: The first complete import opened cleanly and looked plausible, yet the initial native verification reported 50 association mismatches involving 12......
Claude Code PCB Design: Can It Build a Real Board in EasyEDA Pro?
Key Takeaways Claude Code PCB design: Using Claude Opus 5.5 and EasyEDA Pro 3.2.149, I converted a 47-component, three-page schematic from a PDF into a fully routed, two-layer PCB with zero DRC errors. EasyEDA Pro integration: The EasyEDA API skill connects Claude Code to EasyEDA Pro through a local bridge server and the Run API Gateway extension. This allows Claude to control the editor via JavaScript, with a 30-second timeout per API call. Design verification: A successful API response doesn't alway......
Guide to PCB Via Design: Best Practices, Tips, and Key Considerations
High-quality PCB design not only requires innovative concepts but also relies on a deep understanding of PCB manufacturing processes. Via design, as one of the critical steps in PCB design, is crucial for both PCB performance and manufacturing efficiency. Can vias be designed in any size? To answer this question, let’s first understand how holes on a PCB are created. 1. Cutting the Material: PCB manufacturers use automatic cutting machines to slice large copper-clad laminates into substrates of specif......
AI PCB Design: From Prompt to PCB with EasyEDA Pro
Key Takeaways AI PCB design uses AI agents to automate schematic creation, component selection, layout, and verification inside a real EDA editor — not just generate images. The workflow connects EasyEDA Pro to an AI coding agent (Claude Code or Codex) through the EasyEDA API Gateway, the open-source API Skill, and a local bridge server. Setup takes about ten minutes and is fully local-first: designs, API calls, and intermediate code never leave your machine. Because the agent places real library part......