Free Online Circuit Simulator for Electronics Engineers
13 min
- Why LTspice?
- Getting Started with LTspice
- The Amplifier Example: NPN BC547
- Building the Circuit in LTspice
- Running the Simulation
- Why This Matters for PCB Engineers
- Advantages of LTspice for Students and Engineers Include
- Common Pitfalls in LTspice
- Summary of BC547 Amplifier Simulation Results
- FAQs about Online Circuit Simulator
- Conclusion
Key Takeaways
- Simulate First: Free circuit simulators prevent fried components and cut PCB re-spins.
- Fix AC Sweep: Enter pure numbers for points per decade, not time units.
- Use SMD Parts: Swap ideal models for standard SMD resistors and SOT-23 transistors.
- Control Parasitics: Board trace capacitance and via inductance alter high-frequency signals.
- Verify Before Order: Pair SPICE simulation with DFM checks to ensure board success.
If all electronic engineers had a dollar for each burnt-out resistor or fried transistor during physical prototyping, most of us would not be debugging circuits today—we would be sipping coffee on a sunny beach! Thankfully, using a modern circuit simulator allows us to validate electronic designs virtually before taking them to the hardware test bench. With proper SPICE simulation, we ensure no smoke, no component destruction, just smooth signal curves and precise waveforms.
Among the wide variety of circuit simulator tools available today, LTspice stands out as a powerful desktop industry standard due to its speed, free availability, and accuracy. For web-based online workflow, tools like EasyEDA (integrated directly with JLCPCB) also provide seamless browser-based SPICE simulation. Whether you are an engineering student or a professional PCB design engineer, using a circuit simulator makes it easy to analyze AC/DC behavior with just a few clicks. Best of all, once your simulation is validated, you can effortlessly turn your schematics into high-quality physical PCBs with JLCPCB, a trusted global PCB manufacturing leader. This article introduces LTspice fundamentals, walks through a common-emitter amplifier design featuring an NPN BC547 transistor, and demonstrates how simulation translates to physical PCB manufacturing.
Why LTspice?
LTspice is a high-performance, free SPICE-based circuit simulator developed by Analog Devices, widely utilized across educational institutions and professional engineering industries worldwide.
- Free and Cross-Platform: A small installation of LTspice is required for it to work on both Windows PCs and macOS-based machines.
- Fast and Accurate: It is designed to optimize simulation performance for both analog and mixed-signal circuits as well as large designs.
- Extensive Component Library: The software includes a library with plenty of common circuits, such as transistors, operational amplifiers, diodes, MOSFETs, and passive elements. Besides, LTspice is programmed to create your custom SPICE models.
- Capability for Advanced Analysis: LTspice supports both time-domain and frequency-domain simulations. It should be mentioned that it has a single-component noise analysis and a parametric sweep.
- Benefits for Professional Learning and Use: LTspice has a user-friendly interface with a convenient visualization of the circuit’s behavior. It decreases the number of PCB re-spins and validates designs before being physically prototyped.
In short, LTspice is an exceptional free and flexible tool that is the best option for professional circuit design and learning.
Getting Started with LTspice
Download & Install: Free to download directly from the official Analog Devices website.
Interface: Simple schematic editor with toolbar for resistors, capacitors, transistors, and power sources.
Simulation Types:
Simulation types are shown below.
Transient Analysis: Evaluates circuit time-domain responses and dynamic waveforms over a specified duration.
Path: Navigate to Simulate > Edit Simulation Command > Transient, and enter
DC Sweep (.dc): Analyzes how circuit DC operating points, node voltages, and branch currents change while sweeping an independent voltage or current source.
Path: Navigate to Simulate > Edit Simulation Command > DC Sweep, specify the source name, start/stop values, and increment step.
AC Analysis (.ac): Evaluates small-signal frequency response, voltage gain, and phase margin across a frequency spectrum.
Path: Navigate to Simulate > Edit Simulation Command > AC Analysis. Select Type of Sweep = Decade, enter an integer for Number of points per decade = 100 (Note: Do NOT enter time units like "5ms" here, as points per decade requires a pure integer count), Start Frequency = 1, and Stop Frequency = 1MEG
The Amplifier Example: NPN BC547
To demonstrate practical circuit simulator usage, we construct a classic Common-Emitter (CE) BJT voltage amplifier using the BC547 NPN transistor.
Circuit Architecture Overview:
Transistor: BC547 NPN general-purpose bipolar junction transistor.
Voltage Divider Bias (R1, R2): Establishes a stable DC operating (Quiescent) point at the base.
Collector Resistor (RC): Converts collector current variations into amplified output voltage.
Emitter Resistor & Bypass Capacitor (RE, CE): RE provides DC thermal stability, while CE bypasses AC signals to maximize AC voltage gain.
Coupling Capacitors (C1, C2): Block DC bias offsets between stages while passing AC signals.
Power Supply: VCC = +12 V DC.
Input Signal: 10 mV peak amplitude, 1 kHz sinusoidal wave.
Theoretical Simulation Parameters:
R1 = 17.576 kΩ (Upper base bias resistor)
R2 = 17.000 kΩ (Lower base bias resistor)
RC = 350 Ω (Collector load resistor)
RE = 1.040 kΩ (Emitter stabilization resistor)
C1 = C2 = 100μF (Input/Output coupling electrolytic capacitors)
CE = 300μF (Emitter bypass capacitor)
VCC = +12 V, Vin=SINE(0 0.01 1k)
Practical Hardware Tip for JLCPCB Assembly: When transitioning from SPICE simulation to physical PCB layout, exact theoretical values like 17.576kΩ or 1040Ω are substituted with standard E24/E96 SMD values available in the JLCPCB SMT component library—such as 17.4 kΩ (1%) or 18 kΩ , and 1 kΩ (1%). Likewise, the through-hole BC547 is often replaced by its SMD equivalent MMBT3904 or BC847 in SOT-23 packaging for automated SMT mounting.
Circuit Operation
The circuit employs a voltage divider bias network formed by R1 and R2 to establish a stable DC base voltage VB :
VB≈VCC× R2 / R1 + R2 ≈5.89V
Subtracting the base-emitter junction drop (VBE≈0.7V) yields the emitter voltage VE≈5.19 V. The DC emitter current is then IE = VE / RE≈5.19V / 1040Ω≈5.0 mA.The collector resistor RC sets the collector voltage VC = VCC- ICRC, keeping the BJT operating well within its linear active region. For AC signals, capacitor CE shorts RE to ground, driving the small-signal AC voltage gain to :
Av≈-RC/re where re=25mV / IE ≈5Ω is the internal dynamic emitter resistance. This results in significant voltage amplification with a 180° phase inversion at the output VOUT. Coupling capacitors C1 and C2 isolate external DC offsets, making this configuration ideal for audio processing and sensor preamplification.
Building the Circuit in LTspice
1. Create Schematic: Open LTspice and click File > New Schematic (Ctrl+N).
2. Add Components: Press F2 to open the Component Library. Search and place npn transistor, res, cap, and voltage
3. Wire Components: Press F3 to draw interconnections between terminals.
4. Add Ground Reference: Press G to place mandatory SPICE Ground (0) nodes; every SPICE circuit requires ground to calculate node voltages.
5. Configure Values & Directives: Right-click each component to assign resistance, capacitance, and voltage source values. Insert model directives such as .model NPN1 NPN(BF=150 VAF=100) using the Edit SPICE Directive tool (S).
Running the Simulation
Step 1: Bias Verification (DC Operating Point)
Before analyzing AC signals, we verify the DC bias conditions to ensure the transistor stays in the active linear region rather than saturation or cutoff. Running a DC Sweep (.dc VIN 0 5 0.1) sweeps VIN from 0 V to 5 V to observe node voltage transitions.
Results Verification: The simulation confirms VBE ≈ 0.7 V and IC ≈ 5.0 mA, establishing a stable quiescent Q-point (VCE ≈ 5.0 V). This guarantees undistorted AC amplification under rated signal levels.
Step 2: Transient Time-Domain Analysis
Transient analysis reveals how the amplifier responds to dynamic time-varying inputs. Applying a 1 kHz sinusoidal input with a 10 mV peak amplitude (Vin = SINE(0 0.01 1k)) yields the time-domain waveform shown below.
Results Verification: The output node (VOUT) displays a clean, amplified sinusoidal wave inverted by 180°relative to the input, as expected for a common-emitter amplifier. The absence of clipping confirms linear operation without distortion.
Step 3: AC Sweep & Frequency Response Analysis
AC sweep analysis evaluates amplifier gain and bandwidth across 1 Hz to 1 MHz.
Frequency Response Analysis:
Low-Frequency Cutoff ($f_L$): Gain rolls off at low frequencies due to the high reactance of coupling capacitors (C1, C2) and bypass capacitor (CE).
Mid-Band Region: Provides stable maximum voltage gain (Av,mid ≈20 dB to 36 dB, depending on dynamic emitter resistance re).
High-Frequency Cutoff (fH): Gain decreases at high frequencies due to transistor internal junction capacitances (CΠ , Cμ) and PCB stray capacitance.
Why This Matters for PCB Engineers
While SPICE simulation provides a mathematical guarantee of circuit performance, translating a schematic into a physical PCB introduces real-world physical constraints. Understanding how virtual simulation aligns with hardware design is essential for every PCB engineer:
1. Translating Ideal Models to Real-World SMD Components
In LTspice, component values like 17.576 kΩ or ideal 100 μF capacitors are common. However, physical manufacturing requires replacing these with commercial Surface Mount Devices (SMD). During layout, engineers select standard E24/E96 series resistor tolerances (1%) and SOT-23 footprints (such as substituting the through-hole BC547 with an MMBT3904). Checking the JLCPCB Component Library during schematic capture ensures that selected SMD parts are readily available for automated assembly, preventing redesigns due to component stockouts.
2. Accounting for PCB Parasitics and Frequency Response
In high-frequency or sensitive AC simulations, the physical PCB layout alters high-frequency response due to parasitic capacitance between copper traces, via inductances, and ground loop impedance. To closely mirror your LTspice AC sweep in physical hardware:
Keep high-impedance base traces as short as possible to minimize stray capacitance.
Use solid ground planes to reduce ground loop noise and return path inductance.
Place bypass capacitors (CE) adjacent to the transistor emitter pins.
3. Dual-Validation: Electrical Simulation + DFM Check
SPICE simulation verifies electrical functionality, but physical prototyping requires verifying manufacturing tolerances. Before placing an order for PCB prototypes, running a Design for Manufacturability (DFM) check using free tools like the JLCPCB DFM Checker verifies trace spacing, via drill limits, and annular ring tolerances. Combining SPICE simulation with rigorous DFM checks ensures that your physical boards perform on the bench exactly as predicted in LTspice.
Advantages of LTspice for Students and Engineers Include
- Risk-Free Prototyping: Test high-voltage, high-current, or complex analog ideas without blowing up real components or power supplies.
- Instant Visual Feedback: Observe voltage graphs and current node waveforms immediately.
- Complex System Modeling: Capable of simulating advanced Switch-Mode Power Supplies (SMPS), RF front-ends, and mixed-signal systems.
- Thriving Global Community: Access thousands of pre-built third-party LTspice models and community user guides online.
Common Pitfalls in LTspice
- Missing Ground Node (0): SPICE solvers cannot calculate relative node potentials without a ground reference, resulting in matrix errors.
- Ideal vs. Real Component Models: Omitting non-ideal parasitic elements (ESR, ESL, trace inductance) can make simulations look overly optimistic compared to measured physical PCB behavior.
- Unrealistic Parameter Values: Ensure component tolerances and power dissipation values match physical components selectable from JLCPCB's SMT library.
- Misinterpreting Convergence Errors: Tweak SPICE solver tolerances (Gmin, RelTol) when encountering timestep errors in non-linear simulations.
Summary of BC547 Amplifier Simulation Results
| Simulation Type | Purpose | Key Observation | Expected Result |
|---|---|---|---|
| DC Operating Point | To check the transistor bias and verify active region operation | Confirms correct biasing Vbe ≈ 0.7 V, Ic ≈ 1 mA | Stable operating point with proper transistor bias |
| Transient Analysis | To observe time-domain signal behavior | Shows amplified and inverted sine wave output | Clear amplification with 180° phase inversion |
| AC Sweep Analysis | To study frequency response and gain variation | Gain remains stable in the mid-frequency range | Mid-band gain ≈ 13–20 dB; bandwidth defined by cutoff frequencies |
FAQs about Online Circuit Simulator
Q: Is LTspice completely free, and can I run it as an online browser-based circuit simulator?
LTspice is a 100% free desktop application developed by Analog Devices for Windows and macOS rather than a browser-based tool. If you require a web-based circuit simulator that runs directly in your browser without installation, platforms like EasyEDA provide powerful online SPICE simulation capabilities while natively integrating with JLCPCB for seamless PCB layout and component selection.
Q: Why does my LTspice simulation report a syntax error during AC Sweep analysis?
AC Sweep syntax errors are typically caused by entering time-domain parameters into frequency-domain fields. In the AC Analysis setup window, the "Number of points per decade" field requires a pure integer like 100 or 10 rather than time units such as 5ms, which generate invalid SPICE directives like .ac dec 5ms... and crash the solver. Always input pure numbers and ensure your schematic contains a mandatory reference ground node.
Q: How do I transition my circuit simulation schematic into a physical PCB design?
Transitioning from a circuit simulator to physical hardware begins by replacing ideal SPICE models with actual physical footprints, such as swapping a through-hole transistor for an SOT-23 SMD equivalent like MMBT3904. You then select standard E24/E96 resistor values available in component libraries like the JLCPCB Parts Library, export the schematic netlist into your EDA editor to draw the board layout, and perform a Design for Manufacturability (DFM) check prior to ordering.
Q: Why does my actual physical PCB performance differ slightly from my SPICE simulation results?
While SPICE simulations model ideal component environments, physical hardware performance is affected by non-ideal factors like copper trace parasitic resistance and inductance, stray capacitance between adjacent PCB layers, component manufacturing tolerances, and temperature shifts. Keeping high-impedance traces short, adding dedicated ground planes, and placing low-ESR bypass capacitors near IC supply pins will help your physical PCB closely match your simulated waveforms.
Q: What should I check before submitting my PCB layout files for manufacturing?
Beyond validating electrical logic in your circuit simulator, you must ensure your physical layout abides by board fabrication limits. Run a Design Rules Check in your EDA tool to verify trace clearance, drill sizes, and edge margins, and upload your Gerber or EasyEDA files to JLCPCB to run automated DFM checks that detect manufacturing conflicts prior to PCB production and SMT assembly.
Conclusion
In today’s electronics design, circuit simulation is an indispensable process that allows engineers to assess the functionality of their circuits and optimize them before creating physical prototypes. From the above results, we have successfully used LTspice to verify that our BC547 common-emitter amplifier operates correctly by conducting DC, transient, and AC analyses, which confirmed that our circuit was correctly biased, had a stable amplification level, and responded to the signal at expected frequencies. The fact that our results followed the steps that professionals use in their designs means that this method could substantially reduce errors and enhance the resulting circuit performance. Based on the above experience, the free versions of LTspice and other simulators offer a powerful, reliable, and accurate way that leads to the development and validation of perfect electronic designs.
Popular Articles
• GPT-6 Astra PCB Design in EasyEDA Pro: What Worked, What Failed, and What We Learned
• Altium MCP with Claude Code: From Setup to PCB Design
• KiCad MCP: How to Design a PCB with Claude Code [Step-by-Step]
• Altium MCP: AI PCB Design with GPT-6 and Codex [Step-by-Step Guide]
• AI PCB Design: From Prompt to PCB with EasyEDA Pro
Keep Learning
Choosing the Right PCB Shape
key takeaway Choose a PCB shape based on layout, space, and application requirements. Consider edge clearance, cutouts, and manufacturing feasibility early. Select suitable routing and panelization methods for reliable production. Work with JLCPCB to turn custom PCB designs into manufacturable products. Selecting the right PCB shape is an important part of electronic product design. Beyond determining how a circuit board fits inside an enclosure, its geometry also affects component placement, signal r......
Designing Durable Custom Keyboard PCBs: Tailored Solutions and Expert Fabrication
So what's a keyboard PCB? In simple terms, it is the printed circuit board that is contained in the center of any keyboard, connecting the key switches to the controller, which communicates with your computer. Hitting a key closes a circuit on the PCB, which the controller records what key it was and transmits that keycode back to your host device. The mechanical-keyboard community is a subculture that has developed out of a niche hobby to become a successful subculture in the mechanical-keyboard worl......
GPT-6 Astra PCB Design in EasyEDA Pro: What Worked, What Failed, and What We Learned
Key Takeaways What was tested: GPT-6 Astra was given access to a native EasyEDA Pro 3.2.149 installation and asked to design a stereo TPA3116D2 amplifier from a four-line written brief. What it produced: The run resulted in a 44 × 34 mm, two-layer PCB with 40 SMD components and an editable native EasyEDA Pro project with embedded libraries. Where it failed: The first complete import opened cleanly and looked plausible, yet the initial native verification reported 50 association mismatches involving 12......
Claude Code PCB Design: Can It Build a Real Board in EasyEDA Pro?
Key Takeaways Claude Code PCB design: Using Claude Opus 5.5 and EasyEDA Pro 3.2.149, I converted a 47-component, three-page schematic from a PDF into a fully routed, two-layer PCB with zero DRC errors. EasyEDA Pro integration: The EasyEDA API skill connects Claude Code to EasyEDA Pro through a local bridge server and the Run API Gateway extension. This allows Claude to control the editor via JavaScript, with a 30-second timeout per API call. Design verification: A successful API response doesn't alway......
Guide to PCB Via Design: Best Practices, Tips, and Key Considerations
High-quality PCB design not only requires innovative concepts but also relies on a deep understanding of PCB manufacturing processes. Via design, as one of the critical steps in PCB design, is crucial for both PCB performance and manufacturing efficiency. Can vias be designed in any size? To answer this question, let’s first understand how holes on a PCB are created. 1. Cutting the Material: PCB manufacturers use automatic cutting machines to slice large copper-clad laminates into substrates of specif......
AI PCB Design: From Prompt to PCB with EasyEDA Pro
Key Takeaways AI PCB design uses AI agents to automate schematic creation, component selection, layout, and verification inside a real EDA editor — not just generate images. The workflow connects EasyEDA Pro to an AI coding agent (Claude Code or Codex) through the EasyEDA API Gateway, the open-source API Skill, and a local bridge server. Setup takes about ten minutes and is fully local-first: designs, API calls, and intermediate code never leave your machine. Because the agent places real library part......