Graphene vs MXene Inks for Flexible Electronics: Which Is Better?
13 min
- Quick Comparison: Graphene vs MXene Inks at a Glance
- What Are 2D Material Inks, Exactly?
- Conductivity: What You Actually Get in Production
- Water Dispersibility: Why Surface Chemistry Matters
- Production Scale: What's Actually Available
- GO: Easy Coating with a Reduction Step
- MXene: High Conductivity with an Oxidation Clock
- Which Material Should You Choose?
- Hybrid Formulations: Do They Help?
- Key Takeaways
- FAQ About Graphene and MXene
GNP, GO, rGO, and Ti3C2Tx MXene all share a platelet shape, but they differ dramatically in conductivity, water compatibility, production scale, and shelf life. If you're designing flexible electronics, choosing the right 2D material ink means understanding which trade-offs your device can tolerate.
In this guide, we compare the four most common 2D material inks side by side—graphene nanoplatelets (GNP), graphene oxide (GO), reduced graphene oxide (rGO), and Ti3C2Tx MXene—and explain when each one makes the most sense for flexible electronics applications.
Ti3C2Tx MXene offers very high conductivity from a water-based 2D ink, but unprotected aqueous dispersions can oxidize within days in air. GNP is a more mature, generally lower-cost and more oxidation-resistant option. GO suits aqueous coating followed by reduction to conductive rGO; rGO performance depends on the reduction route and formulation.
Quick Comparison: Graphene vs MXene Inks at a Glance
In short: Ti3C2Tx MXene gives the highest conductivity of any water-based 2D ink but oxidizes within days in air, while graphene nanoplatelets are less conductive but mature, cheaper, and stable. GO and rGO suit water-based coating when a post-coating reduction step is acceptable.
Before diving into the details, here's a high-level overview of how these materials stack up:
| Property | GNP | GO | rGO | Ti3C2Tx MXene |
|---|---|---|---|---|
| Typical resistivity (lower = more conductive) | ~10⁻⁴ Ω·m | ~10⁸ Ω·m (insulating) | Varies with reduction and formulation | ~10⁻⁶ Ω·m |
| Water dispersibility | Poor (needs additives) | Excellent | Moderate | Excellent |
| Post-coating reduction | No | Yes (required for conductivity) | N/A (already reduced) | No |
| Production maturity | High (tonne scale) | High | Medium (depends on route) | Low (batch scale) |
| Oxidation stability | Good | N/A (already oxidized) | Good | Poor (major challenge) |
| Best for | Heaters, sensors, shields | Precursor, functional coatings | Flexible conductors | Low-voltage heaters, EMI shields |
Approximate resistivity values from the 2022 review; coating resistivity varies with formulation and processing.
What Are 2D Material Inks, Exactly?
The term "2D ink" covers a family of very different materials. Understanding the distinctions is the first step to making the right choice.
Graphene Nanoplatelets (GNP)
GNPs are stacks of a few to many carbon layers produced at industrial scale. They're the most mature 2D carbon material available commercially, sold by practical attributes like lateral size and surface area.
Graphene Oxide (GO)
GO has oxygen-containing groups and defects that completely change how it interacts with water and surfaces. It disperses easily in water but is electrically insulating—think of it as a processable precursor rather than a finished conductor.
Reduced Graphene Oxide (rGO)
rGO is GO after some of its oxygen chemistry has been removed. The reduction process recovers part of the conductive carbon network, though it never fully rebuilds pristine graphene.
Ti3C2Tx MXene
MXenes are transition-metal carbides or nitrides with surface terminations such as hydroxyl, fluorine, chlorine, or oxygen. Ti3C2Tx is by far the most studied and widely used MXene composition in flexible electronics.
All four share a flake geometry that makes them attractive for flexible devices—thin platelets overlap to form conductive networks, coat fibers and pores, and accommodate deformation through changing contacts. But their chemistry determines almost everything else: conductivity, dispersibility, reduction requirements, oxidation resistance, adhesion, production hazards, and storage.
Conductivity: What You Actually Get in Production
Conductivity is usually the first property designers look at, but the numbers you see in papers don't always match what you can manufacture.
GNP: Good Enough for Many Applications
Ideal single-layer graphene is an extraordinary conductor with intrinsic resistivity near 10⁻⁸ ohm meters and a Young's modulus around 1 TPa. But commercial GNPs are thicker, smaller, and contain more defects.
Real-world GNP inks typically show resistivity around 10⁻⁴ ohm meters. That's still useful for many flexible electronics applications—heaters, sensors, and electromagnetic shields all work well at this level.
GO: An Insulator Until Reduced
GO sits at the opposite extreme. Oxygen groups disrupt the conductive sp² carbon network, pushing resistivity to roughly 10⁸ ohm meters. In this state, GO is better understood as an easily processed precursor or functional coating than as a conductor.
rGO: A Middle Ground
Reduction can improve GO's conductivity by orders of magnitude, but it doesn't perfectly rebuild pristine graphene. Residual defects, incomplete oxygen removal, platelet junctions, and any nonconductive binder all remain part of the final electrical path. The result is conductivity far better than GO; how close it comes to a good GNP coating depends on the reduction route and the formulation.
Ti3C2Tx MXene: High Solution-Processed Conductivity
Ti3C2Tx MXene can achieve resistivity down to about 10⁻⁶ Ω·m, among the lowest values reported for solution-processed 2D materials in the 2022 comparative review. At a given heater geometry and target power, lower resistance can enable lower voltage for Joule heating. High conductivity can also support strong electromagnetic attenuation in thin coatings, although shielding performance depends on the complete structure.
That said, a coated device is not a bulk-material test. Flake contacts, porosity, thickness, additives, pattern geometry, and oxidation all determine the resistance a designer actually receives in practice.
Water Dispersibility: Why Surface Chemistry Matters
How easily a material disperses in water affects everything from manufacturing cost to worker safety to substrate compatibility.
GNP: Needs Help to Stay in Water
Bare graphitic surfaces don't naturally love water. Smaller or thinner GNPs, or platelets decorated with hydrophilic chemistry, can disperse more readily, but aggregation remains a practical problem.
Most GNP formulations rely on organic solvents, binders, or surfactants to help with aqueous dispersibility. These helpers stabilize the ink, but they can also remain between flakes after drying and reduce conductivity.
GO: Naturally Water-Friendly
GO behaves very differently because its oxygen-containing groups make its surface hydrophilic. It forms homogeneous water dispersions without the same level of stabilizing additives, and that surface chemistry may also improve compatibility with polar substrates.
rGO: Somewhere in Between
rGO often retains enough functional chemistry to be easier to handle than pristine graphitic material, although its exact behavior depends strongly on how far reduction proceeds.
Ti3C2Tx MXene: Conductive and Water-Dispersible
Ti3C2Tx combines a metallic conductive backbone with an oxide-like, terminated surface. In a 2022 comparative review of graphene and MXene coatings (Orts Mercadillo et al., Advanced Functional Materials), 60% of the surveyed MXene papers dispersed the material in water alone.
This is a powerful formulation advantage: high conductivity doesn't automatically require a difficult organic carrier. The trade-off is that the same reactive surface that welcomes water also participates in oxidation.
Production Scale: What's Actually Available
Performance numbers don't matter if you can't source the material at the scale and quality you need.
GNP: Mature Supply Chain
GNPs have the most mature production position of the group, with established commercial grades rather than a single standardized ink.
Commercial grades are sold by practical attributes such as lateral size or surface area, and supply is available at tonne scale.
GO/rGO: Grade and Consistency Matter
GO is also available at substantial scale, but consistent purity and grade remain important purchasing criteria.
For conductive rGO, reduction adds another quality-control variable. Compare supplier specifications for the final coating rather than production volume alone.
MXene: Early Stage Production
MXene supply is less mature than GNP supply. The 2022 review described approximately 50-gram batch reactors. Assess current suppliers by their available batch sizes, quality specifications, and delivery commitments.
For material selection, the practical questions are batch consistency, usable shelf life, and dependable delivery. Scaling supply requires control of quality and stability, not merely a bigger mixing operation. For how each ink route maps onto real coating processes, see matching 2D conductive inks to coating processes.
GO: Easy Coating with a Reduction Step
The GO-to-rGO approach is deliberately two-stage: exploit GO's water dispersibility and adhesion to make a uniform coating, then reduce it after deposition. This avoids trying to keep a highly graphitic material suspended before it reaches the substrate.
But reduction becomes part of device fabrication. The substrate, pattern, contacts, and other components must all tolerate that treatment.
Common Reduction Methods
Studies use several reduction approaches, each with different trade-offs:
- Chemical reduction: The most common method, but potent reducing agents add handling and disposal concerns
- Thermal reduction: Fast but may exceed the temperature tolerance of flexible polymers
- Electrochemical, plasma, and microwave routes: Offer alternative processing windows
- Gentler alternatives (ascorbic acid, amino acids, biological agents): Operate at low temperature but can be slower and produce less complete reduction
Decision Rule for GO
Choose GO-to-rGO when conformal aqueous coating and surface compatibility solve a harder problem than the reduction step creates. Don't choose it simply because water appears in the first line of the recipe. The conductivity, cycle time, chemical burden, and yield after reduction determine whether the full route is competitive.
MXene: High Conductivity with an Oxidation Clock
Ti3C2Tx avoids the post-coating reduction required by GO and can disperse directly in water—a rare combination of processability and conductivity. Its vulnerability is environmental stability.
Unprotected aqueous Ti3C2Tx dispersions exposed to air can oxidize toward titanium dioxide within days, with a visible color change and loss of conductivity reported in the 2022 review. The exact lifetime depends on flake quality, concentration, temperature, oxygen, light, and other formulation details.
Managing MXene Stability
Several strategies can extend MXene's usable life:
- Cold storage can extend dispersion stability beyond a month
- Inert storage under argon has been reported to preserve it for more than six months
- Encapsulation and polymer matrices may slow exposure but add their own trade-offs
These measures are feasible in a laboratory and sometimes in manufacturing, but they add logistics. A production line must consider transport, thawing or warming, tank residence time, recirculation, open-air coating, drying, and the lifetime of the finished device.
Protection can also stiffen a flexible device, block ion access in an electrode, alter heat transfer in a heater, or damp a sensor. And electrical degradation has been observed even within polymer matrices, so oxidation cannot be assumed solved just because the coating is embedded.
MXene is compelling when its performance advantage justifies a deliberate stability strategy.
Which Material Should You Choose?
The right material depends on your device's most important constraints. Here's how to match each material to the application where it shines.
Choose MXene When...
- You need the highest possible conductivity from a water-processed ink
- You're building low-voltage heaters or thin EMI shields
- You can control the production environment to manage oxidation
- Your substrate can't tolerate high-temperature GO reduction
- You don't need multi-year shelf stability in ambient conditions
Choose GNP When...
- You need a mature, readily available supply chain
- Carbon robustness and cost are priorities
- You can work with organic solvents or surfactant packages
- The application demands proven long-term stability
- You're building heaters, sensors, shields, or composite electrodes
Choose GO/rGO When...
- Coating uniformity, chemical functionality, or adhesion is the immediate challenge
- You need electrical insulation or specific surface chemistry (use GO as-is)
- Your substrate is compatible with the selected low-temperature reduction route (for rGO)
- Water-based processing is non-negotiable but conductivity requirements are moderate
Application-Specific Guidance
Flexible heaters: MXene's low resistivity can enable low-voltage heating when coating thickness, geometry, and heat loss are controlled, while GNP offers a more oxidation-resistant carbon option. For products that must ship today, etched-foil polyimide and silicone rubber heaters offer an established manufacturing route with specified resistance tolerances.
Strain and pressure sensors: The highest intrinsic conductivity is not automatically best. Sensitivity arises from how junctions make and break as the substrate deforms. A moderately conductive GNP or rGO network can provide a large, interpretable resistance change.
Supercapacitor electrodes: Accessible surface and ion transport compete with flake restacking. Material choice must follow the mechanism that controls device output.
Hybrid Formulations: Do They Help?
Around 40% of the 2D material coatings surveyed in that review used a hybrid formulation. Conductive polymers, silver structures, carbon black, or carbon nanotubes can bridge platelet junctions, adjust mechanical response, or add a second function.
However, graphene and MXene appear together only rarely. Their similar platelet morphology and overlapping strengths may provide less synergy than their added formulation complexity would suggest.
A hybrid should have a clear reason to exist: one filler bridges gaps, another supplies surface area, a polymer holds the network together, or a secondary phase changes the strain response. Adding ingredients simply because each is fashionable makes dispersion, repeatability, recycling, and failure analysis harder.
Key Takeaways
The comparison ends where it began: with the device constraint.
- GNP offers mature carbon platelets but needs dispersion engineering
- GO offers easy aqueous processing but is electrically insulating until reduced
- rGO trades some of that processability for recovered conduction
- Ti3C2Tx MXene offers exceptional solution-processed conductivity and water compatibility but introduces production and oxidation challenges
The winning ink is the one whose unavoidable weakness can be managed most credibly within your specific application and manufacturing constraints.
FAQ About Graphene and MXene
Is MXene always more conductive than graphene ink?
Ti3C2Tx MXene coatings often show a strong conductivity advantage over solution-processed GNP or rGO coatings, but "always" is too strong. Flake quality, oxidation, thickness, additives, junctions, and measurement method all matter. Ideal single-layer graphene is exceptionally conductive, yet that's not the same material as a scalable GNP ink you can actually buy and print.
Why use GO if it's electrically insulating?
GO disperses readily in water and can adhere well to compatible surfaces, making uniform coating easier. It can then be reduced to rGO to recover part of the conductive network. GO can also be useful without reduction when its surface chemistry or insulating behavior, rather than electrical conduction, is the intended function.
What is the biggest practical limitation of Ti3C2Tx MXene ink?
Oxidation is the defining stability challenge. An aqueous dispersion can lose performance as flakes oxidize, so storage, processing time, oxygen exposure, and finished-device protection must all be controlled. Production routes also commonly involve demanding etching chemistry. Those burdens should be weighed against the conductivity and water-processability advantage.
What is the difference between GNP, GO, and rGO?
GNP (graphene nanoplatelets) are stacks of carbon layers produced by exfoliation—conductive and commercially mature but hard to disperse in water. GO (graphene oxide) is chemically oxidized graphene that disperses easily in water but is insulating. rGO (reduced graphene oxide) is GO that has been treated to remove some oxygen groups, partially restoring conductivity while retaining better processability than pristine graphene.
Can you mix graphene and MXene in the same ink?
While technically possible, graphene and MXene hybrids appear rarely in the literature. Their similar platelet morphology and overlapping strengths may provide less synergy than the added formulation complexity justifies. Hybrids work best when each component contributes a distinct mechanism—for example, one bridges gaps while the other supplies surface area.
Which 2D material ink is cheapest?
GNP generally benefits from a mature, high-volume supply chain. GO and rGO costs depend on grade, purification, and reduction requirements, while MXene pricing also depends on batch quality and stability requirements. Compare current supplier quotes and cost per function, such as conductivity at the required thickness, rather than assuming a fixed price ranking.
Keep Learning
Flexible Conductive Coatings: Sheet Resistance, Conductivity, and Durability
Sheet resistance and conductivity describe different aspects of electrical performance. Sheet resistance (Ω/sq) depends on both conductivity and film thickness, while conductivity (S/m) describes charge transport through a material volume. For a uniform thin film, Rₛ = 1/(σ × t), so thickness is essential when converting between them. Neither value alone establishes whether a flexible coating will survive bending, washing, or ageing. This guide explains sheet resistance vs conductivity for flexible co......
How Graphene and MXene Inks Enable Stretchable Circuits
Stretchable circuits must maintain electrical performance while bending, stretching, or twisting. Graphene and MXene inks offer a promising approach by combining electrical conductivity, mechanical flexibility, and printability. But how do these materials actually enable circuits to stretch without losing their electrical function? Graphene and MXene inks enable stretchable circuits by forming interconnected conductive networks that can rearrange as the substrate deforms. Their overlapping 2D platelet......
Graphene vs MXene Inks for Flexible Electronics: Which Is Better?
GNP, GO, rGO, and Ti3C2Tx MXene all share a platelet shape, but they differ dramatically in conductivity, water compatibility, production scale, and shelf life. If you're designing flexible electronics, choosing the right 2D material ink means understanding which trade-offs your device can tolerate. In this guide, we compare the four most common 2D material inks side by side—graphene nanoplatelets (GNP), graphene oxide (GO), reduced graphene oxide (rGO), and Ti3C2Tx MXene—and explain when each one mak......
What Is a Thermoelectric Generator and How Does It Work?
Can heat from an engine, industrial process, or other heat source be turned into useful electricity without moving parts? A thermoelectric generator (TEG) does this by converting a temperature difference directly into electrical power through the Seebeck effect. Its power output depends on the temperature difference across the device, the thermoelectric materials, and the overall system design. What Is a Thermoelectric Generator? A thermoelectric generator (TEG) is a solid-state device that converts h......
What Are Flexible Electronics? How They Work & Where They're Used
Flexible electronics are electronic circuits, devices, and systems designed to maintain their intended functions while bending or conforming to a surface. They enable electronic functions to fit curved, moving, lightweight, or space-constrained products. Common examples include flex circuits in cameras and phones, wearable sensors, flexible heaters, flexible displays, RFID and NFC labels, conformal industrial sensors, and medical patches. Flexible electronics is a broad field that encompasses differen......
What Is a Strip Heater? How It Works: A Complete Guide [2026]
Strip heaters are electric resistance heaters commonly used to heat metal surfaces, machinery, and industrial equipment. Their flat, narrow design allows them to be mounted against surfaces or in spaces where other heater shapes may be less suitable. Understanding how strip heaters are constructed and installed helps determine whether they’re the right choice for a particular heating application. What Is a Strip Heater? A strip heater converts electrical energy into heat through a resistance element h......