The ROI of Nano-Coated Stencils in PCB Assembly Lines
5 min
- Problem with Traditional Stencil Processes:
- Smart Solution with Nano-coated Stencils:
- Cost Drivers in Stencil Printing:
- Return on Investment (ROI) of Nano-Coated Stencils:
- Conclusion:
Nano coatings offer several benefits. They are hydrophobic and repel water-based chemistry or flux, and some are also oleophobic and repel oil-based chemistry or flux. When applied to the bottom or board side of the stencil, these coatings will prevent solder paste squeeze-out during the print process between the stencil and PCB from sticking to the bottom of the stencil when the stencil separates from the board.
As a result, the next print will be as good as the initial print, and bridging is reduced because there is no paste on the bottom of the stencil to transfer to the PCB during the next print. In addition, underside cleaning frequency can be reduced as there is much less solder paste to remove from the stencil. In some cases, I’ve seen customers move from cleaning after every print to cleaning after every 20 prints. This article explores what nano-coating is, the types available, and how it compares to standard SMT stencils in terms of print quality, reliability, and ROI. Get a free coupon for nano-coating
Problem with Traditional Stencil Processes:
Solder paste must stick in acceptable value to the upper side of the stencil, but should not adhere to the bottom side of the stencil and to the aperture walls. Adhering to the wall causes: missing or insufficient solder paste. Adhering to the bottom side of the stencil causes solder paste smearing.
Dealing with this unsolvable production handicap leads to frequent bottom side cleaning – for very advanced boards after every print! This fumbling can not solve the cause of the problem of increasing costs of cleaning material and as a most unlikely effect: slowing down the whole SMD-production line.
Smart Solution with Nano-coated Stencils:
The top side of the stencil is uncoated, the bottom side and the aperture walls are permanently coated with an anti adhesion effect. This nanocoating is a few nanometers thick which does not change the shape and size of the old stencil.
Nano coating is an industry proven process which shows immediate and measurable improvement from the first print. There are many studies on the nano materials going on which have properties to work with stencils. Nano-coatings work by reducing the surface energy of the stencil material and preventing the solder paste from sticking to unwanted areas. As a result, the printed solder paste deposits are cleaner, more uniform, and more repeatable.
Cost Drivers in Stencil Printing:
The main cost areas in solder paste printing include:
- Frequent underside cleaning
- Solder paste waste
- Yield loss due to defects
- Time lost in rework and reprinting
- Equipment wear and cleaning supplies
These recurring costs add up over time, especially in high-volume environments. Standard uncoated stencils often require cleaning after every print, especially when working with fine-pitch components (SAR < 0.55). With nano-coated stencils, cleaning frequency is reduced to once every 20 prints.
- Uncoated stencil: 1 board printed per minute
- Nano-coated stencil: 2 boards printed per minute This doubling of productivity is a game-changer for high-volume PCB assembly lines.
Return on Investment (ROI) of Nano-Coated Stencils:
Investing in nano-coated stencils offers substantial improvements across multiple areas of the solder paste printing process like in cost and efficiency. As seen in the above section the key cost drivers such as cleaning, solder paste wastage and rework are significantly reduced with the use of nano-coatings. While nano-coated stencils may carry a higher initial cost (typically around $40 extra), the ROI is quickly realized often within the first 150 - 180 boards through material savings, process efficiency, and yield improvements. This is the actual data which is provided by PCB manufacturers over a time period.
1. Increased Productivity
Nano-coatings reduce the need for frequent underside cleaning. In high-precision applications, cleaning might be required after every print. With nano-coated stencils, this interval can increase to every 20 prints, effectively doubling throughput in high-volume production environments.
2. Cleaning Material Cost Savings
By reducing cleaning frequency, users can lower cleaning material usage by up to 95%. Which cut down the cleaning cost from $0.20 per board (standard stencil) to just $0.01 per board (nano-coated).
3. Solder Paste Waste Reduction
Traditional stencils often retain solder paste on the underside, leading to material waste. Nano-coatings prevent paste adhesion, reducing solder paste waste to near zero. This results in savings of approximately $0.04–$0.07 per board, depending on paste usage and price.
4. Reduced Rework Costs
Improved print quality means fewer defects and less rework. This thing not only saves on materials and labor but also recovers valuable production time that can be used to build new boards.
Conclusion:
As per the data, nano-coated stencils have a slightly higher upfront cost, their impact on productivity and material savings make them a good investment for PCB manufacturers. Thanks to its large and rapidly growing demand for laser-cut SMT stencils, JLCPCB invested early in advanced nano vacuum-coating equipment. This strategic upgrade enables JLCPCB to scale production efficiently, improve coating consistency, and significantly lower the cost per nano-coating cycle.
As a result, JLCPCB can offer premium nano-coating for only $4.72, making high-performance SMT stencil coatings far more affordable than the industry average. You can even claim a free nano-coating trial coupon to experience the benefits firsthand.
Nano-coated stencils offer a transformative ROI for PCB assembly lines. Nano coatings drastically cut the cleaning costs and lower down solder paste wastage. Transitioning from traditional to nano-coated stencils doubles productivity. The cleaning frequency is reduced up to 95%, making them a smart option specially for high-volume or precision-driven applications.
Keep Learning
Why PCB Stencil Are Key to High-Quality SMT Assembly
PCB(Printed Circuit Board) stencil is a critical component of Surface Mount Technology (SMT) assembly. It plays a vital role in ensuring the accuracy and consistency of SMT assembly results, which directly affects the functionality and performance of the final product. PCB stencil also called SMT stencil, Circuit Board stencil is used to apply solder paste to the PCB, which is then used to attach SMT components to the board. Without the use of PCB stencil, it becomes challenging to achieve high-qualit......
Nano-Coating vs Electropolishing for SMT Stencils
Key Takeaways Electropolishing improves the underlying metal surface by smoothing aperture walls. Nano-coating adds a low-friction, hydrophobic surface that helps paste release and reduces residue. Both treatments can improve fine-pitch paste release and support more consistent deposits and higher first-pass yield. Nano-coating is especially useful for BGA/QFN assemblies and high-volume runs, where cleaning frequency and paste-release consistency matter more. Electropolishing and nano-coating are comp......
Stencil in PCB: A Comprehensive Guide to PCB Stencil Design, Fabrication, and JLCPCB Solutions
Figures 1 Solder paste application using a stainless steel stencil to achieve high-precision results. In PCB assembly based on Surface-Mount Technology (SMT), precision is a key factor that determines the final quality of electronic products. One critical element that strongly influences soldering accuracy is the stencil. The stencil functions as a physical template that controls the distribution of solder paste onto PCB pads before components are placed. Accurate solder paste application produces rel......
Unlocking the Secrets of Nano-Coated Stencil Manufacturing
Nano-Coated Stencil Manufacturing Process The manufacturing of nano-coated stencils involves a series of precision engineering steps including design and drafting, laser cutting, polishing, nano-coating deposition, and quality inspection. Below is a detailed description of each process stage: 1. Design and Drafting (1) Data Acquisition: Accurate data is obtained from customer-supplied design files (e.g., Gerber files, PCB layouts) or physical product samples. This includes stencil dimensions, pad layo......
The ROI of Nano-Coated Stencils in PCB Assembly Lines
Nano coatings offer several benefits. They are hydrophobic and repel water-based chemistry or flux, and some are also oleophobic and repel oil-based chemistry or flux. When applied to the bottom or board side of the stencil, these coatings will prevent solder paste squeeze-out during the print process between the stencil and PCB from sticking to the bottom of the stencil when the stencil separates from the board. As a result, the next print will be as good as the initial print, and bridging is reduced......
What Are Laser Cut Stencils? A Guide for PCB Assembly
Traditional PCB assembly processes require the manual placement of electronic components before soldering. However, the increasing complexity of electronic printed circuit boards, combined with the need for miniaturisation, necessitates mechanical assembly and solder paste application using SMT stencils. Placing and soldering many small components on a small circuit board is no longer practical.Stencils replace the hand soldering of surface mount components and the inconsistencies caused by hand solde......