Unlocking the Secrets of Nano-Coated Stencil Manufacturing
4 min
- Nano-Coated Stencil Manufacturing Process
- 1. Design and Drafting
- 2. Laser Cutting
- 3. Polishing
- 4. Nano Coating Deposition
- 5. Quality Control and Inspection
Nano-Coated Stencil Manufacturing Process
The manufacturing of nano-coated stencils involves a series of precision engineering steps including design and drafting, laser cutting, polishing, nano-coating deposition, and quality inspection. Below is a detailed description of each process stage:
1. Design and Drafting
(1) Data Acquisition:
Accurate data is obtained from customer-supplied design files (e.g., Gerber files, PCB layouts) or physical product samples. This includes stencil dimensions, pad layouts, aperture shapes and sizes, and specific application requirements.
(2) CAD Drafting:
Using professional CAD software such as Auto CAD, the acquired data is converted into precise 2D or 3D engineering drawings. These define the stencil's overall dimensions, aperture locations, shapes, and sizes, serving as the digital blueprint for downstream processing.
2. Laser Cutting
(1) Material Preparation:
High-grade stainless steel sheets, typically SUS 304, are selected as the base material. The material must meet strict criteria for thickness tolerance, flatness, and mechanical integrity.
(2) Machine Setup:
Laser cutting machines are calibrated based on the stencil design. Key parameters include laser power, cutting speed, and pulse frequency. The stainless steel sheet is securely clamped onto the worktable to ensure cutting precision and material stability.
(3) Precision Cutting:
The laser system emits a high-energy beam that locally melts or vaporizes the steel, following the pre-programmed aperture paths. The process yields high-accuracy aperture formation, typically achieving dimensional tolerances within ±0.05 mm.
3. Polishing
(1) Mechanical Polishing:
Rotary polishing wheels or abrasive compounds are applied to remove burrs and improve edge smoothness. Wheel speed and applied pressure are tuned according to stencil thickness and material properties, usually between 1500–3000 RPM.
(2) Chemical Polishing:
The stencil is immersed in a chemical solution that selectively dissolves microscopic surface irregularities. The process typically runs at temperatures between 40°C–80°C for 5–15 minutes, depending on surface condition and required finish.
(3) Electrochemical Polishing (Electropolishing):
The stencil acts as the anode in an electrolytic cell. Anodic dissolution of surface metal occurs under controlled voltage (10–30 V) and current density (1–10 A/cm²). Processing times range from 5–30 minutes. Electropolishing enhances surface finish and ensures uniform treatment across complex geometries and micro-apertures.
4. Nano Coating Deposition
(1) Vacuum Preparation:
After polishing, the stencil is loaded into a high-vacuum deposition chamber. Vacuum levels typically reach 10⁻³ to 10⁻⁵ Pa to ensure uniform deposition of nano-scale coatings.
(2) Coating Material Selection:
Suitable nano-coating materials such as titanium alloy (Ti), titanium nitride (TiN), or silicon dioxide (SiO₂) are selected based on the required functional properties. These materials are introduced into the chamber as targets or evaporation sources.
(3) Deposition Process:
Two main techniques:
A.Physical Vapor Deposition (PVD):
Material atoms are ejected from a solid target by ion bombardment and deposited onto the stencil surface as a thin film.
B.Chemical Vapor Deposition (CVD):
Gaseous reactants undergo chemical reactions on the stencil surface, forming a nano-scale film through in-situ deposition.
These coatings enhance stencil performance, improving wear resistance, anti-adhesion, and print definition in high-precision SMT applications.
5. Quality Control and Inspection
(1) Visual Inspection:
The stencil is examined for surface defects such as non-uniform coating, pinholes, cracks, or delamination. A uniform, smooth, and adherent nano-coating is essential.
(2) Dimensional Verification:
Precise measurement tools (e.g., optical microscopes, micrometers, thickness gauges) are used to validate the overall stencil dimensions, aperture sizes, and coating thickness against design specifications.
(3) Performance Testing:
The stencil’s mechanical and functional properties are tested:
Hardness Testing:
Coating hardness is measured using microhardness testers.
Corrosion Resistance:
Assessed via salt spray testing (ASTM B117 or equivalent).
Hydrophobicity:
Measured using contact angle goniometers to evaluate surface wetting behavior.
These tests ensure the nano-coated stencil meets stringent performance criteria for high-end electronics manufacturing.
The production of nano-coated stencils is a high-precision process that integrates advanced materials science, surface engineering, and microfabrication technology. Each stage — from initial CAD design through to final inspection — is critical to achieving optimal stencil performance, enabling consistent, high-quality solder paste deposition for next-generation electronic assemblies.
Now JLCPCB's Nano-Coated Stencils Are Available — Starting from Just $4.72!
Choosing Nano Coating not only boosts your SMT first-pass yield and improves print quality, but also lets you enjoy a free trial with a $5 coupon. Try it now and get a free quote!
Keep Learning
Why PCB Stencil Are Key to High-Quality SMT Assembly
PCB(Printed Circuit Board) stencil is a critical component of Surface Mount Technology (SMT) assembly. It plays a vital role in ensuring the accuracy and consistency of SMT assembly results, which directly affects the functionality and performance of the final product. PCB stencil also called SMT stencil, Circuit Board stencil is used to apply solder paste to the PCB, which is then used to attach SMT components to the board. Without the use of PCB stencil, it becomes challenging to achieve high-qualit......
Nano-Coating vs Electropolishing for SMT Stencils
Key Takeaways Electropolishing improves the underlying metal surface by smoothing aperture walls. Nano-coating adds a low-friction, hydrophobic surface that helps paste release and reduces residue. Both treatments can improve fine-pitch paste release and support more consistent deposits and higher first-pass yield. Nano-coating is especially useful for BGA/QFN assemblies and high-volume runs, where cleaning frequency and paste-release consistency matter more. Electropolishing and nano-coating are comp......
Stencil in PCB: A Comprehensive Guide to PCB Stencil Design, Fabrication, and JLCPCB Solutions
Figures 1 Solder paste application using a stainless steel stencil to achieve high-precision results. In PCB assembly based on Surface-Mount Technology (SMT), precision is a key factor that determines the final quality of electronic products. One critical element that strongly influences soldering accuracy is the stencil. The stencil functions as a physical template that controls the distribution of solder paste onto PCB pads before components are placed. Accurate solder paste application produces rel......
Unlocking the Secrets of Nano-Coated Stencil Manufacturing
Nano-Coated Stencil Manufacturing Process The manufacturing of nano-coated stencils involves a series of precision engineering steps including design and drafting, laser cutting, polishing, nano-coating deposition, and quality inspection. Below is a detailed description of each process stage: 1. Design and Drafting (1) Data Acquisition: Accurate data is obtained from customer-supplied design files (e.g., Gerber files, PCB layouts) or physical product samples. This includes stencil dimensions, pad layo......
The ROI of Nano-Coated Stencils in PCB Assembly Lines
Nano coatings offer several benefits. They are hydrophobic and repel water-based chemistry or flux, and some are also oleophobic and repel oil-based chemistry or flux. When applied to the bottom or board side of the stencil, these coatings will prevent solder paste squeeze-out during the print process between the stencil and PCB from sticking to the bottom of the stencil when the stencil separates from the board. As a result, the next print will be as good as the initial print, and bridging is reduced......
What Are Laser Cut Stencils? A Guide for PCB Assembly
Traditional PCB assembly processes require the manual placement of electronic components before soldering. However, the increasing complexity of electronic printed circuit boards, combined with the need for miniaturisation, necessitates mechanical assembly and solder paste application using SMT stencils. Placing and soldering many small components on a small circuit board is no longer practical.Stencils replace the hand soldering of surface mount components and the inconsistencies caused by hand solde......