How does Electropolishing Work in PCB Stencil
6 min
- What is Electropolishing?
- Why Electropolishing is Required:
- Manufacturing Process of Electropolished Stencil:
- Science Behind Electropolished Stencils:
- Exact Process of Electropolishing a Stencil:
- Benefits of Electropolishing:
- Electropolishing vs. Other Stencil Finishing Methods
- Standards and Best Practices:
- Conclusion:
To ensure optimum solder paste release, PCB stencil producers must offer superior finishes. One method for enhancing the functionality of stencils is electropolishing. How does electropolishing improve PCB stencils, and what is it?
The continuous application of laser beams during the PCB stencil-making process causes the opening or aperture wall to become rough. This occurs as a result of the sheet material being melted by the laser beam, which causes certain surface irregularities. Electropolishing is used to smooth the aperture wall in order to address this issue. The benefits of electropolishing for SMT assembly, its function in PCB stencil manufacturing, and its operation will all be covered in this article.
JLCPCB provides electropolished stencils as part of its service offerings, ensuring smoother aperture walls for improved solder paste release and higher assembly quality.
What is Electropolishing?
A conductive workpiece can be made smoother, rougher, and free of micro-burrs and other surface flaws by electropolishing, an electrochemical surface finishing technique that removes a thin coating of metal. Electropolishing, also referred to as the "reverse of electroplating," dissolves metal at the tiny level.
Basic Principle of Electropolishing:
- Anodic Process: In an electrolyte bath, the stencil is attached as the anode (+).
- Cathode (-): Usually composed of lead or stainless steel.
- Electrolyte: Acidic fluid, frequently a combination of sulfuric and phosphoric acids.
- Voltage Applied: When metal ions are exposed to a direct current (DC), they dissolve preferentially from surface peaks.
Which results in a smoother, more uniform surface with microscopic imperfections leveled out.
Why Electropolishing is Required:
It is one of the recent technologies which is made to design high quality stencils. What we have traditionally is lasers. By concentrating them on stainless steel they got dissolved by the high intensity of the laser. Which is used to create holes and apertures in laser cutting stencils. Because of this, the laser stencil has metal slag at the opening's edge, and the hole wall's edge is not straight and smooth, which makes it difficult to print solder paste underneath the tin. To address this shortcoming of the laser stencil, electropolishing is being used.
The quality of solder paste printing is directly impacted by stencil performance, particularly for fine-pitch components (0.4 mm or smaller). Microscopic burrs or roughness at the borders of apertures are frequently left by laser-cut stencils, which can:
- Trap solder paste
- Cause inconsistent paste release
- Lead to defects like insufficient solder or bridging
Manufacturers may ensure consistent, flawless printing by employing electropolishing to provide polished aperture walls, which is essential for fine-pitch or high-volume SMT assembly.
Manufacturing Process of Electropolished Stencil:
1. Using the simple process with the stainless steel material we have to create a stencil.
2. To make it electropolished we have to immerse it in an electrolyte solution. Which occurs inside an electrochemical cell.
3. A DC current is applied to the stencil, causing metal ions to dissolve from the surface of the stencil.
4. After these metal ions are dissolved, we can say an upper rough layer is removed. Which causes instabilities in paste applications now we have a smooth polished surface.
Science Behind Electropolished Stencils:
A certain voltage is used during an acid rinse to regulate the roughness of the aperture wall. In essence, metal ions are injected into the acid bath during an inverted galvanizing process.
Step 1: What is done by an electrolytic solution when it is applied is: It leaves positive charges on the stencil and transfers the negative charge to the solution.
Step 2: The stencil is subjected to direct current, which eliminates the metal ions and forces them in the direction of the negative pole.
The whole surface, in particular the laser-cut aperture walls, becomes smooth and devoid of surface irregularities throughout this procedure. Nickel plating is also occasionally used to create smooth aperture walls and openings, although it has the drawback of decreasing the aperture opening's total size and necessitating artwork modification.
Exact Process of Electropolishing a Stencil:
1. Preparation of the PCB Stencil
- To get rid of dust and grease, the laser-cut stainless steel stencil is thoroughly cleaned.
- The stencil is immersed in the acidic electrolyte solution and linked as an anode.
2. Electrochemical Removal of Material
- When direct current is used, the metal dissolves anodically under regulated conditions.
- Uniform smoothing results from surface asperities (peaks) dissolving more quickly than recessed portions (valleys).
3. Post-Electropolishing Treatment
- The stencil is electropolished and then cleaned with deionized water.
- After drying, the surface is examined for homogeneity and smoothness.
Benefits of Electropolishing:
Electropolished stencils provide excellent printing precision, particularly for tiny PCB pads. JLCPCB’s combination of electropolished and nano-coated stencils further enhances these benefits, offering superior paste release and long-lasting performance.Below is a list of some of the benefits:
- Better release results from less paste adherence to aperture walls.
- encourages reliable transmission of solder paste.
- prevents flaws and solder bridging.
- speeds up and improves the thoroughness of post-use stencil cleaning.
- increases the longevity of stencils, particularly in high-humidity settings.
Electropolishing vs. Other Stencil Finishing Methods
Standards and Best Practices:
IPC Guidelines:
- IPC-7525C: Stencil Design Guidelines recommends high-quality aperture finishing for reliable paste transfer.
- IPC-A-610: Acceptability standards highlight the importance of consistent solder deposition for Class 2 (commercial) and Class 3 (high-reliability) products.
Conclusion:
This method applies an electrolytic solution to the stencil material’s surface in order to refine its flatness. This may improve the consistency of solder paste application though it is not essential for every case.
(This electropolishing process is performed by JLCPCB.)
When it comes to SMT stencils the laser cutting is mostly favored because of its accuracy. They have quick turnaround time and adaptability to different designs. If accuracy is a critical aspect then electropolished PCB stencils provide a good choice. The electropolishing step in stencil manufacturing processes becomes imperative when creating stencils for PCBs containing densely packed pitch components. Electropolished stencils enhance SMT production yields and decrease defect rates by improving paste release through smoother aperture walls mercilessly aiding better solder paste deployment during the injection process.With fast production and global shipping, you can trust JLCPCB to support your next project with professional-grade tools.
Keep Learning
Why PCB Stencil Are Key to High-Quality SMT Assembly
PCB(Printed Circuit Board) stencil is a critical component of Surface Mount Technology (SMT) assembly. It plays a vital role in ensuring the accuracy and consistency of SMT assembly results, which directly affects the functionality and performance of the final product. PCB stencil also called SMT stencil, Circuit Board stencil is used to apply solder paste to the PCB, which is then used to attach SMT components to the board. Without the use of PCB stencil, it becomes challenging to achieve high-qualit......
Nano-Coating vs Electropolishing for SMT Stencils
Key Takeaways Electropolishing improves the underlying metal surface by smoothing aperture walls. Nano-coating adds a low-friction, hydrophobic surface that helps paste release and reduces residue. Both treatments can improve fine-pitch paste release and support more consistent deposits and higher first-pass yield. Nano-coating is especially useful for BGA/QFN assemblies and high-volume runs, where cleaning frequency and paste-release consistency matter more. Electropolishing and nano-coating are comp......
Stencil in PCB: A Comprehensive Guide to PCB Stencil Design, Fabrication, and JLCPCB Solutions
Figures 1 Solder paste application using a stainless steel stencil to achieve high-precision results. In PCB assembly based on Surface-Mount Technology (SMT), precision is a key factor that determines the final quality of electronic products. One critical element that strongly influences soldering accuracy is the stencil. The stencil functions as a physical template that controls the distribution of solder paste onto PCB pads before components are placed. Accurate solder paste application produces rel......
Unlocking the Secrets of Nano-Coated Stencil Manufacturing
Nano-Coated Stencil Manufacturing Process The manufacturing of nano-coated stencils involves a series of precision engineering steps including design and drafting, laser cutting, polishing, nano-coating deposition, and quality inspection. Below is a detailed description of each process stage: 1. Design and Drafting (1) Data Acquisition: Accurate data is obtained from customer-supplied design files (e.g., Gerber files, PCB layouts) or physical product samples. This includes stencil dimensions, pad layo......
The ROI of Nano-Coated Stencils in PCB Assembly Lines
Nano coatings offer several benefits. They are hydrophobic and repel water-based chemistry or flux, and some are also oleophobic and repel oil-based chemistry or flux. When applied to the bottom or board side of the stencil, these coatings will prevent solder paste squeeze-out during the print process between the stencil and PCB from sticking to the bottom of the stencil when the stencil separates from the board. As a result, the next print will be as good as the initial print, and bridging is reduced......
What Are Laser Cut Stencils? A Guide for PCB Assembly
Traditional PCB assembly processes require the manual placement of electronic components before soldering. However, the increasing complexity of electronic printed circuit boards, combined with the need for miniaturisation, necessitates mechanical assembly and solder paste application using SMT stencils. Placing and soldering many small components on a small circuit board is no longer practical.Stencils replace the hand soldering of surface mount components and the inconsistencies caused by hand solde......