SAM vs Ceramic: Choosing the Right Nano-Coating for Your PCB Stencil
4 min
- What Are SAM and Ceramic Nano-Coatings?
- Choosing Between SAM and Ceramic:
- Conclusion:
As SMT designs evolve, tighter pitches and smaller components are introduced in electronics. Traditional stencil services can be used for bigger SMD pads but as the innovation goes on nano coated stencils comes to the market. Nano coatings are hydrophobic and oleophobic and repel water, oil and solder paste flux. Some benefits of using these coatings are improved transfer efficiency, reduced need (or frequency) of underside cleaning, and reduced bridging after print.
There are two types of Nano-coatings being used on SMT stencils. The first is the Self Assembled Monolayer (SAM) coating. SAM coatings are manually applied to the underside or board side of the stencil, where the foil contacts the Printed Circuit Board (PCB). The thickness of these coatings are typically 2-4 nanometers and they are invisible. SAM coatings eventually wear off and can be reapplied. The primary benefits of these coatings are reduced underside cleaning and reduced bridging. See the detailed ordering process of nano-coated stencils from here. The other one is ceramic based, lets discuss both of them in detail.
What Are SAM and Ceramic Nano-Coatings?
There are two primary types of nano-coatings used in the PCB industry:
1. Self-Assembled Monolayer (SAM) Coatings:
Self-Assembled Monolayers (SAMs) are molecular coatings consisting of phosphonic acids bonded to the stencil surface. These molecules organize themselves into a manner such as a single-molecule-thick layer on the stencil surface. It bonds chemically with metals like stainless steel and nickel.
- Application: Wipe-on, user-friendly
- Thickness: ~2–4 nm
- Visibility: Invisible, tested via surface energy ink
- Durability: Wears off with time or abrasion
- Reusability: Can be reapplied by user
2. Ceramic Nano-Coatings:
Ceramic nano-coatings are inorganic, spray-applied layers consisting of ceramic particles suspended in a polymer matrix. These coatings are applied by stencil manufacturers using specialized equipment and cured to create a durable anti-adhesive surface.
- Application: Spray-on and cured (by manufacturer)
- Thickness: ~2–4 µm
- Visibility: Colored/UV detectable
- Durability: Excellent abrasion and chemical resistance
- Reusability: Not re-applicable by user
Experimental studies have shown that ceramic nano-coated stencils can improve solder paste transfer efficiency by up to 22% compared to uncoated stencils, especially for small component footprints like 01005 and 0.4 mm BGA. SAM coatings, on the other hand, showed mixed results, sometimes decreasing transfer efficiency for low surface area ratios.
Choosing Between SAM and Ceramic:
Choose SAM if:
- You're producing prototypes or short runs
- You need a quick and affordable coating
- Your stencil has large apertures
Choose Ceramic if:
- You're doing high-volume production
- Your board includes fine-pitch QFNs, BGAs, or 01005s
- Long-term durability and efficiency matter most
Conclusion:
The two types of nanocoatings are self-assembled monolayer (SAM) and ceramic nano-coatings. Each type of coating has specific advantages and there is a significant cost difference in the two coatings. In this article, the impact of these two types of coatings was compared against an uncoated stencil for print solder paste volume, height and area. When comparing the coated stencil data results for print volume in relation to an uncoated stencil, the ceramic nano-coating improved print volume or transfer efficiency on almost all components tested.
The self-assembled monolayer coating, however, showed a decrease in paste height lowering the print height for the 0.4mm pitch CSP component more than 1-mil from the foil thickness. For components larger than 01005, the self-assembled monolayer showed slight improvement over the uncoated stencil and the ceramic nano-coating showed the same or only slightly higher print height than the uncoated stencil. The overall results lead to the conclusion that ceramic nano-coatings should be used to optimize print characteristics when aperture area ratios fall below 0.66. For stencils with all aperture area ratios over 0.66 both ceramic and self-assembled monolayer nano-coatings are beneficial.
Keep Learning
Why PCB Stencil Are Key to High-Quality SMT Assembly
PCB(Printed Circuit Board) stencil is a critical component of Surface Mount Technology (SMT) assembly. It plays a vital role in ensuring the accuracy and consistency of SMT assembly results, which directly affects the functionality and performance of the final product. PCB stencil also called SMT stencil, Circuit Board stencil is used to apply solder paste to the PCB, which is then used to attach SMT components to the board. Without the use of PCB stencil, it becomes challenging to achieve high-qualit......
Nano-Coating vs Electropolishing for SMT Stencils
Key Takeaways Electropolishing improves the underlying metal surface by smoothing aperture walls. Nano-coating adds a low-friction, hydrophobic surface that helps paste release and reduces residue. Both treatments can improve fine-pitch paste release and support more consistent deposits and higher first-pass yield. Nano-coating is especially useful for BGA/QFN assemblies and high-volume runs, where cleaning frequency and paste-release consistency matter more. Electropolishing and nano-coating are comp......
Stencil in PCB: A Comprehensive Guide to PCB Stencil Design, Fabrication, and JLCPCB Solutions
Figures 1 Solder paste application using a stainless steel stencil to achieve high-precision results. In PCB assembly based on Surface-Mount Technology (SMT), precision is a key factor that determines the final quality of electronic products. One critical element that strongly influences soldering accuracy is the stencil. The stencil functions as a physical template that controls the distribution of solder paste onto PCB pads before components are placed. Accurate solder paste application produces rel......
Unlocking the Secrets of Nano-Coated Stencil Manufacturing
Nano-Coated Stencil Manufacturing Process The manufacturing of nano-coated stencils involves a series of precision engineering steps including design and drafting, laser cutting, polishing, nano-coating deposition, and quality inspection. Below is a detailed description of each process stage: 1. Design and Drafting (1) Data Acquisition: Accurate data is obtained from customer-supplied design files (e.g., Gerber files, PCB layouts) or physical product samples. This includes stencil dimensions, pad layo......
The ROI of Nano-Coated Stencils in PCB Assembly Lines
Nano coatings offer several benefits. They are hydrophobic and repel water-based chemistry or flux, and some are also oleophobic and repel oil-based chemistry or flux. When applied to the bottom or board side of the stencil, these coatings will prevent solder paste squeeze-out during the print process between the stencil and PCB from sticking to the bottom of the stencil when the stencil separates from the board. As a result, the next print will be as good as the initial print, and bridging is reduced......
What Are Laser Cut Stencils? A Guide for PCB Assembly
Traditional PCB assembly processes require the manual placement of electronic components before soldering. However, the increasing complexity of electronic printed circuit boards, combined with the need for miniaturisation, necessitates mechanical assembly and solder paste application using SMT stencils. Placing and soldering many small components on a small circuit board is no longer practical.Stencils replace the hand soldering of surface mount components and the inconsistencies caused by hand solde......