Nano-Coatings in PCB Manufacturing: How They Outperform Traditional Stencils
4 min
- Benefits of Nano-coating:
- When to Use Nano-Coated Stencils:
- Types of Nano-Coatings:
- The Science Behind Nano Coating:
- Standard vs Nano-Coated SMT Stencils:
- Conclusion:
Nano coating is a thin hydrophobic (water repellent) and oleophobic (oil repellent) treatment used on the undersides and edges of solder paste stencils. With this the surface becomes non-stick which reduces the number of cleaning cycles required for the solder paste printing process. Upon application, the less than 5 nanometer coating bonds with the stencil foil at the microscopic level, which does not change the size and shape of the stencil.
Nano coating is an industry proven process which shows immediate and measurable improvement from the first print. There are many studies on the nano materials going on which have properties to work with stencils. Nano-coatings work by reducing the surface energy of the stencil material and preventing the solder paste from sticking to unwanted areas. As a result, the printed solder paste deposits are cleaner, more uniform, and more repeatable. This article explores what nano-coating is, the types available, and how it compares to standard SMT stencils in terms of print quality, reliability, and ROI.
Benefits of Nano-coating:
1) Hydrophobic Properties: Nano-coatings repel water-based chemistry (flux), ensuring better performance in environments where moisture could affect stencil efficiency.
2) Oleophobic Properties: By repelling oil-based chemistry (flux), which helps maintain cleanliness and reduces contamination during solder paste application.
3) Improved Transfer Efficiency: Enhance the transfer efficiency, by ensuring precise deposition and reducing defects especially for fine-pitch components
4) Reduced Underside Cleaning Frequency: The combination of ceramic and self-assembled monolayer (SAM) coatings reduces frequent cleaning, saves time and maintenance costs.
When to Use Nano-Coated Stencils:
Nano-coated stencils are ideal for:
- High-density PCB designs with components like 01005, 0201, and fine-pitch BGAs or QFNs
- Aperture area ratios below 0.66
- Environments where print consistency and reduced rework are priorities
- High-volume or automated SMT lines aiming to improve throughput and reduce downtime
Types of Nano-Coatings:
There are two primary types of nano-coatings used in the PCB industry:
1. Self-Assembled Monolayer (SAM) Coatings:
- Thin coating (2–4 nanometers)
- Applied by wiping onto the stencil surface
- Typically clear and invisible
- Easy to reapply by stencil users
- Reduces underside cleaning and bridging
- Less durable, wears off over time with abrasion or cleaning
2. Ceramic Nano-Coatings:
- Thicker coating (2–4 microns)
- Applied by spray and cured using specialized equipment
- Contains colored dye or UV indicator for visibility
- Durable and abrasion-resistant
- Improves transfer efficiency, particularly for area ratios < 0.66
- Cannot be reapplied by users
Experimental studies have shown that ceramic nano-coated stencils can improve solder paste transfer efficiency by up to 22% compared to uncoated stencils, especially for small component footprints like 01005 and 0.4 mm BGA. SAM coatings, on the other hand, showed mixed results, sometimes decreasing transfer efficiency for low surface area ratios.
The Science Behind Nano Coating:
These are also known as nanocoating or nanotechnology coating. It involves applying a liquid polymer containing nanoparticles to the surface of stencils. These nanoparticles are typically composed of materials like silica or titanium dioxide which create an ultra-thin and transparent protective layer. That makes a bond at the nanoscale level which is typically 125 um or 125,000 nanometers.
What sets nano coating apart is its precision and durability is their highly smooth and uniform surface which makes them ideal for intricate stencil designs. They also offer resistance to wear, abrasion, and chemical exposure.
Standard vs Nano-Coated SMT Stencils:
Below is a side-by-side comparison of standard stainless-steel stencils and nano-coated variants:
Conclusion:
Nano-coating technology provides a significant performance upgrade over standard SMT stencils. Factors like ROI and soldering tests will be covered in nano-coated stencil page. Nanocoatings are useful because they reduce cleaning frequency, and improve overall yield. While the upfront cost may be higher, the return on investment especially with ceramic coatings is quickly realized within a few hundred boards. For electronics designers and SMT process engineers aiming for high reliability and precision, nano-coated stencils are a smart, future-forward choice.
Keep Learning
Why PCB Stencil Are Key to High-Quality SMT Assembly
PCB(Printed Circuit Board) stencil is a critical component of Surface Mount Technology (SMT) assembly. It plays a vital role in ensuring the accuracy and consistency of SMT assembly results, which directly affects the functionality and performance of the final product. PCB stencil also called SMT stencil, Circuit Board stencil is used to apply solder paste to the PCB, which is then used to attach SMT components to the board. Without the use of PCB stencil, it becomes challenging to achieve high-qualit......
Nano-Coating vs Electropolishing for SMT Stencils
Key Takeaways Electropolishing improves the underlying metal surface by smoothing aperture walls. Nano-coating adds a low-friction, hydrophobic surface that helps paste release and reduces residue. Both treatments can improve fine-pitch paste release and support more consistent deposits and higher first-pass yield. Nano-coating is especially useful for BGA/QFN assemblies and high-volume runs, where cleaning frequency and paste-release consistency matter more. Electropolishing and nano-coating are comp......
Stencil in PCB: A Comprehensive Guide to PCB Stencil Design, Fabrication, and JLCPCB Solutions
Figures 1 Solder paste application using a stainless steel stencil to achieve high-precision results. In PCB assembly based on Surface-Mount Technology (SMT), precision is a key factor that determines the final quality of electronic products. One critical element that strongly influences soldering accuracy is the stencil. The stencil functions as a physical template that controls the distribution of solder paste onto PCB pads before components are placed. Accurate solder paste application produces rel......
Unlocking the Secrets of Nano-Coated Stencil Manufacturing
Nano-Coated Stencil Manufacturing Process The manufacturing of nano-coated stencils involves a series of precision engineering steps including design and drafting, laser cutting, polishing, nano-coating deposition, and quality inspection. Below is a detailed description of each process stage: 1. Design and Drafting (1) Data Acquisition: Accurate data is obtained from customer-supplied design files (e.g., Gerber files, PCB layouts) or physical product samples. This includes stencil dimensions, pad layo......
The ROI of Nano-Coated Stencils in PCB Assembly Lines
Nano coatings offer several benefits. They are hydrophobic and repel water-based chemistry or flux, and some are also oleophobic and repel oil-based chemistry or flux. When applied to the bottom or board side of the stencil, these coatings will prevent solder paste squeeze-out during the print process between the stencil and PCB from sticking to the bottom of the stencil when the stencil separates from the board. As a result, the next print will be as good as the initial print, and bridging is reduced......
What Are Laser Cut Stencils? A Guide for PCB Assembly
Traditional PCB assembly processes require the manual placement of electronic components before soldering. However, the increasing complexity of electronic printed circuit boards, combined with the need for miniaturisation, necessitates mechanical assembly and solder paste application using SMT stencils. Placing and soldering many small components on a small circuit board is no longer practical.Stencils replace the hand soldering of surface mount components and the inconsistencies caused by hand solde......