This website requires JavaScript.
Coupons
Ship to
Blog

Innovative Uses for Copper Traces in PCB Design

Published Sep 06, 2023, updated Oct 28, 2026

8 min

Table of Contents
  • Choosing the Right Surface Finish for Copper Traces in PCB Design
  • Copper Traces as Capacitors and Inductors: Designing for Efficient PCBs
  • Innovative Uses for Copper Traces in PCB Design
  • Conclusion:

Copper traces are an essential component of printed circuit boards (PCBs), providing the pathways for electric current to flow throughout the board. The surface finish of copper traces plays a crucial role in determining their functionality and reliability. There are several surface finishes available for copper traces, each with its own benefits, and the right choice depends on the intended use of the copper trace. In this article, we will explore the innovative uses of copper traces in PCB design and the surface finishes that can enhance their functionality.


Choosing the Right Surface Finish for Copper Traces in PCB Design

The surface finish of copper traces can have a significant impact on their functionality and reliability. There are several surface finishes available for copper traces, including ENIG, HASL, immersion silver, OSP, and immersion tin. Each surface finish has its own benefits, and the right choice depends on the intended use of the copper trace.
ENIG is a popular surface finish for copper traces that require high reliability and corrosion resistance, making it ideal for aerospace and
industrial electronics applications. HASL is a more affordable option that provides good electrical conductivity but is less reliable than ENIG and can be more prone to corrosion. Immersion silver provides good electrical conductivity and low contact resistance, but it is more prone to oxidation over time. OSP is an inexpensive surface finish that provides good solderability but is less reliable than other finishes and can be more prone to oxidation. Immersion tin provides a uniform surface with excellent solderability, but it is less reliable than other finishes and can be more prone to whisker growth, which can cause short circuits.



Copper Traces as Capacitors and Inductors: Designing for Efficient PCBs

Copper traces

Copper traces can be used as capacitors and inductors, which store electrical energy. By designing the copper trace in a specific shape, it can act as a capacitor or inductor, reducing the need for additional components on the PCB and reducing the overall size and cost of the device. The surface finish chosen for the copper trace depends on its intended use.For copper traces used as capacitors, ENIG is a good surface finish choice, as it provides excellent corrosion resistance and reliability, ensuring optimal functionality over time. For copper traces used as inductors, HASL can be a suitable option, as it is a more affordable choice that can provide adequate resistance to corrosion.


Innovative Uses for Copper Traces in PCB Design

Innovative Uses for Copper Traces in PCB Design

Copper traces are a critical component of PCB design, enabling the flow of electric current throughout the board. The surface finish of copper traces can significantly impact their functionality and reliability, making it essential to choose the right finish for the intended use. Here are some innovative uses for copper traces in PCB design and the surface finishes that can enhance their functionality:


Electromagnetic Compatibility (EMC)
Copper traces can be designed to improve EMC by reducing electromagnetic interference (EMI) and crosstalk. This is particularly important for sensitive electronic devices that require high levels of signal integrity. ENIG is a popular surface finish that can be used for copper traces used to improve EMC, as it provides excellent corrosion resistance and reliability, ensuring the optimal functionality of the copper traces over time.


Microstrip Transmission Lines
Copper traces can be used to create microstrip transmission lines, which are used to transmit high-frequency signals. The thickness and width of the copper trace can be adjusted to achieve the desired impedance. ENIG is a popular surface finish for microstrip transmission lines, as it provides excellent corrosion resistance and reliability, ensuring the optimal functionality of the copper traces over time.


Power Amplifiers
Copper traces can be used in power amplifiers to help distribute power and control the output level. ENIG is a surface finish that can be used for copper traces used in power amplifiers, as it provides excellent corrosion resistance and reliability, ensuring the optimal functionality of the copper traces over time.


High-Frequency Circuits
Copper traces can be designed to improve the performance of high-frequency circuits, such as those used in radar and communication systems. Immersion silver is a surface finish that can be used for copper traces used in high-frequency circuits, providing good electrical conductivity and low contact resistance.


Shielding
Copper traces can be used to create shields that protect sensitive components from electromagnetic interference. These shields can be designed in a specific pattern to block certain frequencies while allowing others to pass through. ENIG is a surface finish that can be used for copper traces used in shielding, as it provides excellent corrosion resistance and reliability, ensuring the optimal functionality of the copper traces over time.


Radio Frequency Identification (RFID)
Copper traces can be used in RFID tags to store and transmit data wirelessly. The surface finish chosen for the copper trace depends on the intended use of the RFID tag. Immersion silver is a surface finish that can be used for copper traces used in RFID tags, providing good electrical conductivity and low contact resistance.


MEMS Devices
Copper traces can be used in microelectromechanical systems (MEMS) devices, which combine mechanical and electronic components on a single chip. The surface finish chosen for the copper trace depends on the specific requirements of the MEMS device. ENIG is a surface finish that can be used for copper traces used in MEMS devices, as it provides excellent corrosion resistance and reliability, ensuring the optimal functionality of the copper traces over time.


Solar Panels
Copper traces can be used in solar panels to help distribute power and control the output level. The surface finish chosen for the copper trace depends on the specific requirements of the solar panel. HASL is a surface finish that can be used for copper traces used in solar panels, as it provides adequate resistance to corrosion.


Heatsinks
Copper traces can be designed in a specific pattern to dissipate heat from hot spots on the PCB. ENIG is a popular surface finish for copper traces used in heatsinks, as it provides excellent corrosion resistance and reliability, ensuring the optimal functionality of the copper traces over time.


Antennas
Copper traces can be used as antennas for wireless communication, such as Bluetooth or Wi-Fi. Immersion silver is a surface finish that can be used for copper traces used as antennas, providing good electrical conductivity and low contact resistance.

Signal Integrity
Copper traces can be designed to improve signal integrity by reducing electromagnetic interference (EMI) and crosstalk. ENIG is a surface finish that can be used for copper traces used to improve signal integrity, as it provides excellent corrosion resistance and reliability, ensuring the optimal functionality of the copper traces over time.


Flexible PCBs
Copper traces can be used in
flexible PCBs, which are designed to bend and flex without cracking or breaking. ENIG is a popular surface finish for copper traces used in flexible PCBs, as it provides excellent corrosion resistance and reliability, ensuring the optimal functionality of the copper traces over time.


LED Lighting
Copper traces can be used in LED lighting to help distribute power and control the brightness of the LEDs. HASL is a surface finish that can be used for copper traces used in LED lighting, as it provides adequate resistance to corrosion.


Touch Panels
Copper traces can be used in touch panels to help detect touch inputs. ENIG is a surface finish that can be used for copper traces used in touch panels, as it provides excellent corrosion resistance and reliability, ensuring the optimal functionality of the copper traces over time.


Power Distribution

Copper traces can be used to distribute power across the PCB, ensuring that each component receives the correct amount of power. Immersion silver is a surface finish that can be used for copper traces used in power distribution, providing good electrical conductivity and low contact resistance.


Conclusion:

Copper traces are a versatile component in PCB design, capable of serving different purposes beyond just electrical conductivity. By choosing the right surface finish, engineers can optimize the functionality and reliability of copper traces for specific applications. From heatsinks to capacitors and inductors, copper traces can be designed in a range of innovative ways, reducing the need for additional components and enhancing the performance of electronic devices. JLCPCB offers a range of surface finishes, including ENIG, HASL, immersion silver, OSP, and immersion tin, ensuring the optimal performance of your copper traces. Our high-quality PCB fabrication and assembly services ensure that our customers receive PCBs that meet their exact specifications. With fast turnaround times, high-quality manufacturing standards, and competitive pricing, JLCPCB is a reliable partner for all your PCB design needs.

GET FREE QUOTE>>


Keep Learning