This website requires JavaScript.
Coupons
Ship to
Blog

Flex PCB Manufacturing Process & Advantages

Published Mar 31, 2023, updated Oct 28, 2026

7 min

Table of Contents
  • Flex Circuit Design:
  • Material selection:
  • Material preparation:
  • Circuit printing:
  • Component placement:
  • Soldering:
  • Testing:
  • Stiffener attachment:
  • Advantages of Flex PCBs
JLCPCB flexible PCB prototype starting at $2 with $20 off

In today's fast-paced and technologically advanced world, printed circuit boards (PCBs) have become an integral part of many electronic devices. However, with the increasing demand for smaller and more flexible electronic devices, the traditional rigid PCBs are proving to be less efficient. This is where Flexible Printed Circuit Boards (Flex PCBs) come in, providing much-needed flexibility while maintaining the same level of functionality as rigid PCBs.

For new users, JLCPCB also prepared up to $70 registration coupons. Never let high development costs limit your creativity.

In this article, we will delve into the manufacturing process of Flex PCBs, from design to production, and explore the various techniques used to produce these innovative circuit boards.

Further Read: Flex PCB Assembly Guide: Process, Challenges, and Solutions

As for several PCB manufacturing, including the JLCPCB Flex PCB manufacturing process, the following steps are the fundamental ones to achieve a successful Flex PCB:

Flex Circuit Design:

The first step is to design the flexible PCB using computer-aided design (CAD) software. The design will include the layout of the circuit, the placement of components, and any specific requirements for the flexing or bending of the PCB.

Material selection:

The next step is to select the appropriate substrate material for the flexible PCB. The most common materials used are polyimide (PI) and polyester (PET) films. These materials have good electrical insulation properties, high-temperature resistance, and are flexible.

Conductive material: This material is used to create electrical pathways on the Flex PCB. Copper is the most commonly used conductive material due to its excellent conductivity, flexibility, and durability.

Adhesive material: This material is used to bond the various layers of the Flex PCB together. The adhesive material is typically made of epoxy, acrylic, or silicone.

Coverlay material: This material is used to protect the conductive material on the Flex PCB from environmental factors such as moisture, dust, and physical damage. Polyimide and polyester are the most commonly used Coverlay materials.

Solder mask material: This material is used to protect the conductive traces on the Flex PCB during the soldering process. The solder mask material is typically made of epoxy or photo-imageable materials.

In addition to these materials, there are other components used in the manufacturing process of Flex PCBs, such as stiffeners, connectors, and component attachment adhesives. The specific materials used depend on the design and application of the Flex PCB.

Material preparation:

The substrate material is then prepared by cleaning and etching the surface to create a clean, smooth surface for the circuit to be printed on.

Circuit printing:

The photolithography process is a critical step in the manufacturing of Flexible PCB. The process involves transferring the circuit pattern from a designed layout to the substrate material using photoresist and etching.

After getting the materials prepared the first step is the photoresist application, a photoresist material is applied to the substrate surface. The photoresist is a light-sensitive material that hardens when exposed to ultraviolet (UV) light. There are two types of photoresist materials used in Flex PCB manufacturing: positive and negative photoresists. After that it comes the photomask alignment, a photomask is placed over the substrate, and UV light is shone through the mask, exposing the photoresist material in the desired pattern. The photomask contains the circuit pattern to be printed on the substrate. Alignment of the photomask is crucial to ensure accurate placement of the circuit pattern on the substrate.

After exposure to UV light, the substrate is developed to remove the photoresist material that was not exposed to UV light. The development process removes the soft, unexposed photoresist material, leaving only the hardened photoresist that corresponds to the circuit pattern. The next step is the etching process which involves removing the copper in areas not protected by the hardened photoresist. This is done using an etchant solution that dissolves the exposed copper, leaving only the desired copper pattern on the substrate.

UV Exposure

Etching

After getting the circuit transferred to the substrate material, the remaining photoresist material is removed from the substrate using a solvent that dissolves the photoresist, leaving only the printed circuit pattern on the substrate.

Component placement:

Once the circuit pattern is printed, the components are placed onto the PCB. Components can be mounted using surface mount technology (SMT) or through-hole technology.

Soldering:

The components are then soldered onto the PCB using either reflow soldering or wave soldering techniques.

Testing:

Testing is a very important step in the manufacturing process of Flexible Printed Circuit Boards. The purpose of testing is to ensure that the Flex PCB meets the required electrical and mechanical specifications and is free from defects.

Flex PCB Testing

Here are some of the commonly used testing methods in Flex PCB manufacturing:

Electrical testing: This involves checking the electrical connectivity of the Flex PCB. The Flex PCB is connected to a test fixture that applies a voltage to the circuit and measures the current flow. Any breaks or shorts in the circuit are detected, and the electrical characteristics of the Flex PCB are measured, including resistance, capacitance, and impedance.

Visual inspection: This involves inspecting the Flex PCB visually to detect any defects such as cracks, scratches, delamination, or misalignments. The inspection is done under a microscope or a magnifying glass to ensure that the Flex PCB meets the required mechanical specifications.

Environmental testing: This involves subjecting the Flex PCB to various environmental conditions such as temperature, humidity, and vibration. The Flex PCB is tested to ensure that it can withstand the expected environmental conditions and perform reliably under these conditions.

Functional testing: This involves testing the Flex PCB to ensure that it performs the intended function. The Flex PCB is connected to a test fixture that simulates the intended application, and its performance is evaluated against the expected specifications.

X-ray inspection: This involves using X-rays to inspect the internal layers of the Flex PCB for any defects such as voids or delamination. X-ray inspection is particularly useful for detecting defects in the solder joints and other hidden areas of the Flex PCB.

Stiffener attachment:

Finally, a stiffener is attached to the flexible PCB to provide support and protection during handling and use. The stiffener can be made from materials such as FR4 or steel, and is typically attached using an adhesive.

Attach Stiffener

Different stiffeners

The stiffener is an important component of the flexible PCB because it provides support and protection to the PCB during handling and use. The stiffener prevents the PCB from bending or flexing beyond its designed limits, which can cause damage to the circuit or components. It also helps to prevent the PCB from cracking or breaking due to stress on the circuit during flexing or bending.

Advantages of Flex PCBs

Flex PCBs offer several advantages over traditional rigid circuit boards. Some of these advantages include:

1. Flexibility

As the name suggests, Flex PCBs are flexible and can bend, twist and flex without damaging the electrical connections on the board. This makes them ideal for applications that require bending or twisting, such as wearable devices or automotive sensors.

2. Space Saving

Flex PCBs can be designed to fit into tight spaces that rigid circuit boards cannot. This allows for smaller and more compact devices.

3. Durability

Flex PCBs are designed to withstand harsh environments, such as extreme temperatures and vibrations. This makes them ideal for applications in the aerospace, industrial automation, and automotive industries.

4. Cost-effective

Flex PCBs can reduce the cost of product development by eliminating the need for connectors and cables. This simplifies the manufacturing process and reduces the number of components required.

Having high-quality PCBs is crucial to bring your excellent PCB designs to life. JLCPCB is committed to ensuring top-notch production standards by investing in cutting-edge equipment and collaborating with leading raw material suppliers from around the world. Additionally, JLCPCB has five intelligent production bases that are self-owned. By leveraging economies of scale, JLCPCB is able to lower production costs and pass on the savings to customers, removing the price barrier to hardware innovation as much as possible. Moreover, JLCPCB offers up to $54 registered coupons for every new user. Sign up and upload your Gerber files here and start ordering premium flex PCBs!

Keep Learning