Low-Temperature Solder Paste: A Practical Sn-Bi Guide
12 min
- Quick Answer: What Is Low-Temperature Solder Paste?
- Low-Temp Alloys and Temperatures
- Why Use Low-Temperature Solder Paste?
- The Trade-offs: When NOT to Use It
- The Low-Temperature Reflow Profile (Sn-Bi)
- Printing Low-Temp Paste: Stencil Considerations
- Common Problems With Low-Temp Solder and Fixes
- FAQ about Low-Temperature Solder Paste
- Conclusion: Use Low-Temp Paste Where It Fits
Key Takeaways
Sn42Bi58 is the mainstream low-temp alloy and melts at 138 C.
Typical reflow peak is 165 to 180 C, about 25 to 30 C above the melt.
It protects heat-sensitive components and reduces warpage on large, thin boards.
It enables step soldering, because 165 to 180 C will not remelt SAC305 joints.
Bismuth joints are more brittle than SAC305, so avoid drop-critical products.
Never mix Sn-Bi with leaded (Sn-Pb) solder. Bi, Sn and Pb form a ternary eutectic that melts near 95 C.
Some parts and some boards simply cannot survive a standard lead-free reflow. SAC305 peaks somewhere around 230 to 250 C, and that is enough to cook heat-sensitive LEDs, melt plastic connectors, drift sensors, or warp a large thin board until the corners lift.
Low-temperature solder paste exists for exactly those cases. It is a lead-free paste, usually tin-bismuth, that melts at 138 C and reflows with a peak near 165 to 180 C, roughly 70 to 80 C cooler than a SAC305 profile.
This guide covers what the alloys actually are, the real temperatures, when low-temp paste is the right call and when it is a bad one, how the reflow profile is shaped, and how to print it.
For the full range of solder alloys and melting points, see our solder alloy guide. Here we focus on Sn-Bi.
Quick Answer: What Is Low-Temperature Solder Paste?
Low-temperature solder paste is a lead-free paste, usually tin-bismuth (Sn-Bi), that melts at about 138 C and reflows with a peak near 165 to 180 C, far below the 230 to 250 C peak a SAC305 profile needs. It protects heat-sensitive parts and thin boards and enables step soldering, but bismuth joints are more brittle.
Low-Temp Alloys and Temperatures
The table below sets the low-temperature alloys against the two baselines most engineers already know. Note that SAC305 is near-eutectic rather than eutectic, so it melts across a range, and note that not every Sn-Bi-Ag alloy is a low-temperature paste.
| Alloy | Melting Point or Range | Typical Reflow Peak | Notes |
|---|---|---|---|
| SAC305 (Sn96.5Ag3Cu0.5) | 217 C solidus to 220 C liquidus | ~230-250 C | The standard lead-free baseline |
| Sn63Pb37 | 183 C (eutectic) | ~210-220 C | Leaded eutectic, for reference only. Never mix with Sn-Bi |
| Sn42Bi58 | 138 C (eutectic) | ~165-180 C | The mainstream low-temp choice |
| Sn-Bi-Ag, near-eutectic (e.g. Sn42Bi57.6Ag0.4) | ~137-142 C | ~165-180 C | A small Ag addition improves wetting |
| Sn-Bi-Ag, off-eutectic (e.g. Sn64Bi35Ag1) | ~138-176 C, a wide pasty range | Higher, follow the datasheet | Not a drop-in low-temp paste |
| Sn-Bi-In | Lower than Sn-Bi | Lower | Indium drops the melt further but adds cost and softness. Niche |
Two rows in that table are worth pausing on, because they are where most confusion starts.
First, silver is not a simple upgrade. A small addition of around 0.5% Ag improves wetting and refines the microstructure, but published work shows that above roughly 1 wt% Ag the Ag3Sn phase grows and ductility actually falls. More silver is not better.
Second, the bismuth content decides everything. Sn-Bi is eutectic near 57 to 58% Bi, which is why Sn42Bi58 melts cleanly at a single temperature. An alloy like Sn64Bi35Ag1 sits far off that eutectic, so it starts softening near 138 C but is not fully liquid until roughly 176 C. That wide pasty range makes it a different tool, not a cooler one.
All of these are lead-free. Bismuth is not a restricted substance under RoHS, so Sn-Bi pastes are RoHS and REACH compatible in the same way SAC305 is.
Why Use Low-Temperature Solder Paste?
It protects heat-sensitive components. LEDs, plastic-bodied connectors, some sensors, cameras, displays and certain electrolytic capacitors have maximum body temperatures well under a 245 C peak. Dropping the peak to 175 C keeps them inside their rating instead of hoping they survive.
It reduces warpage and delamination. Large, thin, or high-density boards bow when heated, because copper, laminate and components expand at different rates. Lower peak temperature means less thermal stress, less bow and twist, and fewer opens on the corners of big BGAs.
It enables step soldering and package-on-package. Solder the first side with SAC305, then run the second side with Sn-Bi at 165 to 180 C. Because that peak sits nearly 40 C below the 217 C point where SAC305 even begins to melt, the first-side joints stay solid and do not slump.
It costs less energy and eases nearby rework. A cooler oven draws less power, and lower heat around a repair site is gentler on neighbouring parts. Low-temp paste is common on LED boards and flex assemblies, and it pairs naturally with the thermal behaviour discussed in our metal-core PCB guide.
The Trade-offs: When NOT to Use It
Low-temperature paste is a real engineering trade, not a free upgrade. These are the reasons to walk away from it.
Never mix Sn-Bi with leaded (Sn-Pb) solder. This is the single most important line in this article. Bismuth, tin and lead together form a ternary eutectic measured by NIST at 95.3 +/- 0.5 C. A joint contaminated that way can soften or fail at temperatures a product might genuinely reach in service. Keep leaded and Sn-Bi pastes, stencils, squeegees and rework tools strictly separate.
That hazard is not only about leaded paste. A leaded HASL surface finish is also a lead source, so check the board finish and component terminations before committing to a low-temp build.
Bismuth joints are more brittle. Eutectic Sn-Bi has a microstructure of ductile beta-Sn mixed with a genuinely brittle bismuth phase, and that shows up as poorer drop, shock and mechanical-stress performance than SAC305. A small silver addition helps, but it does not turn Sn-Bi into a rugged alloy. Avoid it on handhelds, wearables, automotive and anything drop-critical unless the design has been qualified for it.
Compatibility is not automatic. Not every component finish or board finish behaves well with a low-temp alloy, and Sn-Bi can be oxidation-prone, which puts more weight on flux chemistry and on paste storage and handling.
Voiding and material control. Large low-standoff parts such as DPAK can trap outgassing under the tab and void. And because low-temp paste is not the default material in most shops, it needs real inventory discipline so it never gets mixed up with the standard reel of SAC305.
The short decision rule: excellent for heat-sensitive assemblies, thin warping boards and step soldering. Avoid it where mechanical robustness is the priority.
The Low-Temperature Reflow Profile (Sn-Bi)
The shape of a low-temp profile is the same as any reflow curve. Only the numbers move down. Treat the following as typical and always follow the profile on your paste datasheet.
Preheat runs from room temperature to roughly 90 to 110 C, ramping at about 1 to 3 C per second. A soak follows, holding long enough to activate the flux and even out the board temperature before the alloy melts.
The peak sits around 165 to 180 C. The useful way to think about that number is that a reflow peak generally lands 25 to 30 C above the alloy's melting point, and 138 plus 25 to 30 puts you in exactly that window. Time above liquidus is short, usually well under a minute, and cooling is controlled rather than abrupt.
Set against a SAC305 curve, the whole profile drops by roughly 70 to 80 C at the peak. That gap is the entire point of the alloy, and it is what keeps first-side SAC305 joints solid during a second-side low-temp pass.
Do not overcorrect downward. Too low a peak, or too short a time above liquidus, leaves incomplete reflow and dull, grainy joints, because the flux never fully activates in the lower window. Our reflow soldering guide covers profile setup in more depth.
Printing Low-Temp Paste: Stencil Considerations
The stencil rules do not change with the alloy. Match foil thickness and aperture size to the finest pitch on the board and keep the area ratio at or above 0.66, exactly as you would for SAC305. What changes is the tolerance for error, because a low-temp joint has less thermal headroom to pull a marginal deposit into shape.
Sn-Bi paste can also be oxidation-prone, so clean release and crisp print definition matter. Electropolished and nano-coated apertures improve paste release, and our comparison of nano-coating and electropolishing explains when each is worth specifying.
Handle the material properly too. Paste storage, warm-up and working life all affect printability, and our guide on how to use solder paste covers the handling side.
Stencil selection itself is covered in how to choose a solder paste stencil, and the foils themselves come off our precision stencil manufacturingline.
Common Problems With Low-Temp Solder and Fixes
- Brittle or cracked joints - bismuth brittleness under mechanical stress - move to an Ag-bearing Sn-Bi, reduce mechanical stress at the joint, and avoid drop-critical use.
- Voiding under large low-standoff parts - trapped outgassing with nowhere to escape - tune the soak, and use window-pane apertures instead of one large opening.
- Poor wetting or dull, grainy joints - oxidation or weak flux activation - use fresh paste, the right flux chemistry, and confirm the peak is genuinely reaching target.
- Very low remelt or unexpectedly soft joints - accidental mixing with leaded solder - never mix, and segregate materials and tools.
- Incomplete reflow - peak too low or time above liquidus too short - raise the peak toward about 175 C and extend time above liquidus slightly.
Our guide to preventing solder defects during reflow works through the diagnosis process in more detail.
FAQ about Low-Temperature Solder Paste
Q: Is Low-Temperature Solder Paste RoHS Compliant?
Yes. Bismuth is not a restricted substance under RoHS, so Sn-Bi pastes are lead-free and RoHS compatible in the same way SAC305 is. The compliance question that actually matters with Sn-Bi is not the paste itself but contamination: keep it away from leaded solder and leaded board finishes, both for compliance and for the low-melting-phase risk.
Q: Can I Use Low-Temp Paste With a Regular Reflow Oven?
Yes. No special equipment is needed, since you are asking the oven for less heat, not more. You do need a separate profile stored and verified for the low-temp alloy, and you need process discipline so a board never runs on the wrong recipe. Profile with thermocouples on the actual assembly rather than trusting the oven setpoint.
Q: How Strong Is Sn-Bi Compared to SAC305?
Sn-Bi is generally stronger in tensile terms but noticeably less ductile, which is the trade that matters in practice. Its microstructure contains a brittle bismuth phase, so it absorbs less energy before cracking under drop, shock or bending. For static, low-stress assemblies this is rarely an issue. For anything that gets dropped or flexed, SAC305 remains the safer choice.
Q: Does Low-Temp Paste Have a Shorter Shelf Life?
Not inherently, but it is less forgiving of poor handling. Sn-Bi can be oxidation-prone, so refrigerated storage, full warm-up to room temperature before opening, and respecting the stencil life on the printer all matter more than they might with SAC305. Always follow the paste maker's stated storage conditions rather than a general rule.
Q: Can I Rework a Low-Temperature Joint?
Yes, and rework is usually easier because the alloy releases at a much lower temperature, which is gentler on neighbouring parts. The catch is tool contamination. Use a dedicated tip, wick and wire for Sn-Bi work, because touching the joint with leaded solder introduces exactly the low-melting mixture you are trying to avoid.
Q: Is Low-Temp Paste Cheaper Than SAC305?
Not usually on a per-jar basis, since bismuth pricing and lower production volumes often make it comparable or more expensive. The savings show up elsewhere: lower oven energy, less scrap from warped boards, and the ability to use cheaper heat-sensitive components that could not survive a 245 C peak. Judge it on total assembly cost, not paste price.
Conclusion: Use Low-Temp Paste Where It Fits
Sn-Bi low-temperature paste reflows roughly 70 to 80 C cooler than SAC305, which makes it a genuinely good answer for heat-sensitive components, thin boards that warp, and step or sequential soldering.
The conditions attached to it are just as real. Bismuth joints are more brittle, so keep it away from drop-critical products, and never let it meet leaded solder, because the resulting ternary eutectic melts near 95 C.
Match the alloy to the board, print it through a clean and consistent stencil, and profile it properly. Or hand the whole job to an assembly partner and let them run it.
Keep Learning
Manual Pick and Place: A Cost-Effective SMT Alternative
Key Takeaways for Manual Pick and Place Manual pick and place uses a hand-held vacuum wand and positioning stage to place SMD components by hand, replacing tweezers in prototype assembly. It is most cost-effective for production runs of 1 to 50 boards, where an automated SMT pick-and-place machine cannot justify its $10,000+ setup cost. A complete manual workstation runs $300 to $500, compared with $10,000+ for an entry-level automated pick and place machine. SMT stencil quality is the single largest ......
Low-Temperature Solder Paste: A Practical Sn-Bi Guide
Key Takeaways Sn42Bi58 is the mainstream low-temp alloy and melts at 138 C. Typical reflow peak is 165 to 180 C, about 25 to 30 C above the melt. It protects heat-sensitive components and reduces warpage on large, thin boards. It enables step soldering, because 165 to 180 C will not remelt SAC305 joints. Bismuth joints are more brittle than SAC305, so avoid drop-critical products. Never mix Sn-Bi with leaded (Sn-Pb) solder. Bi, Sn and Pb form a ternary eutectic that melts near 95 C. Some parts and som......
Pin-in-Paste: Through-Hole Reflow With a Stencil
Key Takeaways One Reflow Process: Pin-in-paste combines SMT and through-hole soldering into a single reflow pass, eliminating the need for separate wave, selective, or hand-soldering steps when the board has only a few through-hole components. Paste Volume Is Critical: Solder paste is roughly 50% flux by volume, so you need to print about twice the solder volume the finished joint requires. Stencil design—overprint apertures and step-up zones—makes or breaks the process. Target 75% Barrel Fill: Per IP......
Mixed Technology PCB Assembly: Combining SMT and THT on One Board
As technologies become increasingly more complex, the demand for sophisticated printed circuit boards continues to rise. In the electronics industry, the two most prevalent PCB Assembly technologies are SMT and THT, which differ mainly in the manner at which the components are attached. SMT places the components on the surface of the board whereas THT makes use of drilled holes to solder components. While these technologies individually cater to specific applications, advancements in the electronics i......
Moisture Sensitivity Level (MSL): Baking Guide
Key Takeaways Moisture Sensitivity Level (MSL) is a 1-6 classification under IPC/JEDEC J-STD-020 that indicates how quickly a non-hermetic surface-mount package can absorb enough moisture to become vulnerable during reflow. MSL 1 has unlimited floor life at its reference condition, while MSL 6 requires baking before use and reflow within the time printed on the caution label. The floor-life clock begins when the moisture barrier bag is opened and exposure to factory air starts. Baking according to IPC......
Understanding SMT Stencil Printers for Accurate PCB Solder Paste Printing
Stencil printing is a critical process in SMT (Surface Mount Technology) assembly, significantly impacting the quality and reliability of solder joints on PCBs. The crucial machine for implementing this is the SMT Stencil Printer, which applies an appropriate measure of solder paste to each pad of the PCB board before it goes to the placement of components. For those of you looking to work out what a stencil printer is and why it matters in manufacturing, you've come to the right place. This is the ba......