Understanding Electrical Schematics: A Comprehensive Guide
13 min
- What is an Electrical Schematic?
- Understanding the Basics of a Circuit
- Ways to Represent a Circuit Graphically
- How to Read a Simple Circuit
- How to Design a Professional Looking Schematic Diagram
- Bridge to Manufacturing: Transforming Schematics into JLCPCB PCBs
- Troubleshooting with Schematics
- FAQ about Electrical Schematics
- Conclusion
Key Takeaways
- Schematics vs. Block Diagrams: Schematics detail exact components and connections; block diagrams only show high-level functions.
- Mark Polarity: Essential to prevent circuit failure and automated SMT placement errors at JLCPCB.
- Clean Layout: Use modular blocks and net labels (VIN, GND) to eliminate visual clutter.
- Manufacturing Ready: Follow DFM trace rules and export standard Gerber, BOM (LCSC C-IDs), and CPL files.
- Fast Troubleshooting: Isolate schematic blocks to test expected voltages and locate faulty components quickly.
Electrical schematics are essential for understanding and troubleshooting electrical systems. Whether you're an electrician or an engineering student, learning to read schematics is a valuable skill.
What is an Electrical Schematic?
An electrical schematic is a graphical representation of an electrical circuit, using standardized symbols to depict components and their connections. Schematics convey the circuit's design and function, making it easier to understand how it operates
Symbols are the foundation of circuit diagrams, enabling engineers, electricians, and technicians to understand circuit functions without documentation. These symbols are standardized internationally, allowing schematics to be interpreted across languages and regions.
Key elements typically found in an electric schematic include
1. Symbols: Standardized symbols are used to represent components such as resistors, capacitors, diodes, transistors, power sources, and more. A fully detailed article about various symbols and the design physics behind them is attached here.
2. Lines: Lines represent the electrical connections or wires between components. They illustrate how components are connected electrically in the circuit.
3. Nodes : are points where two or more components or wires are connected. They are often represented by dots or junctions, as shown in the figure above.
4. Labels and Annotations: These provide additional information, such as component values (e.g., resistance in ohms, capacitance in farads), part numbers, or specific notes about the circuit's operation.
5. Power and Ground: Symbols indicating the power supply and ground connection points are usually included to show where the circuit connects to its power source.
Electric schematics are essential tools for engineers, technicians, and hobbyists as they provide a clear and concise way to understand and analyze the operation of an electrical circuit. They are used in designing, building, and troubleshooting electrical systems.
Understanding the Basics of a Circuit
Reading a circuit schematic requires a solid understanding of various concepts and components. Here’s a comprehensive guide to the knowledge required.
Basic Electrical Concepts: Ohm's Law states that the current (I: the flow of electric charge) flowing through a conductor between two points is directly proportional to the voltage (V: the potential difference between two points) across the two points and inversely proportional to the resistance (R: the opposition to the flow of current). It is expressed by the formula (V = IR).
Components Working Principle: Various schematic symbols are used to represent actual devices or wires in a circuit. It is crucial to have the expertise to interpret these electrical diagrams accurately, as misinterpretation can lead to errors. Resistors limit current flow and divide voltages according to Ohm’s Law (V = IR). Capacitors store electrical energy and are widely used for decoupling power supply noise, bypassing high-frequency interference, and blocking DC signals while allowing AC signals to pass. When selecting capacitors for JLCPCB SMT assembly, multi-layer ceramic capacitors (MLCCs) in 0603 or 0805 packages are recommended due to lower costs and higher library availability.
Series and Parallel Circuits: Understanding the behavior of components in series and parallel arrangements.
Reading Circuit Flow: Identifying where signals enter and exit the circuit, and understanding how the current flows through the circuit helps in determining the circuit's operation.
Familiarization with SI units: Every scientific discipline relies on a standard chart for SI units, which are universally recognized. Unfortunately, many electricians overlook the significance of these units. It is essential for every electrical technician to be able to interpret this chart. Doing so is advantageous for comprehending the measurement units of various electrical quantities. The SI unit for resistance is ohms, for capacitance is farads, and for inductance is henrys.
The Polarity: Some circuits have polarity. They carry a positive charge and a negative charge. Understanding polarity is important. You should always follow the law of ‘like charges repel’ and ‘unlike charges attract’. So, negative to positive and vice versa. Many electronic components are polarized and must be oriented correctly in the schematic and PCB layout. Polarized components include diodes, LEDs, electrolytic capacitors, tantalum capacitors, and ICs. Non-polarized components include ceramic capacitors (MLCC) and standard resistors. For SMT assembly at JLCPCB, explicitly marking Pin 1 or Cathode polarity in silkscreen/courtyard is crucial to avoid orientation errors during automated pick-and-place assembly.
Practical Application: Using component datasheets for detailed specifications. Employing tools like multimeters to verify circuit behaviour helps in designing as well as in troubleshooting.
By mastering these concepts, you can effectively read and understand circuit schematics, allowing you to build, troubleshoot, and design electronic circuits.
Ways to Represent a Circuit Graphically
There are two methods to represent a circuit: one with the help of a block diagram and the other with a schematic diagram. Both have their advantages and disadvantages. In a schematic diagram, all the circuit components, their connections, and arrangement are shown clearly, but in the block diagram method, the internal circuit is unknown. Block diagrams help in understanding the function of a circuit in a general, not in a specific manner.
Block diagram:
Engineers and technicians utilize block diagrams in various applications. Typically, block diagrams illustrate the connections between small circuits within a larger device or between different devices in a complex system. Block diagrams are also known as functional diagrams as they showcase the fundamental operation of the electronic circuit. The functional diagram provides a basic explanation of the device's functionality, serving as a precursor to the more detailed information presented in a schematic diagram.
Schematic diagram:
Let’s open the audio amplifier block of the above-given block diagram and see what’s inside. According to standard schematic drawing practice, every component should bear a unique alphanumeric label to designate it. The components are identified solely by their schematic symbols along with value designations or industry-standard part designations.
Using the example provided, we know that the transistor is a 2N2222 type, and that the resistors have values of 470, 33k (33,000), 330k (330,000), and 680 ohms. The input capacitor has a value of 0.01 microfarad (μF) and the output capacitor has a value of 0.1 μF. The emitter capacitor, which is connected across the 470-ohm resistor, has a value of 4.7 μF. This is just one component of the block diagram mentioned above. Block diagrams are generally abstract and are used to simplify actual circuit connections.
How to Read a Simple Circuit
Let me briefly explain the purpose of the circuit shown above. It is an amplifier circuit in a voltage divider common emitter configuration. The amplification of the circuit is determined by the resistors within it, and can be calculated using design formulas provided in a book or datasheet.
By reading the circuit from left to right, the input signal is given to C2, which acts as a decoupling capacitor, allowing only the AC signal to pass through for amplification. R3 and R2 set the bias point of the transistor, placing it in the active amplification region. R1 and C1 serve as feedback resistor and bypassing capacitors, providing stability to the circuit. The transistor collector acts as the output, amplifying the signal with some gain. R4 is the loading resistance connected for loading. Finally, C3 is used to produce AC amplified output.
How to Read and Interpret a Schematic Diagram
Schematics may contain multiple circuit blocks, read from left to right or top to bottom. Circuits often have repetitive patterns. Once you understand the basic symbols and their functions, you can recognize these patterns, simplifying the interpretation of complex schematics.
It is divided into 4 sections, every section is labelled properly as per its application. This circuit is for the charging purposes of a 3.7 lithium ion battery with a 1.5 ampere of max current rating.
Section 1: Input
A 2 PIN Connector is connected to 2 different capacitors, this connector is used to connect the battery charge to the external power supply unit. VIN net label is used to connect one block with another without wiring it. In this way a clean schematic can be designed which is easy to read, modify and saves overall time.
Section 2: Main IC
It is a 17 pin IC, all the connections can be made as per given in the datasheet of IC, 2 LEDs are used for charge indication purpose. The grounding, net labels and wires can be properly seen. Mostly while designing a big circuit it is recommended to divide the whole circuit in these types of small blocks and use net labels for connections.
Section 3: Charge Control
The charge control circuit is used to control the IC, designed as per the values and connections given in the datasheet of IC. Inductor and capacitor with diode here acts as buck conversion. Other capacitors are used to keep the output voltage stable, and R10_CC_CTRL resistor to set the max current to 1.5Ampere.
Section 4: Output
Two connectors are used in this section: one serves as the output terminal connected to the battery for charging, and the second is a jumper interface used to select between 1S and 2S battery cell configurations (single-cell or dual-cell) by setting the CS/VREG pins. When designing battery charging circuits based on ICs like TP5100, ensure trace widths on the PCB are sufficiently wide (minimum 20–30 mil per Ampere) to handle continuous high charge currents (e.g., 1.5A) without excessive temperature rise.
Sometimes more than one input and output capacitors of different values are used, because of the power supply noise issues. These capacitors bypass any noise to ground and make the circuit EMI(electromagnetic noise) free.
How to Design a Professional Looking Schematic Diagram
Wires are the heroes of a schematic diagram, because wires are used to connect components together. Readability and reproducibility of a clean and properly labelled circuit is more than a random circuit. Some key aspects of wires and connections in schematics:
Organization: Organize wires logically and label them appropriately to indicate their functions, ensuring that electric current follows the intended paths.
Colours: In some electronic schematics, wires may have colour codes representing specific attributes. Such as power, ground, or signal connections, aiding in quick identification.
Terminations: Connections between wires and components, often represented by dots or junctions, are vital points in the circuit where current joins or divides.
Net label Routing: It identifies and names specific electrical connections or nodes, simplifying the diagram by reducing the number of drawn wires. It helps in clearly indicating which points are electrically connected without visually cluttering the schematic.
Bridge to Manufacturing: Transforming Schematics into JLCPCB PCBs
Translating an electrical schematic into a functional physical printed circuit board (PCB) requires strict adherence to Design for Manufacturing (DFM) guidelines. JLCPCB offers standard 1-60 layer PCB fabrication and SMT assembly services.
Key Design Rules & Capabilities for JLCPCB Fabrication:
| Process Parameter | Standard Capability (1/2-Layer) | Advanced / High-Precision Capability |
|---|---|---|
| Min Trace Width / Clearance | 5/5 mil (0.127mm) | 3.5/3.5 mil (0.09mm) |
| Min Via Hole Size / Diameter | 0.3mm / 0.5mm | 0.15mm / 0.25mm (Laser/Via-in-Pad) |
| Board Thickness Range | 0.4mm - 2.0mm | 0.2mm - 3.2mm |
| Solder Mask Colors | Green, Red, Yellow, Blue, White, Black | Purple, Matte Black, Matte Green |
| SMT Component Package Support | 0402, 0603, QFN, BGA | 0201, Fine-pitch BGA |
Files Required for JLCPCB SMT Production:
1. Gerber Files: Exported RS-274X or X2 format containing copper, solder mask, and silkscreen layer data.
2. BOM (Bill of Materials): Must match JLCPCB Parts Library (LCSC part numbers / Cxxxx Part IDs) for automatic component matching.
3. CPL / Pick and Place File: Contains X/Y coordinates, rotation angle, and layer designation (Top/Bottom) for automated SMT machine placement.
Troubleshooting with Schematics
Isolate Sections: When troubleshooting, isolate specific sections of the circuit using the schematic. This helps narrow down the potential issues and locate faulty components more efficiently.
Check Connections: Examine the connections between components. Look for breaks in the circuit, loose connections, or components that might have failed.
Voltage and Current: Use the schematic to understand the expected voltage and current values at different points in the circuit. This information is invaluable when diagnosing problems.
Practice and Resources
Practice reading electrical schematics by working on simple circuits. Experiment with creating your own schematics for basic circuits to reinforce your understanding. Explore online resources, tutorials, and interactive tools that provide additional guidance on reading electrical schematics. Websites like JLCPCB offer blog articles to deeply explain the concepts of schematic, symbol, PCB design.
FAQ about Electrical Schematics
Q: What is the main difference between a block diagram and a schematic diagram?
A block diagram provides a high-level overview of a circuit's functions and signal flow without showing individual components or connections. In contrast, a schematic diagram details every specific component, such as resistors, ICs, and capacitors, using standardized symbols, precise net labels, and exact pin connections required for circuit analysis and PCB layout.
Q: Why is component polarity important when reading schematics and placing SMT orders?
Polarized components like diodes, LEDs, electrolytic capacitors, and ICs must be connected in a specific direction to function correctly and avoid component failure or circuit damage. When ordering SMT assembly at JLCPCB, clearly marking Pin 1 or Cathode orientations in your schematic and silkscreen ensures automated pick-and-place machines install components accurately.
Q: What files do I need to export from my schematic or EDA tool to manufacture a PCB at JLCPCB?
To fabricate and assemble a PCB, you need Gerber files in RS-274X or X2 format for PCB board manufacturing, a Bill of Materials listing component part numbers matching JLCPCB and LCSC C-number IDs, and a Component Placement List containing X/Y coordinates and rotation angles for automated SMT assembly.
Q: How do net labels help simplify complex schematics?
Net labels assign logical names such as VIN, GND, or VBAT to specific wires or nodes. Instead of drawing cluttering crossover lines across a large diagram, net labels establish electrical connections between identical names automatically, resulting in a cleaner, highly readable, and professional schematic layout.
Q: What layout considerations should be taken when converting high-current schematic sections to PCB?
For high-current paths, such as 1.5A charging circuits based on TP5100, schematic designers must ensure PCB traces are wide enough to handle the current density, typically requiring a trace width of at least 20 to 30 mil per Ampere. Additionally, keeping input bypass capacitors close to IC power pins minimizes noise and voltage ripple.
Conclusion
Reading electrical schematics is a fundamental skill for anyone working with electronics or electrical systems. By familiarising yourself with symbols, understanding the flow of circuits, and practicing with real-world examples, you can gain confidence in interpreting these essential blueprints. Whether you're pursuing a career in electronics or simply want to enhance your DIY skills, the ability to read electrical schematics opens up a world of possibilities in understanding and working with electrical systems.
Popular Articles
• Choosing the Best PCB Color-Enhancing Aesthetics and Functionality
• PCB Silkscreen: All You Need to Know
• The Comprehensive Guide to Circuit Symbols: Key to Understanding Electrical and Electronic Diagrams
• Understanding Electrical Schematics: A Comprehensive Guide
• PCB Board Design: A Step-by-Step Guide for Beginners
Keep Learning
A Beginner's Guide to Basic Electronic Components: Functions, Symbols & Uses
Every circuit, from a simple LED flashlight to a microcontroller board, is built from the same handful of common electronic components. This guide breaks down the ten basic electronic components you will encounter most often: What each component does How it works Key specifications Where engineers use it By the end, you will be able to recognize these electronic circuit components on a schematic, a PCB, or a parts bin, and know exactly why each one is there. These electronic components are the buildin......
Capacitor Voltage Rating Explained with Examples
Capacitors are small components widely used not only for power delivery but also for signal conditioning in electronic circuits. In this article, we focus on the capacitor voltage rating across different types of capacitors. At first glance, capacitors look simple—small cans, discs, or chips on a PCB. However, their markings carry essential design information, including capacitance and voltage rating. These are not arbitrary values but directly affect circuit reliability. Ignoring the voltage rating w......
From Prototype to Product with a Better Development Board
Note Prototype Fast: Development boards integrate power, clock, and programming circuits to validate firmware in hours. Pick the Right Platform: Use ESP32 for Wi-Fi/BLE, Arduino UNO for 5 V sensors, Raspberry Pi Pico for tight I/O timing, and Raspberry Pi 5 for Linux. Scale to Custom PCB: Reuse your prototype's certified module, firmware, and support circuits, but remove unused headers to cut unit cost. Build for Production: Use a 4-layer ground-plane stackup for wireless boards, verify BOM stock earl......
4 Layer vs 6 Layer vs 8 Layer PCB: How to Choose the Right Stackup
Random selection of layers in electronics may lead to serious signal integrity issues. That's why we always design our stackup before designing the PCB. Stackup decides the type of PCB and how it gonna perform under high-frequency conditions. There are a lot of things that directly affect the stackup of the PCB, related to impedance matching, routing density, signal and power integrity, electromagnetic compatibility (EMC), and cost. Knowing the requirements before design and the most critical componen......
Choosing the Best PCB Color-Enhancing Aesthetics and Functionality
Key Takeaways Choosing the best PCB solder mask color involves balancing aesthetics, visibility, and functionality. Green remains the top choice for superior contrast and inspection, while black offers premium appeal, white excels in LED applications, and other colors like purple and red provide unique design options. The ideal color depends on your priorities in inspection ease, thermal performance, and brand image, with minimal impact on electrical performance when using proper silkscreen contrast. ......
Single-Sided PCB Design: Combining Simplicity with Sophistication
Key Takeaways Single-sided PCBs offer a simple, cost-effective solution for many electronic applications. SMT and THT components require different mounting and soldering arrangements. Proper layer orientation, Gerber files, and design rules help ensure manufacturability. Aluminum PCBs require careful attention to insulation, component mounting, and silkscreen placement. A printed circuit board (PCB) provides mechanical support for electronic components and establishes the electrical connections requir......