A Comprehensive Guide to Switch Types in PCB Design
15 min
- What is a PCB Switch?
- How Does a PCB Switch Work?
- How to Design a PCB Switch?
- Other Main Types of Switches Used in Circuit Design
- How to Choose the Right Switch for Your PCB Design
- FAQ about Switch Types in PCB Design
- Conclusion
Key Takeaways
- Understand PCB switch types and their typical applications to select the right switch for your design.
- Create accurate footprints and layouts based on electrical, mechanical, and clearance requirements.
- Consider PCB manufacturing constraints, including trace width, spacing, holes, annular rings, and solder mask.
- Verify the design before production with connectivity checks, DRC, and final manufacturing-file reviews.
Switches are essential components in electronic products, providing a simple way to control, activate, or configure electrical functions. In PCB design, the choice of switch affects not only the user interface but also the component footprint, mechanical clearance, electrical connections, and PCB layout.
From compact tactile switches and push buttons to slide, DIP, rotary, and toggle switches, each type has different electrical and mechanical characteristics. Some PCB designs can also use the PCB itself as part of the switching contact structure, as commonly seen in remote-control interfaces.
This guide explains the main switch types used in PCB design, how they work, how to select and design around them, and which PCB manufacturing considerations should be checked before production.
What is a PCB Switch?
A PCB switch is a switching interface in which conductive contact areas are formed directly on the printed circuit board. When a conductive element in the external pressing mechanism bridges the contact areas, the circuit is closed and current can flow. When the contacts separate, the circuit is opened.
A common example can be found in remote controls, where conductive contacts on the PCB work with a conductive rubber keypad or similar pressing mechanism. In this type of design, the PCB is not simply used to connect a separate switch; the exposed contact areas on the board form part of the switching interface itself.
PCB-based contact switches can be useful when a product requires a compact and integrated user interface. However, the contact geometry, conductive material, mechanical alignment, and PCB surface condition need to be considered together to ensure reliable operation.
How Does a PCB Switch Work?
A PCB-based contact switch generally works by creating or breaking an electrical connection between two conductive contact areas on the PCB.
In a typical design, the PCB contains two separate contact pads with a controlled gap between them. When the user presses the external actuator, a conductive element bridges the gap between the contacts. This creates a closed circuit and allows current to flow. When the pressure is released, the conductive element moves away from the PCB contacts, opening the circuit.
The contact material and mechanical structure should be selected according to the required contact resistance, switching frequency, expected operating life, and mechanical interface. For example, carbon-based conductive contacts may be used in some membrane or remote-control interfaces because they are designed for repeated contact operation.
The conductive contact area should be designed according to the requirements of the switching mechanism. It should not be confused with the conventional PCB surface finish used for soldering.
JLCPCB offers surface-finish options such as HASL, lead-free HASL, and ENIG. ENIG uses an electroless nickel layer with an immersion-gold layer and provides a relatively flat surface, while HASL uses a solder coating on exposed copper. These finishes primarily address PCB protection and solderability requirements. A
How to Design a PCB Switch?
Designing a PCB for a switch requires more than selecting a component and drawing its connections. The design should consider the switch's electrical rating, mechanical dimensions, footprint, contact area, mounting method, surrounding clearance, and PCB manufacturing requirements.
The following steps provide a practical workflow for designing a PCB around a switch.
Step 1: Define Your Requirements
Begin by outlining the purpose of your switch and the way it will be operated. Determine the application's voltage and current requirements, and check the switch's rated load, contact resistance, switching frequency, expected operating life, and mechanical requirements.
The switch's electrical rating should also be considered separately from the PCB trace capability. Both the component and the PCB traces must be suitable for the intended electrical load.
Step 2: Design the Footprint and Schematic Symbol
Schematic Symbol: The symbol should accurately represent the switch's electrical function, such as normally open (NO), normally closed (NC), or changeover operation. Make sure the pin numbers and electrical connections match the selected component.
PCB Footprint: Start with the manufacturer's datasheet and verify the component dimensions, pin configuration, mounting method, actuator position, and recommended land pattern. The footprint should match the physical component and provide sufficient clearance for placement, operation, and surrounding components.
For mechanical switches, also check the actuator height and movement direction. A footprint can be electrically correct but still fail mechanically if the switch interferes with the enclosure or adjacent components.
Step 3: Plan the PCB Layout and Trace Routing
Create a layout for your PCB that accommodates the switch and its associated components. Use PCB design software to draw the circuit traces, component placements, and connection points. Ensure sufficient space around the switch for easy operation. Measure the dimensions of the chosen switch, considering its length, width, and height. These measurements are essential for creating the correct PCB cutouts and designing any housing or casing for the switch.
Pay attention to trace width and spacing according to the electrical load and PCB manufacturing requirements. Keep traces connected to the switch clear of the active contact area and avoid unnecessary routing near mechanical mounting features.
For reference, JLCPCB currently lists a minimum trace width and spacing of 0.10/0.10 mm (4/4 mil) for 1 oz copper on standard 1- and 2-layer PCBs and 0.09/0.09 mm (3.5/3.5 mil) for multilayer PCBs. These are manufacturing capability limits rather than universal design targets, so a larger width and spacing should be used when the electrical or production requirements allow
Design the Contact Area Carefully
If the PCB itself forms part of the switching interface, the contact area requires additional attention. Separate conductive pads should be positioned according to the mechanical actuator, with an appropriate gap between the contacts.
Avoid placing unrelated copper, vias, or traces inside the active switching area unless they are part of the intended contact structure. The contact geometry should be checked together with the mechanical design to prevent misalignment, unintended connections, or interference with the pressing mechanism.
Step 4: Add Cutouts and Mounting Holes
If the switch requires mounting holes, slots, or board-edge cutouts, add these features according to the manufacturer's mechanical drawing. Do not estimate hole or cutout dimensions only from the nominal component size.
Clearance around mounting holes is also important. JLCPCB currently lists a minimum PTH-to-track clearance of 0.28 mm, with 0.35 mm recommended, and a minimum NPTH-to-track clearance of 0.20 mm. These values should be checked against the specific PCB technology and manufacturing requirements before production.
For slots, designers should also check the manufacturing capability of the selected PCB process. JLCPCB currently lists minimum plated-slot widths of 0.50 mm for 2-layer boards and 0.35 mm for multilayer boards, while the listed minimum non-plated slot width is 1.0 mm.
Step 5: Add Supporting Components
Integrate any necessary supporting components around the switch, such as resistors, capacitors, LEDs, or pull-up/pull-down components required by the circuit. Place these components so that they do not interfere with the switch actuator, mounting hardware, or user-access area.
For SMD switches and nearby components, also consider assembly spacing. JLCPCB's current SMT guidance specifies minimum spacing values based on component package combinations to support solder paste printing, placement accuracy, AOI inspection, and rework accessibility.
Step 6:Verify Connectivity and Run DRC
Before manufacturing, use the PCB design software to verify electrical connectivity and run a design-rule check (DRC). Check the switch footprint, pin connections, trace width and spacing, pad clearances, mounting holes, board outline, and other manufacturing constraints.
Pay particular attention to the switch's mechanical area. The electrical design may pass DRC while the physical design still conflicts with the enclosure, actuator, or mounting structure.
Step 7:Finalize the Design and Manufacturing Files
After completing the electrical and mechanical checks, finalize the PCB design and prepare the manufacturing files. Review the Gerber files, drill files, board outline, solder mask openings, silkscreen, and switch contact areas in a Gerber viewer before submitting the design for production.
If the design includes PCB assembly, also verify the bill of materials (BOM), component footprints, polarity information, and placement data. A final review at this stage can help identify design or manufacturing issues before fabrication and assembly.
Other Main Types of Switches Used in Circuit Design
1. Tactile Switches
Tactile switches are commonly used in consumer electronics, especially in handheld devices like smartphones, remote controls, and keyboards. These switches offer a noticeable "click" when pressed, providing feedback to the user that the switch has been activated. Tactile switches are small, reliable, and cost-effective, making them ideal for high-volume production and compact designs.
Tactile switches are commonly used in consumer electronics, handheld devices, remote controls, keyboards, and other user-interface applications. They provide tactile feedback when pressed, helping users confirm that an input has been registered.
From a PCB design perspective, designers should verify the switch footprint, actuator height, mounting method, and clearance from nearby components or enclosure structures. Both through-hole and SMD tactile switches are available, so the PCB footprint should always follow the selected component's datasheet.
Key Features:
- Low profile
- Tactile feedback
- Compact size
2. Push Button Switches
Push-button switches are among the most familiar switch types, ranging from simple control buttons to industrial equipment interfaces. They can be momentary, returning to their original state after being released, or latching, remaining in the selected state until operated again.
When designing a PCB for a push button, consider the actuator direction, mechanical force, mounting method, and clearance around the button. The electrical connections should also be checked against the selected switch's pin configuration.
Key Features:
- Simple user operation
- Momentary or latching configurations
- Through-hole or SMD options depending on the component
- Easy integration into PCB-based control interfaces
3. Slide Switches
Slide switches move a contact back and forth, which opens or closes a circuit. These switches are durable and can be used in various devices that require a simple, manual operation to change states. Slide switches are commonly used for mode selection, power control, and other applications where users need to move between defined switch positions. In PCB design, the designer should consider the actuator direction, number of positions, mounting method, and clearance required for the sliding mechanism.
Key Features:
- Reliable mechanical operation
- Multiple positions (e.g., On/Off/Auto)
- Durable and easy to use
Note
Tactile switches and push-button switches are not always mutually exclusive categories. A tactile switch is generally a type of momentary push-button switch that provides tactile feedback, while push-button switches can include a broader range of mechanical designs and operating modes.
4. DIP Switches
Dual In-line Package (DIP) switches are a series of small switches used for setting up configurations or options in a device. Instead of needing to reprogram or modify a PCB, DIP switches allow for manual configuration changes. These switches are popular in both older electronics and modern devices requiring quick reconfigurations. DIP switches are commonly used when a device needs manual hardware configuration, such as setting operating modes, addresses, or feature options. Because users may need to access the switches after PCB assembly, the layout should provide sufficient physical access and clear labeling where necessary.
Key Features:
- Configurable
- No need for software or reprogramming
- Simple setup changes
5. Rotary Switches
Rotary switches allow users to select different circuit states by rotating a shaft through defined positions. They are useful when an application requires several discrete settings rather than simple on/off control.
PCB designers should check the switch's mounting dimensions, shaft height, rotational clearance, pin arrangement, and panel alignment. Mechanical alignment is particularly important when the rotary switch is connected to a front-panel control.
Key Features:
- Multiple selectable positions
- Precise control
- Rugged and durable
6. Toggle Switches
Toggle switches are widely used for their reliability and simplicity. They feature a lever that can be flipped between two or more positions to open or close a circuit. Toggle switches are often used in applications where users need to easily control functions with a simple, manual action. Toggle switches are widely used when a clearly defined manual switching action is required. Depending on the component, they may provide two or more stable positions.
For PCB design, consider the lever movement, mounting-hole requirements, mechanical stress, and clearance around the switch. If the switch is operated frequently or with relatively high force, the mechanical connection between the switch and PCB should be considered carefully.
Key Features:
- Easy to operate
- Multiple positions
- High durability
7. Rotary Encoders
Rotary encoders are not conventional switches, but they are often discussed alongside switches because they provide a common form of user input. Instead of simply opening or closing a circuit, an encoder detects rotational movement and converts it into electrical signals that a controller can interpret.
Incremental rotary encoders commonly use multiple output signals to indicate rotational movement and direction. Some encoder components also include an integrated push switch, combining rotary input with a button function.
From a PCB design perspective, check the encoder's pin configuration, mounting dimensions, shaft alignment, and mechanical clearance. Signal routing should also follow the requirements of the specific encoder and controller interface.
Key Features:
- Precise rotation detection
- Infinite rotation capability
- Digital and analog output options
Switch Type Comparison for PCB Design
| Switch Type | Operation | Typical Mounting | Main Advantage | PCB Design Consideration |
|---|---|---|---|---|
| Tactile Switch | Momentary press | SMD or through-hole | Compact and tactile feedback | Footprint, actuator height, clearance |
| Push Button | Momentary or latching | SMD or through-hole | Simple user operation | Pin configuration and mechanical force |
| Slide Switch | Sliding movement | SMD or through-hole | Simple state selection | Actuator direction and movement space |
| DIP Switch | Individual toggles | SMD or through-hole | Manual configuration | User access and labeling |
| Rotary Switch | Multiple rotary positions | PCB or panel mount | Multiple discrete states | Shaft alignment and rotational clearance |
| Toggle Switch | Lever movement | PCB/panel mount | Clear manual operation | Mounting holes and mechanical stress |
| Rotary Encoder | Rotary signal output | PCB mount | Precise rotary input | Pinout, signal routing, and alignment |
How to Choose the Right Switch for Your PCB Design
Choosing the right switch requires more than comparing switch types. Designers should consider electrical requirements, mechanical constraints, PCB space, user interaction, and manufacturing requirements.
Electrical requirements: Check operating voltage, current, contact resistance, and expected switching frequency.
Mechanical requirements: Check the actuator, mounting method, dimensions, operating force, and available movement space.
PCB space: Compare the component footprint with the available board area and keep sufficient clearance from nearby components and mechanical structures.
User interaction: Consider whether the application requires tactile feedback, multiple positions, rotary input, or simple momentary operation.
Manufacturing: Verify the footprint, pad dimensions, hole sizes, trace clearance, and assembly spacing against the selected PCB manufacturing and assembly process.
FAQ about Switch Types in PCB Design
Q: What is a PCB switch?
A PCB switch is a switching interface in which conductive contact areas are formed directly on a PCB. An external conductive element can bridge the contacts to close the circuit.
Q: What is the difference between a tactile switch and a push-button switch?
A tactile switch is generally a type of momentary push-button switch designed to provide tactile feedback. Push-button switches are a broader category that can include different mechanical structures and operating modes.
Q: What should I consider when designing a PCB footprint for a switch?
Check the manufacturer's datasheet for the component dimensions, pin configuration, recommended land pattern, actuator position, mounting requirements, and mechanical clearance. The footprint should be verified against both electrical and mechanical requirements.
Q: Do mounting holes affect PCB routing around a switch?
Yes. Mounting holes and slots require sufficient clearance from nearby copper and traces. JLCPCB currently lists minimum PTH-to-track and NPTH-to-track clearances of 0.28 mm and 0.20 mm, respectively.
Q: What PCB manufacturing rules should I check before ordering a switch PCB?
Designers should check trace width and spacing, pad-to-track clearance, hole sizes, mounting-hole clearance, slot dimensions, SMD component spacing, board outline, and manufacturing files before production.
Conclusion
Choosing the right switch is an important part of PCB design because electrical performance, mechanical integration, user experience, and manufacturability all need to work together.
Tactile, push-button, slide, DIP, rotary, toggle, and rotary encoder inputs each serve different design requirements. For PCB-based contact switches, the contact geometry and conductive interface require additional attention.
A reliable switch PCB design should start with the component datasheet and continue through footprint design, contact and clearance planning, trace routing, mounting-hole verification, DRC, and manufacturing-file review.
By considering PCB manufacturing requirements early in the design process, designers can reduce the risk of mechanical conflicts, layout problems, and production issues before the board is manufactured.
Popular Articles
• PCB Silkscreen: All You Need to Know
• The Comprehensive Guide to Circuit Symbols: Key to Understanding Electrical and Electronic Diagrams
• Design Guidelines for PCB Using FR4 Substrates
• Choosing the Best PCB Color-Enhancing Aesthetics and Functionality
• PCB Board Design: A Step-by-Step Guide for Beginners
Keep Learning
Via Stitching Guide : Core Functions, Pitch Rules & Placement
key takeaway Core Purpose: Ties ground layers together to cut EMI, reduce impedance, and shorten return paths. Pitch Rules: Space vias at λ/10 for ground grids and λ/20 for edge rings and shielding fences. Layer Transitions: Place stitching vias adjacent to signal vias to minimize return current loop area. Avoid Over-Stitching: Overuse perforates power planes, alters trace impedance, and increases drilling costs. DFM Control: Follow hole spacing rules, tent non-test vias, and maintain proper edge copp......
Relay Pinout Explained: Diagrams, Pin Functions & Multimeter Testing
Key Takeaways Pin functions: A standard electromechanical relay has two coil pins, and each pole adds a common (COM), normally open (NO), and normally closed (NC) pin. Viewing side: Relay footprints are often drawn in bottom view, with the pins facing you. When a drawing does not state its view, confirm NC and NO with a continuity check. Relay Pin Count: A 5-pin relay is typically SPDT, a 4-pin relay is usually SPST, and an 8-pin relay is commonly DPDT. However, pin arrangements can vary between PCB, ......
How to Connect and Choose a Flyback Diode for a Relay
Key Takeaways Diode Placement: Connect the flyback diode across the relay coil, with its cathode connected to the positive side and its anode to the negative side. Why It Matters: When the relay switches off, the diode provides a safe path for the remaining coil current, preventing a high-voltage spike that could damage the transistor. Choosing the Right Diode: Select a diode with a reverse-voltage rating above the coil supply voltage and a forward-current rating suitable for the coil current. Common ......
A Beginner's Guide to Basic Electronic Components: Functions, Symbols & Uses
Every circuit, from a simple LED flashlight to a microcontroller board, is built from the same handful of common electronic components. This guide breaks down the ten basic electronic components you will encounter most often: What each component does How it works Key specifications Where engineers use it By the end, you will be able to recognize these electronic circuit components on a schematic, a PCB, or a parts bin, and know exactly why each one is there. These electronic components are the buildin......
Reliable BMS Boards Start With Quality PCB Manufacturing
Key Takeaways Dual Duty: BMS PCBs handle heavy currents and millivolt sensing simultaneously, requiring strict layout isolation. Power & Heat: Currents over 10A need 2 oz+ copper pours with via stitching to drop resistance and heat. Clean Sensing: Kelvin differential routing and split grounds prevent load noise from corrupting cell voltage readings. Materials & Finish: High-Tg FR-4 and ENIG surface finishes ensure heat tolerance and flat mounting pads. DFM & Testing: Design for heavy-copper etch toler......
What is Solder Mask and How Does it Impact Your PCB Designs?
Solder mask may not be the most exciting topic in PCB manufacturing, but it's definitely one of the most crucial. Without proper solder mask, your Printed Circuit Boards (PCB's) could suffer from shorts, bridges, corrosion, and other costly and time-consuming issues. So, if you want to ensure the quality, reliability, and longevity of your electronic products, you need to know everything about solder mask - from it's purpose and types to it's application and design implementations. In this ultimate gu......