PCB Gold Fingers: Why They Matter and How to Design Them
10 min
- What is PCB Gold Finger?
- Classification of Goldfingers:
- Design Specifications for PCB Gold Fingers
- Applications of Gold Finger PCBs
- FAQ about PCB Gold Fingers
- Conclusion
Key Takeaways
- PCB gold fingers provide reliable electrical and mechanical contact for PCBs that connect to external connectors or card slots.
- ENIG is suitable for general contact applications, while electroplated hard gold offers higher wear resistance for repeated insertion and removal.
- Gold fingers should remain fully exposed, with solder mask and silkscreen kept away from the contact area.
- Proper chamfering and gold finger orientation are essential to ensure smooth insertion and prevent damage during edge machining.
- Adequate edge clearance, copper-free bevel areas, and proper copper distribution help maintain dimensional accuracy and manufacturing reliability.
What is PCB Gold Finger?
PCB gold fingers are a series of exposed, gold-finished contact pads located along the edge of a printed circuit board. They serve as electrical and mechanical contact points when the PCB is inserted into a mating connector or card slot. Because these contacts may experience repeated insertion and removal, the surface finish and edge geometry must be carefully designed to provide reliable electrical contact and sufficient wear resistance.
Gold is widely used for PCB contact surfaces because it offers good electrical conductivity and excellent resistance to oxidation and corrosion. For gold fingers, these properties help maintain reliable contact performance, while the appropriate plating process also determines how well the surface withstands repeated mechanical contact.
Material and surface-finish selection are important factors in PCB gold finger manufacturing. The selected finish must provide reliable electrical contact while meeting the mechanical and environmental requirements of the application, particularly when the board will be inserted and removed repeatedly.
Two commonly used gold finishes for PCBs are Electroless Nickel Immersion Gold (ENIG) and electroplated hard gold.
Electroless Nickel Immersion Gold (ENIG):
Electroless Nickel Immersion Gold (ENIG) is a widely used PCB surface finish because it provides a flat surface, good solderability, and resistance to oxidation and corrosion. However, the gold layer in ENIG is thin and relatively soft, making it unsuitable for applications that require extensive repeated insertion and removal. Therefore, ENIG is generally better suited to solderable PCB pads and applications with limited mechanical wear.
Electroplated Hard gold :
Electroplated hard gold is designed for contact areas that require higher wear resistance. It is harder and thicker than the gold layer used in ENIG, making it more suitable for edge connectors and gold fingers that undergo repeated mechanical contact. Because electroplated hard gold is more costly, it is typically applied selectively to the required contact areas rather than across the entire PCB surface.
| Feature | ENIG | Electroplated Hard Gold |
|---|---|---|
| Main purpose | Solderable PCB surface finish | Wear-resistant contact surface |
| Surface | Flat and smooth | Harder contact surface |
| Wear resistance | Limited for repeated insertion | Higher resistance to mechanical wear |
| Typical application | SMT pads, fine-pitch components | Gold fingers, edge connectors |
| Mechanical contact | Not ideal for frequent insertion/removal | Suitable for repeated mating |
| Cost | Generally lower | Higher |
| Plating area | Can cover PCB pad areas | Usually applied selectively |
Classification of Goldfingers:
1. Conventional gold fingers (flush fingers)
Rectangular contact pads with consistent lengths arranged along the PCB edge. This configuration is commonly used for card-edge connections such as expansion cards.
2. Long and short gold fingers (i.e. uneven gold fingers)
Gold fingers with different pad lengths. This configuration can be used when the connector requires staggered contact engagement during insertion.
3. Segmented gold fingers (interrupted gold fingers)
Gold fingers with interrupted contact sections designed according to the electrical and mechanical requirements of the connector.
Design Specifications for PCB Gold Fingers
To ensure reliable electrical contact and mechanical performance, PCB designers need to consider several gold finger design requirements before manufacturing. These requirements include gold finger positioning, solder mask and silkscreen clearance, edge chamfering, chamfer depth, copper clearance, and PCB size. Following these guidelines can help ensure that the finished PCB fits properly into the mating connector and that the gold finger area remains reliable during repeated insertion and removal.
Gold Finger Position
Gold fingers are normally located along the PCB edge so that they can directly mate with the corresponding connector. When designing the board, avoid placing PTHs or other features too close to the gold finger area. The available space should also account for the connector structure and the required chamfering area. Proper positioning helps prevent mechanical interference during insertion and removal.
Solder Mask and Silkscreen
The gold finger area should remain fully exposed to provide a clean contact surface. Solder mask should not cover the gold fingers or form bridges between adjacent finger pads. Silkscreen should also be kept away from the contact area to prevent it from interfering with connector mating.
Gold Finger Orientation
Gold fingers should be oriented toward the PCB edge where the bevel will be applied, rather than toward the center of the PCB. Proper orientation ensures that the gold finger area remains clear of the beveling process and allows the PCB to be inserted smoothly into the mating connector.
Gold Finger Chamfering
Gold fingers generally require edge chamfering to help guide the PCB into the mating connector and reduce the risk of damaging the contact area during insertion. The chamfer angle should be selected according to the connector and manufacturing requirements. JLCPCB's gold finger design guidelines use 30° as the default chamfer angle.
Chamfer Depth
Chamfer depth is an important consideration because the bevel must not extend too far into the PCB and damage the gold finger area. JLCPCB provides a calculation for determining the chamfer depth based on PCB thickness, remaining board thickness, and chamfer angle:
L = (D/2 − T/2) / tan α
Where:
D is the PCB thickness.
T is the remaining board thickness after chamfering.
α is the chamfer angle.
L is the chamfer depth measured from the board edge.
For a standard 1.6 mm PCB, JLCPCB specifies a remaining board thickness of 0.5 mm and a default chamfer angle of 30°, resulting in a chamfer depth of approximately 0.6 mm.
Keep Copper Away from the Chamfer Area
The chamfer area should be kept free of copper features. Copper traces or other exposed copper structures within the beveling area may be cut during edge machining, which can damage the circuit or expose copper at the PCB edge. Designers should therefore check the chamfer area during PCB layout and maintain the required copper clearance before manufacturing.
PCB and Panel Size
The overall PCB or panel dimensions should also be considered when designing gold finger boards. According to JLCPCB's gold finger design requirements, the length and width of a single board or panel should each be at least 50 mm. This requirement should be checked during both individual board design and panelization.
Copper Distribution in Multilayer Gold Finger PCBs
For multilayer PCBs with gold fingers, copper distribution should also be considered during the design stage. Large differences in copper coverage between different areas can contribute to thickness variation and affect the mechanical fit of the finished board.
JLCPCB recommends adding copper pours to empty areas of the inner layers when possible, especially in areas corresponding to the gold fingers. When inner-layer copper coverage is below 25%, adding copper pour can help improve copper distribution and support more consistent board thickness.
Gold Finger Orientation and Clearance
Gold fingers should be positioned toward the PCB edge so that they can enter the mating connector correctly. Sufficient clearance must be maintained between the gold finger area and other PCB features. For chamfered designs, the required clearance should also account for the chamfer depth and PCB thickness.
Commonly used gold finger chamfering parameters in JLCPCB
At jlcpcb you can find more design specifications about gold fingers.Failure to adhere to the aforementioned guidelines could result in the PCB being incompatible with the parent PCB. For example, the daughter board may not properly fit into the designated slot on the motherboard.
| Design Item | JLCPCB Gold Finger Requirement |
|---|---|
| Default chamfer angle | 30° |
| Remaining board thickness | 0.5 mm |
| Chamfer depth for 1.6 mm PCB | Approximately 0.6 mm |
| Minimum board/panel length | 50 mm |
| Minimum board/panel width | 50 mm |
| Chamfer area | Keep free of copper |
| Gold finger contact area | Fully exposed |
| Solder mask between fingers | No solder mask bridge |
| Multilayer inner-layer copper coverage | Consider copper pour when coverage is below 25% |
Applications of Gold Finger PCBs
PCB gold fingers are widely used in electronic devices that require reliable electrical connections between a PCB and an external connector or card slot. Their exposed contact surfaces make them particularly suitable for applications where the PCB needs to be inserted into or connected with another component.
| Application | Typical Use of Gold Fingers |
|---|---|
| Mobile Phones | Used in compact electronic assemblies where reliable board-to-board or connector contacts are required. |
| Computers | Commonly used on expansion cards and other PCBs that connect to slots or edge connectors. |
| Automotive Electronics | Used in electronic systems where stable connections are important for reliable operation. |
| Home Entertainment | Applied in electronic devices that use PCB edge connections for removable or modular components. |
| Office Devices | Used in equipment where PCBs need reliable connections with external connectors or modules. |
With the increasing use of modular and connector-based electronic designs, gold fingers remain an important PCB feature for applications that depend on stable contact performance. Selecting an appropriate surface finish and following proper gold finger design requirements can help ensure reliable performance throughout the product's service life.
FAQ about PCB Gold Fingers
Q: What are PCB gold fingers used for?
PCB gold fingers provide exposed electrical contact points along the edge of a PCB, allowing the board to connect with a mating card slot or edge connector.
Q: Is ENIG suitable for gold fingers?
ENIG provides a flat and corrosion-resistant surface, but its thin and relatively soft gold layer has limited resistance to repeated mechanical wear. The appropriate finish should therefore be selected according to the required insertion and removal cycles.
Q: Why do PCB gold fingers need to be chamfered?
Chamfering helps guide the PCB into the mating connector and reduces the risk of damaging the gold finger area during insertion.
Q: What is the minimum board size for gold finger PCBs at JLCPCB?
According to JLCPCB's current Gold Fingers design requirements, the length and width of a single board or panel with gold fingers should not be less than 50 mm.
Q: Can copper be placed in the gold finger chamfer area?
CCopper should not be placed in the chamfered area because the beveling process may damage traces or expose copper.
Conclusion
PCB gold fingers provide a reliable interface between a PCB and its mating connector or card slot. Their performance depends not only on the selected surface finish but also on accurate finger geometry, solder mask opening, board thickness, copper clearance, and bevel design.
For reliable manufacturing, designers should consider these requirements before submitting Gerber files for production. By following JLCPCB's gold finger design guidelines, including beveling, chamfer depth, copper clearance, and board-size requirements, designers can reduce manufacturing risks and achieve more reliable connector performance.
Keep Learning
Avoid PCB Assembly Failures: Mastering Solder Mask Expansion Rules and Best Practices
Solder mask protects copper traces and pads from oxidation, bridges, and contamination during assembly. Incorrect solder mask expansion—the clearance around features where mask is pulled back—leads to defects like shorts or exposed copper. Engineers must set expansion values precisely to ensure reliable soldering and long-term performance. Introduction: Why Solder Mask Expansion is Critical for PCB Reliability Understanding Solder Mask and Expansion Basics Solder mask is a polymer layer applied over t......
Why Copper Oxidation Matters in PCB Design & How to Prevent It
Key Takeaways Copper oxidation is a critical concern in PCB design that directly impacts solderability, contact resistance, and long-term reliability. By understanding how oxidation forms and damages copper surfaces, designers can effectively prevent it through appropriate surface finishes (such as HASL, ENIG, and OSP), strategic solder mask application, and strict adherence to proper storage and handling practices per IPC-1601 guidelines. Protecting copper from oxidation ensures better assembly yield......
Choosing the Right Surface Finish for Your PCB: An Overview of HASL, ENIG, OSP, Immersion Tin and Immersion Silver
Key Takeaways Lead-Free HASL: Best low-cost, RoHS-compliant finish for general PCB builds. ENIG: Superior flatness and 12+ month shelf life for fine-pitch BGAs. OSP: Ultra-flat, lowest-cost option for high-volume SMT (3–6 month shelf life). Immersion Silver: Ideal for high-frequency RF by eliminating nickel signal loss. Immersion Tin: Best for press-fit connectors and fine-pitch assembly. Printed Circuit Boards (PCBs) are essential components in the manufacturing of electronic devices ranging from sma......
Conformal Coating in PCB Technology: Benefits, Challenges, and Future Developments
If you're searching for conformal coating, you're likely looking for a reliable way to protect your PCB from moisture, dust, chemicals, or harsh environments. Choosing the right coating directly affects product reliability, performance, and lifespan. In this guide, you'll learn what conformal coating is, the main types available, and how to select the best option for your application. We'll also cover key benefits, application methods (manual, automated, and selective), as well as inspection, rework, ......
PCB Gold Fingers: Why They Matter and How to Design Them
Key Takeaways PCB gold fingers provide reliable electrical and mechanical contact for PCBs that connect to external connectors or card slots. ENIG is suitable for general contact applications, while electroplated hard gold offers higher wear resistance for repeated insertion and removal. Gold fingers should remain fully exposed, with solder mask and silkscreen kept away from the contact area. Proper chamfering and gold finger orientation are essential to ensure smooth insertion and prevent damage duri......
Comparing HASL and ENIG Surface Finishes for PCBs
Selecting the right surface finish for a printed circuit board (PCB) is crucial to ensuring its performance, reliability, and longevity. Two of the most commonly used finishes are Hot Air Solder Leveling (HASL) and Electroless Nickel Immersion Gold (ENIG). Each of these surface finishes offers distinct advantages and disadvantages, making them suitable for different applications. In this article, we will compare HASL and ENIG to help you determine which finish is best suited for your PCB project. What......