How to Use Solder Paste: Stencil, Syringe, and Iron Methods
11 min
- Before You Start: How to Choose and Prepare Solder Paste
- Method 1: How to Use Solder Paste With a Stencil (Best Practice)
- Method 2: How to Use Solder Paste With a Syringe
- Method 3: How to Use Solder Paste With a Soldering Iron
- How to Reflow Solder Paste After Application
- Troubleshooting: How to Fix Common Solder Paste Defects
- How to Handle and Clean Up Solder Paste Safely
- When You Should NOT Use Solder Paste Manually
- Conclusion
- FAQs about Solder Paste
Key Takeaways: How to Use Solder Paste
- Solder paste must be applied before component placement and reflowed with a controlled heat profile.
- Stencil printing provides the most consistent and reliable results.
- Manual methods (syringe or iron) are suitable only for low-density or repair work.
Solder paste is the foundation of modern electronics assembly. In simple terms, it is a mixture of microscopic solder spheres and flux held together in a creamy consistency. Unlike traditional wire solder, it is applied before components are placed, acting as a temporary adhesive before melting to form permanent electrical joints.
Correct usage is extremely important since a majority of SMT defects, like bridges, cold joints, and shifting of components, are caused by either incorrect paste volume or bad handling. JLCPCB uses automated jet printers and 3D SPI (Solder Paste Inspection) to guarantee perfection.

Applying solder paste on the stencil
Before You Start: How to Choose and Prepare Solder Paste
Before you squeeze the syringe, ensure you have the correct material and that it is ready for use.
How to Choose the Right Solder Paste
Not all pastes are the same. For general SMT work, SAC305 (Sn96.5/Ag3.0/Cu0.5) is the industry standard for lead-free assembly. If you are doing repair work where lower temperatures are needed, leaded paste (Sn63/Pb37) is easier to use but carries health risks.
You also need to choose the right Particle Size (Type).
- Type 3: Standard for most components.
- Type 4: Finer powder, essential for small components (0402 and smaller).
Note: JLCPCB's SMT assembly typically uses Type 4 lead-free solder paste optimized for fine-pitch components, ensuring consistent stencil release and minimal bridging.
|
Paste Type |
Particle Size |
Best For |
Reason |
|---|---|---|---|
|
Type 3 |
25–45 µm |
0603, 0805, SOIC |
Good flow, lower cost, standard shelf life. |
|
Type 4 |
20–38 µm |
0402, 0201, uBGA |
Better release from tiny stencil apertures. |
Note: For hand soldering, "No-Clean" flux is highly recommended so you don't have to wash the board aggressively after reflow.
How to Prepare Solder Paste Correctly
1. Thaw Naturally: Remove the paste from the fridge 3–4 hours before use. Do not open the jar/syringe while cold. If you open it cold, moisture from the air condenses on the paste, causing "solder balls" during heating.
2. Mix Gently: In case of using a jar, gently mix for 1 minute so that the flux is uniformly spread.
Note: After applying the paste on the stencil, it can be worked for approximately 4–8 hours until it dries out. But the humidity and temperature can reduce this to 2–3 hours.
Essential Tools Needed for Using Solder Paste
- Solder Paste: (Syringe or Jar).
- Stencil: Laser-cut stainless steel stencils are best. JLCPCB offers these with "Electropolishing" to smooth the walls for better paste release.
- Squeegee: A metal blade or even an old credit card.
- Tweezers: Fine-tip for placing components.
- Heat Source: Hot air gun, reflow hot plate, or a specialized reflow oven.

Essential Tools Needed for Applying Solder Paste
Note
There are three main ways to apply solder paste, depending on your tools and the complexity of your printed circuit boards.
Method 1: How to Use Solder Paste With a Stencil (Best Practice)
This is the most reliable method and mimics the professional process used at JLCPCB. A personalised stencil makes sure that every pad receives the precise mathematical volume of paste that is needed.

SMT stencil printing process, with the angles of the squeegee and solder paste moving into the apertures.
Using Solder Paste With a Stencil: A Step-by-Step Guide
-
Align & Secure: Tape your PCB to a flat surface. Place scrap PCBs around it to create a flat "surround." Tape the stencil over the PCB, aligning the holes exactly with the pads.
-
Apply Paste: Squeeze a bead of paste onto the stencil (above the pattern, not on it).
-
The Sweep: Hold your scraper/squeegee at a 45° angle. Drag the paste across the pattern with firm, consistent pressure. You want to fill the holes, not leave a thick layer on top of the stencil.
-
Lift: Lift the stencil straight up vertically. Do not slide it.
-
Inspect: The paste deposits should look like little clean bricks on the pads.
-
Place & Reflow: Position the components and then apply heat right away.
Common Mistakes:
- Too much pressure: Soldering material scoops out from the holes (lack of solder).
- Not enough pressure: Leaves a thin layer of paste on top of the stencil (short circuit).
- Misalignment: When the paste touches the solder mask, it could end up as solder balls.
Method 2: How to Use Solder Paste With a Syringe
Best for repairs or one-off prototypes where ordering a stencil isn't feasible.
Applying Solder Paste With a Syringe: A Step-by-Step Guide
-
Needle Selection: Choose either a pink (#20) or blue (#22) tapered tip.
-
Dispense: Keep the syringe in an upright position. Apply a little pressure to come out with a minute dot on every pad.
-
Volume Control: Try to cover just 50-60% of the pad. When it melts, the paste will spread.
-
Place: Drop the component on top. Do not push down hard.
-
Reflow: Heat with hot air.
Practical Tip: Do not use a syringe for QFN or BGA packages. It is impossible to get the volume consistent by hand, leading to hidden shorts. Always use a stencil for these parts.

Use Solder Paste With a Syringe
Method 3: How to Use Solder Paste With a Soldering Iron
This is a specialized method that can be utilized for making fast repairs or for temporarily fixing big parts.
How to do it:
-
Apply a tiny amount of paste to the pad (and component lead if possible).
-
Preheat the pad slightly by holding the iron tip near it.
-
Touch the pad (not the paste directly) with the iron's tip. The heat will flow, making the flux work and melting the paste into the joint.
Warnings:
- Splatter: If a hot iron (350°C+) touches wet paste directly, the solvents can boil instantly, and this will result in the hot solder being splattered.
- Flux Burn: Overheating kills the flux before it can clean the oxide, resulting in a gritty joint.
How to Reflow Solder Paste After Application
Applying the paste is only half the battle. You must heat it correctly (Reflow) to create a solid electrical bond. Professional assembly houses like JLCPCB use 10-zone nitrogen ovens to control this profile perfectly, but you can mimic it at home.
Learn More: Reflow Soldering Principles and Precautions

The solder paste reflow profile with temperature zones: preheat, soak, reflow, and cooling.
#1: Using a Hot Air Gun
- Set air flow to medium (so you don't blow components away).
- Preheat the whole board area to approximately 150°C for half a minute.
- Focus the heat on the component, moving the nozzle in circles. Keep the hot air nozzle 3–5 cm away to avoid blowing components off the pads or overheating them.
- Visual Cue: Look for the gray paste to change to silver and shiny. This is the "wetting" action. Remove heat once all joints are shiny.
#2: Using a Reflow Plate or Mini Oven
- Place the PCB on the cold plate/oven.
- Set temperature to ~230°C (for Sn63) or ~250°C (for SAC305).
- Allow it to ramp up. You will see the flux bubble first, then the solder will melt.
- After the solder has melted, switch off the heat and allow cooling on its own. Do not blow on it because quick cooling could destroy ceramic capacitors.
How to Tell if Solder Paste Reflow Is Successful (Visual Inspection Checklist)
- Self-Alignment: As the solder melts, surface tension naturally pulls the component into the center of the pad. If you see the part wiggle slightly into place, it is a sign of good wetting.
- Good Joints: Joints are smooth, shiny, and concave (fillet shape).
- Poor Joints: Joints appear dull, grainy, or ball-shaped (non-wetting or cold joint).
Troubleshooting: How to Fix Common Solder Paste Defects
Engineers, regardless of experience, encounter problems. Here's a guide to rapid solutions.
|
Problem |
Likely Cause |
Quick Fix |
|---|---|---|
|
Bridging (Shorts) |
Too much paste applied or stencil smeared. |
Wick away excess solder with copper braid. Use a thinner stencil next time. |
|
Cold Joint |
Insufficient heat; the paste didn't fully melt. |
Re-heat the joint with flux. Ensure the profile reaches peak temp. |
|
Poor Wetting |
Oxidized pads or old paste. |
Clean pads with alcohol; add fresh flux before heating. |
|
Tombstoning |
Uneven heating (one pad melts before the other). |
Heat the PCB more evenly (use a hot plate). Check pad design. |
|
Solder Balls |
Heating too fast (explosive boiling). |
Increase the "Preheat" phase to let solvents dry slowly. |

Common SMT solder paste defects: bridging, tombstoning, and solder balls.
How to Handle and Clean Up Solder Paste Safely
Solder paste contains chemicals and metals that require care.
- Clean Immediately: Uncured paste is easy to wipe off with Isopropyl Alcohol (IPA). Cured paste is very hard to remove.
- Don't Reuse: Once paste has been on the stencil, do not scoop it back into the fresh jar. Store it in a "waste" jar.
- Safety: The flux can be a skin irritant, and lead (if using leaded paste) is toxic. Always wear gloves and wash your hands thoroughly. Use a fume extractor when reflowing.
When You Should NOT Use Solder Paste Manually
- Fine-Pitch ICs: For pitch sizes less than 0,5 mm, it is practically impossible to stencil manually without creating a short circuit between the pads.
- QFN / Thermal Pads: It is hard to control the paste coverage on large ground pads manually, leading to parts floating or tilting.
- BGA Parts: These connections need to be verified through X-ray examination.
The Professional Alternative: JLCPCB provides low-cost SMT services where we take care of everything:
-
Automated Printing: Precise electropolished stencils.
-
Type 4 Paste: Standard for high-precision boards.
-
3D SPI: We inspect every single pad for volume and offset.
-
Reflow Ovens: JLCPCB employs contemporary, multi-zone reflow ovens built for uniform thermal control.

Comparison of good shiny solder fillet vs bad cold solder joint.
Conclusion
Gaining the skill to apply solder paste reveals a whole new area of electronic design, which permits the use of smaller, more powerful parts. The method depends on your equipment: a stencil for perfect quality, a syringe for rapid prototyping, or a soldering iron for repairs.
However, the final quality always depends on the heating profile and precise application volume. For complex, high-density boards, save yourself the headache of troubleshooting bridges and cold joints by utilizing JLCPCB's PCBA Service.
FAQs about Solder Paste
Q: What is the appropriate amount of solder paste to use?
In the case of manual syringe application, a dot covering around half the pad area is the target. The height is to be approximately 0.1mm. For stencil usage, the thickness of the stencil sets the volume automatically.
Q: Can I reflow solder paste twice?
Technically, yes, but it is risky. Re-heating increases the intermetallic layer thickness, which can make the joint brittle. It also exhausts the flux. If reworking, always add fresh flux.
Q: What is the best temperature for solder paste?
For Leaded (Sn63/Pb37) paste, the peak temperature should be ~210–220°C. For Lead-free (SAC305) paste, the peak should reach ~235–245°C.
Q: How long can solder paste stay on the PCB before reflow?
The best-case scenario would be the formation getting done within two hours of the paste being applied. In the case of a longer time, the flux solvents will evaporate, and the paste will become "tack dry," which will then cause poor wetting and component adhesion problems.
Q: Is solder paste or wire solder better for SMD?
Solder paste is far superior for SMD assembly because it allows you to place components flat on the board and reflow them all at once. Wire solder requires holding the part with tweezers while manipulating the iron and wire, which is difficult for tiny parts.
Popular Articles
• SMD Soldering Tools You Need: Complete Guide from Beginner to Pro
• SMT Assembly Process Explained and Equipment Used: A Step-by-Step Guide to PCBA Manufacturing
• Common PCB Assembly Methods and Soldering Techniques Explained
• What Is BGA Void? Causes, IPC Limits, and Solutions
• Reflow Soldering: Everything You Need to Know
Keep Learning
Wire Bonding vs Flip Chip: Key Differences in Semiconductor Packaging
In the rapidly evolving world of semiconductor packaging, the choice between Wire Bonding and Flip Chip technology is more than just a mechanical decision—it is a strategic pivot that dictates your product’s performance, thermal limits, and bottom line. Are you looking for the cost-effective reliability of traditional interconnects, or does your application demand the high I/O density and superior signal integrity of modern flip-chip architectures? In this comprehensive guide, we draw on years of high......
Chip Scale Package (CSP) Explained: Types, Benefits & More
Open any flagship smartphone motherboard and the ICs look almost like bare silicon - no chunky leads, no oversized housings. That is chip scale packaging in action. By definition, a chip scale package (CSP) is an IC package where the total body area is ≤1.2× the die size, adhering to rigorous JEDEC and IPC standards. This design philosophy translates directly into smaller boards, shorter signal paths, and superior electrical performance, which is why CSPs now ship in everything from wireless earbuds t......
How to Solder Wires to a Circuit Board Properly: Step-by-Step Guide
Learning how to solder wires to a circuit board is a fundamental skill for electronics repair, prototyping, and PCB assembly. Whether you are attaching power leads, signal wires, or test connections, a weak solder joint can cause intermittent failures, lifted pads, or long-term reliability issues. In this step-by-step guide, you'll learn the correct tools, preparation methods, and soldering techniques needed to create strong, clean, and reliable wire-to-PCB connections. From preparing the wire and PCB......
BGA Reballing Explained: Complete Process, Tools, Risks, and Best Practices
In modern electronics design, the Ball Grid Array (BGA) is the standard for high-performance silicon, enabling thousands of I/O connections in a tiny footprint. However, this density creates a "black box" scenario: connections are hidden, and defects like cold joints or thermal fatigue cracks are invisible to the naked eye. Unlike a QFP that can be fixed with a soldering iron, a failed BGA threatens the viability of the entire board. BGA reballing is the critical solution to this problem. It is the pr......
SMD Soldering Tools You Need: Complete Guide from Beginner to Pro
Surface Mount Devices (SMDs) are essential components in modern electronic devices, including smartphones, tablets, and IoT systems. Unlike older through-hole methods, where components were inserted through drilled PCB holes, soldering SMD components manually can be challenging, especially for beginners. The extremely small sizes and tight spacing on modern PCBs require high precision, and achieving reliable solder joints often depends on using the best SMD soldering tools. Common issues arising from ......
IC Package Types Explained: A Practical Guide for PCB Designers
Walk into any electronics lab, and you'll hear the same debate: "Which IC package should I use here?" It sounds like a simple question until you realise the answer determines your PCB footprint, thermal headroom, assembly process, rework feasibility, and field reliability - all at once. This guide breaks down every major IC package type used in modern PCB design, helping you understand the differences between common IC package types in plain engineering language so you can make the right call from the......