Exploring the Differences Between Reflow Soldering and Wave Soldering in PCB Assembly
5 min
- Principles and Applications of Wave Soldering
- Principles and Applications of Reflow Soldering
- Comparison between reflow soldering and wave soldering
In PCB assembly processing, wave soldering and reflow soldering are two common soldering processes, but the choice of soldering method varies depending on the scenario. What is the difference between these two welding processes?
Principles and Applications of Wave Soldering
Wave soldering is a batch PCB soldering process mainly used for soldering through-hole devices (THD). The wave soldering process consists of four steps: flux spraying, pre-coating, wave soldering, and cooling.
1.Flux is primarily used to remove oxides from the board, which results in lower surface tension, enhanced heat transmittance, and a smoother soldering process.
2. Preheating: The PCB passes through a thermal channel for preheating and activation of flux.
3. Wave soldering: As the temperature rises, the solder paste transforms into a liquid, creating a wave that allows the components to be securely bonded to the board.
4. Cooling: The wave soldering process follows the temperature curve. During the wave soldering stage, as the temperature reaches its peak, it subsequently decreases in what is known as the cooling zone.
Wave Soldering progress
Advantages and Disadvantages of wave soldering:
Advantage
Fast Welding Speed: Wave soldering is suitable for soldering large-scale, high-density electronic components because of its rapid welding speed.
Stable welding quality: The solder joints are strong and reliable, making them suitable for applications with high welding quality requirements, such as the aerospace, and other fields.
Suitable for high-reliability connections: Ideal for applications that require highly reliable connections and electrical performance.
Shortcoming
Thermal Stress Effects: Welding-induced thermal stress may affect sensitive components.
Challenges with Soldering Complex PCBs: Wave soldering may not be ideal for intricate PCBs due to the requirement of exposing the entire board to a wave of molten solder.
Principles and Applications of Reflow Soldering
Reflow soldering is a common process used to connect electronic components to PCBs. The principle involves assembling PCBs and components pre-coated with solder paste, and then using high-temperature hot air or hot plates to melt the solder paste. This process forms solder joints, completing the soldering process. Reflow soldering can achieve efficient mass production, is suitable for SMT (surface mount technology) processes, and is widely used in the manufacturing of various electronic products.
The processing flow can be divided into two types: single-sided mounting and double-sided mounting.
Single-sided mounting involves pre-coating solder paste, mounting side A, reflow soldering, and power-on testing.
Double-sided mounting: Pre-coat the A-side with solder paste → Surface Mount Technology (SMT) → Reflow soldering → Apply solder paste to the B-side → Reflow soldering → Power-on inspection
With double side mounting, top and bottom sides doesn’t use same solder paste. Solder paste with higher reflow temperature goes on the first layer. After assembly and reflow of first layer is finished, second layer uses solder paste that melts on lower temperature point. This technique or trick is used to accomplish the effect that first layer doesn’t get melted while second one is being soldered.
Advantage
Fast welding speed: Reflow soldering offers high production efficiency and is suitable for mass production.
Stable welding quality: By accurately controlling the temperature curve and welding process, stable welding quality can be achieved.
Strong adaptability: Suitable for various types of electronic assembly, including small electronic equipment, SMT assembly, and welding of precision components.
High-density component welding: This process enables the welding of high-density components, enhancing the reliability and performance of the product.
Shortcoming
High equipment cost: Special equipment and process control are required, leading to high costs.
High-temperature control requirements: Precise control of parameters such as temperature curve and welding atmosphere is necessary.
Thermal Sensitivity: Some components may be sensitive to heat, posing a risk of thermal damage.
Comparison between reflow soldering and wave soldering
Welding Process
Applicability
Wave soldering is suitable for soldering large-scale, high-density electronic components, such as power boards and motherboards. It is typically used in applications that require highly reliable connections and electrical performance.
wave soldering
Reflow soldering is suitable for various types of electronic assembly, including small electronic devices, SMT assembly, and soldering of precision components. It allows for more flexible production since the application of solder paste can adapt to a variety of PCB designs and component arrangements.
Reflow soldering
Welding Temperature
Wave soldering typically involves higher soldering temperatures because it requires exposing the entire PCB to waves of molten solder. This can cause thermal stress on some sensitive electronic components.
Reflow soldering temperatures are typically lower because only the solder paste and solder joints need to be heated to the melting point. This helps reduce thermal damage to components.
Control and Precision
Wave soldering is generally easier to control because soldering parameters, such as the temperature and speed of the solder wave, can be adjusted more accurately.
Reflow soldering: The control of reflow soldering is more complex because the speed of heating and cooling needs to be considered, as well as the thermal sensitivity of different components. Requires more complex equipment and control systems
In summary, reflow soldering and wave soldering are two commonly used soldering technologies in industrial electronics manufacturing, each with unique advantages and applications. In practical applications, choosing suitable welding methods according to specific requirements and component characteristics can enhance production efficiency and welding quality.
Popular Articles
• SMT Assembly Process Explained and Equipment Used: A Step-by-Step Guide to PCBA Manufacturing
• Common PCB Assembly Methods and Soldering Techniques Explained
• SMD Soldering Tools You Need: Complete Guide from Beginner to Pro
• What Is BGA Void? Causes, IPC Limits, and Solutions
• Reflow Soldering: Everything You Need to Know
Keep Learning
Everything You Need to Know About Solder Wire
The Latin word solidare means "to make solid," this is where the term solder gets its start. For joining two metal parts, this alloy is used because of its low melting point. Solder is a substance that is used to attach items, basically we can say wires and leads components together. Soldering is considered a skill in electronics for assembly of components onto a bare board PCB. The solder wire used has a significant impact on how well a soldering project turns out. It consists of alloys, mostly based......
SMT vs Through Hole: Which PCB Assembly is Most Cost-Effective?
Performance and cost in the realm of electronics production depend on choosing the correct assembly method. Of the several approaches accessible, Surface Mount Technology (SMT) and Through-Hole Technology (THT) are the two most often used ones for PCB assembly. These two assemblies can be combined to create some products or used as individual technologies. Though seemingly little, this variance affects several aspects including board design, materials and techniques employed, heat dissipation, and rel......
PCB Soldering Basic Techniques and Overview
Soldering means joining metal components with a melted metal called solder, which has a low melting point compared to other metals. Soldering is crucial in the electronics industry and is the primary method of joining electrical components. There are different types of soldering materials based on quality and their melting points. The most common combination is a tin or lead metal alloy mixed with silver or brass. The soldering iron melts the metal so it can be used like glue to connect two pieces. On......
Lead-Free Solder vs Lead Solder : What is the Difference?
Solder is used by the majority of electrical devices to connect components to PCBs. The procedure of soldering is, when a solder melts down it will make a connection. This connection can be between pads or wires. Soldering is not like welding, we can attach the two joints by heating them again a lil bit. Although after performing the soldering step the curing and cooling is required. If during the cooling step there is any disturbance occur in the system it will lead to dry joints. Two main varieties ......
How to Repair a Burnt Circuit Board (and When to Replace It)
Key Takeaways Find out why the board burnt before you repair anything. The part that charred is often a victim of a fault somewhere else. Charred FR-4 conducts. A repair only lasts if every trace of carbon is cut out and the area measures as an insulator again. Heat that went through the board, blistering, or a burn among vias or under a BGA usually means replacing the board. Rebuild a burnt trace heavier than the original, and keep conductive epoxy off power paths. Power the repaired board from a cur......
How to Set the Temperature for Wave Soldering and What Are the Soldering Temperature Standards?
Wave soldering is a process used for soldering electronic components by inserting them into the holes on a Printed Circuit Board (PCB) and securing the components to the board using a molten solder wave generated by a wave soldering machine. Temperature is a crucial parameter during the wave soldering process, as it directly affects the quality and efficiency of soldering. Therefore, setting the temperature correctly for wave soldering is essential. Temperature for Wave Soldering Wave soldering machin......