Common PCB Assembly Methods and Soldering Techniques Explained
7 min
- Main PCB Assembly Methods
- Main PCB Soldering Techniques
- FAQs about PCB Assembly and Soldering
- Conclusion
Whether you're designing your first prototype or scaling up to production, understanding PCB assembly methods and soldering techniques is crucial to achieving reliable, high-performance circuit boards. Modern PCBA primarily relies on Surface Mount Technology (SMT) and Through-Hole Technology (THT)—each offering unique advantages for component density, durability, and manufacturability.
In this guide, we'll break down the major PCB assembly methods, key soldering techniques such as reflow and wave soldering, and the step-by-step PCB assembly process. You'll also learn how to identify and fix common defects like tombstoning, voids, and cold joints, helping you build cleaner, more consistent boards.
Main PCB Assembly Methods
PCB assembly is not a single technique but a collection of manufacturing strategies optimized for different component types, reliability requirements, and cost targets. The main PCB assembly approaches include Surface Mount Technology (SMT), Through-Hole Technology (THT), and mixed assembly, each with unique implications for signal integrity, thermal management, and manufacturability.
1Surface Mount Technology (SMT)
Surface Mount Technology (SMT) dominates modern PCBA because it enables miniaturization and high-density layouts. Instead of long leads, Surface Mount Device (SMD) has flat terminations or solder balls that sit directly on copper pads.
Stencil Printing
A stainless steel stencil deposits solder paste with precise volume control.
Pick-and-Place
High-speed machines place SMDs at ±25 μm accuracy.
Reflow Soldering
Thermal profile (preheat, soak, peak ~245 °C, controlled cool-down) forms intermetallic solder joints.

2Through-Hole Technology (THT)
Through-Hole Technology (THT) refers to the process of inserting component leads into drilled holes that are plated with copper, and then it is soldered either by wave soldering or selective soldering.
Hole Drilling
CNC drilling, plating to create conductive barrels.
Component Insertion
Manual or robotic insertion (axial or radial insertion machine).
Wave/Selective Soldering
Molten solder bonds leads to barrels.

3Mixed Assembly (SMT + THT)
Most real-world boards will use a combination of SMT and THT:
- SMT for ICs, passives, and RF circuits.
- THT for connectors, power semiconductors, and relays.
Challenges of Mixed Assembly
- Need to manage two different soldering processes (reflow + wave/selective)
- Thermal management has to address two different solder types.
- Board warpage may introduce alignment issues during the second soldering step.
To simplify this, JLCPCB offers hybrid assembly services, integrating SMT reflow and THT selective soldering.
4PCB Assembly Options: Single vs Double-Sided, Manual, and Turnkey Approaches
Single-Sided vs Double-Sided SMT: Double-sided requires more than one reflow cycle, and must be thermally balanced.
Manual Assembly: Still used for prototypes or specialized low-volume boards.
Turnkey vs Consignment PCB Assembly:
- Turnkey PCB Assembly → Manufacturer sources all parts.
- Consignment PCB Assembly → Customer supplies parts; manufacturer only assembles.
Also Read: How to Consign Parts to JLCPCB

Main PCB Soldering Techniques
1Reflow Soldering
Reflow soldering is the primary method for soldering SMT components. The reflow soldering process includes applying solder paste via a stencil, accurately picking and placing components, and passing the assembled PCB through a reflow oven with multiple thermal zones.
A lead-free solder reflow profile, such as for SAC305 alloy, typically consists of four stages: preheat (120–150 °C), soak (150–180 °C), peak (230–250 °C), and controlled cooling. Mechanical integrity depends on proper intermetallic compound (IMC) formation, while poor thermal management can cause common reflow defects such as tombstoning, voids, or popcorning.

2Wave Soldering
Wave soldering is used for through-hole (THT) components and larger surface-mount (SMT) components; a PCB board is pre-fluxed and passed across molten solder (approximately 250 degrees Celsius).
Wave soldering creates strong solder joints; it is ideal for high pin-count connectors or dual-in-line package integrated circuits (DIP ICs).
Note
Wave soldering is not recommended for small/pitch SMT components or SMT components due to potential risks of bridging and thermal stresses.

3Selective Soldering
Selective soldering applies solder in a localized area (pin) using a computer numeric controlled (CNC) soldering nozzle, which can be ideal for hybrid assemblies, i.e., an SMT component that has already been reflowed. By using selective soldering, you do not risk damaging the existing connections and minimize thermal stress on the adjacent components. Selective soldering is slower than wave soldering, but a stronger joint can be achieved.

4Hand Soldering
Manual soldering is mostly used for prototyping, rework, and low-volume boards. Hand soldering is flexible and labor-intensive, but errors can and will occur. For example, cold joints and inconsistent wetting. Hence, for high-volume productions, hand soldering should not be recommended.
FAQs about PCB Assembly and Soldering
Q: What is the difference between SMT and THT assembly?
SMT places components directly on the PCB surface using solder paste and reflow soldering, enabling miniaturization and high-density layouts. THT inserts component leads through drilled and plated holes, then solders them via wave or selective soldering for stronger mechanical bonds—ideal for connectors, power components, and high-reliability applications.
Q: What is the most common soldering method for SMT components?
Reflow soldering is the primary method for SMT components. It involves applying solder paste via a stencil, placing components, and passing the PCB through a reflow oven with controlled thermal zones (preheat, soak, peak ~245 °C, cooling) to form reliable intermetallic solder joints.
Q: Can SMT and THT be used on the same PCB?
Yes, this is called mixed assembly. SMT components are placed and reflowed first, then THT components are inserted and soldered via wave or selective soldering. Challenges include managing two different soldering processes and potential board warpage during the second soldering step.
Q: What is the difference between turnkey and consignment PCB assembly?
In turnkey assembly, the manufacturer sources all components and handles the entire process. In consignment assembly, the customer supplies the parts and the manufacturer only performs the assembly. Turnkey reduces procurement burden, while consignment gives the customer more control over component sourcing.
Q: What are common PCB assembly defects and how can they be prevented?
Common defects include tombstoning (uneven solder wetting causing components to stand up), voids (trapped gas in solder joints), cold joints (insufficient heat/dull appearance), and bridging (unintended solder connections between pins). Prevention requires proper stencil design, optimized thermal profiles, controlled cooling rates, and thorough inspection using AOI or X-ray.
Conclusion
Mastering PCB assembly is about precision, consistency, and quality control—from selecting the right assembly method (SMT, THT, or mixed) to applying the proper soldering technique for each component type. Understanding how to prevent and fix assembly defects not only improves circuit board reliability but also reduces production waste and rework.
Popular Articles
• SMD Soldering Tools You Need: Complete Guide from Beginner to Pro
• SMT Assembly Process Explained and Equipment Used: A Step-by-Step Guide to PCBA Manufacturing
• Common PCB Assembly Methods and Soldering Techniques Explained
• What Is BGA Void? Causes, IPC Limits, and Solutions
• Reflow Soldering: Everything You Need to Know
Keep Learning
What Is Tombstoning? A Practical Guide to Causes, Reflow Risks, Prevention, and Rework
Key Takeaways Definition: Tombstoning occurs when a small two-terminal component lifts off one pad during reflow and stands upright, leaving one end without a proper solder connection. Root Cause: Unequal solder wetting forces act on the two terminals, often due to differences in pad temperature, solder-paste volume, pad geometry, or thermal mass. Highest Risk: Small passive components, such as 0201 and 0402 resistors and capacitors, are especially susceptible because their low mass and small terminat......
12 Professional Soldering Tips and Tricks Every Beginner Should Know
Soldering is not merely "gluing" metal; it is a metallurgical process that creates an intermetallic compound (IMC). This molecular bond ensures the electrical and mechanical integrity of your device. A poor joint might pass a quick visual check but will inevitably fail under vibration or thermal stress, leading to "ghost" bugs and hardware failures. These soldering tips and tricks focus on practical, repeatable techniques used in professional electronics soldering—from correct heat transfer and flux u......
Wire Bonding vs Flip Chip: Key Differences in Semiconductor Packaging
In the rapidly evolving world of semiconductor packaging, the choice between Wire Bonding and Flip Chip technology is more than just a mechanical decision—it is a strategic pivot that dictates your product’s performance, thermal limits, and bottom line. Are you looking for the cost-effective reliability of traditional interconnects, or does your application demand the high I/O density and superior signal integrity of modern flip-chip architectures? In this comprehensive guide, we draw on years of high......
Chip Scale Package (CSP) Explained: Types, Benefits & More
Open any flagship smartphone motherboard and the ICs look almost like bare silicon - no chunky leads, no oversized housings. That is chip scale packaging in action. By definition, a chip scale package (CSP) is an IC package where the total body area is ≤1.2× the die size, adhering to rigorous JEDEC and IPC standards. This design philosophy translates directly into smaller boards, shorter signal paths, and superior electrical performance, which is why CSPs now ship in everything from wireless earbuds t......
How to Solder Wires to a Circuit Board Properly: Step-by-Step Guide
Learning how to solder wires to a circuit board is a fundamental skill for electronics repair, prototyping, and PCB assembly. Whether you are attaching power leads, signal wires, or test connections, a weak solder joint can cause intermittent failures, lifted pads, or long-term reliability issues. In this step-by-step guide, you'll learn the correct tools, preparation methods, and soldering techniques needed to create strong, clean, and reliable wire-to-PCB connections. From preparing the wire and PCB......
BGA Reballing Explained: Complete Process, Tools, Risks, and Best Practices
In modern electronics design, the Ball Grid Array (BGA) is the standard for high-performance silicon, enabling thousands of I/O connections in a tiny footprint. However, this density creates a "black box" scenario: connections are hidden, and defects like cold joints or thermal fatigue cracks are invisible to the naked eye. Unlike a QFP that can be fixed with a soldering iron, a failed BGA threatens the viability of the entire board. BGA reballing is the critical solution to this problem. It is the pr......