PCB Design : How to Resolve Short Circuit Defects Caused by HASL
9 min
- Introduction
- Understanding the HASL Process and Why Short Circuits Occur
- Why ENIG is the Recommended Solution for Dense Designs
- Detailed Comparison: HASL vs. ENIG at JLCPCB
- Practical PCB Design Recommendations to Minimize Risks
- FAQ about Short Circuit Defects Caused by HASL
- Conclusion and Actionable Advice
Key Takeaways
In high-density PCB designs, HASL frequently causes solder bridging and short circuits due to its uneven surface and molten solder flow, especially on fine-pitch and dense traces. The most effective solution is to switch to ENIG (Electroless Nickel Immersion Gold), which provides superior planarity, significantly reduces bridging risks, and improves assembly yield. By selecting ENIG for dense layouts, optimizing solder mask design, and running DFM checks, designers can effectively eliminate HASL-related defects while achieving higher reliability at JLCPCB.
Introduction
In modern high-density PCB designs, short circuits caused by surface finish processes remain a frequent challenge during manufacturing and assembly. Hot Air Solder Leveling (HASL) is still one of the most economical surface finishes offered by JLCPCB. However, for boards with dense traces, fine-pitch components, or coil patterns, HASL can easily cause solder bridging and short circuits. This article provides a comprehensive analysis of the root causes and recommends effective solutions, focusing on Electroless Nickel Immersion Gold (ENIG), fully aligned with JLCPCB’s actual manufacturing capabilities.

Understanding the HASL Process and Why Short Circuits Occur
HASL Process Steps (JLCPCB Implementation)
HASL, also known as Hot Air Solder Leveling, is a traditional surface finish method. The bare PCB, after etching and solder mask application, is first cleaned and fluxed. It is then dipped vertically into a molten solder bath (leaded SnPb or lead-free SnAgCu alloy). As the board is withdrawn, high-pressure hot air knives level the excess molten solder, leaving a thin coating on exposed copper pads and traces.
While this process is reliable and cost-effective for standard designs, it presents significant challenges in high-density layouts. The molten solder has high surface tension and fluidity. In regions with narrow solder mask openings or closely spaced traces, it tends to adhere to adjacent copper features before solidifying, forming unwanted bridges that result in short circuits.
Common Scenarios Prone to HASL Bridging
- Dense SMD pads with pitch ≤ 0.5 mm (e.g., QFN, BGA, 0201 components)
- Coil boards or RF circuits with numerous parallel fine traces
- Areas with small “window openings” in solder mask where clearance is insufficient
- Multi-layer or HDI boards with varying thermal mass
Production experience and JLCPCB guidelines show that these issues become prominent when trace spacing approaches the practical limits for uniform solder distribution.
Root Technical Causes
The primary reasons stem from the inherent characteristics of the HASL process. The resulting surface is non-planar, with solder thickness varying significantly (approximately 5–50 μm), creating peaks and valleys. During hot air leveling, excess solder can migrate laterally in dense regions. Narrow solder mask dams or insufficient clearance allow molten solder to wet unintended areas. Variations in board thickness, copper weight, and preheat conditions can further worsen bridging. These factors ultimately lead to higher defect rates in SMT assembly, increased rework costs, and reduced yield.
Why ENIG is the Recommended Solution for Dense Designs
ENIG Process Overview and Advantages
ENIG (Electroless Nickel / Immersion Gold) uses a chemical plating process that deposits a nickel barrier layer (typically 3–6 μm thick) followed by a thin gold layer (0.05–0.2 μm). This creates a mirror-flat, highly uniform surface. Unlike HASL’s physical leveling, ENIG completely avoids solder flow variability. JLCPCB offers ENIG as a standard option for most board types, including 6+ layer boards and RF applications.

Key Benefits for Short Circuit Prevention
- Superior planarity that virtually eliminates bridging risks even at fine pitches below 0.5 mm
- Consistent thickness with no peaks or valleys that trap or redirect solder during reflow
- Excellent compatibility with high-density interconnects (HDI), coil patterns, and dense mask openings
- Longer shelf life and strong oxidation resistance, ideal for humid environments
- Full RoHS compliance as it is chemically lead-free
While ENIG has a higher cost than HASL, the investment is often offset by significantly improved first-pass yield and fewer assembly defects.
Detailed Comparison: HASL vs. ENIG at JLCPCB
Overview of HASL and ENIG
HASL and ENIG represent two fundamentally different approaches to PCB surface finishing. HASL relies on a physical process (molten solder dipping + hot air leveling), while ENIG uses a chemical deposition method. This difference directly impacts surface flatness, bridging risk, cost, and suitability for dense designs. Understanding these trade-offs helps designers make informed decisions to avoid short circuit defects.
Performance Metrics Table (Based on JLCPCB Data)
| Feature | HASL / Lead-free HASL | ENIG (Immersion Gold) | Best Use Case Recommendation |
|---|---|---|---|
| Cost | Lowest | Moderate to Higher | HASL for simple; ENIG for dense |
| Surface Flatness | Uneven (prone to bridging) | Excellent (planar) | ENIG for fine-pitch |
| Fine Pitch Compatibility | Limited (≥ 0.5 mm recommended) | Excellent (< 0.5 mm, down to 0.3 mm+) | ENIG |
| Solderability | Good (but variable) | Excellent & consistent | ENIG |
| Shelf Life | 6–12 months | >12 months | ENIG |
| RoHS Compliance | Lead-free version available | Fully compliant | ENIG |
| Typical Thickness | Variable (5–50+ μm) | Ni: 3–6 μm, Au: 0.05–0.2 μm | - |
| Applications | Through-hole, low-density, prototypes | HDI, BGA/QFN, coil/RF, high-reliability | See design section |
This comparison clearly shows when to choose each finish. HASL suits cost-sensitive, coarse-pitch boards, while ENIG excels in dense and high-reliability designs.
In-Depth Analysis of Key Differences
HASL remains the most cost-effective choice for many standard applications. Its pre-tinned surface offers excellent initial solderability, making it suitable for through-hole and coarser-pitch SMD components. However, the uneven topography created by the hot air leveling process increases the risk of solder bridging in dense areas — precisely the short circuit issue this article addresses.
In contrast, ENIG provides a flat, uniform surface that significantly reduces bridging risks and improves assembly yield for fine-pitch components such as BGAs, QFNs, and 0201 packages. The nickel barrier layer also prevents copper diffusion, while the thin gold layer offers superior corrosion resistance and longer shelf life. Although ENIG costs more due to the precious metals and additional chemical steps, it is often the more economical choice overall for high-density or high-reliability boards because it minimizes defects and rework.
Practical PCB Design Recommendations to Minimize Risks
Surface Finish Selection Strategy
Evaluate your design’s minimum pitch and density early in the layout stage. In the JLCPCB ordering interface, select ENIG for any board containing features prone to HASL bridging. Always run the free online DFM analysis on your Gerber files before submission to catch potential issues.
Solder Mask and Clearance Optimization
- Maintain adequate solder mask dam width (minimum ~0.1 mm depending on process)
- Follow JLCPCB’s recommended solder mask expansion (typically 0.05–0.1 mm)
- Consider Non-Solder Mask Defined (NSMD) pads in dense areas
- Slightly increase trace-to-trace spacing in critical zones if HASL must be used
Trace Spacing and Layout Best Practices
Follow JLCPCB’s minimum trace/space rules based on copper weight and layer count. Adding teardrops on pads improves reliability. For coil and RF sections, route critical signals on inner layers with proper ground plane shielding. Perform thorough DRC and consider thermal profile simulation for reflow assembly.
Additional Manufacturing and Assembly Tips
- Use proper panelization with appropriate array spacing and fiducials for better SMT handling
- For ENIG boards, standard stencil thickness (0.1–0.12 mm) usually works well due to excellent flatness
- Order Flying Probe or fixture electrical testing to detect latent shorts early
- Start with small prototype runs to validate the surface finish choice before scaling to volume production
FAQ about Short Circuit Defects Caused by HASL
Q: What is the main cause of short circuits when using HASL?
The main cause is the uneven, non-planar solder surface created during vertical immersion and hot air leveling. In dense areas or with fine pitches, molten solder easily bridges adjacent traces or pads before it solidifies.
Q: When should I choose ENIG instead of HASL at JLCPCB?
Choose ENIG when your design has trace spacing or component pitch ≤ 0.5 mm, dense SMD pads, coil/RF patterns, BGA/QFN packages, or when you need high assembly yield and reliability. For simple, low-density, or cost-sensitive boards with pitch > 0.65 mm, HASL is usually sufficient.
Q: How much more expensive is ENIG compared to HASL?
ENIG is moderately more expensive than HASL or Lead-free HASL, but the price difference at JLCPCB is reasonable and often offset by reduced defects and rework. Check the real-time quote in the JLCPCB ordering system for your specific board parameters.
Q: Does switching to ENIG affect signal integrity or impedance control?
ENIG has excellent planarity and minimal impact on impedance. Its thin, uniform coating (Ni + Au) is well-suited for high-frequency and RF boards. It is often preferred over HASL for impedance-critical designs because of its consistency.
Q: Can I still use HASL safely for dense designs?
It is possible but risky. You would need to increase trace spacing, enlarge solder mask openings carefully, and accept potentially lower yield. For most dense or fine-pitch boards, JLCPCB recommends ENIG to avoid bridging issues.
Q:How do I specify the surface finish when ordering at JLCPCB?
In the JLCPCB online order page, simply select “ENIG” or “Immersion Gold” under Surface Finish options. Upload your Gerber files and run the DFM check — the system will flag potential issues. You can also add notes in the order comments if needed.
Conclusion and Actionable Advice
Switching from HASL to ENIG for dense-circuit or fine-feature PCBs is one of the most effective ways to resolve short circuit defects caused by solder adhesion. JLCPCB makes this transition easy with clear options, competitive pricing, and robust DFM support. By combining the right surface finish with good layout practices, you can significantly improve manufacturing yield, reduce assembly defects, and enhance overall product reliability.
Keep Learning
Implications of border lines and 3D footprint lines on Mechanical Layer 1
Key Takeaways Mastering Mechanical Layer 1 is essential for accurate PCB manufacturing. Always place the complete board outline, mounting holes, and irregular slots on Mechanical Layer 1 (GM1), as JLCPCB prioritizes the lowest-numbered Mechanical Layer while ignoring KEEP-OUT and higher Mechanical Layers. 3D footprint lines serve only as design references and will not be fabricated. Following these layer priority rules and best practices ensures correct board dimensions, proper slot formation, and avo......
The Role of PCB Test Fixtures in High-Volume Manufacturing
In high-volume manufacturing of Printed Circuit Boards (PCBs), quality, efficiency, and reliability are paramount. One of the most crucial tools in achieving these goals is the PCB test fixture. These fixtures play a vital role in ensuring that PCBs meet the required performance standards before they are integrated into electronic devices. This article delves into the importance of PCB test fixtures, their types, and how they contribute to the efficiency of high-volume manufacturing. Specialized and c......
SMT or Through Hole Technology?Which is Better for Your Project?
When designing and manufacturing electronics, one of the most important steps is selecting the appropriate assembly method. Nowadays we have through-hole technology and surface mount technology, which become the industry standards and are the two main approaches. The surface-mount technology (SMT) uses components that are perfectly aligned with the PCB surface. On the other hand through-hole technology (THT) uses leads that are placed into pre-drilled holes in the PCB and thereafter soldered. Consider......
PCB temperature: Tips regarding improving the thermal management of PCBs
Thermal management is of utmost importance while designing PCBs. This is because the temperature of PCBs can guarantee the reliability, performance, and longevity of PCBs and the electronic equipment of which they are an integral component. Thus, enhanced Printed Circuit Board heat management is a necessity for reliable operation and to protect against damage to electronic components. In the upcoming chapter, we will discuss several approaches to strengthen PCB temperature management. Reasons of heat ......
Design for Manufacturing (DFM): A Comprehensive Guide for Optimizing Production
Maintaining quality while improving the manufacturing process is critically important in the competitive fields of electronics and industry. Design for Manufacturing (DFM) here comes in handy. DFM is a design tool stressing the simplicity of manufacturing during the product development stage. Early on manufacturing limitations help DFM to guarantee that goods are not only useful but also reasonably priced, dependable, and easily produced at large-scale production. This article covers the importance of......
Design for Manufacturing and Assembly: A Complete DFMA for PCB Design Guide
Key Takeaways DFMA covers both PCB fabrication and assembly: DFM addresses bare-board fabrication, while DFA addresses component assembly and related process constraints. The biggest decisions happen early: Package choice, layer count, and board outline are usually set well before Gerber export and become expensive to change later. Passing DRC does not guarantee a good footprint: Design rules can verify clearances and copper geometry, but they cannot confirm that a footprint matches the component data......