The Ultimate Guide to PCB Panelization: Tools and Techniques
13 min
- What is Panelization in PCB?
- Tools for PCB Panelization
- Techniques for Making a PCB Panel
- Challenges and Solutions in Panelization
- FAQ about Guide to PCB Panelization
- Conclusion
Printed circuit boards (PCBs) are the backbone of modern electronics. One critical aspect of PCB manufacturing is panelization — the process of arranging multiple PCBs onto a single larger panel for efficient manufacturing and assembly. This technique allows multiple boards to be processed simultaneously, significantly reducing costs and improving production efficiency.
In this article, we will provide a comprehensive guide to PCB panelization, covering the tools and techniques required for successful panelization, as well as design considerations and common challenges. Let's dive into the world of PCB panelization and explore the tools, techniques, and best practices for successful panelization.
What is Panelization in PCB?
Panelization is the process of arranging multiple PCBs onto a single panel for efficient manufacturing and assembly. The panel is then processed as a single unit, rather than processing each PCB individually. Panelization can significantly improve the efficiency and reduce the cost of PCB manufacturing and assembly.
Types of Panelization:
Panelization is a critical process in PCB manufacturing and assembly, allowing for more efficient and cost-effective production. There are several types of panelization methods used in the industry. Each method has its own benefits and drawbacks, and the appropriate method should be selected based on the specific requirements of the project.
V-Cut Panelization:
V-cut panelization is a process in which a V-shaped groove is created in the panel, allowing for easy separation of the individual PCBs. The V-cut tool is a specialized cutting tool that is designed to create a clean and precise groove. Once the groove is created, the panel can be easily bent along the groove to separate the individual PCBs. V-cut panelization is a popular method due to its simplicity and low cost. However, it may not be suitable for PCBs with components located close to the edge of the PCB, as the bending process may damage these components.
| Method | Best For | Key JLCPCB Specs | Advantages | Disadvantages | Post-Separation Edge |
|---|---|---|---|---|---|
| V-Cut (V-Scoring) | Rectangular boards, straight lines | 25° angle, min panel 70×70 mm, straight H/V lines only, min connecting edge 3 mm (5 mm for ≤0.8 mm thick), clearance ≥0.4 mm from centerline, tolerance ±0.4 mm | Lowest cost, minimal waste, fast | Only straight lines, higher stress | Relatively smooth (possible minor fibers) |
| Mouse Bites (Tab Routing) | Irregular shapes, components near edges | 0.60 mm dia. holes (5–8 per set), 0.35–0.4 mm edge-to-edge spacing (min 0.3 mm), ≥2 symmetric sets, panel gap 1.6–2 mm (min 1.2 mm), add set every 50–60 mm | Versatile, lower component stress | Slightly more waste, serrated edges (may need sanding) | Serrated (cleanable) |
Tab Routing Panelization:
Tab routing panelization is a process in which small tabs are created between the individual PCBs, allowing for easy separation from the panel. The routing tool is a specialized cutting tool that is designed to create a precise cut in the panel. Once the tabs are created, the panel can be easily broken along the cut line to separate the individual PCBs. Tab routing panelization is a popular method due to its versatility and ability to accommodate PCBs with components located close to the edge of the PCB. However, it may be more time-consuming and expensive compared to other methods.
Mouse Bites Panelization:
Mouse bites panelization creates arrays of small perforations, typically consisting of 5 to 8 holes of 0.60 mm diameter with edge-to-edge spacing of 0.35–0.4 mm (minimum 0.3 mm for structural integrity). Designers should place at least two symmetric sets per board, adding more sets every 50–60 mm for longer boards. This approach is particularly suitable for complex or irregular board outlines and situations where components are located close to the edges. The gap between adjacent boards is usually 1.6 mm or 2 mm. After snapping, the edges may exhibit a serrated finish that can be cleaned or lightly sanded if a smoother appearance is required.
Advantages of Panelization:
Reduced Costs:
Panelization can significantly reduce the cost of PCB manufacturing and assembly, as it allows for more efficient use of materials, equipment, and labor. By processing multiple PCBs simultaneously, manufacturers can reduce the amount of waste material and the time required for setup and teardown of equipment.
Improved Efficiency:
Panelization can also improve the efficiency of PCB manufacturing and assembly, as it allows for more consistent and reliable processing. By processing multiple PCBs simultaneously, manufacturers can reduce the variability in production and improve the overall quality and reliability of the final product.
Easier Assembly:
Panelization can also make the assembly process easier and more efficient. By arranging multiple PCBs onto a single panel, the assembly process can be streamlined, reducing the time and effort required for assembly.
Tools for PCB Panelization
Panelization is a critical process in PCB manufacturing and assembly, allowing for more efficient and cost-effective production. Several tools are available to aid in the panelization process, including software tools, panelization equipment, and specialized tooling.
PCB Design Software:
PCB design software is a critical tool for panelization, as it allows for the design and layout of the individual PCBs to be optimized for panelization. Software tools such as EasyEDA, Altium Designer, Eagle PCB and KiCad allow for the creation of panelized PCB designs, with features such as panelization templates, array tools, and step-and-repeat functions.
Panelization Equipment:
Panelization equipment is used to physically separate the individual PCBs from the panel once the manufacturing process is complete. Equipment such as V-cut tools, routing tools, and punching tools are commonly used for this purpose. These tools are designed to create clean and precise cuts or perforations in the panel, allowing for easy separation of the individual PCBs.
Specialized Tooling:
Specialized tooling is used to aid in the panelization process, such as pick-and-place machines, stencil printers, and reflow ovens. These tools are designed to automate and streamline the manufacturing and assembly process, reducing the time and effort required for manual assembly.
Quality Control Tools:
Quality control tools such as inspection cameras, X-ray machines, and testing equipment are used to ensure the quality and reliability of the final product. These tools allow for the detection of defects or issues that may arise during the panelization process, allowing for corrective action to be taken before the final product is shipped.
Advanced Software Features for Panelization:
Modern PCB design tools provide powerful panelization capabilities. Features such as automatic array generation, step-and-repeat functions, panel border creation, fiducial placement, and 3D panel preview help designers create optimized layouts quickly. Popular software including KiCad, EasyEDA, and Altium Designer offer dedicated panelization plugins or built-in tools that automatically handle clearances, tab placement, and V-cut lines while performing design rule checks.
Techniques for Making a PCB Panel
The process of making a PCB panel involves several steps, including designing the panel layout, selecting the appropriate panelization method, and manufacturing the panel. Here are some techniques for making a PCB panel:
Design the Panel Layout:
Design the Panel Layout: Begin by determining the optimal arrangement of individual boards to maximize panel utilization while maintaining required clearances. Include process rails (typically 5–10 mm wide) along the panel edges with fiducial markers for automated assembly equipment. Consider thermal expansion, component orientation, and separation method when placing boards. Modern PCB design software provides array and step-and-repeat functions to streamline this process. It is highly recommended to simulate the full panel in 3D and perform a design rule check (DRC) before finalizing the layout.
Select the Panelization Method:
Once the panel layout has been designed, the appropriate panelization method should be selected. The selection should be based on the specific requirements of the project, including the density and complexity of the PCBs, the location of components on the PCBs, and the desired cost and efficiency.
Create the Panel:
Once the panelization method has been selected, the panel can be created. This process will vary depending on the selected panelization method. For example, for V-Cut panelization, a V-shaped groove is created in the panel using a specialized cutting tool. For tab routing panelization, small tabs are created between the individual PCBs using a routing tool. For mouse bite panelization, small perforations, or "mouse bites", are created in the panel using a punching tool.
Separate the Individual PCBs:
Once the panel has been created, the individual PCBs can be separated. This process will vary depending on the selected panelization method. For V-Cut panelization, the panel can be bent along the V-shaped groove to separate the individual PCBs. For tab routing panelization, the panel can be broken along the cut lines between the PCBs. For mouse bite panelization, the panel can be broken along the perforations.
Test and Verify:
Before beginning production, it is important to test and verify the panelized design using simulation and testing tools. This can help to ensure that the design meets the required specifications and standards, and can help to identify any issues or defects that may affect the quality and reliability of the final product.
Best Practices for Successful Panelization:
To achieve optimal results, always follow these guidelines: maintain consistent board orientation when possible, avoid placing components or critical traces within 3–5 mm of separation lines, include adequate tooling holes and fiducials on the panel rails, and verify panel flatness for multi-layer boards. For high-volume production, consider prototype runs with the chosen panelization method first. Proper documentation of panel drawings and separation instructions is also essential for smooth communication with manufacturing partners.
Challenges and Solutions in Panelization
Panelization is a common process in PCB manufacturing, but it can also present several challenges. Here are some common challenges and solutions in panelization:
Component Placement:
One of the challenges in panelization is ensuring that the components on the individual PCBs are placed in a way that allows for easy separation from the panel without damaging the components. To address this challenge, designers can use specialized panelization software that allows them to easily adjust the placement of components on the individual PCBs to ensure that they are located away from the edges of the PCBs.
Trace Routing:
Another challenge in panelization is ensuring that the traces on the individual PCBs are routed in a way that allows for easy separation from the panel without damaging the traces. To address this challenge, designers can use specialized routing software that allows them to easily adjust the routing of the traces on the individual PCBs to ensure that they are located away from the edges of the PCBs.
Thermal Management:
Thermal management is another challenge in panelization, as components that generate heat must be placed and routed in a way that allows for adequate heat dissipation. To address this challenge, designers can use specialized thermal management software that allows them to simulate the thermal performance of the panelized design and identify any potential issues or hotspots.
Manufacturing Tolerances:
Manufacturing tolerances can also present a challenge in panelization, as the manufacturing process can introduce variations in the dimensions of the panel and the individual PCBs. To address this challenge, designers can use specialized panelization software that allows them to adjust the layout of the individual PCBs to accommodate any variations in the dimensions of the panel.
Assembly and Testing:
Another challenge in panelization is ensuring that the individual PCBs can be assembled and tested after separation from the panel. To address this challenge, designers can use specialized software that allows them to design the panel in a way that allows for easy assembly and testing of the individual PCBs.
Panel Utilization and Cost Optimization:
One of the main challenges in panelization is controlling costs, as improper design can lead to excessive material waste or complex manufacturing processes. Achieving high panel utilization (ideally 70–85%) is crucial for maximizing cost savings. Designers should carefully balance the number of boards per panel, spacing requirements, and assembly constraints. Techniques such as nested or rotated placements for irregular boards, combined with optimized clearances, can significantly improve material efficiency. Selecting the right panelization method (V-Cut or Mouse Bites) and maintaining good communication with the fabrication team during the design phase will help minimize unexpected expenses.
FAQ about Guide to PCB Panelization
Q: What is PCB panelization and why is it important?
PCB panelization is the process of arranging multiple individual circuit boards onto a single larger panel for manufacturing and assembly. It is important because it significantly reduces production costs, minimizes material waste, improves manufacturing efficiency, and makes automated assembly easier and more reliable.
Q: What are the main differences between V-Cut and Mouse Bites panelization?
V-Cut (V-Scoring) uses V-shaped grooves for straight-line separation and is the most cost-effective option for rectangular boards. Mouse Bites (Tab Routing with perforations) uses small drilled holes to create breakaway tabs and offers greater flexibility for irregular board shapes or when components are placed close to the edges. V-Cut provides cleaner edges but limited layout options, while Mouse Bites are more versatile but may leave slightly serrated edges.
Q: How much clearance should I keep between components and panel separation lines?
For V-Cut, maintain at least 3–4 mm clearance from the groove centerline. For Mouse Bites, keep components at least 3–5 mm away from the perforation lines. These clearances help prevent damage to components, traces, and pads during depanelization.
Q: Which panelization method should I choose for my project?
Choose V-Cut for rectangular boards with straight edges and high-volume production where cost is the top priority. Use Mouse Bites when your design has irregular shapes, rounded corners, or components located near the board edges. Consider your board outline, component placement, and separation requirements when making the decision.
Q: How can I maximize panel utilization and reduce manufacturing costs?
Aim for a panel utilization rate of 70–85%. Optimize board arrangement using nesting or rotation for irregular shapes, minimize unnecessary spacing, include efficient process rails (5–10 mm), and perform thorough Design Rule Checks (DRC). Selecting the appropriate panelization method and testing the layout in advance are also critical for cost optimization.
Q: What are the most common mistakes in PCB panelization and how can they be avoided?
Common mistakes include insufficient clearance for components near separation lines, improper tab or V-cut placement, missing fiducials on rails, and poor panel utilization. These can be avoided by following manufacturer design guidelines, using panelization tools in software like KiCad or Altium, simulating the full panel layout, and verifying the design with a prototype run before mass production.
Conclusion
Panelization remains one of the most effective ways to optimize PCB manufacturing, reduce costs, and enhance production efficiency. By carefully selecting the appropriate method, following best design practices, and paying attention to clearances and tolerances, engineers can overcome common challenges and deliver high-quality products. As PCB designs grow increasingly complex, mastering panelization techniques becomes ever more valuable for both prototype and high-volume production.
Keep Learning
The Ultimate Guide to PCB Panelization: Tools and Techniques
Printed circuit boards (PCBs) are the backbone of modern electronics. One critical aspect of PCB manufacturing is panelization — the process of arranging multiple PCBs onto a single larger panel for efficient manufacturing and assembly. This technique allows multiple boards to be processed simultaneously, significantly reducing costs and improving production efficiency. In this article, we will provide a comprehensive guide to PCB panelization, covering the tools and techniques required for successful......
PCB File Formats
Ordering printed circuit boards (PCBs) involves providing precise and detailed information about the design and specifications of the board. This is why specific PCB file formats are necessary. Manufacturing can only take place successfully with a completed PCB file. Designing a PCB and communicating those design decisions depends on files such as circuit schematic designs, Bill-of-Materials, PCB layouts, and stack-up design information. To ensure interoperability among various electronics design soft......
How to Run a Design Rule Check (DRC) for Your PCBs
Any time you design a PCB, and you want to turn it into a real product, you will have to make sure the design obeys all the constraints within the standard PCB manufacturing process. These constraints in the PCB design are known as Design rules and to check these rules in a CAD software we have to run the DRC(Design Rule Check) algorithm. The ever-increasing complexity of boards has made it nearly impossible to carry out the design rule verification process manually, so designers have to program the r......
Using Via-in-Pad Technology: What You Need to Know, Design Guidelines, and More…
In the world of multi-layer PCB (Printed Circuit Board) design, vias are essential parts that connect different layers of a board. As electronic devices become more compact and complex, designers must employ advanced technologies to optimize board space and performance. One such technology is via-in-pad technology, which has become increasingly popular in high-density and high-performance PCB designs. This article explores the essentials of via-in-pad technology, including guidelines for its implement......
Castellated PCBs: Introduction and Design Requirements
With the rapid development of electronic technology, electronic products are moving towards miniaturization, portability, multi-functionality, high integration, and high reliability.Consequently, printed circuit boards (PCBs) are frequently designed to integrate pre-existing, off-the-shelf modules. For example, IoT Bluetooth modules or NB-IoT modules, which are indispensable communication modules, can be soldered onto PCBs just like chips. These carrier boards are characterized by their small size and......
Implications of border lines and 3D footprint lines on Mechanical Layer 1
Key Takeaways Mastering Mechanical Layer 1 is essential for accurate PCB manufacturing. Always place the complete board outline, mounting holes, and irregular slots on Mechanical Layer 1 (GM1), as JLCPCB prioritizes the lowest-numbered Mechanical Layer while ignoring KEEP-OUT and higher Mechanical Layers. 3D footprint lines serve only as design references and will not be fabricated. Following these layer priority rules and best practices ensures correct board dimensions, proper slot formation, and avo......