Implications of border lines and 3D footprint lines on Mechanical Layer 1
6 min
- Example Scenario:
- Guidelines for Proper Component Placement and Slot Recognition:
- FAQ about Mechanical Layer 1
- Conclusion
Key Takeaways
Mastering Mechanical Layer 1 is essential for accurate PCB manufacturing. Always place the complete board outline, mounting holes, and irregular slots on Mechanical Layer 1 (GM1), as JLCPCB prioritizes the lowest-numbered Mechanical Layer while ignoring KEEP-OUT and higher Mechanical Layers. 3D footprint lines serve only as design references and will not be fabricated. Following these layer priority rules and best practices ensures correct board dimensions, proper slot formation, and avoids costly manufacturing errors.
In the process of PCB (Printed Circuit Board) design, the Mechanical Layer plays a crucial role in defining the physical aspects of the board. It helps in determining the placement of components, recognition of slots, and creation of drilled holes. In this article, we will explore the implications of border lines and 3D footprint lines on Mechanical Layer 1 in PCB manufacturing using an example. Mechanical layers (often denoted as GM1, GM2, etc. in Gerber files) are critical for board outline definition, with JLCPCB prioritizing the lowest-numbered Mechanical layer for routing and panelization.
Example Scenario:
Let's consider a scenario where Mechanical Layer 1 has placed border lines and 3D footprint lines for components. The image provided below showcases the design:
Analyzing the Design:
In the given design, the 3D footprint lines of the components are drawn on Mechanical Layer 1. However, it is important to note that in the final product, these 3D footprint lines will not be included as they serve primarily as assembly and 3D modeling references (e.g., component height and courtyard visualization in CAD tools). Instead, the design includes four circles that are intended to produce drilled holes. Ensure hole diameters meet JLCPCB's minimum drill size (typically 0.15-0.2mm depending on layer count) and maintain proper annular ring (≥0.1mm recommended).
Guidelines for Proper Component Placement and Slot Recognition:
Based on the provided design, we can identify certain aspects that need to be addressed to ensure accurate manufacturing and avoidance of unnecessary slots or missing holes. Here are the key guidelines:
Placement of Edge Lines and Circles:
To optimize design clarity and accuracy, it is generally recommended to use Mechanical Layer 1 (GM1) exclusively for the complete board outline and critical features such as mounting holes. Non-outline elements like 3D footprints should be moved to Mechanical Layer 2 or higher. If four circles are needed for drilled holes, ensure they are properly defined in the Drill layer as well.
Unique Edge Layer for Irregular Slots:
For screw holes or irregular slots (shapes drawn) that need to be formed within the board, it is crucial to draw them correctly on a unique edge layer. This allows for precise recognition and implementation of the desired slot shapes during manufacturing.
| Feature | Recommended Layer | Notes / Capabilities |
|---|---|---|
| Board Outline & V-Cut | Mechanical 1 (GM1) | Lowest number priority; Line width ~0.15mm |
| Irregular Slots/Cutouts | Same as Outline (GM1) | Min plated slot width 0.5mm; Length ≥ 2x width |
| Mounting Holes | Drill + Mechanical 1 | Tolerance ±0.1mm (regular) |
| 3D Footprint / Courtyard | Mechanical 2+ | Not manufactured; Reference only |
Consideration of Layer Priority:
It's important to understand how layers are prioritized for routing purposes. In situations where both the KEEP-OUT layer and Mechanical Layer have complete borders, JLCPCB (the PCB manufacturer) will prioritize the elements from the Mechanical Layer and disregard data from the KEEP-OUT layer.This ensures consistent manufacturing even if multiple outline definitions exist.
In cases where multiple Mechanical Layers exist, all with complete borders, the lowest numbered Mechanical Layer will be considered as the outline layer. For instance, if there are Mechanical 1, Mechanical 2, Mechanical 3, and Mechanical 4 layers, the elements from Mechanical 1 will be used for routing purposes, while data from Mechanical 2, Mechanical 3, and Mechanical 4 will be ignored.
FAQ about Mechanical Layer 1
Q: Will the 3D footprint lines drawn on Mechanical Layer 1 appear on the final manufactured PCB?
No. 3D footprint lines are for design reference and 3D modeling only. They will not be fabricated. JLCPCB treats them as non-manufacturing elements.
Q: Which Mechanical Layer should I use for the board outline?
It is strongly recommended to use Mechanical Layer 1 (GM1) as the primary board outline layer. JLCPCB prioritizes the lowest numbered Mechanical Layer when multiple outlines exist.
Q: What should I do if I have board borders on both KEEP-OUT layer and Mechanical Layer?
JLCPCB will prioritize the Mechanical Layer and ignore the KEEP-OUT layer data. For best results, keep only one complete outline on Mechanical Layer 1.
Q: How do I correctly define irregular slots or cutouts?
Draw the exact slot shape using closed contours on Mechanical Layer 1 (or the same layer as your board outline). For plated slots, also define them properly in the Drill files. Minimum plated slot width is 0.5mm.
Q: Can I place mounting holes (circles) on Mechanical Layer 2 instead of Layer 1?
Yes, but it is better to define all critical holes on Mechanical Layer 1 together with the outline. The actual holes must also be defined in the Drill layer for manufacturing.
Q: What happens if I have complete borders on multiple Mechanical Layers (e.g. Mech1, Mech2, Mech3)?
JLCPCB will only use the lowest numbered Mechanical Layer (Mechanical 1) as the board outline. Data from higher-numbered Mechanical Layers will be ignored for routing and panelization.
Conclusion
Understanding the role of the Mechanical Layer in PCB design is crucial for accurate component placement and slot recognition. By following the guidelines provided in this article and considering the example scenario, you can ensure their designs are optimized for manufacturing processes. Proper utilization of the Mechanical Layer, along with other relevant layers and adherence to JLCPCB's DFM guidelines, will result in high-quality PCBs that meet the desired specifications.
Keep Learning
Common Design Issues and Recommendations for PCB Optimized Design
To help customers avoid common issues that may arise during the PCB production process due to design problems, we' ve summarized the most frequent cases below. These issues have been detailed on our website to assist customers in identifying and addressing them more effectively. The following points include important design considerations and suggested modifications: 1. Missing Slots, Cutouts, Millings and V-Cut Issue: Missing Slots, Cutouts, Millings and V-Cut due to improper design. Recommendation: ......
How to Run a Design Rule Check (DRC) for Your PCBs
Any time you design a PCB, and you want to turn it into a real product, you will have to make sure the design obeys all the constraints within the standard PCB manufacturing process. These constraints in the PCB design are known as Design rules and to check these rules in a CAD software we have to run the DRC(Design Rule Check) algorithm. The ever-increasing complexity of boards has made it nearly impossible to carry out the design rule verification process manually, so designers have to program the r......
Thermal Vias in PCB Design for Heat Management
Thermal vias are specialized vias designed to transfer heat from one layer of a PCB to another. These vias are placed near heat-generating components to create a thermal pathway, helping to dissipate heat and reduce the risk of overheating. They are often used with heat sinks, thermal pads, or copper planes to enhance their effectiveness. They are simply plated through holes (PTHs) that are located under a surface-mounted heat source component in a printed circuit board (PCB) that allow heat transfer.......
The Ultimate Guide to PCB Panelization: Tools and Techniques
Printed circuit boards (PCBs) are the backbone of modern electronics. One critical aspect of PCB manufacturing is panelization — the process of arranging multiple PCBs onto a single larger panel for efficient manufacturing and assembly. This technique allows multiple boards to be processed simultaneously, significantly reducing costs and improving production efficiency. In this article, we will provide a comprehensive guide to PCB panelization, covering the tools and techniques required for successful......
PCB File Formats
Ordering printed circuit boards (PCBs) involves providing precise and detailed information about the design and specifications of the board. This is why specific PCB file formats are necessary. Manufacturing can only take place successfully with a completed PCB file. Designing a PCB and communicating those design decisions depends on files such as circuit schematic designs, Bill-of-Materials, PCB layouts, and stack-up design information. To ensure interoperability among various electronics design soft......
Using Via-in-Pad Technology: What You Need to Know, Design Guidelines, and More…
In the world of multi-layer PCB (Printed Circuit Board) design, vias are essential parts that connect different layers of a board. As electronic devices become more compact and complex, designers must employ advanced technologies to optimize board space and performance. One such technology is via-in-pad technology, which has become increasingly popular in high-density and high-performance PCB designs. This article explores the essentials of via-in-pad technology, including guidelines for its implement......