This website requires JavaScript.
Coupons
Ship to
Blog

FPC Soldering Methods: A Complete Guide to Techniques and Their Applications

Published Mar 26, 2025, updated Oct 19, 2026

3 min

Table of Contents
  • 1. Hot Press Soldering
  • 2. Reflow Soldering
  • 3. Wave Soldering
  • 4. Manual Soldering
  • Summary
JLCPCB flexible PCB prototype starting at $2 with $20 off

Flexible Printed Circuits (FPC) are extensively utilized in a variety of electronic devices because of their flexibility, lightweight design, and high-density attributes. FPC soldering is a critical process for connecting components to circuit boards, and the selection of soldering method directly impacts the performance and reliability of the circuit board. This article will examine four common FPC soldering techniques—hot pressing soldering, reflow soldering, wave soldering, and manual soldering—emphasizing their characteristics and optimal application scenarios.

1. Hot Press Soldering

Hot press soldering is a technique that employs heat and pressure to bond flexible printed circuits (FPCs) to solder joints. This method is commonly utilized in applications that demand high reliability and precise control.

Process: Conductive adhesive or solder is placed between the FPC and the solder joints. The assembly is then heated to a specific temperature and pressurized using a hot press machine. Once cooled, a reliable electrical connection is established.

Advantages: Ideal for small solder joints and fine-pitch components. It offers high reliability and stable electrical connections, making it ideal for mass production.

Applications: Liquid Crystal Display (LCD) modules, touch screen components, medical equipment connections.

2. Reflow Soldering

Reflow soldering involves heating solder paste until it melts, forming solder joints. This method is widely used in Surface Mount Technology (SMT).

Process: Solder paste is applied to the FPC’s pads, and components are placed onto the paste. The assembly is then heated in a reflow oven, causing the solder paste to melt, form joints, and solidify upon cooling.

Advantages: Highly efficient for mass production, with stable soldering quality. It is ideal for fine-pitch components and intricate designs.

Applications: Consumer electronics such as smartphones, tablets, automotive electronics, and communication equipment.

3. Wave Soldering

Wave soldering involves immersing the FPC in a wave of molten solder to create joints, typically used for through-hole components in double-sided or multi-layer circuit boards.

Process: Components are inserted into the FPC’s through-holes, and the assembly is passed through a wave soldering machine, where the molten solder forms joints. After cooling, the solder solidifies.

Advantages: Perfect for soldering through-hole components, offering high efficiency. It is ideal for applications requiring high power and reliability.

Applications: High-power modules, industrial control systems, communication base station equipment.

4. Manual Soldering

Manual soldering is conducted using a handheld soldering iron, making it ideal for small-batch production, prototyping, and equipment repair.

Process: A soldering iron is used to heat the solder joint, melting the solder and connecting component leads to the pads. After cooling, the solder solidifies, completing the connection.

Advantages: Offers high flexibility, requires no complex equipment, and is ideal for small-batch production and repairs.

Applications: Prototyping, small-batch production, electronic equipment repair.

Summary

FPC soldering methods vary, each offering distinct advantages and specific use cases. Hot press soldering is ideal for high-precision and high-reliability connections. Reflow soldering excels in mass production and is particularly effective for fine-pitch components. Wave soldering is well-suited for through-hole components, while manual soldering is essential for small-batch production and repairs. Selecting the appropriate soldering method based on the specific application can enhance FPC performance and improve the overall quality of electronic devices.

Keep Learning