Flexible Meets Durable: Understanding Rigid-Flex PCB Technology
7 min
- Rigid-Flex design
- The Evolution of Rigid Flex PCB Technology
- Rigid Flex PCB Types Based on Application
- Key Advantages of Rigid-Flex PCBs
- Design Considerations for Rigid-Flex PCBs
- The Manufacturing Process of Rigid-Flex PCBs
- What Are the Challenges in Designing Rigid-Flex?
- Conclusion
In the rapidly evolving world of electronics, the demand for smaller, more reliable, and more versatile devices continues to grow. To meet these demands, engineers and designers are increasingly turning to Rigid-Flex PCBs. The circuit boards combine rigid and flexible substrates into a single interconnected structure. This combination allows for complex designs that can bend and flex in specific areas while maintaining rigidity in others. To manufacture rigid flex PCBs, IPC offers advice and best practices. Technically speaking, rigid flex designs combine two or more conductive layers with flexible or rigid insulation in between them.
The rigid sections typically house components and provide structural support, while the flexible sections allow for bending and folding, enabling more compact and intricate designs. Most rigid flex boards consist of multiple layers of flexible circuit substrates attached to one or more rigid boards externally and/or internally, depending upon the design of the application. In this comprehensive guide, we’ll explore the fundamentals of Rigid-Flex PCBs, their benefits, design considerations, and typical applications.
Rigid-Flex design
The designs of Rigid-Flex PCBs are a little more complex as these boards are designed in 3D, which allows the board to be folded or twisted to create the desired shape for the product. This 3D flexibility enhances spatial efficiency, making them ideal for compact, weight-sensitive applications like medical equipment.
Rigid-Flex PCBs are usually thinner than other boards, meaning it’s a great option for any thin or light packaging needs your products may have. With thin copper layers and adhesive-less laminates, it is the best possible small, thin and light solution for your circuit design needs.
The Evolution of Rigid Flex PCB Technology
PCB technology has evolved significantly, with ongoing advancements addressing earlier limitations. Rigid PCBs were once widely used but had several drawbacks, such as the inability to bend, making them prone to breakage and unsuitable for compact devices. Rigid-Flex PCBs have solved many of these issues. While originally developed for spacecraft, they are now commonly used in electronics like smartphones and laptops. Rigid-Flex PCBs combine the benefits of rigid and flexible PCBs, offering both durability and flexibility. The flexible part is typically made of Polyimide (PI), while the rigid part uses FR4. Common designs include 4, 6, or 8 layers.
Rigid Flex PCB Types Based on Application
There are two main functional applications for rigid flex. These are static (flex-to-install) and dynamic (continuous flexing over the life of the product). The design and construction of the rigid flex will be dependent on whether the application is static or dynamic.
- Static Application: An application where the flex circuit is only required to flex during installation in order to fit it into its application (also known as flex-to-install).
- Dynamic Flexing Applications: An application where the flexible area is dynamically flexed during normal operation. This can range from a few hundred cycles up to over 1 million cycles.
Key Advantages of Rigid-Flex PCBs
Rigid-Flex PCBs offer several advantages over traditional rigid or flexible PCBs, making them an attractive choice for many applications, here are some main points:
1. Space and Weight Savings: By integrating rigid and flexible sections, Rigid-Flex PCBs eliminate the need for connectors, cables, and other interconnections, reducing the overall size and weight of the assembly.
Further Read: Rigid-Flex PCB Assembly: Design, Process, Quality & Cost
2. Enhanced Reliability: The elimination of connectors and solder joints in the flex areas reduces potential failure points, leading to improved reliability and longer product lifespans.
3. Three-Dimensional Design: Rigid-Flex PCBs can be designed to fit into three-dimensional spaces, allowing for more creative and efficient layouts. This capability is crucial in applications where space is at a premium.
4. Mechanical Strength: The rigid sections of Rigid-Flex PCBs provide the necessary mechanical support for components, while the flexible sections offer resistance to mechanical stress and vibration.
Design Considerations for Rigid-Flex PCBs
Designing Rigid-Flex PCBs requires careful consideration of several factors to ensure optimal performance and manufacturability:
Material Selection: Choose compatible materials like FR-4 for rigid sections and polyimide for flexible parts, ensuring they withstand operating conditions.
Layer Stack-Up: Ensure the right balance of electrical performance, mechanical strength, and flexibility when stacking rigid and flexible layers.
Bending and Flexing: Design flexible sections with appropriate bend radius and stress reduction techniques to prevent trace damage.
Component Placement: Position components on rigid sections to avoid stress on solder joints during flexing.
Trace Routing: Plan trace routing to handle bending and minimize stress, ensuring integrity.
Impedance Control: Maintain consistent impedance in high-speed designs through careful control of trace widths and spacing.
Manufacturability: Collaborate with manufacturers early to address complexities and ensure smooth production.
The Manufacturing Process of Rigid-Flex PCBs
The manufacturing process of Rigid-Flex PCBs is more intricate than that of traditional PCBs due to the combination of rigid and flexible materials. Here are the key steps involved:
- Material Preparation: Selection of material for Rigid and Flex section.
- Layer Lamination: layer bonding and adhesive application.
- Drilling and Plating: Stitching via's between different layers.
- Imaging and Etching: Pattern transferring and removing unwanted copper.
- Soldermask and Silkscreen: Color and Annotations.
- Final Testing and Inspection: For performance matching
For a detailed breakdown of the manufacturing process of Rigid-Flex designs, check out our comprehensive guide on PCB manufacturing.
What Are the Challenges in Designing Rigid-Flex?
Rigid-flex PCBs often have more complex design rules compared to rigid PCBs. These designs must address both the mechanical and electrical needs of rigid and flexible parts. Here are some main points including bend radii, layer stackup, and material constraints:
Bend Radius Importance: A key consideration in rigid-flex design is selecting an appropriate bend radius for flexible sections. If the radius is too small, it can lead to mechanical failures and impact signal quality.
Tear Drop Design with Flex: Tear drops can be added to make the through holes more stable and rigid. To know more about how to add teardrops to your design have a look on this EasyEDA tutorial page.
Signal Integrity and EMI: Maintaining signal integrity and controlling electromagnetic interference (EMI) in the flexible sections can be challenging. The flexibility of the substrate and the proximity of signals to the bend region can affect signal quality.
Round Corner Design: Make the corners round and a little bigger to avoid any corner tear of the PCB. Ensuring that the flexible sections can withstand repeated bending and flexing without mechanical failure is essential in designs.
Layer Transition: Properly transitioning signal layers from the rigid to the flexible sections can be challenging. Misalignment or improper layer transitions can result in impedance mismatches and signal degradation.
Conclusion
Rigid-Flex PCBs offer a powerful solution for modern electronic devices that require compact, reliable, and flexible circuit designs. By combining the strengths of both rigid and flexible PCBs, they enable innovative design possibilities across a wide range of industries. However, designing Rigid-Flex PCBs requires careful planning, material selection, and collaboration with manufacturers to ensure a successful outcome.
As technology continues to advance, the role of Rigid-Flex PCBs in electronic design will only grow, driving innovation in everything from consumer gadgets to critical aerospace systems. Whether you’re designing a new product or improving an existing one, understanding the intricacies of Rigid-Flex PCB design is key to staying ahead in the competitive world of electronics.
Popular Articles
Keep Learning
Medical Flex Circuits: Manufacturing, Applications, Materials, and Design Guide
Medical flex circuits made to fit inside a 1.0 mm disposable endoscope, wrap around a hearing aid shell, and sit on a patient's arm for ten straight days. When one fails, it is not a warranty return but a device history file and a regulatory conversation. In this guide, you will learn: What separates a medical flex circuit from a consumer one How they are built, tested, and released Polyimide, copper, coverlay, and stiffener choices Fine line, bend radius, and layer count limits What to check before c......
Flexible Meets Durable: Understanding Rigid-Flex PCB Technology
In the rapidly evolving world of electronics, the demand for smaller, more reliable, and more versatile devices continues to grow. To meet these demands, engineers and designers are increasingly turning to Rigid-Flex PCBs. The circuit boards combine rigid and flexible substrates into a single interconnected structure. This combination allows for complex designs that can bend and flex in specific areas while maintaining rigidity in others. To manufacture rigid flex PCBs, IPC offers advice and best prac......
PCB Stiffeners: An Essential Requirement for Flexible Circuits
A printed circuit board stiffener plays an important role when it comes to offering mechanical support to a PCB. They are particularly helpful for flexible circuit boards, that given their name, are flexible and in need of stiffness in certain places. Stiffeners are particularly required when components are placed in a flex zone & the weight of these components stresses the flex material. These components provide a rigid connection from the flexible portion to the solid board. This solidity makes appl......
Choosing the Right Bend Radius for Durable Flexible PCBs
Key Takeaways Mastering the bend radius is essential for reliable flexible PCB design. Following IPC-2223 guidelines, maintain a minimum of 6× total thickness for static bends and 100× for dynamic applications, while using thinner RA copper, adhesiveless polyimide, staggered traces, and cross-hatched patterns in flex zones. Proper material selection, layer stackup optimization, and adequate clearance from stiffeners can dramatically extend flex life and prevent premature trace cracking or delamination......
Flex PCB Cost: Complete Pricing Guide & Ways to Reduce Costs
Flex PCB cost is the number that stops most projects cold. You finish a clean polyimide design, upload the Gerbers, and the quote comes back at several times higher than what the same circuit would cost on FR4. Knowing which line items drive that number is what lets you bring it down. In this guide, you will learn: Real flex PCB price ranges for prototypes and production The factors that move an FPC quote the most How does the layer count and quantity change per-board price Why flex costs more than ri......
Flexible Circuit Connector: Types, Features & Selection Guide
A flexible circuit connector clamps onto the bare copper at the end of a flex circuit, so nothing is soldered at that joint. The tail slides into the housing, and an actuator presses a row of spring contacts onto the pads. Every connector is built around one tail thickness. TE's 0.5 mm pitch 2328702 family expects 0.30 mm (12 mil) of flex, because the contact beams are deflected by exactly that dimension. Figure 1: Cross-section of a 0.5 mm pitch FPC connector with the tail inserted Feed it a bare sin......