FPC Design Rules: 13 Safety Distances You Can’t Ignore
6 min
- 1. Solder Mask Design
- Outline Design
- Via Design
- Spacing Design
- Stiffener Design
In FPC (Flexible Printed Circuit Board) design, neglecting safety distances can lead to issues such as pad detachment or circuit short circuits. For example, insufficient solder mask bridge distance (less than 0.5mm) can cause it to break, pads placed too close to the edge (less than 0.2mm) may result in carbonization and short circuits, and improper via placement can lead to fractures. Precisely controlling these details is key to ensuring design reliability.
Some people believe that safety distances in FPC design don't need to be strictly followed, and approximate measurements are good enough. Others think that as long as the circuits work, the design is fine. But did you know? In FPC design, many seemingly insignificant safety distances, if overlooked, can lead to serious problems! Today, let’s take a closer look at those easily ignored safety distances in FPC design—how many do you know?
1. Solder Mask Design
Insufficient Solder Mask Bridge Distance
A solder mask bridge refers to the solder mask film between two pads. The distance between the pads should be at least 0.5mm to ensure the solder mask bridge doesn’t break. If the distance is too small, the solder mask bridge is prone to breaking.
Before After
Solder Mask Window to Copper Distance
The distance between the solder mask window and the copper should be greater than 0. solder mask window and the copper should be greater than 0.15mm. If the distance is too small, the solder mask may shift, causing copper exposure, which increases the risk of a short circuit.
Wrong Right
Solder Mask Window Length
The length of the solder mask window should generally not exceed 20mm, and large-area windows should be avoided. If the window is too large, the solder mask may deform during application, leading to poor fit or misalignment.
Wrong Right
Outline Design
Pad to Outline Distance
The pad must be at least 0.2mm away from the outline. Otherwise, during laser cutting, the pad may carbonize, causing a short circuit.
Via Design
1. Via to Edge Distance
The distance from the via edge to the center of the board outline should be at least 0.5mm, to prevent laser damage to the via during cutting, which may cause pad detachment. Additionally, vias should not be arranged in a straight line but should be staggered either horizontally or vertically.
2. Via to Window Distance
Vias should not be designed at the edge of a window and should maintain at least a 0.3mm distance from the solder mask’s edge. This area is where welding fingers are applied, and during welding, bending could concentrate stress at the junction of the uncovered and covered areas, which may cause copper at the hole to break.
Not recommend Recommend
Spacing Design
1. BGA Pad Diameter
The BGA pad diameter must be greater than or equal to 0.25mm. If it's smaller, the pad may be too small or may detach.
BGA pad diameter less than 0.25mm
2. Edge Pad Width
The width of edge pads should be at least 0.5mm. When placing orders, be sure to specify that pads should not be shaved. If not specified, JLCPCB will default to shaving 0.2mm off the pad’s edge, which could cause the pad to detach or lead to a cold solder joint.
Wrong Right
3. Trace or Copper Pour to Edge Distance
To prevent copper damage during the formation process, traces or copper pours should be at least 0.2mm away from the board edge. If the copper pour is flush with the edge of the board, it could lead to an open circuit during CAM processing.
4. Pad to Trace Distance
When the pad spacing is less than 0.5mm, avoid routing traces between pads. The minimum distance between a pad and a trace should be 0.20mm. It is recommended to route the traces from the back side or accept exposed traces.
The distance between IC pad and trace is only 0.1mm
Stiffener Design
1. Stiffener to Pad Distance
The stiffener area should be at least 1.0mm larger than the pad. If the distance is insufficient, bending can lead to fractures at the junction between the pad and the trace, causing an open circuit.
Wrong Right
2. Minimum Width of Stiffener
If the stiffener is too narrow, it may cause difficulty in fitting and could easily fracture.
FR4 stiffener is too narrow and more prone to breaking.
The minimum width for stiffener materials is as follows:
FR4 Stiffener: Minimum width 3mm;
PI Stiffener: Minimum width 2mm;
Stainless Steel Stiffener: Minimum width 3mm (1mm is possible with 2.5mm length).
3. EM Shielding Film to Pad Distance
EM Shielding Film are conductors, so the distance between the electromagnetic film and the pad window must be at least 0.8mm to avoid interference.
The safety distance data above is derived from JLCPCB’s experience in the FPC production process. Mastering these design details can effectively avoid common issues in the design and ensure the reliability and stability of FPCs.
Popular Articles
Keep Learning
Medical Flex Circuits: Manufacturing, Applications, Materials, and Design Guide
Medical flex circuits made to fit inside a 1.0 mm disposable endoscope, wrap around a hearing aid shell, and sit on a patient's arm for ten straight days. When one fails, it is not a warranty return but a device history file and a regulatory conversation. In this guide, you will learn: What separates a medical flex circuit from a consumer one How they are built, tested, and released Polyimide, copper, coverlay, and stiffener choices Fine line, bend radius, and layer count limits What to check before c......
Flexible Meets Durable: Understanding Rigid-Flex PCB Technology
In the rapidly evolving world of electronics, the demand for smaller, more reliable, and more versatile devices continues to grow. To meet these demands, engineers and designers are increasingly turning to Rigid-Flex PCBs. The circuit boards combine rigid and flexible substrates into a single interconnected structure. This combination allows for complex designs that can bend and flex in specific areas while maintaining rigidity in others. To manufacture rigid flex PCBs, IPC offers advice and best prac......
PCB Stiffeners: An Essential Requirement for Flexible Circuits
A printed circuit board stiffener plays an important role when it comes to offering mechanical support to a PCB. They are particularly helpful for flexible circuit boards, that given their name, are flexible and in need of stiffness in certain places. Stiffeners are particularly required when components are placed in a flex zone & the weight of these components stresses the flex material. These components provide a rigid connection from the flexible portion to the solid board. This solidity makes appl......
Choosing the Right Bend Radius for Durable Flexible PCBs
Key Takeaways Mastering the bend radius is essential for reliable flexible PCB design. Following IPC-2223 guidelines, maintain a minimum of 6× total thickness for static bends and 100× for dynamic applications, while using thinner RA copper, adhesiveless polyimide, staggered traces, and cross-hatched patterns in flex zones. Proper material selection, layer stackup optimization, and adequate clearance from stiffeners can dramatically extend flex life and prevent premature trace cracking or delamination......
Flex PCB Cost: Complete Pricing Guide & Ways to Reduce Costs
Flex PCB cost is the number that stops most projects cold. You finish a clean polyimide design, upload the Gerbers, and the quote comes back at several times higher than what the same circuit would cost on FR4. Knowing which line items drive that number is what lets you bring it down. In this guide, you will learn: Real flex PCB price ranges for prototypes and production The factors that move an FPC quote the most How does the layer count and quantity change per-board price Why flex costs more than ri......
Flexible Circuit Connector: Types, Features & Selection Guide
A flexible circuit connector clamps onto the bare copper at the end of a flex circuit, so nothing is soldered at that joint. The tail slides into the housing, and an actuator presses a row of spring contacts onto the pads. Every connector is built around one tail thickness. TE's 0.5 mm pitch 2328702 family expects 0.30 mm (12 mil) of flex, because the contact beams are deflected by exactly that dimension. Figure 1: Cross-section of a 0.5 mm pitch FPC connector with the tail inserted Feed it a bare sin......