45 Must-Know Flex PCB Design Tips You Can't Afford to Miss!
8 min
- Outline and Drilling
- Copper Surface and Solder Pad Design
- Gold Fingers and Soldering
- Connector Pads and IC Design
- Silkscreen and Text Design
- Panelization Design
- Reinforcement Design
- Board Thickness
Achieving perfection in product design requires a careful balance between meeting design requirements and manufacturing standards. However, when it comes to flex PCB (FPC) design, many engineers find themselves at a loss, unsure of where to begin.
In this insightful guide, we will delve into 45 essential design guidelines for FPC. By the end, you'll have the knowledge and confidence to navigate the complexities of flex PCB design.
Outline and Drilling
1. The minimum distance from through-holes to the board frame should be 0.5mm. If less than 0.5mm, change to U-shaped holes (slots open towards the board frame).
2. Ensure via holes are at least 0.2mm away from the solder mask window to prevent exposed copper around the hole edges.
3. Avoid designing vias in pads in FPC, as unlike rigid PCBs, FPC cannot do resin plugging for such holes, leading to solder wicking.
Copper Surface and Solder Pad Design
4. Large Copper Surface Oxidation: Large copper areas can trap air during coverlay application, leading to oxidation in high temperature and pressure, affecting appearance but not function. To avoid this, design hatched copper or add solder mask windows on large copper surfaces.
5. Avoid Independent Pads: Independent pads, especially those overlapping on both sides, can easily detach since the FPC core is only 25μm thick. It’s recommended to add copper reinforcement around the pad and connect pad corners to the copper area, and offset pads on opposite sides for better adhesion.
6. Pad Detachment: Connector pads are prone to detachment. Design soldermask defined pads to prevent this, as the soldermask coverage on the pad’s rim provides mechanical strength.
7. Avoid Large Exposed Copper Areas: This can lead to wrinkling.
8. Coverlay Requirements: For flexible boards, coverlay acts as the solder mask. It needs to be pre-windowed before application. Ensure a 0.2mm gap between pads and adjacent traces, and a 0.5mm spacing between pads. Otherwise, bridged apertures should be used, accepting exposed traces.
9. Prevent Tearing at Corners: Sparse routing can cause tearing at board corners. Add anti-tear copper strips at the edges or add hatched copper on the back.
10. Grid Pattern Routing: Use a 45-degree angle for the grid pattern to improve signal transmission. Line width and spacing should be 0.2/0.2mm.
Gold Fingers and Soldering
11. Gold Fingers: Shrink gold fingers by 0.2mm to avoid micro-shorts caused by carbonization from laser cutting. (JLCPCB will do this by default; special requirements should be mentioned.)
12. Vias on Solder Pads: Avoid placing vias in a straight line on solder pads to prevent stress concentration and potential cracking.
13. Coverlay Offset: Ensure a 0.3mm offset for the coverlay on either side of gold fingers to prevent breakage.
14. Soldermask Defined Pads: Design solder pads with extended coverlay to ensure the coverlay overlaps the pad by more than 0.3mm.
15. Gold Finger Solder Mask Windows: Ensure windows overlap pads by more than 0.3mm to prevent disconnection at the joint.
16. Hollow Boards: JLCPCB currently does not support hollow boards. Reverse-side gold fingers need additional pads and vias for layer transitions.
17. Extra Copper on Pads: Avoid extra copper on IC pads, as this can enlarge pads and reduce spacing, leading to shorts during soldering.
18. Independent Gold Finger Pads: Design gold finger pads as independent pads. If there’s copper or traces overlapping the gold fingers, solder mask windows will expose the copper or traces.
19. Gold Finger Tolerance: Default tolerance is +/-0.1mm. If +/-0.05mm is required, specify when ordering.
Connector Pads and IC Design
20. Connector Pads: Connector pads in FPCs are prone to detachment. Design with soldermask defined pads to provide mechanical strength.
21. IC Bridges: Include coverlay bridges in the middle of ICs to retain the solder mask.
22. Gold Finger Solder Mask Windows: Gold finger pads must have solder mask windows to enable connection with the connector.
23. Default Solder Mask: Ensure the correct solder mask layer is used as the default.
24. Via Covering: To prevent cracking of via copper during bending, vias in FPCs are usually tented by default. Specify when ordering if coverlay windows are required.
25. Test Points: Do not attribute test points as vias, or separately add a window for test points.
26. Exposed Copper Edges: Large exposed copper areas on double-sided boards can blacken board edges. Add a coverlay ring around the edges.
Silkscreen and Text Design
27. If you need legend or silkscreen on the reinforcement, make sure to specify this when ordering to prevent process errors.
28. Avoid placing annotation text inside the board area or on the same layers as the rest of the design, as this could lead to unfortunate outcomes.
Panelization Design
29. For steel-reinforced boards, maintain a minimum distance of 3 mm between boards and a slot width of 0.5 mm, with connection points of 1 mm width spaced approximately every 15 mm. When ordering, specify paper to be placed between each PCB and sandwich between cardboard.
30. Avoid placing connection points on the same board edge as gold fingers, as this can cause unevenness at the front of the gold fingers.
31. Ensure there are enough connection points; each PCB should have at least two connection points of 0.8 mm width. The number of connection points should increase with the board size.
32. If the board is very small and has too many connection points, it can be hard to separate. If not for SMT, small PCBs need only two 0.3 mm connection points for easy manual separation.
33. Low utilization in panelization can lead to high costs (example below). Aim for a panel width of 119 mm or 240/250 mm, and consider choosing third-party panelization.
34. For very small boards less than 20 × 20 mm, panelize them to prevent the boards from being sucked away during laser dust collection. You can either deliver them as a panel or have JLCPCB help with the separation.
Reinforcement Design
Reinforcement involves adding rigid materials to specific areas of the FPC for easier assembly. PI reinforcement is suitable for products with gold finger insertion; FR4 is used for lower-end products; steel reinforcement is ideal for products requiring chip mounting due to its flatness and resistance to deformation.
35. Avoid using steel reinforcement over exposed pads as it may cause shorts. Additionally, steel has weak magnetism, making it unsuitable near Hall sensors. Steel reinforcement is also not recommended for gold finger areas.
36. Specify the total thickness requirement for gold finger insertion when ordering. The total thickness is usually in the connector specification sheet. Use JLCPCB's gold finger PI thickness calculator to determine the correct PI reinforcement thickness.
37. Reinforcement Cutouts: Design the reinforcement to avoid covering components or pads. Ideally, the customer should design this. If no cutouts are designed by the customer, JLCPCB defaults to cutouts for pads with a clearance of 0.3 mm. Any remaining reinforcement with width less than 2 mm will be removed, unless special requirements are specified in the order notes.
38. The reinforcement for gold fingers should extend at least 1.0 mm beyond the pad to prevent breakage during use.
39. Double-sided EMI films are electrically connected on both sides and cannot be separated. Consider removing EMI films if this is not acceptable for your design.
40. If a specific impedance to ground is required for the EMI film, design a soldermask opening over the ground trace/plane as the connection point to the film. Without specific requirements, JLCPCB defaults to adding a 1.0 mm solder mask window in a random location. Note: An ungrounded electromagnetic film may absorb significant electromagnetic waves, potentially causing signal issues, so verify with a prototype first.
41. Steel reinforcement on pads can cause shorts.
42. Reinforcement Width: FR4 reinforcement width less than 5 mm is prone to breaking and carbonization. Switch to PI or steel reinforcement. The minimum width for adhesive should be at least 3 mm.
43. Do not place reinforcement or adhesive near SMT pads, as it can interfere with stencil printing. If necessary, reinforcement or adhesive can be added after SMT.
Board Thickness
44. The selected board thickness includes coverlay, copper thickness, and PI board material thickness. If the board has non-copper areas or no coverlay, the thickness will be reduced accordingly. Pay special attention to this in your design.
45. FPC impedance calculations using simulation software can be inaccurate. JLCPCB’s empirical experience for designing line widths is available for reference, but always validate with a prototype first. This parameter applies to double-sided boards with 0.11 mm thickness.

1. Recommended line width/spacing for hatched copper: 200 μm.
2. Grounding points (coverlay opening over ground place) are recommended on both sides when using EMI films. Recommended size: 1 × 1 mm.
3. The ground planes on both sides should be electrically connected by vias.
Note: All parameters above are based on the 0.11 mm 2-layer FPC stack-up.
JLCPCB’s design guidelines cover potential manufacturing issues, helping engineers identify manufacturability problems before production. This ensures various scenarios are met, minimizing design iterations and reducing costs!
Keep Learning
Choosing the Right Bend Radius for Durable Flexible PCBs
Key Takeaways Mastering the bend radius is essential for reliable flexible PCB design. Following IPC-2223 guidelines, maintain a minimum of 6× total thickness for static bends and 100× for dynamic applications, while using thinner RA copper, adhesiveless polyimide, staggered traces, and cross-hatched patterns in flex zones. Proper material selection, layer stackup optimization, and adequate clearance from stiffeners can dramatically extend flex life and prevent premature trace cracking or delamination......
Flex PCB Cost: Complete Pricing Guide & Ways to Reduce Costs
Flex PCB cost is the number that stops most projects cold. You finish a clean polyimide design, upload the Gerbers, and the quote comes back at several times higher than what the same circuit would cost on FR4. Knowing which line items drive that number is what lets you bring it down. In this guide, you will learn: Real flex PCB price ranges for prototypes and production The factors that move an FPC quote the most How does the layer count and quantity change per-board price Why flex costs more than ri......
Flexible Circuit Connector: Types, Features & Selection Guide
A flexible circuit connector clamps onto the bare copper at the end of a flex circuit, so nothing is soldered at that joint. The tail slides into the housing, and an actuator presses a row of spring contacts onto the pads. Every connector is built around one tail thickness. TE's 0.5 mm pitch 2328702 family expects 0.30 mm (12 mil) of flex, because the contact beams are deflected by exactly that dimension. Figure 1: Cross-section of a 0.5 mm pitch FPC connector with the tail inserted Feed it a bare sin......
Polyimide Flex PCB: A Complete Guide for Engineers
A polyimide flex PCB can be folded about 285,000 times when the base film is 25 µm (1 mil) thick. Make that film 75 µm (3 mil), and the same MIT fold test gives up near 6,000 cycles. Bending is a strain problem, not a material problem. Copper sits above the center of the stack, so a bend forces it to stretch around the longer outer path. Figure 1: A polyimide flex circuit folded tight, with a stiffener holding the connector A thicker stack places the copper farther out, resulting in more stretch at th......
Flex PCB Bend Radius: Calculation, Minimum Radius & Design Guidelines
Flex PCB bend radius is the one dimension on an FPC that no design rule check will catch. Bend the circuit tighter than its material allows; the outer copper stretches from its elongation limit, and then it cracks. Figure 1: A flex circuit formed around a mandrel, with bend radius and stack thickness A flex circuit bends around a neutral axis near the middle of its stack. Copper below that line is squeezed, and copper above it is pulled. So the further a layer sits from the line, the harder it is to w......
FPC vs FFC: Understanding the Key Differences Between Flexible Circuit Technologies
The FPC vs FFC decision is really a question about how the copper was made. An FFC consists of flat copper strips laminated between two PET films. Every conductor runs straight from end to end at one fixed pitch, because nothing in that process can make a trace turn or branch. An FPC starts as copper-clad polyimide and is etched exactly like a rigid board. Traces can turn, taper, split onto a second layer, and land under a soldered component. The finished circuit can be as thin as 0.1 mm (4 mil). Figu......