Flex PCB Manufacturing Process: From Prototyping To Mass Production
7 min
- Application of Flex PCBs:
- Manufacturing Steps Of Flex PCBs :
- Detailed Manufacturing Process
- Transition to Mass Production :
- FAQ about Flex PCB Manufacturing
- Conclusion :
Flexible Printed Circuit Board commonly known as flex PCBs are a revolutionary step in modern electronics that offer compact, lightweight, dynamic and precise designs. Flex PCBs are designed to bend, twist, and fold, which rigid boards are incapable of. These characteristics have led to their widespread adoption in industries like wearable technology to consumer electronics to aerospace and medical technologies.
With demands increasing day by day for miniaturized and ergonomic product designs, understanding the process of a flex PCB from its prototyping phase to mass production has become a must. In this article the journey of a flex PCB from prototype to mass production will be covered.
Application of Flex PCBs:
The rise of flex PCBs is because of their versatility. They're mostly used in -
● Medical Devices: Pacemaker, Cochlear implants and Wearable diagnostics.
● Consumer Electronics: Smartphones, Foldable Screens and Fitness bands and so on.
● Automotive Systems : Airbag Controllers, Dashboard interfaces and sensors.
● Aerospace: Satellite, Avionics and high reliability communication systems.
Manufacturing Steps Of Flex PCBs :
Flex PCB manufacturing is almost similar to the traditional PCB manufacturing process but here the use of specialized materials and procedures are needed to ensure flexibility, durability and quality control. Here are the steps to do this right-
Flex PCB Core Capability Parameters:
| Process Item | JLCPCB Standard Capability |
|---|---|
| Layer Count | 1-Layer / 2-Layer |
| Base Material | Polyimide (PI) |
| Base PI Thickness | 12.5um / 25um |
| Finished Thickness | 0.07mm / 0.11mm / 0.12mm / 0.20mm |
| Copper Weight | 1/3 oz (12um) / 0.5 oz (18um) / 1 oz (35um) |
| Min Trace Width/Spacing | 0.075mm / 0.075mm |
| Surface Finish | Electroless Nickel Immersion Gold (ENIG - Default) |
| Coverlay Color | Yellow / Black / White |
| Stiffener Material | Polyimide (PI) / FR4 / Stainless Steel |
| Min Drilling Hole Size | Mechanical Drilling: 0.2mm / Laser Drilling: 0.1mm |
1. Material Selection: The most suitable base substrate is Polyimide. It is chosen because of its top notch thermal stability and amazing flexibility. It is actually copper-clad on one or both sides, depending on requirements.
2. Cleaning and Preparation : The copper-clad polyimide is thoroughly cleaned to remove oxidation and contaminants before proceeding to the next step.
3. Photo Imaging and Patterning : The Copper surface is laminated with a Photoresist . A UV light source projects the circuit pattern into a photomask which hardens the exposed areas.
4. Etching and Stripping : The unwanted copper is etched away, and the remaining photoresist is stripped, leaving only the designed circuit traces.
5. Drilling and Plating : In multilayer designs precise drilling is performed then the vias are plated with copper to create electrical connection between layers.
6. Coverlay Application : Here a coverlay made of Polyimide and adhesive is applied to protect the circuit. It's laminated and cured to bond securely with substrate.
7. Surface Finish: Immersion Silver or OSP or ENIG surface finish is applied to prepare the pads for soldering this also protects the exposed copper from oxidation.
8. Laser or Die Cutting : The board outline is cut using laser for precision.
9. Electrical Testing : Automated test equipment ensures that all traces and vias are correctly placed and checks for violations.
10. Inspection and Quality Control : The board now undergoes flex testing and visual inspection according to industry standards.
Detailed Manufacturing Process
Material Cutting & Pre-treatment
The production begins with cutting advanced roll-based flexible copper-clad laminates (FCCL), typically consisting of polyimide film base bonded with copper foil (0.5 oz or 1 oz). JLCPCB uses adhesive-less base materials to ensure thinner profiles and superior thermal stability during lead-free soldering.
CNC Drilling & Automated Copper Plating
Micro-vias are drilled using high-speed mechanical CNC drilling machines operating at up to 200,000 RPM, or advanced UV lasers for high-density interconnect (HDI) designs. To establish electrical continuity between layers, specialized roll-to-roll or vertical conveyorized plating systems deposit a uniform layer of copper inside the drilled vias.
Photolithography & Etching
A photosensitive dry film (photoresist) is laminated onto the cleaned copper surfaces under heat and pressure. Using Laser Direct Imaging (LDI) technology, the precise circuit pattern is digitally exposed via UV light, hardening the trace areas. The unexposed film is developed away, and the board passes through a high-precision acid etching chemical line to remove unwanted copper, perfectly forming traces down to 0.05mm/0.05mm width/spacing.
Coverlay Alignment & Vacuum Lamination
Unlike rigid PCBs that use liquid photoimageable solder mask, flex PCBs require a solid coverlay (a combination of polyimide film and thermo-setting acrylic adhesive) to protect the delicate copper traces from oxidation and dynamic bending fatigue. Openings for SMT pads are pre-cut via CNC laser, aligned precisely over the circuit, and bonded using high-temperature industrial vacuum presses to eliminate air traps.
Surface Finish & Stiffener Application
Electroless Nickel Immersion Gold (ENIG) is applied as the standard surface finish at JLCPCB. This provides a perfectly flat surface for fine-pitch SMT components and excellent shelf life. Following this, FR4, PI, or Aluminum stiffeners are precisely bonded to the designated areas (such as underneath ZIF connectors or heavy components) using thermosetting or pressure-sensitive tape to provide localized rigidity.
Laser Contour Cutting & 100% Electrical Test
Individual boards are profiled out of the panels using precise UV Laser Cutting machines, which prevent any mechanical stress or delamination at the flexible edges. Finally, 100% Flying Probe or dedicated fixture Electronic Testing is executed alongside Automated Optical Inspection (AOI) to guarantee zero open or short circuit defects before shipping.
Transition to Mass Production :
Once the prototypes are done and pass all performance and durability tests the product then goes into mass production.
Steps in Mass Production :
1. Design Freeze: Lock in all specifics after rigorous testing and stakeholder approval.
2. Tooling Setup: Create precise stencils for high speed fabrication and assembly.
3. Process Optimization: Fine tune lamination, drilling and plating processes for volume efficiency.
4. Quality Control Scaling: Implement in line testing and automated visual inspection.
5. Planning: Coordinate supply of polyimide, adhesive and finishes.
FAQ about Flex PCB Manufacturing
Q: What is the main difference between the materials used in rigid PCBs and Flex PCBs?
Rigid PCBs primarily use FR4 (fiberglass and epoxy resin) as the rigid substrate. In contrast, Flex PCBs use Polyimide (PI) as the base material, which provides excellent thermal stability, electrical insulation, and the ability to bend and twist dynamically.
Q: Does JLCPCB use adhesive or adhesive-less base materials for FPC production?
JLCPCB utilizes premium adhesive-less base materials (FCCL) for flexible PCBs. This ensures a thinner overall profile, superior flexibility, and better thermal stability to prevent delamination during high-temperature lead-free reflow soldering.
Q: What coverlay options and colors are available at JLCPCB?
Coverlay serves as the flexible equivalent of a rigid board's solder mask. JLCPCB offers standard solid polyimide coverlays in three colors: Yellow (standard), Black, and White, protecting the underlying copper traces from oxidation and dynamic bending fatigue.
Q:Why are stiffeners added to flexible PCBs, and what types does JLCPCB support?
Stiffeners are added to provide localized rigidity in areas that require mechanical strength, such as underneath heavy SMT components or ZIF connectors. JLCPCB supports three primary stiffener materials: Polyimide (PI), FR4, and Stainless Steel.
Q: What are the minimum trace width and drilling hole limits for JLCPCB's Flex PCB process?
To ensure excellent manufacturing yield and stability, JLCPCB's flexible PCB process supports a minimum trace width and spacing of 0.075mm / 0.075mm, and a minimum mechanical drilling hole size of 0.2mm.
Conclusion :
Flex PCBs are an indispensable part of modern electronics enabling innovation across diverse sectors. Their ability to combine flexibility, durability and compact design unlocks new possibilities for product engineers and system designers.
From the initial stages of design and prototyping to the demands of high volume manufacturing each step of the flex PCB process requires precision, expertise and careful coordination. By understanding the intricacies of the flex PCB manufacturing process, organizations can harness the full potential of this powerful technology and bring next generation products to life faster, smaller and smarter than ever before.
Keep Learning
Flex PCB Cost: Complete Pricing Guide & Ways to Reduce Costs
Flex PCB cost is the number that stops most projects cold. You finish a clean polyimide design, upload the Gerbers, and the quote comes back at several times higher than what the same circuit would cost on FR4. Knowing which line items drive that number is what lets you bring it down. In this guide, you will learn: Real flex PCB price ranges for prototypes and production The factors that move an FPC quote the most How does the layer count and quantity change per-board price Why flex costs more than ri......
Flexible Circuit Connector: Types, Features & Selection Guide
A flexible circuit connector clamps onto the bare copper at the end of a flex circuit, so nothing is soldered at that joint. The tail slides into the housing, and an actuator presses a row of spring contacts onto the pads. Every connector is built around one tail thickness. TE's 0.5 mm pitch 2328702 family expects 0.30 mm (12 mil) of flex, because the contact beams are deflected by exactly that dimension. Figure 1: Cross-section of a 0.5 mm pitch FPC connector with the tail inserted Feed it a bare sin......
Polyimide Flex PCB: A Complete Guide for Engineers
A polyimide flex PCB can be folded about 285,000 times when the base film is 25 µm (1 mil) thick. Make that film 75 µm (3 mil), and the same MIT fold test gives up near 6,000 cycles. Bending is a strain problem, not a material problem. Copper sits above the center of the stack, so a bend forces it to stretch around the longer outer path. Figure 1: A polyimide flex circuit folded tight, with a stiffener holding the connector A thicker stack places the copper farther out, resulting in more stretch at th......
Flex PCB Bend Radius: Calculation, Minimum Radius & Design Guidelines
Flex PCB bend radius is the one dimension on an FPC that no design rule check will catch. Bend the circuit tighter than its material allows; the outer copper stretches from its elongation limit, and then it cracks. Figure 1: A flex circuit formed around a mandrel, with bend radius and stack thickness A flex circuit bends around a neutral axis near the middle of its stack. Copper below that line is squeezed, and copper above it is pulled. So the further a layer sits from the line, the harder it is to w......
FPC vs FFC: Understanding the Key Differences Between Flexible Circuit Technologies
The FPC vs FFC decision is really a question about how the copper was made. An FFC consists of flat copper strips laminated between two PET films. Every conductor runs straight from end to end at one fixed pitch, because nothing in that process can make a trace turn or branch. An FPC starts as copper-clad polyimide and is etched exactly like a rigid board. Traces can turn, taper, split onto a second layer, and land under a soldered component. The finished circuit can be as thin as 0.1 mm (4 mil). Figu......
Flex PCB Stackup Design Guide: Layers, Materials & Reliability
Key Takeaways A reliable flex PCB starts with the right stackup design. The layer structure, material selection, and copper arrangement directly affect flexibility, bend life, electrical performance, and manufacturing reliability. This guide explains single-sided, double-sided, and multilayer flex PCB stackups, including polyimide materials, coverlay, copper types, and key design considerations for creating durable flexible circuits with JLCPCB. Did you ever wonder how a foldable phone can last for 20......