A Complete Guide to IC Package: Types, Properties, PCB Design Rules & Selection Tips
9 min
- What is an IC Package?
- IC Package Types and Typical Dimensions
- What Information Does an IC Package Define?
- Key International Standards for IC Package, Schematic Symbols, and 3D Models
- PCB Design Rules for IC Packages
- How to Choose the Right IC Package
- FAQ
What is an IC Package?
An IC package is the physical enclosure that houses an integrated circuit or electronic component, providing mechanical protection, electrical connections, and thermal management. It ensures that the component can be reliably mounted on a PCB and integrated into circuits.
Key Functions of an IC Package:
IC Package Types and Typical Dimensions
IC packages are categorized based on their mounting style, pin configuration, and physical form factor. Each package type follows standardized dimensions and footprints, which are critical for PCB layout and assembly.
Below are some of the most commonly used IC package types along with their typical dimensions:
SMT Packages
QFP (Quad Flat Package)
QFP (Quad Flat Package) is a larger PCB footprint commonly used for ICs and integrated circuits. Common sizes include 7x7mm, 10x10mm, 14x14mm, etc., and the number of pins ranges from dozens to hundreds.
BGA(Ball Grid Array)
BGA packages typically have spherical pads, with a package pitch generally ranging from 0.75mm to 1.0mm, and the number of pins can vary from dozens to hundreds.
Features: BGA packaging is suitable for high-performance chips and large-scale integrated circuits, offering good heat dissipation and electrical performance.
SOIC (Small Outline Integrated Circuit)
SOIC (Small Outline Integrated Circuit) is a common type of integrated circuit packaging. It has a compact shape and a small pitch pin layout, making it suitable for packaging medium-sized integrated circuits. The sizes are usually 3x3mm, 5x5mm, 7x7mm, etc., and the number of pins generally ranges from 8 to 48.
Plug-in Package (THT) - Through-hole Technology Package
DIP (Dual Inline Package)
The common size is 7.62mm (0.3 inches) pitch, and the number of pins ranges from 8 to hundreds.
TO-220 Package
TO-220 packages are typically used for power devices. They are approximately 10x15mm in size and have three pins.
TO-92 Package
The dimensions are approximately 5x5mm, with a pin count of 3.
Legacy or Specialty Packages
COB (Chip on Board) Package
The chip is directly mounted on the PCB. The package size is typically very small and is commonly used in compact equipment and products with high integration requirements.
PLCC (Plastic Leaded Chip Carrier)
PLCC (Plastic Leaded Chip Carrier) is typically used for highly integrated digital circuits. The package size is approximately 20x20mm, and the number of pins usually ranges from 20 to 84.
What Information Does an IC Package Define?
- Package type: Indicate the package type of the component, such as QFP, BGA, SMD, etc.
- Package size: Describes the overall dimensions of the package, usually expressed in terms of length, width, and height.
- Pin layout refers to the arrangement of pins in a pin package, which can be single row, double row, grid, etc.
- Pin Count: This term refers to the number of pins in the package, which dictates the function of the component and the number of interfaces.
- Material Type: The packaging material type, such as plastic, ceramic, etc., influences the mechanical strength, heat resistance, and other characteristics of the package.
- Pad Information: Describes the location, shape, and size of solder pins to ensure proper solder connections.
- Thermal management involves designing and setting parameters for heat dissipation structures for high-power components to ensure they operate within the normal temperature range.
- Package Identification: The package may contain the manufacturer's logo, model number, date code, and other information for traceability and identification.
- Pin function: For complex packages, a functional description of the pin may be included to guide correct circuit connections.
- Environmental adaptability: This refers to the package's ability to adapt to different environments, including being waterproof, dustproof, and other characteristics.
This information is crucial for designing and producing PCB boards to ensure that components are correctly integrated into the circuit, meeting design requirements and performance specifications.
Key International Standards for IC Package, Schematic Symbols, and 3D Models
For IC packaging, there are specific internationally applicable standards that define packages, schematic symbols, and 3D models.
1. IPC-7351 — PCB Land Pattern / Footprint Standard
The IPC-7351 standard defines recommended land patterns, pad geometry, and pin layouts for SMD components, enabling PCB designers to create manufacturable and assembly-ready footprints efficiently.
2. ANSI Y32.2-1975 — Schematic Symbols
The standard defines symbols for various electrical and electronic components, such as resistors, capacitors, inductors, diodes, transistors, operational switches, power supplies, sensors, connectors, etc. Each component symbol has a unique shape and identification that is utilized to represent the component's type and function in the schematic.
3. ISO 10303-21 — STEP File Format for 3D Models
The ISO 10303-21 standard defines the file format used for STEP models that can be imported into 3D CAD software. The standard is more of a file format specification than a requirement for encapsulating drawing components.
PCB Design Rules for IC Packages
- Package size: It is important to ensure that the size and shape of the package meet the component specifications to avoid being either too large or too small. Incorrect sizing may lead to installation difficulties or electrical problems.
- Pin arrangement: Pay attention to the arrangement of the pins. Avoid overlapping or placing them too densely. Ensure there is sufficient spacing between pins for soldering.
- Pad design: It is important to determine the correct pad size and shape, taking into account welding quality and reliability, and to avoid poor welding caused by excessive or insufficient welding.
- Thermal Heat Dissipation: Design suitable heat dissipation structures for components requiring heat dissipation to maintain the components' operating temperature within a safe range.
- Symbol marking: Design an accurate symbolic representation of the package in the schematic diagram to aid identification and comprehension by designers and maintenance personnel.
- 3D Model: This feature offers a 3D representation of the package following IPC standards to assist with PCB layout and collision detection.
- Prohibited Areas: Ensure there are sufficient prohibited areas designated during the package design process to prevent collisions with other components or packages.
- Manufacturability Considerations: It is important to consider limitations in the PCB manufacturing and assembly process during the design phase to ensure that the design aligns with actual production requirements.
How to Choose the Right IC Package
1. Different IC Packaging Types
Surface Mount Technology (SMT) packaging is suitable for small electronic products like smartphones, tablets, etc.
Plug-in packaging is suitable for applications that require larger electrical and mechanical connections, such as industrial control systems and automotive electronics.
System-in-Package (SiP) packaging integrates multiple functional modules into one package to provide higher integration and performance.
Ball Grid Array (BGA) package features a high-density solder ball array designed for high-performance and high-power applications.
2. Determine functional and performance requirements
Signal integrity is crucial. It is important to consider the quality and stability of signal transmission when selecting a packaging type that can meet the signal requirements. For high-frequency or high-speed signals, it is essential to select a package with excellent signal integrity.
Size restrictions: Choose the suitable package size according to the space limitations of the PCB and the needs of the assembly process. Ensure that the package size matches the PCB layout to prevent installation issues resulting from a size mismatch.
3. Consider cooling and thermal management
For integrated circuits (ICs) that need to handle high power, heat dissipation and thermal management are crucial considerations. Choosing a package with a good heat dissipation design, such as one with heat dissipation pins or a heat sink plate, can effectively dissipate heat and prevent the integrated circuit (IC) from overheating.
4. Consider layout and routing
The layout and pinout of the package are critical for the performance and reliability of the circuit. Make sure the package you choose matches your PCB layout to ensure good signal integrity and electrical connections.
5. Cost and Supply Chain Availability
Finally, consider the cost and availability of the supply chain. Some packaging types may be more expensive or have tighter supply chains than others. Therefore, consider the cost versus performance and ensure that the packaging you select can meet your project requirements and timelines.
Further reading: How to Choose the Right SMD Resistor: A Beginner's Guide
FAQ
Q: What is the difference between SMT and THT IC packages?
The main difference between SMT (Surface Mount Technology) and THT (Through-Hole Technology) IC packages is how they are mounted on a PCB. SMT components are soldered directly onto the PCB surface, while THT components use leads inserted into drilled holes for stronger mechanical connections.
- SMT: Smaller size, higher density, automated assembly
- THT: Stronger mechanical bonding, better for high-power applications
Q: Why is BGA packaging used for high-performance chips?
BGA (Ball Grid Array) packaging is preferred for high-performance ICs because it supports a higher pin count in a compact footprint and improves both thermal and electrical performance.
Key Benefits:
- Shorter signal paths → better signal integrity
- Lower inductance → suitable for high-speed designs
- Efficient heat dissipation via solder ball array
Q: What standards define IC package footprints and symbols?
IC package footprints and symbols are defined by international standards to ensure compatibility and manufacturability.
Key Standards:
- IPC-7351: PCB footprint and land pattern design
- ANSI Y32.2: Schematic symbols
- ISO 10303-21: STEP format for 3D models
Q: Does IC packaging affect signal integrity?
Yes, IC packaging significantly affects signal integrity due to parasitic capacitance and inductance introduced by the package structure.
Impact Factors:
- Longer leads → higher inductance
- Package structure → affects EMI and signal loss
- High-speed designs → require low-inductance packages like BGA or flip-chip
Q: What is the difference between BGA and QFP packages?
The primary difference between BGA (Ball Grid Array) and QFP (Quad Flat Package) lies in the pin layout and electrical performance.
Comparison:
BGA: Uses an array of solder balls on the bottom of the package. Provides high pin density, excellent thermal performance, and reduced signal distortion due to shorter interconnections. Ideal for high-performance and high-speed ICs.
QFP: Has leads extending from all four sides. Offers moderate pin density and easier visual inspection during soldering but is less optimal for very high-speed applications compared to BGA.
Summary: BGA excels in performance and thermal management for dense, high-speed ICs, while QFP is simpler to handle and suitable for medium-pin-count devices.
Keep Learning
QFN Package: Structure, PCB Design, and Assembly
Key Takeaways Choose the correct PCB footprint: Follow the QFN manufacturer’s recommended land pattern and package datasheet. Optimize thermal management: Use appropriate thermal pads and thermal vias to improve heat transfer. Control solder paste application: Design stencil apertures to achieve suitable solder volume and reduce assembly defects. Inspect hidden solder joints: Use X-ray inspection when required by the product’s reliability needs and inspection plan. Design for manufacturability (DFM): ......
Navigating Automotive PCB Manufacturing Standards and High-Reliability Fabrication
Key Takeaways Harsh Operating Environments: Engineered to survive 15 years under thermal cycling (-40 °C to 150 °C) and severe vibration. Strict Compliance: Guided by IATF 16949, AEC-Q200 components, and IPC Class 3 standards. Targeted Materials: Leverages high-Tg/heavy copper for power and Rogers substrates for 77 GHz radar. Zero-Defect Inspection: Employs 3D AOI and X-ray testing to eliminate hidden solder joints failures. An automotive PCB has to keep working for fifteen years in the same place. Bo......
Battery PCB Board: What You Need to Know
Key Takeaways Battery PCB boards support power distribution, protection, monitoring, and cell balancing. PCB types include single-layer, multilayer, flexible, and HDI designs. Current capacity, thermal management, and routing density are key design considerations. Reliable manufacturing depends on proper materials, fabrication, assembly, and testing. Battery PCB boards are used in a wide range of battery-powered electronics, from smartphones and laptops to electric vehicles and energy storage systems.......
Medical PCB Manufacturing: Key Standards, Types, and High-Reliability Fabrication
Key Takeaways Strict Compliance: Demands ISO 13485 QMS certification, IPC Class 3 specs (25 µm copper barrels), and IEC 60601-1 safety rules. Targeted Substrates: High-Tg FR-4 handles autoclave heat, polyimide flex serves wearables, and metal/ceramic cores manage high power. Quality & Traceability: Layered AOI, X-ray inspection, and full IPC-1782 lot tracking prevent critical field failures. A medical PCB carries a level of responsibility that consumer electronics rarely face, because a patient’s diag......
A Complete Guide to Package Substrates: Materials, Structure, Types, and PCB Differences
Key Takeaways Definition: A package substrate is the fine-pitch organic carrier connecting a bare die to the system board. Not a PCB: Substrates are routed several times finer than advanced HDI and use entirely different dielectrics. Materials: BT resin cores carry wire-bond and CSP work, while glass-free ABF build-up film carries flip chip. Process: Semi-additive plating, not etching, is what makes single-digit micrometer lines possible. Constraint: Substrate capacity, not wafer supply, now limits hi......
Comprehensive Guide to QFN Packages: Advantages, Types, and Applications in Electronics
Key Takeaways Thermal Vias: Place 0.3mm vias in the exposed pad to draw heat away from the IC. Voiding Control: Apply a window-pane stencil (50–75% coverage) to prevent solder voids. Prevent Wicking: Use tented vias or Via-in-Pad to stop solder from leaking. Hidden Joints: Require X-ray inspection (AXI) since QFN leads are under the package. JLCPCB SMT: Fully supports 0.4mm pitch QFNs, Via-in-Pad, and AXI quality checks. Quad flat no-lead (QFN) packages are a type of IC package that are small, lightwe......